diff options
author | Steven Rostedt | 2012-12-11 16:37:41 -0600 |
---|---|---|
committer | Steven Rostedt | 2012-12-11 17:18:46 -0600 |
commit | 7786954c95dbeba26ef39d2b6899bf06fbf2b629 (patch) | |
tree | 07b916a88e539aff2bf00836511251e58cfdab8d /tools | |
parent | a496872212e50a7e543a027faf35b0909459ec9e (diff) | |
download | kernel-omap-7786954c95dbeba26ef39d2b6899bf06fbf2b629.tar.gz kernel-omap-7786954c95dbeba26ef39d2b6899bf06fbf2b629.tar.xz kernel-omap-7786954c95dbeba26ef39d2b6899bf06fbf2b629.zip |
ktest: Add native support for syslinux boot loader
I installed Fedora 17 which no longer supports grub v1. I worked
with grub2 for a while, but there's so many issues with it and automated
rebooting, that I decided to switch to syslinux. Instead of using
the REBOOT_SCRIPT and add customized changes to get syslinux booted,
I thought it better to make ktest aware of syslinux and add options
to simplify the use of syslinux on a target test box.
Acked-by: H. Peter Anvin <hpa@zytor.com>
Cc: John 'Warthog9' Hawley <warthog9@kernel.org>
Signed-off-by: Steven Rostedt <rostedt@goodmis.org>
Diffstat (limited to 'tools')
-rwxr-xr-x | tools/testing/ktest/ktest.pl | 28 | ||||
-rw-r--r-- | tools/testing/ktest/sample.conf | 22 |
2 files changed, 48 insertions, 2 deletions
diff --git a/tools/testing/ktest/ktest.pl b/tools/testing/ktest/ktest.pl index f4b8f96a9430..067337bbce7b 100755 --- a/tools/testing/ktest/ktest.pl +++ b/tools/testing/ktest/ktest.pl | |||
@@ -54,6 +54,8 @@ my %default = ( | |||
54 | "STOP_TEST_AFTER" => 600, | 54 | "STOP_TEST_AFTER" => 600, |
55 | "MAX_MONITOR_WAIT" => 1800, | 55 | "MAX_MONITOR_WAIT" => 1800, |
56 | "GRUB_REBOOT" => "grub2-reboot", | 56 | "GRUB_REBOOT" => "grub2-reboot", |
57 | "SYSLINUX" => "extlinux", | ||
58 | "SYSLINUX_PATH" => "/boot/extlinux", | ||
57 | 59 | ||
58 | # required, and we will ask users if they don't have them but we keep the default | 60 | # required, and we will ask users if they don't have them but we keep the default |
59 | # value something that is common. | 61 | # value something that is common. |
@@ -109,6 +111,9 @@ my $grub_menu; | |||
109 | my $grub_file; | 111 | my $grub_file; |
110 | my $grub_number; | 112 | my $grub_number; |
111 | my $grub_reboot; | 113 | my $grub_reboot; |
114 | my $syslinux; | ||
115 | my $syslinux_path; | ||
116 | my $syslinux_label; | ||
112 | my $target; | 117 | my $target; |
113 | my $make; | 118 | my $make; |
114 | my $pre_install; | 119 | my $pre_install; |
@@ -237,6 +242,9 @@ my %option_map = ( | |||
237 | "GRUB_MENU" => \$grub_menu, | 242 | "GRUB_MENU" => \$grub_menu, |
238 | "GRUB_FILE" => \$grub_file, | 243 | "GRUB_FILE" => \$grub_file, |
239 | "GRUB_REBOOT" => \$grub_reboot, | 244 | "GRUB_REBOOT" => \$grub_reboot, |
245 | "SYSLINUX" => \$syslinux, | ||
246 | "SYSLINUX_PATH" => \$syslinux_path, | ||
247 | "SYSLINUX_LABEL" => \$syslinux_label, | ||
240 | "PRE_INSTALL" => \$pre_install, | 248 | "PRE_INSTALL" => \$pre_install, |
241 | "POST_INSTALL" => \$post_install, | 249 | "POST_INSTALL" => \$post_install, |
242 | "NO_INSTALL" => \$no_install, | 250 | "NO_INSTALL" => \$no_install, |
@@ -373,7 +381,7 @@ EOF | |||
373 | ; | 381 | ; |
374 | $config_help{"REBOOT_TYPE"} = << "EOF" | 382 | $config_help{"REBOOT_TYPE"} = << "EOF" |
375 | Way to reboot the box to the test kernel. | 383 | Way to reboot the box to the test kernel. |
376 | Only valid options so far are "grub", "grub2", and "script". | 384 | Only valid options so far are "grub", "grub2", "syslinux", and "script". |
377 | 385 | ||
378 | If you specify grub, it will assume grub version 1 | 386 | If you specify grub, it will assume grub version 1 |
379 | and will search in /boot/grub/menu.lst for the title \$GRUB_MENU | 387 | and will search in /boot/grub/menu.lst for the title \$GRUB_MENU |
@@ -386,6 +394,11 @@ $config_help{"REBOOT_TYPE"} = << "EOF" | |||
386 | 394 | ||
387 | If you specify grub2, then you also need to specify both \$GRUB_MENU | 395 | If you specify grub2, then you also need to specify both \$GRUB_MENU |
388 | and \$GRUB_FILE. | 396 | and \$GRUB_FILE. |
397 | |||
398 | If you specify syslinux, then you may use SYSLINUX to define the syslinux | ||
399 | command (defaults to extlinux), and SYSLINUX_PATH to specify the path to | ||
400 | the syslinux install (defaults to /boot/extlinux). But you have to specify | ||
401 | SYSLINUX_LABEL to define the label to boot to for the test kernel. | ||
389 | EOF | 402 | EOF |
390 | ; | 403 | ; |
391 | $config_help{"GRUB_MENU"} = << "EOF" | 404 | $config_help{"GRUB_MENU"} = << "EOF" |
@@ -414,6 +427,11 @@ $config_help{"GRUB_FILE"} = << "EOF" | |||
414 | here. Use something like /boot/grub2/grub.cfg to search. | 427 | here. Use something like /boot/grub2/grub.cfg to search. |
415 | EOF | 428 | EOF |
416 | ; | 429 | ; |
430 | $config_help{"SYSLINUX_LABEL"} = << "EOF" | ||
431 | If syslinux is used, the label that boots the target kernel must | ||
432 | be specified with SYSLINUX_LABEL. | ||
433 | EOF | ||
434 | ; | ||
417 | $config_help{"REBOOT_SCRIPT"} = << "EOF" | 435 | $config_help{"REBOOT_SCRIPT"} = << "EOF" |
418 | A script to reboot the target into the test kernel | 436 | A script to reboot the target into the test kernel |
419 | (Only mandatory if REBOOT_TYPE = script) | 437 | (Only mandatory if REBOOT_TYPE = script) |
@@ -545,6 +563,10 @@ sub get_ktest_configs { | |||
545 | get_ktest_config("GRUB_MENU"); | 563 | get_ktest_config("GRUB_MENU"); |
546 | get_ktest_config("GRUB_FILE"); | 564 | get_ktest_config("GRUB_FILE"); |
547 | } | 565 | } |
566 | |||
567 | if ($rtype eq "syslinux") { | ||
568 | get_ktest_config("SYSLINUX_LABEL"); | ||
569 | } | ||
548 | } | 570 | } |
549 | 571 | ||
550 | sub process_variables { | 572 | sub process_variables { |
@@ -1589,6 +1611,8 @@ sub reboot_to { | |||
1589 | run_ssh "'(echo \"savedefault --default=$grub_number --once\" | grub --batch)'"; | 1611 | run_ssh "'(echo \"savedefault --default=$grub_number --once\" | grub --batch)'"; |
1590 | } elsif ($reboot_type eq "grub2") { | 1612 | } elsif ($reboot_type eq "grub2") { |
1591 | run_ssh "$grub_reboot $grub_number"; | 1613 | run_ssh "$grub_reboot $grub_number"; |
1614 | } elsif ($reboot_type eq "syslinux") { | ||
1615 | run_ssh "$syslinux --once \\\"$syslinux_label\\\" $syslinux_path"; | ||
1592 | } elsif (defined $reboot_script) { | 1616 | } elsif (defined $reboot_script) { |
1593 | run_command "$reboot_script"; | 1617 | run_command "$reboot_script"; |
1594 | } | 1618 | } |
@@ -3768,6 +3792,8 @@ for (my $i = 1; $i <= $opt{"NUM_TESTS"}; $i++) { | |||
3768 | } elsif ($reboot_type eq "grub2") { | 3792 | } elsif ($reboot_type eq "grub2") { |
3769 | dodie "GRUB_MENU not defined" if (!defined($grub_menu)); | 3793 | dodie "GRUB_MENU not defined" if (!defined($grub_menu)); |
3770 | dodie "GRUB_FILE not defined" if (!defined($grub_file)); | 3794 | dodie "GRUB_FILE not defined" if (!defined($grub_file)); |
3795 | } elsif ($reboot_type eq "syslinux") { | ||
3796 | dodie "SYSLINUX_LABEL not defined" if (!defined($syslinux_label)); | ||
3771 | } | 3797 | } |
3772 | } | 3798 | } |
3773 | 3799 | ||
diff --git a/tools/testing/ktest/sample.conf b/tools/testing/ktest/sample.conf index 57617ec88c3b..4012e9330344 100644 --- a/tools/testing/ktest/sample.conf +++ b/tools/testing/ktest/sample.conf | |||
@@ -364,6 +364,22 @@ | |||
364 | # | 364 | # |
365 | #GRUB_MENU = Test Kernel | 365 | #GRUB_MENU = Test Kernel |
366 | 366 | ||
367 | # For REBOOT_TYPE = syslinux, the name of the syslinux executable | ||
368 | # (on the target) to use to set up the next reboot to boot the | ||
369 | # test kernel. | ||
370 | # (default extlinux) | ||
371 | #SYSLINUX = syslinux | ||
372 | |||
373 | # For REBOOT_TYPE = syslinux, the path that is passed to to the | ||
374 | # syslinux command where syslinux is installed. | ||
375 | # (default /boot/extlinux) | ||
376 | #SYSLINUX_PATH = /boot/syslinux | ||
377 | |||
378 | # For REBOOT_TYPE = syslinux, the syslinux label that references the | ||
379 | # test kernel in the syslinux config file. | ||
380 | # (default undefined) | ||
381 | #SYSLINUX_LABEL = "test-kernel" | ||
382 | |||
367 | # A script to reboot the target into the test kernel | 383 | # A script to reboot the target into the test kernel |
368 | # This and SWITCH_TO_TEST are about the same, except | 384 | # This and SWITCH_TO_TEST are about the same, except |
369 | # SWITCH_TO_TEST is run even for REBOOT_TYPE = grub. | 385 | # SWITCH_TO_TEST is run even for REBOOT_TYPE = grub. |
@@ -516,7 +532,7 @@ | |||
516 | #POST_BUILD_DIE = 1 | 532 | #POST_BUILD_DIE = 1 |
517 | 533 | ||
518 | # Way to reboot the box to the test kernel. | 534 | # Way to reboot the box to the test kernel. |
519 | # Only valid options so far are "grub", "grub2" and "script" | 535 | # Only valid options so far are "grub", "grub2", "syslinux" and "script" |
520 | # (default grub) | 536 | # (default grub) |
521 | # If you specify grub, it will assume grub version 1 | 537 | # If you specify grub, it will assume grub version 1 |
522 | # and will search in /boot/grub/menu.lst for the title $GRUB_MENU | 538 | # and will search in /boot/grub/menu.lst for the title $GRUB_MENU |
@@ -527,6 +543,10 @@ | |||
527 | # For REBOOT_TYPE = grub2, you must define both GRUB_MENU and | 543 | # For REBOOT_TYPE = grub2, you must define both GRUB_MENU and |
528 | # GRUB_FILE. | 544 | # GRUB_FILE. |
529 | # | 545 | # |
546 | # For REBOOT_TYPE = syslinux, you must define SYSLINUX_LABEL, and | ||
547 | # perhaps modify SYSLINUX (default extlinux) and SYSLINUX_PATH | ||
548 | # (default /boot/extlinux) | ||
549 | # | ||
530 | # The entry in /boot/grub/menu.lst must be entered in manually. | 550 | # The entry in /boot/grub/menu.lst must be entered in manually. |
531 | # The test will not modify that file. | 551 | # The test will not modify that file. |
532 | #REBOOT_TYPE = grub | 552 | #REBOOT_TYPE = grub |