diff options
author | Sam Ravnborg | 2005-08-10 13:44:50 -0500 |
---|---|---|
committer | Sam Ravnborg | 2005-08-10 13:44:50 -0500 |
commit | dbec486632d2303f5c0e75af7a8473fa4c4a145a (patch) | |
tree | 2597d1fd4f095dd29e30ae5614240a59eb635c2c /usr | |
parent | fb7f6ff614f3ead2ca41bb4a348b9ea431d95176 (diff) | |
download | kernel-omap-dbec486632d2303f5c0e75af7a8473fa4c4a145a.tar.gz kernel-omap-dbec486632d2303f5c0e75af7a8473fa4c4a145a.tar.xz kernel-omap-dbec486632d2303f5c0e75af7a8473fa4c4a145a.zip |
kconfig: move initramfs options to General Setup
Move initramfs options from Device Drivers | Block Drivers to General Setup
This is a more natural place for this option.
Furthermore separate out intramfs options to usr/Kconfig
Signed-off-by: Sam Ravnborg <sam@ravnborg.org>
Diffstat (limited to 'usr')
-rw-r--r-- | usr/Kconfig | 46 |
1 files changed, 46 insertions, 0 deletions
diff --git a/usr/Kconfig b/usr/Kconfig new file mode 100644 index 000000000000..07727f3c7cea --- /dev/null +++ b/usr/Kconfig | |||
@@ -0,0 +1,46 @@ | |||
1 | # | ||
2 | # Configuration for initramfs | ||
3 | # | ||
4 | |||
5 | config INITRAMFS_SOURCE | ||
6 | string "Initramfs source file(s)" | ||
7 | default "" | ||
8 | help | ||
9 | This can be either a single cpio archive with a .cpio suffix or a | ||
10 | space-separated list of directories and files for building the | ||
11 | initramfs image. A cpio archive should contain a filesystem archive | ||
12 | to be used as an initramfs image. Directories should contain a | ||
13 | filesystem layout to be included in the initramfs image. Files | ||
14 | should contain entries according to the format described by the | ||
15 | "usr/gen_init_cpio" program in the kernel tree. | ||
16 | |||
17 | When multiple directories and files are specified then the | ||
18 | initramfs image will be the aggregate of all of them. | ||
19 | |||
20 | See <file:Documentation/early-userspace/README for more details. | ||
21 | |||
22 | If you are not sure, leave it blank. | ||
23 | |||
24 | config INITRAMFS_ROOT_UID | ||
25 | int "User ID to map to 0 (user root)" | ||
26 | depends on INITRAMFS_SOURCE!="" | ||
27 | default "0" | ||
28 | help | ||
29 | This setting is only meaningful if the INITRAMFS_SOURCE is | ||
30 | contains a directory. Setting this user ID (UID) to something | ||
31 | other than "0" will cause all files owned by that UID to be | ||
32 | owned by user root in the initial ramdisk image. | ||
33 | |||
34 | If you are not sure, leave it set to "0". | ||
35 | |||
36 | config INITRAMFS_ROOT_GID | ||
37 | int "Group ID to map to 0 (group root)" | ||
38 | depends on INITRAMFS_SOURCE!="" | ||
39 | default "0" | ||
40 | help | ||
41 | This setting is only meaningful if the INITRAMFS_SOURCE is | ||
42 | contains a directory. Setting this group ID (GID) to something | ||
43 | other than "0" will cause all files owned by that GID to be | ||
44 | owned by group root in the initial ramdisk image. | ||
45 | |||
46 | If you are not sure, leave it set to "0". | ||