diff options
Diffstat (limited to 'Documentation/BK-usage/bk-kernel-howto.txt')
-rw-r--r-- | Documentation/BK-usage/bk-kernel-howto.txt | 283 |
1 files changed, 283 insertions, 0 deletions
diff --git a/Documentation/BK-usage/bk-kernel-howto.txt b/Documentation/BK-usage/bk-kernel-howto.txt new file mode 100644 index 000000000000..b7b9075d2910 --- /dev/null +++ b/Documentation/BK-usage/bk-kernel-howto.txt | |||
@@ -0,0 +1,283 @@ | |||
1 | |||
2 | Doing the BK Thing, Penguin-Style | ||
3 | |||
4 | |||
5 | |||
6 | |||
7 | This set of notes is intended mainly for kernel developers, occasional | ||
8 | or full-time, but sysadmins and power users may find parts of it useful | ||
9 | as well. It assumes at least a basic familiarity with CVS, both at a | ||
10 | user level (use on the cmd line) and at a higher level (client-server model). | ||
11 | Due to the author's background, an operation may be described in terms | ||
12 | of CVS, or in terms of how that operation differs from CVS. | ||
13 | |||
14 | This is -not- intended to be BitKeeper documentation. Always run | ||
15 | "bk help <command>" or in X "bk helptool <command>" for reference | ||
16 | documentation. | ||
17 | |||
18 | |||
19 | BitKeeper Concepts | ||
20 | ------------------ | ||
21 | |||
22 | In the true nature of the Internet itself, BitKeeper is a distributed | ||
23 | system. When applied to revision control, this means doing away with | ||
24 | client-server, and changing to a parent-child model... essentially | ||
25 | peer-to-peer. On the developer's end, this also represents a | ||
26 | fundamental disruption in the standard workflow of changes, commits, | ||
27 | and merges. You will need to take a few minutes to think about | ||
28 | how to best work under BitKeeper, and re-optimize things a bit. | ||
29 | In some sense it is a bit radical, because it might described as | ||
30 | tossing changes out into a maelstrom and having them magically | ||
31 | land at the right destination... but I'm getting ahead of myself. | ||
32 | |||
33 | Let's start with this progression: | ||
34 | Each BitKeeper source tree on disk is a repository unto itself. | ||
35 | Each repository has a parent (except the root/original, of course). | ||
36 | Each repository contains a set of a changesets ("csets"). | ||
37 | Each cset is one or more changed files, bundled together. | ||
38 | |||
39 | Each tree is a repository, so all changes are checked into the local | ||
40 | tree. When a change is checked in, all modified files are grouped | ||
41 | into a logical unit, the changeset. Internally, BK links these | ||
42 | changesets in a tree, representing various converging and diverging | ||
43 | lines of development. These changesets are the bread and butter of | ||
44 | the BK system. | ||
45 | |||
46 | After the concept of changesets, the next thing you need to get used | ||
47 | to is having multiple copies of source trees lying around. This -really- | ||
48 | takes some getting used to, for some people. Separate source trees | ||
49 | are the means in BitKeeper by which you delineate parallel lines | ||
50 | of development, both minor and major. What would be branches in | ||
51 | CVS become separate source trees, or "clones" in BitKeeper [heh, | ||
52 | or Star Wars] terminology. | ||
53 | |||
54 | Clones and changesets are the tools from which most of the power of | ||
55 | BitKeeper is derived. As mentioned earlier, each clone has a parent, | ||
56 | the tree used as the source when the new clone was created. In a | ||
57 | CVS-like setup, the parent would be a remote server on the Internet, | ||
58 | and the child is your local clone of that tree. | ||
59 | |||
60 | Once you have established a common baseline between two source trees -- | ||
61 | a common parent -- then you can merge changesets between those two | ||
62 | trees with ease. Merging changes into a tree is called a "pull", and | ||
63 | is analagous to 'cvs update'. A pull downloads all the changesets in | ||
64 | the remote tree you do not have, and merges them. Sending changes in | ||
65 | one tree to another tree is called a "push". Push sends all changes | ||
66 | in the local tree the remote does not yet have, and merges them. | ||
67 | |||
68 | From these concepts come some initial command examples: | ||
69 | |||
70 | 1) bk clone -q http://linux.bkbits.net/linux-2.5 linus-2.5 | ||
71 | Download a 2.5 stock kernel tree, naming it "linus-2.5" in the local dir. | ||
72 | The "-q" disables listing every single file as it is downloaded. | ||
73 | |||
74 | 2) bk clone -ql linus-2.5 alpha-2.5 | ||
75 | Create a separate source tree for the Alpha AXP architecture. | ||
76 | The "-l" uses hard links instead of copying data, since both trees are | ||
77 | on the local disk. You can also replace the above with "bk lclone -q ..." | ||
78 | |||
79 | You only clone a tree -once-. After cloning the tree lives a long time | ||
80 | on disk, being updating by pushes and pulls. | ||
81 | |||
82 | 3) cd alpha-2.5 ; bk pull http://gkernel.bkbits.net/alpha-2.5 | ||
83 | Download changes in "alpha-2.5" repository which are not present | ||
84 | in the local repository, and merge them into the source tree. | ||
85 | |||
86 | 4) bk -r co -q | ||
87 | Because every tree is a repository, files must be checked out before | ||
88 | they will be in their standard places in the source tree. | ||
89 | |||
90 | 5) bk vi fs/inode.c # example change... | ||
91 | bk citool # checkin, using X tool | ||
92 | bk push bk://gkernel@bkbits.net/alpha-2.5 # upload change | ||
93 | Typical example of a BK sequence that would replace the analagous CVS | ||
94 | situation, | ||
95 | vi fs/inode.c | ||
96 | cvs commit | ||
97 | |||
98 | As this is just supposed to be a quick BK intro, for more in-depth | ||
99 | tutorials, live working demos, and docs, see http://www.bitkeeper.com/ | ||
100 | |||
101 | |||
102 | |||
103 | BK and Kernel Development Workflow | ||
104 | ---------------------------------- | ||
105 | Currently the latest 2.5 tree is available via "bk clone $URL" | ||
106 | and "bk pull $URL" at http://linux.bkbits.net/linux-2.5 | ||
107 | This should change in a few weeks to a kernel.org URL. | ||
108 | |||
109 | |||
110 | A big part of using BitKeeper is organizing the various trees you have | ||
111 | on your local disk, and organizing the flow of changes among those | ||
112 | trees, and remote trees. If one were to graph the relationships between | ||
113 | a desired BK setup, you are likely to see a few-many-few graph, like | ||
114 | this: | ||
115 | |||
116 | linux-2.5 | ||
117 | | | ||
118 | merge-to-linus-2.5 | ||
119 | / | | | ||
120 | / | | | ||
121 | vm-hacks bugfixes filesys personal-hacks | ||
122 | \ | | / | ||
123 | \ | | / | ||
124 | \ | | / | ||
125 | testing-and-validation | ||
126 | |||
127 | Since a "bk push" sends all changes not in the target tree, and | ||
128 | since a "bk pull" receives all changes not in the source tree, you want | ||
129 | to make sure you are only pushing specific changes to the desired tree, | ||
130 | not all changes from "peer parent" trees. For example, pushing a change | ||
131 | from the testing-and-validation tree would probably be a bad idea, | ||
132 | because it will push all changes from vm-hacks, bugfixes, filesys, and | ||
133 | personal-hacks trees into the target tree. | ||
134 | |||
135 | One would typically work on only one "theme" at a time, either | ||
136 | vm-hacks or bugfixes or filesys, keeping those changes isolated in | ||
137 | their own tree during development, and only merge the isolated with | ||
138 | other changes when going upstream (to Linus or other maintainers) or | ||
139 | downstream (to your "union" trees, like testing-and-validation above). | ||
140 | |||
141 | It should be noted that some of this separation is not just recommended | ||
142 | practice, it's actually [for now] -enforced- by BitKeeper. BitKeeper | ||
143 | requires that changesets maintain a certain order, which is the reason | ||
144 | that "bk push" sends all local changesets the remote doesn't have. This | ||
145 | separation may look like a lot of wasted disk space at first, but it | ||
146 | helps when two unrelated changes may "pollute" the same area of code, or | ||
147 | don't follow the same pace of development, or any other of the standard | ||
148 | reasons why one creates a development branch. | ||
149 | |||
150 | Small development branches (clones) will appear and disappear: | ||
151 | |||
152 | -------- A --------- B --------- C --------- D ------- | ||
153 | \ / | ||
154 | -----short-term devel branch----- | ||
155 | |||
156 | While long-term branches will parallel a tree (or trees), with period | ||
157 | merge points. In this first example, we pull from a tree (pulls, | ||
158 | "\") periodically, such as what occurs when tracking changes in a | ||
159 | vendor tree, never pushing changes back up the line: | ||
160 | |||
161 | -------- A --------- B --------- C --------- D ------- | ||
162 | \ \ \ | ||
163 | ----long-term devel branch----------------- | ||
164 | |||
165 | And then a more common case in Linux kernel development, a long term | ||
166 | branch with periodic merges back into the tree (pushes, "/"): | ||
167 | |||
168 | -------- A --------- B --------- C --------- D ------- | ||
169 | \ \ / \ | ||
170 | ----long-term devel branch----------------- | ||
171 | |||
172 | |||
173 | |||
174 | |||
175 | |||
176 | Submitting Changes to Linus | ||
177 | --------------------------- | ||
178 | There's a bit of an art, or style, of submitting changes to Linus. | ||
179 | Since Linus's tree is now (you might say) fully integrated into the | ||
180 | distributed BitKeeper system, there are several prerequisites to | ||
181 | properly submitting a BitKeeper change. All these prereq's are just | ||
182 | general cleanliness of BK usage, so as people become experts at BK, feel | ||
183 | free to optimize this process further (assuming Linus agrees, of | ||
184 | course). | ||
185 | |||
186 | |||
187 | |||
188 | 0) Make sure your tree was originally cloned from the linux-2.5 tree | ||
189 | created by Linus. If your tree does not have this as its ancestor, it | ||
190 | is impossible to reliably exchange changesets. | ||
191 | |||
192 | |||
193 | |||
194 | 1) Pay attention to your commit text. The commit message that | ||
195 | accompanies each changeset you submit will live on forever in history, | ||
196 | and is used by Linus to accurately summarize the changes in each | ||
197 | pre-patch. Remember that there is no context, so | ||
198 | "fix for new scheduler changes" | ||
199 | would be too vague, but | ||
200 | "fix mips64 arch for new scheduler switch_to(), TIF_xxx semantics" | ||
201 | would be much better. | ||
202 | |||
203 | You can and should use the command "bk comment -C<rev>" to update the | ||
204 | commit text, and improve it after the fact. This is very useful for | ||
205 | development: poor, quick descriptions during development, which get | ||
206 | cleaned up using "bk comment" before issuing the "bk push" to submit the | ||
207 | changes. | ||
208 | |||
209 | |||
210 | |||
211 | 2) Include an Internet-available URL for Linus to pull from, such as | ||
212 | |||
213 | Pull from: http://gkernel.bkbits.net/net-drivers-2.5 | ||
214 | |||
215 | |||
216 | |||
217 | 3) Include a summary and "diffstat -p1" of each changeset that will be | ||
218 | downloaded, when Linus issues a "bk pull". The author auto-generates | ||
219 | these summaries using "bk changes -L <parent>", to obtain a listing | ||
220 | of all the pending-to-send changesets, and their commit messages. | ||
221 | |||
222 | It is important to show Linus what he will be downloading when he issues | ||
223 | a "bk pull", to reduce the time required to sift the changes once they | ||
224 | are downloaded to Linus's local machine. | ||
225 | |||
226 | IMPORTANT NOTE: One of the features of BK is that your repository does | ||
227 | not have to be up to date, in order for Linus to receive your changes. | ||
228 | It is considered a courtesy to keep your repository fairly recent, to | ||
229 | lessen any potential merge work Linus may need to do. | ||
230 | |||
231 | |||
232 | 4) Split up your changes. Each maintainer<->Linus situation is likely | ||
233 | to be slightly different here, so take this just as general advice. The | ||
234 | author splits up changes according to "themes" when merging with Linus. | ||
235 | Simultaneous pushes from local development go to special trees which | ||
236 | exist solely to house changes "queued" for Linus. Example of the trees: | ||
237 | |||
238 | net-drivers-2.5 -- on-going net driver maintenance | ||
239 | vm-2.5 -- VM-related changes | ||
240 | fs-2.5 -- filesystem-related changes | ||
241 | |||
242 | Linus then has much more freedom for pulling changes. He could (for | ||
243 | example) issue a "bk pull" on vm-2.5 and fs-2.5 trees, to merge their | ||
244 | changes, but hold off net-drivers-2.5 because of a change that needs | ||
245 | more discussion. | ||
246 | |||
247 | Other maintainers may find that a single linus-pull-from tree is | ||
248 | adequate for passing BK changesets to him. | ||
249 | |||
250 | |||
251 | |||
252 | Frequently Answered Questions | ||
253 | ----------------------------- | ||
254 | 1) How do I change the e-mail address shown in the changelog? | ||
255 | A. When you run "bk citool" or "bk commit", set environment | ||
256 | variables BK_USER and BK_HOST to the desired username | ||
257 | and host/domain name. | ||
258 | |||
259 | |||
260 | 2) How do I use tags / get a diff between two kernel versions? | ||
261 | A. Pass the tags Linus uses to 'bk export'. | ||
262 | |||
263 | ChangeSets are in a forward-progressing order, so it's pretty easy | ||
264 | to get a snapshot starting and ending at any two points in time. | ||
265 | Linus puts tags on each release and pre-release, so you could use | ||
266 | these two examples: | ||
267 | |||
268 | bk export -tpatch -hdu -rv2.5.4,v2.5.5 | less | ||
269 | # creates patch-2.5.5 essentially | ||
270 | bk export -tpatch -du -rv2.5.5-pre1,v2.5.5 | less | ||
271 | # changes from pre1 to final | ||
272 | |||
273 | A tag is just an alias for a specific changeset... and since changesets | ||
274 | are ordered, a tag is thus a marker for a specific point in time (or | ||
275 | specific state of the tree). | ||
276 | |||
277 | |||
278 | 3) Is there an easy way to generate One Big Patch versus mainline, | ||
279 | for my long-lived kernel branch? | ||
280 | A. Yes. This requires BK 3.x, though. | ||
281 | |||
282 | bk export -tpatch -r`bk repogca bk://linux.bkbits.net/linux-2.5`,+ | ||
283 | |||