summaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
Diffstat (limited to 'Documentation/DocBook/mtdnand.tmpl')
-rw-r--r--Documentation/DocBook/mtdnand.tmpl1320
1 files changed, 1320 insertions, 0 deletions
diff --git a/Documentation/DocBook/mtdnand.tmpl b/Documentation/DocBook/mtdnand.tmpl
new file mode 100644
index 000000000000..6e463d0db266
--- /dev/null
+++ b/Documentation/DocBook/mtdnand.tmpl
@@ -0,0 +1,1320 @@
1<?xml version="1.0" encoding="UTF-8"?>
2<!DOCTYPE book PUBLIC "-//OASIS//DTD DocBook XML V4.1.2//EN"
3 "http://www.oasis-open.org/docbook/xml/4.1.2/docbookx.dtd" []>
4
5<book id="MTD-NAND-Guide">
6 <bookinfo>
7 <title>MTD NAND Driver Programming Interface</title>
8
9 <authorgroup>
10 <author>
11 <firstname>Thomas</firstname>
12 <surname>Gleixner</surname>
13 <affiliation>
14 <address>
15 <email>tglx@linutronix.de</email>
16 </address>
17 </affiliation>
18 </author>
19 </authorgroup>
20
21 <copyright>
22 <year>2004</year>
23 <holder>Thomas Gleixner</holder>
24 </copyright>
25
26 <legalnotice>
27 <para>
28 This documentation is free software; you can redistribute
29 it and/or modify it under the terms of the GNU General Public
30 License version 2 as published by the Free Software Foundation.
31 </para>
32
33 <para>
34 This program is distributed in the hope that it will be
35 useful, but WITHOUT ANY WARRANTY; without even the implied
36 warranty of MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.
37 See the GNU General Public License for more details.
38 </para>
39
40 <para>
41 You should have received a copy of the GNU General Public
42 License along with this program; if not, write to the Free
43 Software Foundation, Inc., 59 Temple Place, Suite 330, Boston,
44 MA 02111-1307 USA
45 </para>
46
47 <para>
48 For more details see the file COPYING in the source
49 distribution of Linux.
50 </para>
51 </legalnotice>
52 </bookinfo>
53
54<toc></toc>
55
56 <chapter id="intro">
57 <title>Introduction</title>
58 <para>
59 The generic NAND driver supports almost all NAND and AG-AND based
60 chips and connects them to the Memory Technology Devices (MTD)
61 subsystem of the Linux Kernel.
62 </para>
63 <para>
64 This documentation is provided for developers who want to implement
65 board drivers or filesystem drivers suitable for NAND devices.
66 </para>
67 </chapter>
68
69 <chapter id="bugs">
70 <title>Known Bugs And Assumptions</title>
71 <para>
72 None.
73 </para>
74 </chapter>
75
76 <chapter id="dochints">
77 <title>Documentation hints</title>
78 <para>
79 The function and structure docs are autogenerated. Each function and
80 struct member has a short description which is marked with an [XXX] identifier.
81 The following chapters explain the meaning of those identifiers.
82 </para>
83 <sect1>
84 <title>Function identifiers [XXX]</title>
85 <para>
86 The functions are marked with [XXX] identifiers in the short
87 comment. The identifiers explain the usage and scope of the
88 functions. Following identifiers are used:
89 </para>
90 <itemizedlist>
91 <listitem><para>
92 [MTD Interface]</para><para>
93 These functions provide the interface to the MTD kernel API.
94 They are not replacable and provide functionality
95 which is complete hardware independent.
96 </para></listitem>
97 <listitem><para>
98 [NAND Interface]</para><para>
99 These functions are exported and provide the interface to the NAND kernel API.
100 </para></listitem>
101 <listitem><para>
102 [GENERIC]</para><para>
103 Generic functions are not replacable and provide functionality
104 which is complete hardware independent.
105 </para></listitem>
106 <listitem><para>
107 [DEFAULT]</para><para>
108 Default functions provide hardware related functionality which is suitable
109 for most of the implementations. These functions can be replaced by the
110 board driver if neccecary. Those functions are called via pointers in the
111 NAND chip description structure. The board driver can set the functions which
112 should be replaced by board dependend functions before calling nand_scan().
113 If the function pointer is NULL on entry to nand_scan() then the pointer
114 is set to the default function which is suitable for the detected chip type.
115 </para></listitem>
116 </itemizedlist>
117 </sect1>
118 <sect1>
119 <title>Struct member identifiers [XXX]</title>
120 <para>
121 The struct members are marked with [XXX] identifiers in the
122 comment. The identifiers explain the usage and scope of the
123 members. Following identifiers are used:
124 </para>
125 <itemizedlist>
126 <listitem><para>
127 [INTERN]</para><para>
128 These members are for NAND driver internal use only and must not be
129 modified. Most of these values are calculated from the chip geometry
130 information which is evaluated during nand_scan().
131 </para></listitem>
132 <listitem><para>
133 [REPLACEABLE]</para><para>
134 Replaceable members hold hardware related functions which can be
135 provided by the board driver. The board driver can set the functions which
136 should be replaced by board dependend functions before calling nand_scan().
137 If the function pointer is NULL on entry to nand_scan() then the pointer
138 is set to the default function which is suitable for the detected chip type.
139 </para></listitem>
140 <listitem><para>
141 [BOARDSPECIFIC]</para><para>
142 Board specific members hold hardware related information which must
143 be provided by the board driver. The board driver must set the function
144 pointers and datafields before calling nand_scan().
145 </para></listitem>
146 <listitem><para>
147 [OPTIONAL]</para><para>
148 Optional members can hold information relevant for the board driver. The
149 generic NAND driver code does not use this information.
150 </para></listitem>
151 </itemizedlist>
152 </sect1>
153 </chapter>
154
155 <chapter id="basicboarddriver">
156 <title>Basic board driver</title>
157 <para>
158 For most boards it will be sufficient to provide just the
159 basic functions and fill out some really board dependend
160 members in the nand chip description structure.
161 See drivers/mtd/nand/skeleton for reference.
162 </para>
163 <sect1>
164 <title>Basic defines</title>
165 <para>
166 At least you have to provide a mtd structure and
167 a storage for the ioremap'ed chip address.
168 You can allocate the mtd structure using kmalloc
169 or you can allocate it statically.
170 In case of static allocation you have to allocate
171 a nand_chip structure too.
172 </para>
173 <para>
174 Kmalloc based example
175 </para>
176 <programlisting>
177static struct mtd_info *board_mtd;
178static unsigned long baseaddr;
179 </programlisting>
180 <para>
181 Static example
182 </para>
183 <programlisting>
184static struct mtd_info board_mtd;
185static struct nand_chip board_chip;
186static unsigned long baseaddr;
187 </programlisting>
188 </sect1>
189 <sect1>
190 <title>Partition defines</title>
191 <para>
192 If you want to divide your device into parititions, then
193 enable the configuration switch CONFIG_MTD_PARITIONS and define
194 a paritioning scheme suitable to your board.
195 </para>
196 <programlisting>
197#define NUM_PARTITIONS 2
198static struct mtd_partition partition_info[] = {
199 { .name = "Flash partition 1",
200 .offset = 0,
201 .size = 8 * 1024 * 1024 },
202 { .name = "Flash partition 2",
203 .offset = MTDPART_OFS_NEXT,
204 .size = MTDPART_SIZ_FULL },
205};
206 </programlisting>
207 </sect1>
208 <sect1>
209 <title>Hardware control function</title>
210 <para>
211 The hardware control function provides access to the
212 control pins of the NAND chip(s).
213 The access can be done by GPIO pins or by address lines.
214 If you use address lines, make sure that the timing
215 requirements are met.
216 </para>
217 <para>
218 <emphasis>GPIO based example</emphasis>
219 </para>
220 <programlisting>
221static void board_hwcontrol(struct mtd_info *mtd, int cmd)
222{
223 switch(cmd){
224 case NAND_CTL_SETCLE: /* Set CLE pin high */ break;
225 case NAND_CTL_CLRCLE: /* Set CLE pin low */ break;
226 case NAND_CTL_SETALE: /* Set ALE pin high */ break;
227 case NAND_CTL_CLRALE: /* Set ALE pin low */ break;
228 case NAND_CTL_SETNCE: /* Set nCE pin low */ break;
229 case NAND_CTL_CLRNCE: /* Set nCE pin high */ break;
230 }
231}
232 </programlisting>
233 <para>
234 <emphasis>Address lines based example.</emphasis> It's assumed that the
235 nCE pin is driven by a chip select decoder.
236 </para>
237 <programlisting>
238static void board_hwcontrol(struct mtd_info *mtd, int cmd)
239{
240 struct nand_chip *this = (struct nand_chip *) mtd->priv;
241 switch(cmd){
242 case NAND_CTL_SETCLE: this->IO_ADDR_W |= CLE_ADRR_BIT; break;
243 case NAND_CTL_CLRCLE: this->IO_ADDR_W &amp;= ~CLE_ADRR_BIT; break;
244 case NAND_CTL_SETALE: this->IO_ADDR_W |= ALE_ADRR_BIT; break;
245 case NAND_CTL_CLRALE: this->IO_ADDR_W &amp;= ~ALE_ADRR_BIT; break;
246 }
247}
248 </programlisting>
249 </sect1>
250 <sect1>
251 <title>Device ready function</title>
252 <para>
253 If the hardware interface has the ready busy pin of the NAND chip connected to a
254 GPIO or other accesible I/O pin, this function is used to read back the state of the
255 pin. The function has no arguments and should return 0, if the device is busy (R/B pin
256 is low) and 1, if the device is ready (R/B pin is high).
257 If the hardware interface does not give access to the ready busy pin, then
258 the function must not be defined and the function pointer this->dev_ready is set to NULL.
259 </para>
260 </sect1>
261 <sect1>
262 <title>Init function</title>
263 <para>
264 The init function allocates memory and sets up all the board
265 specific parameters and function pointers. When everything
266 is set up nand_scan() is called. This function tries to
267 detect and identify then chip. If a chip is found all the
268 internal data fields are initialized accordingly.
269 The structure(s) have to be zeroed out first and then filled with the neccecary
270 information about the device.
271 </para>
272 <programlisting>
273int __init board_init (void)
274{
275 struct nand_chip *this;
276 int err = 0;
277
278 /* Allocate memory for MTD device structure and private data */
279 board_mtd = kmalloc (sizeof(struct mtd_info) + sizeof (struct nand_chip), GFP_KERNEL);
280 if (!board_mtd) {
281 printk ("Unable to allocate NAND MTD device structure.\n");
282 err = -ENOMEM;
283 goto out;
284 }
285
286 /* Initialize structures */
287 memset ((char *) board_mtd, 0, sizeof(struct mtd_info) + sizeof(struct nand_chip));
288
289 /* map physical adress */
290 baseaddr = (unsigned long)ioremap(CHIP_PHYSICAL_ADDRESS, 1024);
291 if(!baseaddr){
292 printk("Ioremap to access NAND chip failed\n");
293 err = -EIO;
294 goto out_mtd;
295 }
296
297 /* Get pointer to private data */
298 this = (struct nand_chip *) ();
299 /* Link the private data with the MTD structure */
300 board_mtd->priv = this;
301
302 /* Set address of NAND IO lines */
303 this->IO_ADDR_R = baseaddr;
304 this->IO_ADDR_W = baseaddr;
305 /* Reference hardware control function */
306 this->hwcontrol = board_hwcontrol;
307 /* Set command delay time, see datasheet for correct value */
308 this->chip_delay = CHIP_DEPENDEND_COMMAND_DELAY;
309 /* Assign the device ready function, if available */
310 this->dev_ready = board_dev_ready;
311 this->eccmode = NAND_ECC_SOFT;
312
313 /* Scan to find existance of the device */
314 if (nand_scan (board_mtd, 1)) {
315 err = -ENXIO;
316 goto out_ior;
317 }
318
319 add_mtd_partitions(board_mtd, partition_info, NUM_PARTITIONS);
320 goto out;
321
322out_ior:
323 iounmap((void *)baseaddr);
324out_mtd:
325 kfree (board_mtd);
326out:
327 return err;
328}
329module_init(board_init);
330 </programlisting>
331 </sect1>
332 <sect1>
333 <title>Exit function</title>
334 <para>
335 The exit function is only neccecary if the driver is
336 compiled as a module. It releases all resources which
337 are held by the chip driver and unregisters the partitions
338 in the MTD layer.
339 </para>
340 <programlisting>
341#ifdef MODULE
342static void __exit board_cleanup (void)
343{
344 /* Release resources, unregister device */
345 nand_release (board_mtd);
346
347 /* unmap physical adress */
348 iounmap((void *)baseaddr);
349
350 /* Free the MTD device structure */
351 kfree (board_mtd);
352}
353module_exit(board_cleanup);
354#endif
355 </programlisting>
356 </sect1>
357 </chapter>
358
359 <chapter id="boarddriversadvanced">
360 <title>Advanced board driver functions</title>
361 <para>
362 This chapter describes the advanced functionality of the NAND
363 driver. For a list of functions which can be overridden by the board
364 driver see the documentation of the nand_chip structure.
365 </para>
366 <sect1>
367 <title>Multiple chip control</title>
368 <para>
369 The nand driver can control chip arrays. Therefor the
370 board driver must provide an own select_chip function. This
371 function must (de)select the requested chip.
372 The function pointer in the nand_chip structure must
373 be set before calling nand_scan(). The maxchip parameter
374 of nand_scan() defines the maximum number of chips to
375 scan for. Make sure that the select_chip function can
376 handle the requested number of chips.
377 </para>
378 <para>
379 The nand driver concatenates the chips to one virtual
380 chip and provides this virtual chip to the MTD layer.
381 </para>
382 <para>
383 <emphasis>Note: The driver can only handle linear chip arrays
384 of equally sized chips. There is no support for
385 parallel arrays which extend the buswidth.</emphasis>
386 </para>
387 <para>
388 <emphasis>GPIO based example</emphasis>
389 </para>
390 <programlisting>
391static void board_select_chip (struct mtd_info *mtd, int chip)
392{
393 /* Deselect all chips, set all nCE pins high */
394 GPIO(BOARD_NAND_NCE) |= 0xff;
395 if (chip >= 0)
396 GPIO(BOARD_NAND_NCE) &amp;= ~ (1 &lt;&lt; chip);
397}
398 </programlisting>
399 <para>
400 <emphasis>Address lines based example.</emphasis>
401 Its assumed that the nCE pins are connected to an
402 address decoder.
403 </para>
404 <programlisting>
405static void board_select_chip (struct mtd_info *mtd, int chip)
406{
407 struct nand_chip *this = (struct nand_chip *) mtd->priv;
408
409 /* Deselect all chips */
410 this->IO_ADDR_R &amp;= ~BOARD_NAND_ADDR_MASK;
411 this->IO_ADDR_W &amp;= ~BOARD_NAND_ADDR_MASK;
412 switch (chip) {
413 case 0:
414 this->IO_ADDR_R |= BOARD_NAND_ADDR_CHIP0;
415 this->IO_ADDR_W |= BOARD_NAND_ADDR_CHIP0;
416 break;
417 ....
418 case n:
419 this->IO_ADDR_R |= BOARD_NAND_ADDR_CHIPn;
420 this->IO_ADDR_W |= BOARD_NAND_ADDR_CHIPn;
421 break;
422 }
423}
424 </programlisting>
425 </sect1>
426 <sect1>
427 <title>Hardware ECC support</title>
428 <sect2>
429 <title>Functions and constants</title>
430 <para>
431 The nand driver supports three different types of
432 hardware ECC.
433 <itemizedlist>
434 <listitem><para>NAND_ECC_HW3_256</para><para>
435 Hardware ECC generator providing 3 bytes ECC per
436 256 byte.
437 </para> </listitem>
438 <listitem><para>NAND_ECC_HW3_512</para><para>
439 Hardware ECC generator providing 3 bytes ECC per
440 512 byte.
441 </para> </listitem>
442 <listitem><para>NAND_ECC_HW6_512</para><para>
443 Hardware ECC generator providing 6 bytes ECC per
444 512 byte.
445 </para> </listitem>
446 <listitem><para>NAND_ECC_HW8_512</para><para>
447 Hardware ECC generator providing 6 bytes ECC per
448 512 byte.
449 </para> </listitem>
450 </itemizedlist>
451 If your hardware generator has a different functionality
452 add it at the appropriate place in nand_base.c
453 </para>
454 <para>
455 The board driver must provide following functions:
456 <itemizedlist>
457 <listitem><para>enable_hwecc</para><para>
458 This function is called before reading / writing to
459 the chip. Reset or initialize the hardware generator
460 in this function. The function is called with an
461 argument which let you distinguish between read
462 and write operations.
463 </para> </listitem>
464 <listitem><para>calculate_ecc</para><para>
465 This function is called after read / write from / to
466 the chip. Transfer the ECC from the hardware to
467 the buffer. If the option NAND_HWECC_SYNDROME is set
468 then the function is only called on write. See below.
469 </para> </listitem>
470 <listitem><para>correct_data</para><para>
471 In case of an ECC error this function is called for
472 error detection and correction. Return 1 respectively 2
473 in case the error can be corrected. If the error is
474 not correctable return -1. If your hardware generator
475 matches the default algorithm of the nand_ecc software
476 generator then use the correction function provided
477 by nand_ecc instead of implementing duplicated code.
478 </para> </listitem>
479 </itemizedlist>
480 </para>
481 </sect2>
482 <sect2>
483 <title>Hardware ECC with syndrome calculation</title>
484 <para>
485 Many hardware ECC implementations provide Reed-Solomon
486 codes and calculate an error syndrome on read. The syndrome
487 must be converted to a standard Reed-Solomon syndrome
488 before calling the error correction code in the generic
489 Reed-Solomon library.
490 </para>
491 <para>
492 The ECC bytes must be placed immidiately after the data
493 bytes in order to make the syndrome generator work. This
494 is contrary to the usual layout used by software ECC. The
495 seperation of data and out of band area is not longer
496 possible. The nand driver code handles this layout and
497 the remaining free bytes in the oob area are managed by
498 the autoplacement code. Provide a matching oob-layout
499 in this case. See rts_from4.c and diskonchip.c for
500 implementation reference. In those cases we must also
501 use bad block tables on FLASH, because the ECC layout is
502 interferring with the bad block marker positions.
503 See bad block table support for details.
504 </para>
505 </sect2>
506 </sect1>
507 <sect1>
508 <title>Bad block table support</title>
509 <para>
510 Most NAND chips mark the bad blocks at a defined
511 position in the spare area. Those blocks must
512 not be erased under any circumstances as the bad
513 block information would be lost.
514 It is possible to check the bad block mark each
515 time when the blocks are accessed by reading the
516 spare area of the first page in the block. This
517 is time consuming so a bad block table is used.
518 </para>
519 <para>
520 The nand driver supports various types of bad block
521 tables.
522 <itemizedlist>
523 <listitem><para>Per device</para><para>
524 The bad block table contains all bad block information
525 of the device which can consist of multiple chips.
526 </para> </listitem>
527 <listitem><para>Per chip</para><para>
528 A bad block table is used per chip and contains the
529 bad block information for this particular chip.
530 </para> </listitem>
531 <listitem><para>Fixed offset</para><para>
532 The bad block table is located at a fixed offset
533 in the chip (device). This applies to various
534 DiskOnChip devices.
535 </para> </listitem>
536 <listitem><para>Automatic placed</para><para>
537 The bad block table is automatically placed and
538 detected either at the end or at the beginning
539 of a chip (device)
540 </para> </listitem>
541 <listitem><para>Mirrored tables</para><para>
542 The bad block table is mirrored on the chip (device) to
543 allow updates of the bad block table without data loss.
544 </para> </listitem>
545 </itemizedlist>
546 </para>
547 <para>
548 nand_scan() calls the function nand_default_bbt().
549 nand_default_bbt() selects appropriate default
550 bad block table desriptors depending on the chip information
551 which was retrieved by nand_scan().
552 </para>
553 <para>
554 The standard policy is scanning the device for bad
555 blocks and build a ram based bad block table which
556 allows faster access than always checking the
557 bad block information on the flash chip itself.
558 </para>
559 <sect2>
560 <title>Flash based tables</title>
561 <para>
562 It may be desired or neccecary to keep a bad block table in FLASH.
563 For AG-AND chips this is mandatory, as they have no factory marked
564 bad blocks. They have factory marked good blocks. The marker pattern
565 is erased when the block is erased to be reused. So in case of
566 powerloss before writing the pattern back to the chip this block
567 would be lost and added to the bad blocks. Therefor we scan the
568 chip(s) when we detect them the first time for good blocks and
569 store this information in a bad block table before erasing any
570 of the blocks.
571 </para>
572 <para>
573 The blocks in which the tables are stored are procteted against
574 accidental access by marking them bad in the memory bad block
575 table. The bad block table managment functions are allowed
576 to circumvernt this protection.
577 </para>
578 <para>
579 The simplest way to activate the FLASH based bad block table support
580 is to set the option NAND_USE_FLASH_BBT in the option field of
581 the nand chip structure before calling nand_scan(). For AG-AND
582 chips is this done by default.
583 This activates the default FLASH based bad block table functionality
584 of the NAND driver. The default bad block table options are
585 <itemizedlist>
586 <listitem><para>Store bad block table per chip</para></listitem>
587 <listitem><para>Use 2 bits per block</para></listitem>
588 <listitem><para>Automatic placement at the end of the chip</para></listitem>
589 <listitem><para>Use mirrored tables with version numbers</para></listitem>
590 <listitem><para>Reserve 4 blocks at the end of the chip</para></listitem>
591 </itemizedlist>
592 </para>
593 </sect2>
594 <sect2>
595 <title>User defined tables</title>
596 <para>
597 User defined tables are created by filling out a
598 nand_bbt_descr structure and storing the pointer in the
599 nand_chip structure member bbt_td before calling nand_scan().
600 If a mirror table is neccecary a second structure must be
601 created and a pointer to this structure must be stored
602 in bbt_md inside the nand_chip structure. If the bbt_md
603 member is set to NULL then only the main table is used
604 and no scan for the mirrored table is performed.
605 </para>
606 <para>
607 The most important field in the nand_bbt_descr structure
608 is the options field. The options define most of the
609 table properties. Use the predefined constants from
610 nand.h to define the options.
611 <itemizedlist>
612 <listitem><para>Number of bits per block</para>
613 <para>The supported number of bits is 1, 2, 4, 8.</para></listitem>
614 <listitem><para>Table per chip</para>
615 <para>Setting the constant NAND_BBT_PERCHIP selects that
616 a bad block table is managed for each chip in a chip array.
617 If this option is not set then a per device bad block table
618 is used.</para></listitem>
619 <listitem><para>Table location is absolute</para>
620 <para>Use the option constant NAND_BBT_ABSPAGE and
621 define the absolute page number where the bad block
622 table starts in the field pages. If you have selected bad block
623 tables per chip and you have a multi chip array then the start page
624 must be given for each chip in the chip array. Note: there is no scan
625 for a table ident pattern performed, so the fields
626 pattern, veroffs, offs, len can be left uninitialized</para></listitem>
627 <listitem><para>Table location is automatically detected</para>
628 <para>The table can either be located in the first or the last good
629 blocks of the chip (device). Set NAND_BBT_LASTBLOCK to place
630 the bad block table at the end of the chip (device). The
631 bad block tables are marked and identified by a pattern which
632 is stored in the spare area of the first page in the block which
633 holds the bad block table. Store a pointer to the pattern
634 in the pattern field. Further the length of the pattern has to be
635 stored in len and the offset in the spare area must be given
636 in the offs member of the nand_bbt_descr stucture. For mirrored
637 bad block tables different patterns are mandatory.</para></listitem>
638 <listitem><para>Table creation</para>
639 <para>Set the option NAND_BBT_CREATE to enable the table creation
640 if no table can be found during the scan. Usually this is done only
641 once if a new chip is found. </para></listitem>
642 <listitem><para>Table write support</para>
643 <para>Set the option NAND_BBT_WRITE to enable the table write support.
644 This allows the update of the bad block table(s) in case a block has
645 to be marked bad due to wear. The MTD interface function block_markbad
646 is calling the update function of the bad block table. If the write
647 support is enabled then the table is updated on FLASH.</para>
648 <para>
649 Note: Write support should only be enabled for mirrored tables with
650 version control.
651 </para></listitem>
652 <listitem><para>Table version control</para>
653 <para>Set the option NAND_BBT_VERSION to enable the table version control.
654 It's highly recommended to enable this for mirrored tables with write
655 support. It makes sure that the risk of loosing the bad block
656 table information is reduced to the loss of the information about the
657 one worn out block which should be marked bad. The version is stored in
658 4 consecutive bytes in the spare area of the device. The position of
659 the version number is defined by the member veroffs in the bad block table
660 descriptor.</para></listitem>
661 <listitem><para>Save block contents on write</para>
662 <para>
663 In case that the block which holds the bad block table does contain
664 other useful information, set the option NAND_BBT_SAVECONTENT. When
665 the bad block table is written then the whole block is read the bad
666 block table is updated and the block is erased and everything is
667 written back. If this option is not set only the bad block table
668 is written and everything else in the block is ignored and erased.
669 </para></listitem>
670 <listitem><para>Number of reserved blocks</para>
671 <para>
672 For automatic placement some blocks must be reserved for
673 bad block table storage. The number of reserved blocks is defined
674 in the maxblocks member of the babd block table description structure.
675 Reserving 4 blocks for mirrored tables should be a reasonable number.
676 This also limits the number of blocks which are scanned for the bad
677 block table ident pattern.
678 </para></listitem>
679 </itemizedlist>
680 </para>
681 </sect2>
682 </sect1>
683 <sect1>
684 <title>Spare area (auto)placement</title>
685 <para>
686 The nand driver implements different possibilities for
687 placement of filesystem data in the spare area,
688 <itemizedlist>
689 <listitem><para>Placement defined by fs driver</para></listitem>
690 <listitem><para>Automatic placement</para></listitem>
691 </itemizedlist>
692 The default placement function is automatic placement. The
693 nand driver has built in default placement schemes for the
694 various chiptypes. If due to hardware ECC functionality the
695 default placement does not fit then the board driver can
696 provide a own placement scheme.
697 </para>
698 <para>
699 File system drivers can provide a own placement scheme which
700 is used instead of the default placement scheme.
701 </para>
702 <para>
703 Placement schemes are defined by a nand_oobinfo structure
704 <programlisting>
705struct nand_oobinfo {
706 int useecc;
707 int eccbytes;
708 int eccpos[24];
709 int oobfree[8][2];
710};
711 </programlisting>
712 <itemizedlist>
713 <listitem><para>useecc</para><para>
714 The useecc member controls the ecc and placement function. The header
715 file include/mtd/mtd-abi.h contains constants to select ecc and
716 placement. MTD_NANDECC_OFF switches off the ecc complete. This is
717 not recommended and available for testing and diagnosis only.
718 MTD_NANDECC_PLACE selects caller defined placement, MTD_NANDECC_AUTOPLACE
719 selects automatic placement.
720 </para></listitem>
721 <listitem><para>eccbytes</para><para>
722 The eccbytes member defines the number of ecc bytes per page.
723 </para></listitem>
724 <listitem><para>eccpos</para><para>
725 The eccpos array holds the byte offsets in the spare area where
726 the ecc codes are placed.
727 </para></listitem>
728 <listitem><para>oobfree</para><para>
729 The oobfree array defines the areas in the spare area which can be
730 used for automatic placement. The information is given in the format
731 {offset, size}. offset defines the start of the usable area, size the
732 length in bytes. More than one area can be defined. The list is terminated
733 by an {0, 0} entry.
734 </para></listitem>
735 </itemizedlist>
736 </para>
737 <sect2>
738 <title>Placement defined by fs driver</title>
739 <para>
740 The calling function provides a pointer to a nand_oobinfo
741 structure which defines the ecc placement. For writes the
742 caller must provide a spare area buffer along with the
743 data buffer. The spare area buffer size is (number of pages) *
744 (size of spare area). For reads the buffer size is
745 (number of pages) * ((size of spare area) + (number of ecc
746 steps per page) * sizeof (int)). The driver stores the
747 result of the ecc check for each tuple in the spare buffer.
748 The storage sequence is
749 </para>
750 <para>
751 &lt;spare data page 0&gt;&lt;ecc result 0&gt;...&lt;ecc result n&gt;
752 </para>
753 <para>
754 ...
755 </para>
756 <para>
757 &lt;spare data page n&gt;&lt;ecc result 0&gt;...&lt;ecc result n&gt;
758 </para>
759 <para>
760 This is a legacy mode used by YAFFS1.
761 </para>
762 <para>
763 If the spare area buffer is NULL then only the ECC placement is
764 done according to the given scheme in the nand_oobinfo structure.
765 </para>
766 </sect2>
767 <sect2>
768 <title>Automatic placement</title>
769 <para>
770 Automatic placement uses the built in defaults to place the
771 ecc bytes in the spare area. If filesystem data have to be stored /
772 read into the spare area then the calling function must provide a
773 buffer. The buffer size per page is determined by the oobfree array in
774 the nand_oobinfo structure.
775 </para>
776 <para>
777 If the spare area buffer is NULL then only the ECC placement is
778 done according to the default builtin scheme.
779 </para>
780 </sect2>
781 <sect2>
782 <title>User space placement selection</title>
783 <para>
784 All non ecc functions like mtd->read and mtd->write use an internal
785 structure, which can be set by an ioctl. This structure is preset
786 to the autoplacement default.
787 <programlisting>
788 ioctl (fd, MEMSETOOBSEL, oobsel);
789 </programlisting>
790 oobsel is a pointer to a user supplied structure of type
791 nand_oobconfig. The contents of this structure must match the
792 criteria of the filesystem, which will be used. See an example in utils/nandwrite.c.
793 </para>
794 </sect2>
795 </sect1>
796 <sect1>
797 <title>Spare area autoplacement default schemes</title>
798 <sect2>
799 <title>256 byte pagesize</title>
800<informaltable><tgroup cols="3"><tbody>
801<row>
802<entry>Offset</entry>
803<entry>Content</entry>
804<entry>Comment</entry>
805</row>
806<row>
807<entry>0x00</entry>
808<entry>ECC byte 0</entry>
809<entry>Error correction code byte 0</entry>
810</row>
811<row>
812<entry>0x01</entry>
813<entry>ECC byte 1</entry>
814<entry>Error correction code byte 1</entry>
815</row>
816<row>
817<entry>0x02</entry>
818<entry>ECC byte 2</entry>
819<entry>Error correction code byte 2</entry>
820</row>
821<row>
822<entry>0x03</entry>
823<entry>Autoplace 0</entry>
824<entry></entry>
825</row>
826<row>
827<entry>0x04</entry>
828<entry>Autoplace 1</entry>
829<entry></entry>
830</row>
831<row>
832<entry>0x05</entry>
833<entry>Bad block marker</entry>
834<entry>If any bit in this byte is zero, then this block is bad.
835This applies only to the first page in a block. In the remaining
836pages this byte is reserved</entry>
837</row>
838<row>
839<entry>0x06</entry>
840<entry>Autoplace 2</entry>
841<entry></entry>
842</row>
843<row>
844<entry>0x07</entry>
845<entry>Autoplace 3</entry>
846<entry></entry>
847</row>
848</tbody></tgroup></informaltable>
849 </sect2>
850 <sect2>
851 <title>512 byte pagesize</title>
852<informaltable><tgroup cols="3"><tbody>
853<row>
854<entry>Offset</entry>
855<entry>Content</entry>
856<entry>Comment</entry>
857</row>
858<row>
859<entry>0x00</entry>
860<entry>ECC byte 0</entry>
861<entry>Error correction code byte 0 of the lower 256 Byte data in
862this page</entry>
863</row>
864<row>
865<entry>0x01</entry>
866<entry>ECC byte 1</entry>
867<entry>Error correction code byte 1 of the lower 256 Bytes of data
868in this page</entry>
869</row>
870<row>
871<entry>0x02</entry>
872<entry>ECC byte 2</entry>
873<entry>Error correction code byte 2 of the lower 256 Bytes of data
874in this page</entry>
875</row>
876<row>
877<entry>0x03</entry>
878<entry>ECC byte 3</entry>
879<entry>Error correction code byte 0 of the upper 256 Bytes of data
880in this page</entry>
881</row>
882<row>
883<entry>0x04</entry>
884<entry>reserved</entry>
885<entry>reserved</entry>
886</row>
887<row>
888<entry>0x05</entry>
889<entry>Bad block marker</entry>
890<entry>If any bit in this byte is zero, then this block is bad.
891This applies only to the first page in a block. In the remaining
892pages this byte is reserved</entry>
893</row>
894<row>
895<entry>0x06</entry>
896<entry>ECC byte 4</entry>
897<entry>Error correction code byte 1 of the upper 256 Bytes of data
898in this page</entry>
899</row>
900<row>
901<entry>0x07</entry>
902<entry>ECC byte 5</entry>
903<entry>Error correction code byte 2 of the upper 256 Bytes of data
904in this page</entry>
905</row>
906<row>
907<entry>0x08 - 0x0F</entry>
908<entry>Autoplace 0 - 7</entry>
909<entry></entry>
910</row>
911</tbody></tgroup></informaltable>
912 </sect2>
913 <sect2>
914 <title>2048 byte pagesize</title>
915<informaltable><tgroup cols="3"><tbody>
916<row>
917<entry>Offset</entry>
918<entry>Content</entry>
919<entry>Comment</entry>
920</row>
921<row>
922<entry>0x00</entry>
923<entry>Bad block marker</entry>
924<entry>If any bit in this byte is zero, then this block is bad.
925This applies only to the first page in a block. In the remaining
926pages this byte is reserved</entry>
927</row>
928<row>
929<entry>0x01</entry>
930<entry>Reserved</entry>
931<entry>Reserved</entry>
932</row>
933<row>
934<entry>0x02-0x27</entry>
935<entry>Autoplace 0 - 37</entry>
936<entry></entry>
937</row>
938<row>
939<entry>0x28</entry>
940<entry>ECC byte 0</entry>
941<entry>Error correction code byte 0 of the first 256 Byte data in
942this page</entry>
943</row>
944<row>
945<entry>0x29</entry>
946<entry>ECC byte 1</entry>
947<entry>Error correction code byte 1 of the first 256 Bytes of data
948in this page</entry>
949</row>
950<row>
951<entry>0x2A</entry>
952<entry>ECC byte 2</entry>
953<entry>Error correction code byte 2 of the first 256 Bytes data in
954this page</entry>
955</row>
956<row>
957<entry>0x2B</entry>
958<entry>ECC byte 3</entry>
959<entry>Error correction code byte 0 of the second 256 Bytes of data
960in this page</entry>
961</row>
962<row>
963<entry>0x2C</entry>
964<entry>ECC byte 4</entry>
965<entry>Error correction code byte 1 of the second 256 Bytes of data
966in this page</entry>
967</row>
968<row>
969<entry>0x2D</entry>
970<entry>ECC byte 5</entry>
971<entry>Error correction code byte 2 of the second 256 Bytes of data
972in this page</entry>
973</row>
974<row>
975<entry>0x2E</entry>
976<entry>ECC byte 6</entry>
977<entry>Error correction code byte 0 of the third 256 Bytes of data
978in this page</entry>
979</row>
980<row>
981<entry>0x2F</entry>
982<entry>ECC byte 7</entry>
983<entry>Error correction code byte 1 of the third 256 Bytes of data
984in this page</entry>
985</row>
986<row>
987<entry>0x30</entry>
988<entry>ECC byte 8</entry>
989<entry>Error correction code byte 2 of the third 256 Bytes of data
990in this page</entry>
991</row>
992<row>
993<entry>0x31</entry>
994<entry>ECC byte 9</entry>
995<entry>Error correction code byte 0 of the fourth 256 Bytes of data
996in this page</entry>
997</row>
998<row>
999<entry>0x32</entry>
1000<entry>ECC byte 10</entry>
1001<entry>Error correction code byte 1 of the fourth 256 Bytes of data
1002in this page</entry>
1003</row>
1004<row>
1005<entry>0x33</entry>
1006<entry>ECC byte 11</entry>
1007<entry>Error correction code byte 2 of the fourth 256 Bytes of data
1008in this page</entry>
1009</row>
1010<row>
1011<entry>0x34</entry>
1012<entry>ECC byte 12</entry>
1013<entry>Error correction code byte 0 of the fifth 256 Bytes of data
1014in this page</entry>
1015</row>
1016<row>
1017<entry>0x35</entry>
1018<entry>ECC byte 13</entry>
1019<entry>Error correction code byte 1 of the fifth 256 Bytes of data
1020in this page</entry>
1021</row>
1022<row>
1023<entry>0x36</entry>
1024<entry>ECC byte 14</entry>
1025<entry>Error correction code byte 2 of the fifth 256 Bytes of data
1026in this page</entry>
1027</row>
1028<row>
1029<entry>0x37</entry>
1030<entry>ECC byte 15</entry>
1031<entry>Error correction code byte 0 of the sixt 256 Bytes of data
1032in this page</entry>
1033</row>
1034<row>
1035<entry>0x38</entry>
1036<entry>ECC byte 16</entry>
1037<entry>Error correction code byte 1 of the sixt 256 Bytes of data
1038in this page</entry>
1039</row>
1040<row>
1041<entry>0x39</entry>
1042<entry>ECC byte 17</entry>
1043<entry>Error correction code byte 2 of the sixt 256 Bytes of data
1044in this page</entry>
1045</row>
1046<row>
1047<entry>0x3A</entry>
1048<entry>ECC byte 18</entry>
1049<entry>Error correction code byte 0 of the seventh 256 Bytes of
1050data in this page</entry>
1051</row>
1052<row>
1053<entry>0x3B</entry>
1054<entry>ECC byte 19</entry>
1055<entry>Error correction code byte 1 of the seventh 256 Bytes of
1056data in this page</entry>
1057</row>
1058<row>
1059<entry>0x3C</entry>
1060<entry>ECC byte 20</entry>
1061<entry>Error correction code byte 2 of the seventh 256 Bytes of
1062data in this page</entry>
1063</row>
1064<row>
1065<entry>0x3D</entry>
1066<entry>ECC byte 21</entry>
1067<entry>Error correction code byte 0 of the eigth 256 Bytes of data
1068in this page</entry>
1069</row>
1070<row>
1071<entry>0x3E</entry>
1072<entry>ECC byte 22</entry>
1073<entry>Error correction code byte 1 of the eigth 256 Bytes of data
1074in this page</entry>
1075</row>
1076<row>
1077<entry>0x3F</entry>
1078<entry>ECC byte 23</entry>
1079<entry>Error correction code byte 2 of the eigth 256 Bytes of data
1080in this page</entry>
1081</row>
1082</tbody></tgroup></informaltable>
1083 </sect2>
1084 </sect1>
1085 </chapter>
1086
1087 <chapter id="filesystems">
1088 <title>Filesystem support</title>
1089 <para>
1090 The NAND driver provides all neccecary functions for a
1091 filesystem via the MTD interface.
1092 </para>
1093 <para>
1094 Filesystems must be aware of the NAND pecularities and
1095 restrictions. One major restrictions of NAND Flash is, that you cannot
1096 write as often as you want to a page. The consecutive writes to a page,
1097 before erasing it again, are restricted to 1-3 writes, depending on the
1098 manufacturers specifications. This applies similar to the spare area.
1099 </para>
1100 <para>
1101 Therefor NAND aware filesystems must either write in page size chunks
1102 or hold a writebuffer to collect smaller writes until they sum up to
1103 pagesize. Available NAND aware filesystems: JFFS2, YAFFS.
1104 </para>
1105 <para>
1106 The spare area usage to store filesystem data is controlled by
1107 the spare area placement functionality which is described in one
1108 of the earlier chapters.
1109 </para>
1110 </chapter>
1111 <chapter id="tools">
1112 <title>Tools</title>
1113 <para>
1114 The MTD project provides a couple of helpful tools to handle NAND Flash.
1115 <itemizedlist>
1116 <listitem><para>flasherase, flasheraseall: Erase and format FLASH partitions</para></listitem>
1117 <listitem><para>nandwrite: write filesystem images to NAND FLASH</para></listitem>
1118 <listitem><para>nanddump: dump the contents of a NAND FLASH partitions</para></listitem>
1119 </itemizedlist>
1120 </para>
1121 <para>
1122 These tools are aware of the NAND restrictions. Please use those tools
1123 instead of complaining about errors which are caused by non NAND aware
1124 access methods.
1125 </para>
1126 </chapter>
1127
1128 <chapter id="defines">
1129 <title>Constants</title>
1130 <para>
1131 This chapter describes the constants which might be relevant for a driver developer.
1132 </para>
1133 <sect1>
1134 <title>Chip option constants</title>
1135 <sect2>
1136 <title>Constants for chip id table</title>
1137 <para>
1138 These constants are defined in nand.h. They are ored together to describe
1139 the chip functionality.
1140 <programlisting>
1141/* Chip can not auto increment pages */
1142#define NAND_NO_AUTOINCR 0x00000001
1143/* Buswitdh is 16 bit */
1144#define NAND_BUSWIDTH_16 0x00000002
1145/* Device supports partial programming without padding */
1146#define NAND_NO_PADDING 0x00000004
1147/* Chip has cache program function */
1148#define NAND_CACHEPRG 0x00000008
1149/* Chip has copy back function */
1150#define NAND_COPYBACK 0x00000010
1151/* AND Chip which has 4 banks and a confusing page / block
1152 * assignment. See Renesas datasheet for further information */
1153#define NAND_IS_AND 0x00000020
1154/* Chip has a array of 4 pages which can be read without
1155 * additional ready /busy waits */
1156#define NAND_4PAGE_ARRAY 0x00000040
1157 </programlisting>
1158 </para>
1159 </sect2>
1160 <sect2>
1161 <title>Constants for runtime options</title>
1162 <para>
1163 These constants are defined in nand.h. They are ored together to describe
1164 the functionality.
1165 <programlisting>
1166/* Use a flash based bad block table. This option is parsed by the
1167 * default bad block table function (nand_default_bbt). */
1168#define NAND_USE_FLASH_BBT 0x00010000
1169/* The hw ecc generator provides a syndrome instead a ecc value on read
1170 * This can only work if we have the ecc bytes directly behind the
1171 * data bytes. Applies for DOC and AG-AND Renesas HW Reed Solomon generators */
1172#define NAND_HWECC_SYNDROME 0x00020000
1173 </programlisting>
1174 </para>
1175 </sect2>
1176 </sect1>
1177
1178 <sect1>
1179 <title>ECC selection constants</title>
1180 <para>
1181 Use these constants to select the ECC algorithm.
1182 <programlisting>
1183/* No ECC. Usage is not recommended ! */
1184#define NAND_ECC_NONE 0
1185/* Software ECC 3 byte ECC per 256 Byte data */
1186#define NAND_ECC_SOFT 1
1187/* Hardware ECC 3 byte ECC per 256 Byte data */
1188#define NAND_ECC_HW3_256 2
1189/* Hardware ECC 3 byte ECC per 512 Byte data */
1190#define NAND_ECC_HW3_512 3
1191/* Hardware ECC 6 byte ECC per 512 Byte data */
1192#define NAND_ECC_HW6_512 4
1193/* Hardware ECC 6 byte ECC per 512 Byte data */
1194#define NAND_ECC_HW8_512 6
1195 </programlisting>
1196 </para>
1197 </sect1>
1198
1199 <sect1>
1200 <title>Hardware control related constants</title>
1201 <para>
1202 These constants describe the requested hardware access function when
1203 the boardspecific hardware control function is called
1204 <programlisting>
1205/* Select the chip by setting nCE to low */
1206#define NAND_CTL_SETNCE 1
1207/* Deselect the chip by setting nCE to high */
1208#define NAND_CTL_CLRNCE 2
1209/* Select the command latch by setting CLE to high */
1210#define NAND_CTL_SETCLE 3
1211/* Deselect the command latch by setting CLE to low */
1212#define NAND_CTL_CLRCLE 4
1213/* Select the address latch by setting ALE to high */
1214#define NAND_CTL_SETALE 5
1215/* Deselect the address latch by setting ALE to low */
1216#define NAND_CTL_CLRALE 6
1217/* Set write protection by setting WP to high. Not used! */
1218#define NAND_CTL_SETWP 7
1219/* Clear write protection by setting WP to low. Not used! */
1220#define NAND_CTL_CLRWP 8
1221 </programlisting>
1222 </para>
1223 </sect1>
1224
1225 <sect1>
1226 <title>Bad block table related constants</title>
1227 <para>
1228 These constants describe the options used for bad block
1229 table descriptors.
1230 <programlisting>
1231/* Options for the bad block table descriptors */
1232
1233/* The number of bits used per block in the bbt on the device */
1234#define NAND_BBT_NRBITS_MSK 0x0000000F
1235#define NAND_BBT_1BIT 0x00000001
1236#define NAND_BBT_2BIT 0x00000002
1237#define NAND_BBT_4BIT 0x00000004
1238#define NAND_BBT_8BIT 0x00000008
1239/* The bad block table is in the last good block of the device */
1240#define NAND_BBT_LASTBLOCK 0x00000010
1241/* The bbt is at the given page, else we must scan for the bbt */
1242#define NAND_BBT_ABSPAGE 0x00000020
1243/* The bbt is at the given page, else we must scan for the bbt */
1244#define NAND_BBT_SEARCH 0x00000040
1245/* bbt is stored per chip on multichip devices */
1246#define NAND_BBT_PERCHIP 0x00000080
1247/* bbt has a version counter at offset veroffs */
1248#define NAND_BBT_VERSION 0x00000100
1249/* Create a bbt if none axists */
1250#define NAND_BBT_CREATE 0x00000200
1251/* Search good / bad pattern through all pages of a block */
1252#define NAND_BBT_SCANALLPAGES 0x00000400
1253/* Scan block empty during good / bad block scan */
1254#define NAND_BBT_SCANEMPTY 0x00000800
1255/* Write bbt if neccecary */
1256#define NAND_BBT_WRITE 0x00001000
1257/* Read and write back block contents when writing bbt */
1258#define NAND_BBT_SAVECONTENT 0x00002000
1259 </programlisting>
1260 </para>
1261 </sect1>
1262
1263 </chapter>
1264
1265 <chapter id="structs">
1266 <title>Structures</title>
1267 <para>
1268 This chapter contains the autogenerated documentation of the structures which are
1269 used in the NAND driver and might be relevant for a driver developer. Each
1270 struct member has a short description which is marked with an [XXX] identifier.
1271 See the chapter "Documentation hints" for an explanation.
1272 </para>
1273!Iinclude/linux/mtd/nand.h
1274 </chapter>
1275
1276 <chapter id="pubfunctions">
1277 <title>Public Functions Provided</title>
1278 <para>
1279 This chapter contains the autogenerated documentation of the NAND kernel API functions
1280 which are exported. Each function has a short description which is marked with an [XXX] identifier.
1281 See the chapter "Documentation hints" for an explanation.
1282 </para>
1283!Edrivers/mtd/nand/nand_base.c
1284!Edrivers/mtd/nand/nand_bbt.c
1285!Edrivers/mtd/nand/nand_ecc.c
1286 </chapter>
1287
1288 <chapter id="intfunctions">
1289 <title>Internal Functions Provided</title>
1290 <para>
1291 This chapter contains the autogenerated documentation of the NAND driver internal functions.
1292 Each function has a short description which is marked with an [XXX] identifier.
1293 See the chapter "Documentation hints" for an explanation.
1294 The functions marked with [DEFAULT] might be relevant for a board driver developer.
1295 </para>
1296!Idrivers/mtd/nand/nand_base.c
1297!Idrivers/mtd/nand/nand_bbt.c
1298!Idrivers/mtd/nand/nand_ecc.c
1299 </chapter>
1300
1301 <chapter id="credits">
1302 <title>Credits</title>
1303 <para>
1304 The following people have contributed to the NAND driver:
1305 <orderedlist>
1306 <listitem><para>Steven J. Hill<email>sjhill@realitydiluted.com</email></para></listitem>
1307 <listitem><para>David Woodhouse<email>dwmw2@infradead.org</email></para></listitem>
1308 <listitem><para>Thomas Gleixner<email>tglx@linutronix.de</email></para></listitem>
1309 </orderedlist>
1310 A lot of users have provided bugfixes, improvements and helping hands for testing.
1311 Thanks a lot.
1312 </para>
1313 <para>
1314 The following people have contributed to this document:
1315 <orderedlist>
1316 <listitem><para>Thomas Gleixner<email>tglx@linutronix.de</email></para></listitem>
1317 </orderedlist>
1318 </para>
1319 </chapter>
1320</book>