summaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
Diffstat (limited to 'Documentation/digiepca.txt')
-rw-r--r--Documentation/digiepca.txt98
1 files changed, 98 insertions, 0 deletions
diff --git a/Documentation/digiepca.txt b/Documentation/digiepca.txt
new file mode 100644
index 000000000000..88820fe38dad
--- /dev/null
+++ b/Documentation/digiepca.txt
@@ -0,0 +1,98 @@
1NOTE: This driver is obsolete. Digi provides a 2.6 driver (dgdm) at
2http://www.digi.com for PCI cards. They no longer maintain this driver,
3and have no 2.6 driver for ISA cards.
4
5This driver requires a number of user-space tools. They can be aquired from
6http://www.digi.com, but only works with 2.4 kernels.
7
8
9The Digi Intl. epca driver.
10----------------------------
11The Digi Intl. epca driver for Linux supports the following boards:
12
13Digi PC/Xem, PC/Xr, PC/Xe, PC/Xi, PC/Xeve
14Digi EISA/Xem, PCI/Xem, PCI/Xr
15
16Limitations:
17------------
18Currently the driver only autoprobes for supported PCI boards.
19
20The Linux MAKEDEV command does not support generating the Digiboard
21Devices. Users executing digiConfig to setup EISA and PC series cards
22will have their device nodes automatically constructed (cud?? for ~CLOCAL,
23and ttyD?? for CLOCAL). Users wishing to boot their board from the LILO
24prompt, or those users booting PCI cards may use buildDIGI to construct
25the necessary nodes.
26
27Notes:
28------
29This driver may be configured via LILO. For users who have already configured
30their driver using digiConfig, configuring from LILO will override previous
31settings. Multiple boards may be configured by issuing multiple LILO command
32lines. For examples see the bottom of this document.
33
34Device names start at 0 and continue up. Beware of this as previous Digi
35drivers started device names with 1.
36
37PCI boards are auto-detected and configured by the driver. PCI boards will
38be allocated device numbers (internally) beginning with the lowest PCI slot
39first. In other words a PCI card in slot 3 will always have higher device
40nodes than a PCI card in slot 1.
41
42LILO config examples:
43---------------------
44Using LILO's APPEND command, a string of comma separated identifiers or
45integers can be used to configure supported boards. The six values in order
46are:
47
48 Enable/Disable this card or Override,
49 Type of card: PC/Xe (AccelePort) (0), PC/Xeve (1), PC/Xem or PC/Xr (2),
50 EISA/Xem (3), PC/64Xe (4), PC/Xi (5),
51 Enable/Disable alternate pin arrangement,
52 Number of ports on this card,
53 I/O Port where card is configured (in HEX if using string identifiers),
54 Base of memory window (in HEX if using string identifiers),
55
56NOTE : PCI boards are auto-detected and configured. Do not attempt to
57configure PCI boards with the LILO append command. If you wish to override
58previous configuration data (As set by digiConfig), but you do not wish to
59configure any specific card (Example if there are PCI cards in the system)
60the following override command will accomplish this:
61-> append="digi=2"
62
63Samples:
64 append="digiepca=E,PC/Xe,D,16,200,D0000"
65 or
66 append="digi=1,0,0,16,512,851968"
67
68Supporting Tools:
69-----------------
70Supporting tools include digiDload, digiConfig, buildPCI, and ditty. See
71drivers/char/README.epca for more details. Note,
72this driver REQUIRES that digiDload be executed prior to it being used.
73Failure to do this will result in an ENODEV error.
74
75Documentation:
76--------------
77Complete documentation for this product may be found in the tool package.
78
79Sources of information and support:
80-----------------------------------
81Digi Intl. support site for this product:
82
83-> http://www.digi.com
84
85Acknowledgments:
86----------------
87Much of this work (And even text) was derived from a similar document
88supporting the original public domain DigiBoard driver Copyright (C)
891994,1995 Troy De Jongh. Many thanks to Christoph Lameter
90(christoph@lameter.com) and Mike McLagan (mike.mclagan@linux.org) who authored
91and contributed to the original document.
92
93Changelog:
94----------
9510-29-04: Update status of driver, remove dead links in document
96 James Nelson <james4765@gmail.com>
97
982000 (?) Original Document