summaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
Diffstat (limited to 'Documentation/driver-model/bus.txt')
-rw-r--r--Documentation/driver-model/bus.txt160
1 files changed, 160 insertions, 0 deletions
diff --git a/Documentation/driver-model/bus.txt b/Documentation/driver-model/bus.txt
new file mode 100644
index 000000000000..dd62c7b80b3f
--- /dev/null
+++ b/Documentation/driver-model/bus.txt
@@ -0,0 +1,160 @@
1
2Bus Types
3
4Definition
5~~~~~~~~~~
6
7struct bus_type {
8 char * name;
9
10 struct subsystem subsys;
11 struct kset drivers;
12 struct kset devices;
13
14 struct bus_attribute * bus_attrs;
15 struct device_attribute * dev_attrs;
16 struct driver_attribute * drv_attrs;
17
18 int (*match)(struct device * dev, struct device_driver * drv);
19 int (*hotplug) (struct device *dev, char **envp,
20 int num_envp, char *buffer, int buffer_size);
21 int (*suspend)(struct device * dev, u32 state);
22 int (*resume)(struct device * dev);
23};
24
25int bus_register(struct bus_type * bus);
26
27
28Declaration
29~~~~~~~~~~~
30
31Each bus type in the kernel (PCI, USB, etc) should declare one static
32object of this type. They must initialize the name field, and may
33optionally initialize the match callback.
34
35struct bus_type pci_bus_type = {
36 .name = "pci",
37 .match = pci_bus_match,
38};
39
40The structure should be exported to drivers in a header file:
41
42extern struct bus_type pci_bus_type;
43
44
45Registration
46~~~~~~~~~~~~
47
48When a bus driver is initialized, it calls bus_register. This
49initializes the rest of the fields in the bus object and inserts it
50into a global list of bus types. Once the bus object is registered,
51the fields in it are usable by the bus driver.
52
53
54Callbacks
55~~~~~~~~~
56
57match(): Attaching Drivers to Devices
58~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
59
60The format of device ID structures and the semantics for comparing
61them are inherently bus-specific. Drivers typically declare an array
62of device IDs of devices they support that reside in a bus-specific
63driver structure.
64
65The purpose of the match callback is provide the bus an opportunity to
66determine if a particular driver supports a particular device by
67comparing the device IDs the driver supports with the device ID of a
68particular device, without sacrificing bus-specific functionality or
69type-safety.
70
71When a driver is registered with the bus, the bus's list of devices is
72iterated over, and the match callback is called for each device that
73does not have a driver associated with it.
74
75
76
77Device and Driver Lists
78~~~~~~~~~~~~~~~~~~~~~~~
79
80The lists of devices and drivers are intended to replace the local
81lists that many buses keep. They are lists of struct devices and
82struct device_drivers, respectively. Bus drivers are free to use the
83lists as they please, but conversion to the bus-specific type may be
84necessary.
85
86The LDM core provides helper functions for iterating over each list.
87
88int bus_for_each_dev(struct bus_type * bus, struct device * start, void * data,
89 int (*fn)(struct device *, void *));
90
91int bus_for_each_drv(struct bus_type * bus, struct device_driver * start,
92 void * data, int (*fn)(struct device_driver *, void *));
93
94These helpers iterate over the respective list, and call the callback
95for each device or driver in the list. All list accesses are
96synchronized by taking the bus's lock (read currently). The reference
97count on each object in the list is incremented before the callback is
98called; it is decremented after the next object has been obtained. The
99lock is not held when calling the callback.
100
101
102sysfs
103~~~~~~~~
104There is a top-level directory named 'bus'.
105
106Each bus gets a directory in the bus directory, along with two default
107directories:
108
109 /sys/bus/pci/
110 |-- devices
111 `-- drivers
112
113Drivers registered with the bus get a directory in the bus's drivers
114directory:
115
116 /sys/bus/pci/
117 |-- devices
118 `-- drivers
119 |-- Intel ICH
120 |-- Intel ICH Joystick
121 |-- agpgart
122 `-- e100
123
124Each device that is discovered on a bus of that type gets a symlink in
125the bus's devices directory to the device's directory in the physical
126hierarchy:
127
128 /sys/bus/pci/
129 |-- devices
130 | |-- 00:00.0 -> ../../../root/pci0/00:00.0
131 | |-- 00:01.0 -> ../../../root/pci0/00:01.0
132 | `-- 00:02.0 -> ../../../root/pci0/00:02.0
133 `-- drivers
134
135
136Exporting Attributes
137~~~~~~~~~~~~~~~~~~~~
138struct bus_attribute {
139 struct attribute attr;
140 ssize_t (*show)(struct bus_type *, char * buf);
141 ssize_t (*store)(struct bus_type *, const char * buf, size_t count);
142};
143
144Bus drivers can export attributes using the BUS_ATTR macro that works
145similarly to the DEVICE_ATTR macro for devices. For example, a definition
146like this:
147
148static BUS_ATTR(debug,0644,show_debug,store_debug);
149
150is equivalent to declaring:
151
152static bus_attribute bus_attr_debug;
153
154This can then be used to add and remove the attribute from the bus's
155sysfs directory using:
156
157int bus_create_file(struct bus_type *, struct bus_attribute *);
158void bus_remove_file(struct bus_type *, struct bus_attribute *);
159
160