aboutsummaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
Diffstat (limited to 'Documentation/i2c/ten-bit-addresses')
-rw-r--r--Documentation/i2c/ten-bit-addresses36
1 files changed, 19 insertions, 17 deletions
diff --git a/Documentation/i2c/ten-bit-addresses b/Documentation/i2c/ten-bit-addresses
index e9890709c508..cdfe13901b99 100644
--- a/Documentation/i2c/ten-bit-addresses
+++ b/Documentation/i2c/ten-bit-addresses
@@ -1,22 +1,24 @@
1The I2C protocol knows about two kinds of device addresses: normal 7 bit 1The I2C protocol knows about two kinds of device addresses: normal 7 bit
2addresses, and an extended set of 10 bit addresses. The sets of addresses 2addresses, and an extended set of 10 bit addresses. The sets of addresses
3do not intersect: the 7 bit address 0x10 is not the same as the 10 bit 3do not intersect: the 7 bit address 0x10 is not the same as the 10 bit
4address 0x10 (though a single device could respond to both of them). You 4address 0x10 (though a single device could respond to both of them).
5select a 10 bit address by adding an extra byte after the address
6byte:
7 S Addr7 Rd/Wr ....
8becomes
9 S 11110 Addr10 Rd/Wr
10S is the start bit, Rd/Wr the read/write bit, and if you count the number
11of bits, you will see the there are 8 after the S bit for 7 bit addresses,
12and 16 after the S bit for 10 bit addresses.
13 5
14WARNING! The current 10 bit address support is EXPERIMENTAL. There are 6I2C messages to and from 10-bit address devices have a different format.
15several places in the code that will cause SEVERE PROBLEMS with 10 bit 7See the I2C specification for the details.
16addresses, even though there is some basic handling and hooks. Also,
17almost no supported adapter handles the 10 bit addresses correctly.
18 8
19As soon as a real 10 bit address device is spotted 'in the wild', we 9The current 10 bit address support is minimal. It should work, however
20can and will add proper support. Right now, 10 bit address devices 10you can expect some problems along the way:
21are defined by the I2C protocol, but we have never seen a single device 11* Not all bus drivers support 10-bit addresses. Some don't because the
22which supports them. 12 hardware doesn't support them (SMBus doesn't require 10-bit address
13 support for example), some don't because nobody bothered adding the
14 code (or it's there but not working properly.) Software implementation
15 (i2c-algo-bit) is known to work.
16* Some optional features do not support 10-bit addresses. This is the
17 case of automatic detection and instantiation of devices by their,
18 drivers, for example.
19* Many user-space packages (for example i2c-tools) lack support for
20 10-bit addresses.
21
22Note that 10-bit address devices are still pretty rare, so the limitations
23listed above could stay for a long time, maybe even forever if nobody
24needs them to be fixed.