diff options
Diffstat (limited to 'Documentation/power/freezing-of-tasks.txt')
-rw-r--r-- | Documentation/power/freezing-of-tasks.txt | 47 |
1 files changed, 36 insertions, 11 deletions
diff --git a/Documentation/power/freezing-of-tasks.txt b/Documentation/power/freezing-of-tasks.txt index 38b57248fd61..6ccb68f68da6 100644 --- a/Documentation/power/freezing-of-tasks.txt +++ b/Documentation/power/freezing-of-tasks.txt | |||
@@ -21,18 +21,18 @@ freeze_processes() (defined in kernel/power/process.c) is called. It executes | |||
21 | try_to_freeze_tasks() that sets TIF_FREEZE for all of the freezable tasks and | 21 | try_to_freeze_tasks() that sets TIF_FREEZE for all of the freezable tasks and |
22 | either wakes them up, if they are kernel threads, or sends fake signals to them, | 22 | either wakes them up, if they are kernel threads, or sends fake signals to them, |
23 | if they are user space processes. A task that has TIF_FREEZE set, should react | 23 | if they are user space processes. A task that has TIF_FREEZE set, should react |
24 | to it by calling the function called refrigerator() (defined in | 24 | to it by calling the function called __refrigerator() (defined in |
25 | kernel/power/process.c), which sets the task's PF_FROZEN flag, changes its state | 25 | kernel/freezer.c), which sets the task's PF_FROZEN flag, changes its state |
26 | to TASK_UNINTERRUPTIBLE and makes it loop until PF_FROZEN is cleared for it. | 26 | to TASK_UNINTERRUPTIBLE and makes it loop until PF_FROZEN is cleared for it. |
27 | Then, we say that the task is 'frozen' and therefore the set of functions | 27 | Then, we say that the task is 'frozen' and therefore the set of functions |
28 | handling this mechanism is referred to as 'the freezer' (these functions are | 28 | handling this mechanism is referred to as 'the freezer' (these functions are |
29 | defined in kernel/power/process.c and include/linux/freezer.h). User space | 29 | defined in kernel/power/process.c, kernel/freezer.c & include/linux/freezer.h). |
30 | processes are generally frozen before kernel threads. | 30 | User space processes are generally frozen before kernel threads. |
31 | 31 | ||
32 | It is not recommended to call refrigerator() directly. Instead, it is | 32 | __refrigerator() must not be called directly. Instead, use the |
33 | recommended to use the try_to_freeze() function (defined in | 33 | try_to_freeze() function (defined in include/linux/freezer.h), that checks |
34 | include/linux/freezer.h), that checks the task's TIF_FREEZE flag and makes the | 34 | the task's TIF_FREEZE flag and makes the task enter __refrigerator() if the |
35 | task enter refrigerator() if the flag is set. | 35 | flag is set. |
36 | 36 | ||
37 | For user space processes try_to_freeze() is called automatically from the | 37 | For user space processes try_to_freeze() is called automatically from the |
38 | signal-handling code, but the freezable kernel threads need to call it | 38 | signal-handling code, but the freezable kernel threads need to call it |
@@ -61,13 +61,13 @@ wait_event_freezable() and wait_event_freezable_timeout() macros. | |||
61 | After the system memory state has been restored from a hibernation image and | 61 | After the system memory state has been restored from a hibernation image and |
62 | devices have been reinitialized, the function thaw_processes() is called in | 62 | devices have been reinitialized, the function thaw_processes() is called in |
63 | order to clear the PF_FROZEN flag for each frozen task. Then, the tasks that | 63 | order to clear the PF_FROZEN flag for each frozen task. Then, the tasks that |
64 | have been frozen leave refrigerator() and continue running. | 64 | have been frozen leave __refrigerator() and continue running. |
65 | 65 | ||
66 | III. Which kernel threads are freezable? | 66 | III. Which kernel threads are freezable? |
67 | 67 | ||
68 | Kernel threads are not freezable by default. However, a kernel thread may clear | 68 | Kernel threads are not freezable by default. However, a kernel thread may clear |
69 | PF_NOFREEZE for itself by calling set_freezable() (the resetting of PF_NOFREEZE | 69 | PF_NOFREEZE for itself by calling set_freezable() (the resetting of PF_NOFREEZE |
70 | directly is strongly discouraged). From this point it is regarded as freezable | 70 | directly is not allowed). From this point it is regarded as freezable |
71 | and must call try_to_freeze() in a suitable place. | 71 | and must call try_to_freeze() in a suitable place. |
72 | 72 | ||
73 | IV. Why do we do that? | 73 | IV. Why do we do that? |
@@ -95,7 +95,7 @@ after the memory for the image has been freed, we don't want tasks to allocate | |||
95 | additional memory and we prevent them from doing that by freezing them earlier. | 95 | additional memory and we prevent them from doing that by freezing them earlier. |
96 | [Of course, this also means that device drivers should not allocate substantial | 96 | [Of course, this also means that device drivers should not allocate substantial |
97 | amounts of memory from their .suspend() callbacks before hibernation, but this | 97 | amounts of memory from their .suspend() callbacks before hibernation, but this |
98 | is e separate issue.] | 98 | is a separate issue.] |
99 | 99 | ||
100 | 3. The third reason is to prevent user space processes and some kernel threads | 100 | 3. The third reason is to prevent user space processes and some kernel threads |
101 | from interfering with the suspending and resuming of devices. A user space | 101 | from interfering with the suspending and resuming of devices. A user space |
@@ -176,3 +176,28 @@ tasks, since it generally exists anyway. | |||
176 | A driver must have all firmwares it may need in RAM before suspend() is called. | 176 | A driver must have all firmwares it may need in RAM before suspend() is called. |
177 | If keeping them is not practical, for example due to their size, they must be | 177 | If keeping them is not practical, for example due to their size, they must be |
178 | requested early enough using the suspend notifier API described in notifiers.txt. | 178 | requested early enough using the suspend notifier API described in notifiers.txt. |
179 | |||
180 | VI. Are there any precautions to be taken to prevent freezing failures? | ||
181 | |||
182 | Yes, there are. | ||
183 | |||
184 | First of all, grabbing the 'pm_mutex' lock to mutually exclude a piece of code | ||
185 | from system-wide sleep such as suspend/hibernation is not encouraged. | ||
186 | If possible, that piece of code must instead hook onto the suspend/hibernation | ||
187 | notifiers to achieve mutual exclusion. Look at the CPU-Hotplug code | ||
188 | (kernel/cpu.c) for an example. | ||
189 | |||
190 | However, if that is not feasible, and grabbing 'pm_mutex' is deemed necessary, | ||
191 | it is strongly discouraged to directly call mutex_[un]lock(&pm_mutex) since | ||
192 | that could lead to freezing failures, because if the suspend/hibernate code | ||
193 | successfully acquired the 'pm_mutex' lock, and hence that other entity failed | ||
194 | to acquire the lock, then that task would get blocked in TASK_UNINTERRUPTIBLE | ||
195 | state. As a consequence, the freezer would not be able to freeze that task, | ||
196 | leading to freezing failure. | ||
197 | |||
198 | However, the [un]lock_system_sleep() APIs are safe to use in this scenario, | ||
199 | since they ask the freezer to skip freezing this task, since it is anyway | ||
200 | "frozen enough" as it is blocked on 'pm_mutex', which will be released | ||
201 | only after the entire suspend/hibernation sequence is complete. | ||
202 | So, to summarize, use [un]lock_system_sleep() instead of directly using | ||
203 | mutex_[un]lock(&pm_mutex). That would prevent freezing failures. | ||