summaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
Diffstat (limited to 'Documentation/scsi/megaraid.txt')
-rw-r--r--Documentation/scsi/megaraid.txt70
1 files changed, 70 insertions, 0 deletions
diff --git a/Documentation/scsi/megaraid.txt b/Documentation/scsi/megaraid.txt
new file mode 100644
index 000000000000..ff864c0f494c
--- /dev/null
+++ b/Documentation/scsi/megaraid.txt
@@ -0,0 +1,70 @@
1 Notes on Management Module
2 ~~~~~~~~~~~~~~~~~~~~~~~~~~
3
4Overview:
5--------
6
7Different classes of controllers from LSI Logic, accept and respond to the
8user applications in a similar way. They understand the same firmware control
9commands. Furthermore, the applications also can treat different classes of
10the controllers uniformly. Hence it is logical to have a single module that
11interefaces with the applications on one side and all the low level drivers
12on the other.
13
14The advantages, though obvious, are listed for completeness:
15
16 i. Avoid duplicate code from the low level drivers.
17 ii. Unburden the low level drivers from having to export the
18 character node device and related handling.
19 iii. Implement any policy mechanisms in one place.
20 iv. Applications have to interface with only module instead of
21 multiple low level drivers.
22
23Currently this module (called Common Management Module) is used only to issue
24ioctl commands. But this module is envisioned to handle all user space level
25interactions. So any 'proc', 'sysfs' implementations will be localized in this
26common module.
27
28Credits:
29-------
30
31"Shared code in a third module, a "library module", is an acceptable
32solution. modprobe automatically loads dependent modules, so users
33running "modprobe driver1" or "modprobe driver2" would automatically
34load the shared library module."
35
36 - Jeff Garzik (jgarzik@pobox.com), 02.25.2004 LKML
37
38"As Jeff hinted, if your userspace<->driver API is consistent between
39your new MPT-based RAID controllers and your existing megaraid driver,
40then perhaps you need a single small helper module (lsiioctl or some
41better name), loaded by both mptraid and megaraid automatically, which
42handles registering the /dev/megaraid node dynamically. In this case,
43both mptraid and megaraid would register with lsiioctl for each
44adapter discovered, and lsiioctl would essentially be a switch,
45redirecting userspace tool ioctls to the appropriate driver."
46
47 - Matt Domsch, (Matt_Domsch@dell.com), 02.25.2004 LKML
48
49Design:
50------
51
52The Common Management Module is implemented in megaraid_mm.[ch] files. This
53module acts as a registry for low level hba drivers. The low level drivers
54(currently only megaraid) register each controller with the common module.
55
56The applications interface with the common module via the character device
57node exported by the module.
58
59The lower level drivers now understand only a new improved ioctl packet called
60uioc_t. The management module converts the older ioctl packets from the older
61applications into uioc_t. After driver handles the uioc_t, the common module
62will convert that back into the old format before returning to applications.
63
64As new applications evolve and replace the old ones, the old packet format
65will be retired.
66
67Common module dedicates one uioc_t packet to each controller registered. This
68can easily be more than one. But since megaraid is the only low level driver
69today, and it can handle only one ioctl, there is no reason to have more. But
70as new controller classes get added, this will be tuned appropriately.