summaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
Diffstat (limited to 'Documentation/sx.txt')
-rw-r--r--Documentation/sx.txt294
1 files changed, 294 insertions, 0 deletions
diff --git a/Documentation/sx.txt b/Documentation/sx.txt
new file mode 100644
index 000000000000..cb4efa0fb5cc
--- /dev/null
+++ b/Documentation/sx.txt
@@ -0,0 +1,294 @@
1
2 sx.txt -- specialix SX/SI multiport serial driver readme.
3
4
5
6 Copyright (C) 1997 Roger Wolff (R.E.Wolff@BitWizard.nl)
7
8 Specialix pays for the development and support of this driver.
9 Please DO contact support@specialix.co.uk if you require
10 support.
11
12 This driver was developed in the BitWizard linux device
13 driver service. If you require a linux device driver for your
14 product, please contact devices@BitWizard.nl for a quote.
15
16 (History)
17 There used to be an SI driver by Simon Allan. This is a complete
18 rewrite from scratch. Just a few lines-of-code have been snatched.
19
20 (Sources)
21 Specialix document number 6210028: SX Host Card and Download Code
22 Software Functional Specification.
23
24 (Copying)
25 This program is free software; you can redistribute it and/or
26 modify it under the terms of the GNU General Public License as
27 published by the Free Software Foundation; either version 2 of
28 the License, or (at your option) any later version.
29
30 This program is distributed in the hope that it will be
31 useful, but WITHOUT ANY WARRANTY; without even the implied
32 warranty of MERCHANTABILITY or FITNESS FOR A PARTICULAR
33 PURPOSE. See the GNU General Public License for more details.
34
35 You should have received a copy of the GNU General Public
36 License along with this program; if not, write to the Free
37 Software Foundation, Inc., 675 Mass Ave, Cambridge, MA 02139,
38 USA.
39
40 (Addendum)
41 I'd appreciate it that if you have fixes, that you send them
42 to me first.
43
44
45Introduction
46============
47
48This file contains some random information, that I like to have online
49instead of in a manual that can get lost. Ever misplace your Linux
50kernel sources? And the manual of one of the boards in your computer?
51
52
53Theory of operation
54===================
55
56An important thing to know is that the driver itself doesn't have the
57firmware for the card. This means that you need the separate package
58"sx_firmware". For now you can get the source at
59
60 ftp://ftp.bitwizard.nl/specialix/sx_firmware_<version>.tgz
61
62The firmware load needs a "misc" device, so you'll need to enable the
63"Support for user misc device modules" in your kernel configuration.
64The misc device needs to be called "/dev/specialix_sxctl". It needs
65misc major 10, and minor number 167 (assigned by HPA). The section
66on creating device files below also creates this device.
67
68After loading the sx.o module into your kernel, the driver will report
69the number of cards detected, but because it doesn't have any
70firmware, it will not be able to determine the number of ports. Only
71when you then run "sx_firmware" will the firmware be downloaded and
72the rest of the driver initialized. At that time the sx_firmware
73program will report the number of ports installed.
74
75In contrast with many other multi port serial cards, some of the data
76structures are only allocated when the card knows the number of ports
77that are connected. This means we won't waste memory for 120 port
78descriptor structures when you only have 8 ports. If you experience
79problems due to this, please report them: I haven't seen any.
80
81
82Interrupts
83==========
84
85A multi port serial card, would generate a horrendous amount of
86interrupts if it would interrupt the CPU for every received
87character. Even more than 10 years ago, the trick not to use
88interrupts but to poll the serial cards was invented.
89
90The SX card allow us to do this two ways. First the card limits its
91own interrupt rate to a rate that won't overwhelm the CPU. Secondly,
92we could forget about the cards interrupt completely and use the
93internal timer for this purpose.
94
95Polling the card can take up to a few percent of your CPU. Using the
96interrupts would be better if you have most of the ports idle. Using
97timer-based polling is better if your card almost always has work to
98do. You save the separate interrupt in that case.
99
100In any case, it doesn't really matter all that much.
101
102The most common problem with interrupts is that for ISA cards in a PCI
103system the BIOS has to be told to configure that interrupt as "legacy
104ISA". Otherwise the card can pull on the interrupt line all it wants
105but the CPU won't see this.
106
107If you can't get the interrupt to work, remember that polling mode is
108more efficient (provided you actually use the card intensively).
109
110
111Allowed Configurations
112======================
113
114Some configurations are disallowed. Even though at a glance they might
115seem to work, they are known to lockup the bus between the host card
116and the device concentrators. You should respect the drivers decision
117not to support certain configurations. It's there for a reason.
118
119Warning: Seriously technical stuff ahead. Executive summary: Don't use
120SX cards except configured at a 64k boundary. Skip the next paragraph.
121
122The SX cards can theoretically be placed at a 32k boundary. So for
123instance you can put an SX card at 0xc8000-0xd7fff. This is not a
124"recommended configuration". ISA cards have to tell the bus controller
125how they like their timing. Due to timing issues they have to do this
126based on which 64k window the address falls into. This means that the
12732k window below and above the SX card have to use exactly the same
128timing as the SX card. That reportedly works for other SX cards. But
129you're still left with two useless 32k windows that should not be used
130by anybody else.
131
132
133Configuring the driver
134======================
135
136PCI cards are always detected. The driver auto-probes for ISA cards at
137some sensible addresses. Please report if the auto-probe causes trouble
138in your system, or when a card isn't detected.
139
140I'm afraid I haven't implemented "kernel command line parameters" yet.
141This means that if the default doesn't work for you, you shouldn't use
142the compiled-into-the-kernel version of the driver. Use a module
143instead. If you convince me that you need this, I'll make it for
144you. Deal?
145
146I'm afraid that the module parameters are a bit clumsy. If you have a
147better idea, please tell me.
148
149You can specify several parameters:
150
151 sx_poll: number of jiffies between timer-based polls.
152
153 Set this to "0" to disable timer based polls.
154 Initialization of cards without a working interrupt
155 will fail.
156
157 Set this to "1" if you want a polling driver.
158 (on Intel: 100 polls per second). If you don't use
159 fast baud rates, you might consider a value like "5".
160 (If you don't know how to do the math, use 1).
161
162 sx_slowpoll: Number of jiffies between timer-based polls.
163 Set this to "100" to poll once a second.
164 This should get the card out of a stall if the driver
165 ever misses an interrupt. I've never seen this happen,
166 and if it does, that's a bug. Tell me.
167
168 sx_maxints: Number of interrupts to request from the card.
169 The card normally limits interrupts to about 100 per
170 second to offload the host CPU. You can increase this
171 number to reduce latency on the card a little.
172 Note that if you give a very high number you can overload
173 your CPU as well as the CPU on the host card. This setting
174 is inaccurate and not recommended for SI cards (But it
175 works).
176
177 sx_irqmask: The mask of allowable IRQs to use. I suggest you set
178 this to 0 (disable IRQs all together) and use polling if
179 the assignment of IRQs becomes problematic. This is defined
180 as the sum of (1 << irq) 's that you want to allow. So
181 sx_irqmask of 8 (1 << 3) specifies that only irq 3 may
182 be used by the SX driver. If you want to specify to the
183 driver: "Either irq 11 or 12 is ok for you to use", then
184 specify (1 << 11) | (1 << 12) = 0x1800 .
185
186 sx_debug: You can enable different sorts of debug traces with this.
187 At "-1" all debugging traces are active. You'll get several
188 times more debugging output than you'll get characters
189 transmitted.
190
191
192Baud rates
193==========
194
195Theoretically new SXDCs should be capable of more than 460k
196baud. However the line drivers usually give up before that. Also the
197CPU on the card may not be able to handle 8 channels going at full
198blast at that speed. Moreover, the buffers are not large enough to
199allow operation with 100 interrupts per second. You'll have to realize
200that the card has a 256 byte buffer, so you'll have to increase the
201number of interrupts per second if you have more than 256*100 bytes
202per second to transmit. If you do any performance testing in this
203area, I'd be glad to hear from you...
204
205(Psst Linux users..... I think the Linux driver is more efficient than
206the driver for other OSes. If you can and want to benchmark them
207against each other, be my guest, and report your findings...... :-)
208
209
210Ports and devices
211=================
212
213Port 0 is the top connector on the module closest to the host
214card. Oh, the ports on the SXDCs and TAs are labelled from 1 to 8
215instead of from 0 to 7, as they are numbered by linux. I'm stubborn in
216this: I know for sure that I wouldn't be able to calculate which port
217is which anymore if I would change that....
218
219
220Devices:
221
222You should make the device files as follows:
223
224#!/bin/sh
225# (I recommend that you cut-and-paste this into a file and run that)
226cd /dev
227t=0
228mknod specialix_sxctl c 10 167
229while [ $t -lt 64 ]
230 do
231 echo -n "$t "
232 mknod ttyX$t c 32 $t
233 mknod cux$t c 33 $t
234 t=`expr $t + 1`
235done
236echo ""
237rm /etc/psdevtab
238ps > /dev/null
239
240
241This creates 64 devices. If you have more, increase the constant on
242the line with "while". The devices start at 0, as is customary on
243Linux. Specialix seems to like starting the numbering at 1.
244
245If your system doesn't come with these devices pre-installed, bug your
246linux-vendor about this. They should have these devices
247"pre-installed" before the new millennium. The "ps" stuff at the end
248is to "tell" ps that the new devices exist.
249
250Officially the maximum number of cards per computer is 4. This driver
251however supports as many cards in one machine as you want. You'll run
252out of interrupts after a few, but you can switch to polled operation
253then. At about 256 ports (More than 8 cards), we run out of minor
254device numbers. Sorry. I suggest you buy a second computer.... (Or
255switch to RIO).
256
257------------------------------------------------------------------------
258
259
260 Fixed bugs and restrictions:
261 - Hangup processing.
262 -- Done.
263
264 - the write path in generic_serial (lockup / oops).
265 -- Done (Ugly: not the way I want it. Copied from serial.c).
266
267 - write buffer isn't flushed at close.
268 -- Done. I still seem to lose a few chars at close.
269 Sorry. I think that this is a firmware issue. (-> Specialix)
270
271 - drain hardware before changing termios
272 - Change debug on the fly.
273 - ISA free irq -1. (no firmware loaded).
274 - adding c8000 as a probe address. Added warning.
275 - Add a RAMtest for the RAM on the card.c
276 - Crash when opening a port "way" of the number of allowed ports.
277 (for example opening port 60 when there are only 24 ports attached)
278 - Sometimes the use-count strays a bit. After a few hours of
279 testing the use count is sometimes "3". If you are not like
280 me and can remember what you did to get it that way, I'd
281 appreciate an Email. Possibly fixed. Tell me if anyone still
282 sees this.
283 - TAs don't work right if you don't connect all the modem control
284 signals. SXDCs do. T225 firmware problem -> Specialix.
285 (Mostly fixed now, I think. Tell me if you encounter this!)
286
287 Bugs & restrictions:
288
289 - Arbitrary baud rates. Requires firmware update. (-> Specialix)
290
291 - Low latency (mostly firmware, -> Specialix)
292
293
294