diff options
Diffstat (limited to 'Documentation')
-rw-r--r-- | Documentation/filesystems/caching/backend-api.txt | 38 | ||||
-rw-r--r-- | Documentation/filesystems/caching/netfs-api.txt | 46 | ||||
-rw-r--r-- | Documentation/filesystems/caching/object.txt | 23 | ||||
-rw-r--r-- | Documentation/filesystems/caching/operations.txt | 2 | ||||
-rw-r--r-- | Documentation/hwmon/it87 | 10 |
5 files changed, 101 insertions, 18 deletions
diff --git a/Documentation/filesystems/caching/backend-api.txt b/Documentation/filesystems/caching/backend-api.txt index 382d52cdaf2d..d78bab9622c6 100644 --- a/Documentation/filesystems/caching/backend-api.txt +++ b/Documentation/filesystems/caching/backend-api.txt | |||
@@ -308,6 +308,18 @@ performed on the denizens of the cache. These are held in a structure of type: | |||
308 | obtained by calling object->cookie->def->get_aux()/get_attr(). | 308 | obtained by calling object->cookie->def->get_aux()/get_attr(). |
309 | 309 | ||
310 | 310 | ||
311 | (*) Invalidate data object [mandatory]: | ||
312 | |||
313 | int (*invalidate_object)(struct fscache_operation *op) | ||
314 | |||
315 | This is called to invalidate a data object (as pointed to by op->object). | ||
316 | All the data stored for this object should be discarded and an | ||
317 | attr_changed operation should be performed. The caller will follow up | ||
318 | with an object update operation. | ||
319 | |||
320 | fscache_op_complete() must be called on op before returning. | ||
321 | |||
322 | |||
311 | (*) Discard object [mandatory]: | 323 | (*) Discard object [mandatory]: |
312 | 324 | ||
313 | void (*drop_object)(struct fscache_object *object) | 325 | void (*drop_object)(struct fscache_object *object) |
@@ -419,7 +431,10 @@ performed on the denizens of the cache. These are held in a structure of type: | |||
419 | 431 | ||
420 | If an I/O error occurs, fscache_io_error() should be called and -ENOBUFS | 432 | If an I/O error occurs, fscache_io_error() should be called and -ENOBUFS |
421 | returned if possible or fscache_end_io() called with a suitable error | 433 | returned if possible or fscache_end_io() called with a suitable error |
422 | code.. | 434 | code. |
435 | |||
436 | fscache_put_retrieval() should be called after a page or pages are dealt | ||
437 | with. This will complete the operation when all pages are dealt with. | ||
423 | 438 | ||
424 | 439 | ||
425 | (*) Request pages be read from cache [mandatory]: | 440 | (*) Request pages be read from cache [mandatory]: |
@@ -526,6 +541,27 @@ FS-Cache provides some utilities that a cache backend may make use of: | |||
526 | error value should be 0 if successful and an error otherwise. | 541 | error value should be 0 if successful and an error otherwise. |
527 | 542 | ||
528 | 543 | ||
544 | (*) Record that one or more pages being retrieved or allocated have been dealt | ||
545 | with: | ||
546 | |||
547 | void fscache_retrieval_complete(struct fscache_retrieval *op, | ||
548 | int n_pages); | ||
549 | |||
550 | This is called to record the fact that one or more pages have been dealt | ||
551 | with and are no longer the concern of this operation. When the number of | ||
552 | pages remaining in the operation reaches 0, the operation will be | ||
553 | completed. | ||
554 | |||
555 | |||
556 | (*) Record operation completion: | ||
557 | |||
558 | void fscache_op_complete(struct fscache_operation *op); | ||
559 | |||
560 | This is called to record the completion of an operation. This deducts | ||
561 | this operation from the parent object's run state, potentially permitting | ||
562 | one or more pending operations to start running. | ||
563 | |||
564 | |||
529 | (*) Set highest store limit: | 565 | (*) Set highest store limit: |
530 | 566 | ||
531 | void fscache_set_store_limit(struct fscache_object *object, | 567 | void fscache_set_store_limit(struct fscache_object *object, |
diff --git a/Documentation/filesystems/caching/netfs-api.txt b/Documentation/filesystems/caching/netfs-api.txt index 7cc6bf2871eb..97e6c0ecc5ef 100644 --- a/Documentation/filesystems/caching/netfs-api.txt +++ b/Documentation/filesystems/caching/netfs-api.txt | |||
@@ -35,8 +35,9 @@ This document contains the following sections: | |||
35 | (12) Index and data file update | 35 | (12) Index and data file update |
36 | (13) Miscellaneous cookie operations | 36 | (13) Miscellaneous cookie operations |
37 | (14) Cookie unregistration | 37 | (14) Cookie unregistration |
38 | (15) Index and data file invalidation | 38 | (15) Index invalidation |
39 | (16) FS-Cache specific page flags. | 39 | (16) Data file invalidation |
40 | (17) FS-Cache specific page flags. | ||
40 | 41 | ||
41 | 42 | ||
42 | ============================= | 43 | ============================= |
@@ -767,13 +768,42 @@ the cookies for "child" indices, objects and pages have been relinquished | |||
767 | first. | 768 | first. |
768 | 769 | ||
769 | 770 | ||
770 | ================================ | 771 | ================== |
771 | INDEX AND DATA FILE INVALIDATION | 772 | INDEX INVALIDATION |
772 | ================================ | 773 | ================== |
774 | |||
775 | There is no direct way to invalidate an index subtree. To do this, the caller | ||
776 | should relinquish and retire the cookie they have, and then acquire a new one. | ||
777 | |||
778 | |||
779 | ====================== | ||
780 | DATA FILE INVALIDATION | ||
781 | ====================== | ||
782 | |||
783 | Sometimes it will be necessary to invalidate an object that contains data. | ||
784 | Typically this will be necessary when the server tells the netfs of a foreign | ||
785 | change - at which point the netfs has to throw away all the state it had for an | ||
786 | inode and reload from the server. | ||
787 | |||
788 | To indicate that a cache object should be invalidated, the following function | ||
789 | can be called: | ||
790 | |||
791 | void fscache_invalidate(struct fscache_cookie *cookie); | ||
792 | |||
793 | This can be called with spinlocks held as it defers the work to a thread pool. | ||
794 | All extant storage, retrieval and attribute change ops at this point are | ||
795 | cancelled and discarded. Some future operations will be rejected until the | ||
796 | cache has had a chance to insert a barrier in the operations queue. After | ||
797 | that, operations will be queued again behind the invalidation operation. | ||
798 | |||
799 | The invalidation operation will perform an attribute change operation and an | ||
800 | auxiliary data update operation as it is very likely these will have changed. | ||
801 | |||
802 | Using the following function, the netfs can wait for the invalidation operation | ||
803 | to have reached a point at which it can start submitting ordinary operations | ||
804 | once again: | ||
773 | 805 | ||
774 | There is no direct way to invalidate an index subtree or a data file. To do | 806 | void fscache_wait_on_invalidate(struct fscache_cookie *cookie); |
775 | this, the caller should relinquish and retire the cookie they have, and then | ||
776 | acquire a new one. | ||
777 | 807 | ||
778 | 808 | ||
779 | =========================== | 809 | =========================== |
diff --git a/Documentation/filesystems/caching/object.txt b/Documentation/filesystems/caching/object.txt index 58313348da87..100ff41127e4 100644 --- a/Documentation/filesystems/caching/object.txt +++ b/Documentation/filesystems/caching/object.txt | |||
@@ -216,7 +216,14 @@ servicing netfs requests: | |||
216 | The normal running state. In this state, requests the netfs makes will be | 216 | The normal running state. In this state, requests the netfs makes will be |
217 | passed on to the cache. | 217 | passed on to the cache. |
218 | 218 | ||
219 | (6) State FSCACHE_OBJECT_UPDATING. | 219 | (6) State FSCACHE_OBJECT_INVALIDATING. |
220 | |||
221 | The object is undergoing invalidation. When the state comes here, it | ||
222 | discards all pending read, write and attribute change operations as it is | ||
223 | going to clear out the cache entirely and reinitialise it. It will then | ||
224 | continue to the FSCACHE_OBJECT_UPDATING state. | ||
225 | |||
226 | (7) State FSCACHE_OBJECT_UPDATING. | ||
220 | 227 | ||
221 | The state machine comes here to update the object in the cache from the | 228 | The state machine comes here to update the object in the cache from the |
222 | netfs's records. This involves updating the auxiliary data that is used | 229 | netfs's records. This involves updating the auxiliary data that is used |
@@ -225,13 +232,13 @@ servicing netfs requests: | |||
225 | And there are terminal states in which an object cleans itself up, deallocates | 232 | And there are terminal states in which an object cleans itself up, deallocates |
226 | memory and potentially deletes stuff from disk: | 233 | memory and potentially deletes stuff from disk: |
227 | 234 | ||
228 | (7) State FSCACHE_OBJECT_LC_DYING. | 235 | (8) State FSCACHE_OBJECT_LC_DYING. |
229 | 236 | ||
230 | The object comes here if it is dying because of a lookup or creation | 237 | The object comes here if it is dying because of a lookup or creation |
231 | error. This would be due to a disk error or system error of some sort. | 238 | error. This would be due to a disk error or system error of some sort. |
232 | Temporary data is cleaned up, and the parent is released. | 239 | Temporary data is cleaned up, and the parent is released. |
233 | 240 | ||
234 | (8) State FSCACHE_OBJECT_DYING. | 241 | (9) State FSCACHE_OBJECT_DYING. |
235 | 242 | ||
236 | The object comes here if it is dying due to an error, because its parent | 243 | The object comes here if it is dying due to an error, because its parent |
237 | cookie has been relinquished by the netfs or because the cache is being | 244 | cookie has been relinquished by the netfs or because the cache is being |
@@ -241,27 +248,27 @@ memory and potentially deletes stuff from disk: | |||
241 | can destroy themselves. This object waits for all its children to go away | 248 | can destroy themselves. This object waits for all its children to go away |
242 | before advancing to the next state. | 249 | before advancing to the next state. |
243 | 250 | ||
244 | (9) State FSCACHE_OBJECT_ABORT_INIT. | 251 | (10) State FSCACHE_OBJECT_ABORT_INIT. |
245 | 252 | ||
246 | The object comes to this state if it was waiting on its parent in | 253 | The object comes to this state if it was waiting on its parent in |
247 | FSCACHE_OBJECT_INIT, but its parent died. The object will destroy itself | 254 | FSCACHE_OBJECT_INIT, but its parent died. The object will destroy itself |
248 | so that the parent may proceed from the FSCACHE_OBJECT_DYING state. | 255 | so that the parent may proceed from the FSCACHE_OBJECT_DYING state. |
249 | 256 | ||
250 | (10) State FSCACHE_OBJECT_RELEASING. | 257 | (11) State FSCACHE_OBJECT_RELEASING. |
251 | (11) State FSCACHE_OBJECT_RECYCLING. | 258 | (12) State FSCACHE_OBJECT_RECYCLING. |
252 | 259 | ||
253 | The object comes to one of these two states when dying once it is rid of | 260 | The object comes to one of these two states when dying once it is rid of |
254 | all its children, if it is dying because the netfs relinquished its | 261 | all its children, if it is dying because the netfs relinquished its |
255 | cookie. In the first state, the cached data is expected to persist, and | 262 | cookie. In the first state, the cached data is expected to persist, and |
256 | in the second it will be deleted. | 263 | in the second it will be deleted. |
257 | 264 | ||
258 | (12) State FSCACHE_OBJECT_WITHDRAWING. | 265 | (13) State FSCACHE_OBJECT_WITHDRAWING. |
259 | 266 | ||
260 | The object transits to this state if the cache decides it wants to | 267 | The object transits to this state if the cache decides it wants to |
261 | withdraw the object from service, perhaps to make space, but also due to | 268 | withdraw the object from service, perhaps to make space, but also due to |
262 | error or just because the whole cache is being withdrawn. | 269 | error or just because the whole cache is being withdrawn. |
263 | 270 | ||
264 | (13) State FSCACHE_OBJECT_DEAD. | 271 | (14) State FSCACHE_OBJECT_DEAD. |
265 | 272 | ||
266 | The object transits to this state when the in-memory object record is | 273 | The object transits to this state when the in-memory object record is |
267 | ready to be deleted. The object processor shouldn't ever see an object in | 274 | ready to be deleted. The object processor shouldn't ever see an object in |
diff --git a/Documentation/filesystems/caching/operations.txt b/Documentation/filesystems/caching/operations.txt index b6b070c57cbf..bee2a5f93d60 100644 --- a/Documentation/filesystems/caching/operations.txt +++ b/Documentation/filesystems/caching/operations.txt | |||
@@ -174,7 +174,7 @@ Operations are used through the following procedure: | |||
174 | necessary (the object might have died whilst the thread was waiting). | 174 | necessary (the object might have died whilst the thread was waiting). |
175 | 175 | ||
176 | When it has finished doing its processing, it should call | 176 | When it has finished doing its processing, it should call |
177 | fscache_put_operation() on it. | 177 | fscache_op_complete() and fscache_put_operation() on it. |
178 | 178 | ||
179 | (4) The operation holds an effective lock upon the object, preventing other | 179 | (4) The operation holds an effective lock upon the object, preventing other |
180 | exclusive ops conflicting until it is released. The operation can be | 180 | exclusive ops conflicting until it is released. The operation can be |
diff --git a/Documentation/hwmon/it87 b/Documentation/hwmon/it87 index 87850d86c559..8386aadc0a82 100644 --- a/Documentation/hwmon/it87 +++ b/Documentation/hwmon/it87 | |||
@@ -209,3 +209,13 @@ doesn't use CPU cycles. | |||
209 | Trip points must be set properly before switching to automatic fan speed | 209 | Trip points must be set properly before switching to automatic fan speed |
210 | control mode. The driver will perform basic integrity checks before | 210 | control mode. The driver will perform basic integrity checks before |
211 | actually switching to automatic control mode. | 211 | actually switching to automatic control mode. |
212 | |||
213 | |||
214 | Temperature offset attributes | ||
215 | ----------------------------- | ||
216 | |||
217 | The driver supports temp[1-3]_offset sysfs attributes to adjust the reported | ||
218 | temperature for thermal diodes or diode-connected thermal transistors. | ||
219 | If a temperature sensor is configured for thermistors, the attribute values | ||
220 | are ignored. If the thermal sensor type is Intel PECI, the temperature offset | ||
221 | must be programmed to the critical CPU temperature. | ||