aboutsummaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
Diffstat (limited to 'Documentation')
-rw-r--r--Documentation/filesystems/caching/backend-api.txt26
-rw-r--r--Documentation/filesystems/caching/operations.txt2
2 files changed, 26 insertions, 2 deletions
diff --git a/Documentation/filesystems/caching/backend-api.txt b/Documentation/filesystems/caching/backend-api.txt
index 382d52cdaf2d..f4769b9399df 100644
--- a/Documentation/filesystems/caching/backend-api.txt
+++ b/Documentation/filesystems/caching/backend-api.txt
@@ -419,7 +419,10 @@ performed on the denizens of the cache. These are held in a structure of type:
419 419
420 If an I/O error occurs, fscache_io_error() should be called and -ENOBUFS 420 If an I/O error occurs, fscache_io_error() should be called and -ENOBUFS
421 returned if possible or fscache_end_io() called with a suitable error 421 returned if possible or fscache_end_io() called with a suitable error
422 code.. 422 code.
423
424 fscache_put_retrieval() should be called after a page or pages are dealt
425 with. This will complete the operation when all pages are dealt with.
423 426
424 427
425 (*) Request pages be read from cache [mandatory]: 428 (*) Request pages be read from cache [mandatory]:
@@ -526,6 +529,27 @@ FS-Cache provides some utilities that a cache backend may make use of:
526 error value should be 0 if successful and an error otherwise. 529 error value should be 0 if successful and an error otherwise.
527 530
528 531
532 (*) Record that one or more pages being retrieved or allocated have been dealt
533 with:
534
535 void fscache_retrieval_complete(struct fscache_retrieval *op,
536 int n_pages);
537
538 This is called to record the fact that one or more pages have been dealt
539 with and are no longer the concern of this operation. When the number of
540 pages remaining in the operation reaches 0, the operation will be
541 completed.
542
543
544 (*) Record operation completion:
545
546 void fscache_op_complete(struct fscache_operation *op);
547
548 This is called to record the completion of an operation. This deducts
549 this operation from the parent object's run state, potentially permitting
550 one or more pending operations to start running.
551
552
529 (*) Set highest store limit: 553 (*) Set highest store limit:
530 554
531 void fscache_set_store_limit(struct fscache_object *object, 555 void fscache_set_store_limit(struct fscache_object *object,
diff --git a/Documentation/filesystems/caching/operations.txt b/Documentation/filesystems/caching/operations.txt
index b6b070c57cbf..bee2a5f93d60 100644
--- a/Documentation/filesystems/caching/operations.txt
+++ b/Documentation/filesystems/caching/operations.txt
@@ -174,7 +174,7 @@ Operations are used through the following procedure:
174 necessary (the object might have died whilst the thread was waiting). 174 necessary (the object might have died whilst the thread was waiting).
175 175
176 When it has finished doing its processing, it should call 176 When it has finished doing its processing, it should call
177 fscache_put_operation() on it. 177 fscache_op_complete() and fscache_put_operation() on it.
178 178
179 (4) The operation holds an effective lock upon the object, preventing other 179 (4) The operation holds an effective lock upon the object, preventing other
180 exclusive ops conflicting until it is released. The operation can be 180 exclusive ops conflicting until it is released. The operation can be