diff options
Diffstat (limited to 'arch/x86/include/asm/elf.h')
-rw-r--r-- | arch/x86/include/asm/elf.h | 4 |
1 files changed, 2 insertions, 2 deletions
diff --git a/arch/x86/include/asm/elf.h b/arch/x86/include/asm/elf.h index 07cf288b692e..bcd3d6199464 100644 --- a/arch/x86/include/asm/elf.h +++ b/arch/x86/include/asm/elf.h | |||
@@ -247,11 +247,11 @@ extern int force_personality32; | |||
247 | 247 | ||
248 | /* | 248 | /* |
249 | * This is the base location for PIE (ET_DYN with INTERP) loads. On | 249 | * This is the base location for PIE (ET_DYN with INTERP) loads. On |
250 | * 64-bit, this is raised to 4GB to leave the entire 32-bit address | 250 | * 64-bit, this is above 4GB to leave the entire 32-bit address |
251 | * space open for things that want to use the area for 32-bit pointers. | 251 | * space open for things that want to use the area for 32-bit pointers. |
252 | */ | 252 | */ |
253 | #define ELF_ET_DYN_BASE (mmap_is_ia32() ? 0x000400000UL : \ | 253 | #define ELF_ET_DYN_BASE (mmap_is_ia32() ? 0x000400000UL : \ |
254 | 0x100000000UL) | 254 | (TASK_SIZE / 3 * 2)) |
255 | 255 | ||
256 | /* This yields a mask that user programs can use to figure out what | 256 | /* This yields a mask that user programs can use to figure out what |
257 | instruction set this CPU supports. This could be done in user space, | 257 | instruction set this CPU supports. This could be done in user space, |