diff options
Diffstat (limited to 'arch/x86/kernel/cpu/bugs_64.c')
-rw-r--r-- | arch/x86/kernel/cpu/bugs_64.c | 33 |
1 files changed, 0 insertions, 33 deletions
diff --git a/arch/x86/kernel/cpu/bugs_64.c b/arch/x86/kernel/cpu/bugs_64.c deleted file mode 100644 index 04f0fe5af83e..000000000000 --- a/arch/x86/kernel/cpu/bugs_64.c +++ /dev/null | |||
@@ -1,33 +0,0 @@ | |||
1 | /* | ||
2 | * Copyright (C) 1994 Linus Torvalds | ||
3 | * Copyright (C) 2000 SuSE | ||
4 | */ | ||
5 | |||
6 | #include <linux/kernel.h> | ||
7 | #include <linux/init.h> | ||
8 | #include <asm/alternative.h> | ||
9 | #include <asm/bugs.h> | ||
10 | #include <asm/processor.h> | ||
11 | #include <asm/mtrr.h> | ||
12 | #include <asm/cacheflush.h> | ||
13 | |||
14 | void __init check_bugs(void) | ||
15 | { | ||
16 | identify_boot_cpu(); | ||
17 | #if !defined(CONFIG_SMP) | ||
18 | printk(KERN_INFO "CPU: "); | ||
19 | print_cpu_info(&boot_cpu_data); | ||
20 | #endif | ||
21 | alternative_instructions(); | ||
22 | |||
23 | /* | ||
24 | * Make sure the first 2MB area is not mapped by huge pages | ||
25 | * There are typically fixed size MTRRs in there and overlapping | ||
26 | * MTRRs into large pages causes slow downs. | ||
27 | * | ||
28 | * Right now we don't do that with gbpages because there seems | ||
29 | * very little benefit for that case. | ||
30 | */ | ||
31 | if (!direct_gbpages) | ||
32 | set_memory_4k((unsigned long)__va(0), 1); | ||
33 | } | ||