aboutsummaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
Diffstat (limited to 'include/linux/fscache-cache.h')
-rw-r--r--include/linux/fscache-cache.h1
1 files changed, 1 insertions, 0 deletions
diff --git a/include/linux/fscache-cache.h b/include/linux/fscache-cache.h
index 604e1526cd00..eb19bf2b2a81 100644
--- a/include/linux/fscache-cache.h
+++ b/include/linux/fscache-cache.h
@@ -360,6 +360,7 @@ struct fscache_object {
360#define FSCACHE_OBJECT_IS_AVAILABLE 5 /* T if object has become active */ 360#define FSCACHE_OBJECT_IS_AVAILABLE 5 /* T if object has become active */
361#define FSCACHE_OBJECT_RETIRED 6 /* T if object was retired on relinquishment */ 361#define FSCACHE_OBJECT_RETIRED 6 /* T if object was retired on relinquishment */
362#define FSCACHE_OBJECT_KILLED_BY_CACHE 7 /* T if object was killed by the cache */ 362#define FSCACHE_OBJECT_KILLED_BY_CACHE 7 /* T if object was killed by the cache */
363#define FSCACHE_OBJECT_RUN_AFTER_DEAD 8 /* T if object has been dispatched after death */
363 364
364 struct list_head cache_link; /* link in cache->object_list */ 365 struct list_head cache_link; /* link in cache->object_list */
365 struct hlist_node cookie_link; /* link in cookie->backing_objects */ 366 struct hlist_node cookie_link; /* link in cookie->backing_objects */