aboutsummaryrefslogtreecommitdiffstats
Commit message (Collapse)AuthorAgeFilesLines
* tty/serial: Add support for Altera serial portLey Foon Tan2013-03-201-0/+3
| | | | | | | | | | commit e06c93cacb82dd147266fd1bdb2d0a0bd45ff2c1 upstream. Add support for Altera 8250/16550 compatible serial port. Signed-off-by: Ley Foon Tan <lftan@altera.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* doc, kernel-parameters: Document 'console=hvc<n>'Konrad Rzeszutek Wilk2013-03-031-0/+2
| | | | | | | | | | | | | commit a2fd6419174470f5ae6383f5037d0ee21ed9833f upstream. Both the PowerPC hypervisor and Xen hypervisor can utilize the hvc driver. Signed-off-by: Konrad Rzeszutek Wilk <konrad.wilk@oracle.com> Link: http://lkml.kernel.org/r/1361825650-14031-3-git-send-email-konrad.wilk@oracle.com Signed-off-by: H. Peter Anvin <hpa@linux.intel.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* doc, xen: Mention 'earlyprintk=xen' in the documentation.Konrad Rzeszutek Wilk2013-03-031-0/+3
| | | | | | | | | | | | | | | | | commit 2482a92e7d17187301d7313cfe5021b13393a0b4 upstream. The earlyprintk for Xen PV guests utilizes a simple hypercall (console_io) to provide output to Xen emergency console. Note that the Xen hypervisor should be booted with 'loglevel=all' to output said information. Reported-by: H. Peter Anvin <hpa@zytor.com> Signed-off-by: Konrad Rzeszutek Wilk <konrad.wilk@oracle.com> Link: http://lkml.kernel.org/r/1361825650-14031-2-git-send-email-konrad.wilk@oracle.com Signed-off-by: H. Peter Anvin <hpa@linux.intel.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* x86, doc: Add a bootloader ID for OVMFH. Peter Anvin2013-02-081-0/+1
| | | | | | | | | | | OVMF (an implementation of UEFI based on TianoCore used in virtual environments) now has the ability to boot Linux natively; this is used for "qemu -kernel" and similar things in a UEFI environment. Accordingly, assign it a bootloader ID. Signed-off-by: H. Peter Anvin <hpa@linux.intel.com> Cc: David Woodhouse <dwmw2@infradead.org>
* Merge branch 'x86-urgent-for-linus' of ↵Linus Torvalds2013-02-041-1/+1
|\ | | | | | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/tip/tip Pull x86 fixes from Ingo Molnar: "Three small fixlets" * 'x86-urgent-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/tip/tip: x86/intel/cacheinfo: Shut up annoying warning x86, doc: Boot protocol 2.12 is in 3.8 x86-64: Replace left over sti/cli in ia32 audit exit code
| * x86, doc: Boot protocol 2.12 is in 3.8H. Peter Anvin2013-01-311-1/+1
| | | | | | | | | | | | | | The boot protocol 2.12 changes were pulled for 3.8, so update the documentation accordingly. Signed-off-by: H. Peter Anvin <hpa@linux.intel.com>
* | Merge branch 'core-urgent-for-linus' of ↵Linus Torvalds2013-02-041-1/+1
|\ \ | |/ |/| | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/tip/tip Pull two small RCU fixlets from Ingo Molnar. * 'core-urgent-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/tip/tip: rcu: Make rcu_nocb_poll an early_param instead of module_param rcu: Prevent soft-lockup complaints about no-CBs CPUs
| * Merge branch 'rcu/urgent' of ↵Ingo Molnar2013-01-241-1/+1
| |\ | | | | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/paulmck/linux-rcu into core/urgent Pull RCU fixes from Paul E. McKenney. Signed-off-by: Ingo Molnar <mingo@kernel.org>
| | * rcu: Make rcu_nocb_poll an early_param instead of module_paramPaul Gortmaker2013-01-081-1/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | The as-documented rcu_nocb_poll will fail to enable this feature for two reasons. (1) there is an extra "s" in the documented name which is not in the code, and (2) since it uses module_param, it really is expecting a prefix, akin to "rcutree.fanout_leaf" and the prefix isn't documented. However, there are several reasons why we might not want to simply fix the typo and add the prefix: 1) we'd end up with rcutree.rcu_nocb_poll, and rather probably make a change to rcutree.nocb_poll 2) if we did #1, then the prefix wouldn't be consistent with the rcu_nocbs=<cpumap> parameter (i.e. one with, one without prefix) 3) the use of module_param in a header file is less than desired, since it isn't immediately obvious that it will get processed via rcutree.c and get the prefix from that (although use of module_param_named() could clarify that.) 4) the implied export of /sys/module/rcutree/parameters/rcu_nocb_poll data to userspace via module_param() doesn't really buy us anything, as it is read-only and we can tell if it is enabled already without it, since there is a printk at early boot telling us so. In light of all that, just change it from a module_param() to an early_setup() call, and worry about adding it to /sys later on if we decide to allow a dynamic setting of it. Also change the variable to be tagged as read_mostly, since it will only ever be fiddled with at most, once at boot. Signed-off-by: Paul Gortmaker <paul.gortmaker@windriver.com> Signed-off-by: Paul E. McKenney <paulmck@linux.vnet.ibm.com>
* | | Merge branch 'for-3.8/upstream-fixes' of ↵Linus Torvalds2013-01-311-0/+0
|\ \ \ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/jikos/hid PullHID fixes from Jiri Kosina: - fix i2c-hid and hidraw interaction, by Benjamin Tissoires - a quirk to make a particular device (Formosa IR receiver) work properly, by Nicholas Santos * 'for-3.8/upstream-fixes' of git://git.kernel.org/pub/scm/linux/kernel/git/jikos/hid: HID: i2c-hid: fix i2c_hid_output_raw_report HID: usbhid: quirk for Formosa IR receiver HID: remove x bit from sensor doc
| * | | HID: remove x bit from sensor docJiri Kosina2012-12-141-0/+0
| | | | | | | | | | | | | | | | | | | | Reported-by: Xose Vazquez Perez <xose.vazquez@gmail.com> Signed-off-by: Jiri Kosina <jkosina@suse.cz>
* | | | Merge branch 'x86-efi-for-linus' of ↵Linus Torvalds2013-01-312-1/+30
|\ \ \ \ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/tip/tip Pull x86 EFI fixes from Peter Anvin: "This is a collection of fixes for the EFI support. The controversial bit here is a set of patches which bumps the boot protocol version as part of fixing some serious problems with the EFI handover protocol, used when booting under EFI using a bootloader as opposed to directly from EFI. These changes should also make it a lot saner to support cross-mode 32/64-bit EFI booting in the future. Getting these changes into 3.8 means we avoid presenting an inconsistent ABI to bootloaders. Other changes are display detection and fixing efivarfs." * 'x86-efi-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/tip/tip: x86, efi: remove attribute check from setup_efi_pci x86, build: Dynamically find entry points in compressed startup code x86, efi: Fix PCI ROM handing in EFI boot stub, in 32-bit mode x86, efi: Fix 32-bit EFI handover protocol entry point x86, efi: Fix display detection in EFI boot stub x86, boot: Define the 2.12 bzImage boot protocol x86/boot: Fix minor fd leakage in tools/relocs.c x86, efi: Set runtime_version to the EFI spec revision x86, efi: fix 32-bit warnings in setup_efi_pci() efivarfs: Delete dentry from dcache in efivarfs_file_write() efivarfs: Never return ENOENT from firmware efi, x86: Pass a proper identity mapping in efi_call_phys_prelog efivarfs: Drop link count of the right inode
| * | | | x86, boot: Define the 2.12 bzImage boot protocolH. Peter Anvin2013-01-272-1/+30
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Define the 2.12 bzImage boot protocol: add xloadflags and additional fields to allow the command line, initramfs and struct boot_params to live above the 4 GiB mark. The xloadflags now communicates if this is a 64-bit kernel with the legacy 64-bit entry point and which of the EFI handover entry points are supported. Avoid adding new read flags to loadflags because of claimed bootloaders testing the whole byte for == 1 to determine bzImageness at least until the issue can be researched further. This is based on patches by Yinghai Lu and David Woodhouse. Originally-by: Yinghai Lu <yinghai@kernel.org> Originally-by: David Woodhouse <dwmw2@infradead.org> Acked-by: Yinghai Lu <yinghai@kernel.org> Acked-by: David Woodhouse <dwmw2@infradead.org> Acked-by: Matt Fleming <matt.fleming@intel.com> Signed-off-by: H. Peter Anvin <hpa@linux.intel.com> Link: http://lkml.kernel.org/r/1359058816-7615-26-git-send-email-yinghai@kernel.org Cc: Rob Landley <rob@landley.net> Cc: Gokul Caushik <caushik1@gmail.com> Cc: Josh Triplett <josh@joshtriplett.org> Cc: Joe Millenbach <jmillenbach@gmail.com>
* | | | | Merge tag 'md-3.8-fixes' of git://neil.brown.name/mdLinus Torvalds2013-01-281-0/+1
|\ \ \ \ \ | |/ / / / |/| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Pull dmraid fix from NeilBrown: "Just one fix for md in 3.8 dmraid assess redundancy and replacements slightly inaccurately which could lead to some degraded arrays failing to assemble." * tag 'md-3.8-fixes' of git://neil.brown.name/md: DM-RAID: Fix RAID10's check for sufficient redundancy
| * | | | DM-RAID: Fix RAID10's check for sufficient redundancyJonathan Brassow2013-01-231-0/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Before attempting to activate a RAID array, it is checked for sufficient redundancy. That is, we make sure that there are not too many failed devices - or devices specified for rebuild - to undermine our ability to activate the array. The current code performs this check twice - once to ensure there were not too many devices specified for rebuild by the user ('validate_rebuild_devices') and again after possibly experiencing a failure to read the superblock ('analyse_superblocks'). Neither of these checks are sufficient. The first check is done properly but with insufficient information about the possible failure state of the devices to make a good determination if the array can be activated. The second check is simply done wrong in the case of RAID10 because it doesn't account for the independence of the stripes (i.e. mirror sets). The solution is to use the properly written check ('validate_rebuild_devices'), but perform the check after the superblocks have been read and we know which devices have failed. This gives us one check instead of two and performs it in a location where it can be done right. Only RAID10 was affected and it was affected in the following ways: - the code did not properly catch the condition where a user specified a device for rebuild that already had a failed device in the same mirror set. (This condition would, however, be caught at a deeper level in MD.) - the code triggers a false positive and denies activation when devices in independent mirror sets have failed - counting the failures as though they were all in the same set. The most likely place this error was introduced (or this patch should have been included) is in commit 4ec1e369 - first introduced in v3.7-rc1. Consequently this fix should also go in v3.7.y, however there is a small conflict on the .version in raid_target, so I'll submit a separate patch to -stable. Cc: stable@vger.kernel.org Signed-off-by: Jonathan Brassow <jbrassow@redhat.com> Signed-off-by: NeilBrown <neilb@suse.de>
* | | | | Merge tag 'fixes-for-linus2' of ↵Linus Torvalds2013-01-241-2/+3
|\ \ \ \ \ | |_|_|/ / |/| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/arm/arm-soc Pull ARM SoC fixes from Olof Johansson: "Here's a long-pending fixes pull request for arm-soc (I didn't send one in the -rc4 cycle). The larger deltas are from: - A fixup of error paths in the mvsdio driver - Header file move for a driver that hadn't been properly converted to multiplatform on i.MX, which was causing build failures when included - Device tree updates for at91 dealing mostly with their new pinctrl setup merged in 3.8 and mistakes in those initial configs The rest are the normal mix of small fixes all over the place; sunxi, omap, imx, mvebu, etc, etc." * tag 'fixes-for-linus2' of git://git.kernel.org/pub/scm/linux/kernel/git/arm/arm-soc: (40 commits) mfd: vexpress-sysreg: Don't skip initialization on probe ARM: vexpress: Enable A7 cores in V2P-CA15_A7's Device Tree ARM: vexpress: extend the MPIDR range used for pen release check ARM: at91/dts: correct comment in at91sam9x5.dtsi for mii ARM: at91/at91_dt_defconfig: add at91sam9n12 SoC to DT defconfig ARM: at91/at91_dt_defconfig: remove memory specification to cmdline ARM: at91/dts: add macb mii pinctrl config for kizbox ARM: at91: rm9200: remake the BGA as default version ARM: at91: fix gpios on i2c-gpio for RM9200 DT ARM: at91/at91sam9x5 DTS: add SCK USART pins ARM: at91/at91sam9x5 DTS: correct wrong PIO BANK values on u(s)arts ARM: at91/at91-pinctrl documentation: fix typo and add some details ARM: kirkwood: fix missing #interrupt-cells property mmc: mvsdio: use devm_ API to simplify/correct error paths. clk: mvebu/clk-cpu.c: fix memory leakage ARM: OMAP2+: omap4-panda: add UART2 muxing for WiLink shared transport ARM: OMAP2+: DT node Timer iteration fix ARM: OMAP2+: Fix section warning for omap_init_ocp2scp() ARM: OMAP2+: fix build break for omapdrm ARM: OMAP2: Fix missing omap2xxx_clkt_vps_late_init function calls ...
| * | | | ARM: at91/at91-pinctrl documentation: fix typo and add some detailsRichard Genoud2013-01-231-2/+3
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | The relation between PIN_BANK numbers and pio letters wasn't made very clear. Signed-off-by: Richard Genoud <richard.genoud@gmail.com> Acked-by: Jean-Christophe PLAGNIOL-VILLARD <plagnioj@jcrosoft.com> Signed-off-by: Nicolas Ferre <nicolas.ferre@atmel.com>
* | | | | Merge tag 'f2fs-for-3.8-rc5' of ↵Linus Torvalds2013-01-221-9/+9
|\ \ \ \ \ | |/ / / / |/| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/jaegeuk/f2fs Pull f2fs fixes from Jaegeuk Kim: o Support swap file and link generic_file_remap_pages o Enhance the bio streaming flow and free section control o Major bug fix on recovery routine o Minor bug/warning fixes and code cleanups * tag 'f2fs-for-3.8-rc5' of git://git.kernel.org/pub/scm/linux/kernel/git/jaegeuk/f2fs: (22 commits) f2fs: use _safe() version of list_for_each f2fs: add comments of start_bidx_of_node f2fs: avoid issuing small bios due to several dirty node pages f2fs: support swapfile f2fs: add remap_pages as generic_file_remap_pages f2fs: add __init to functions in init_f2fs_fs f2fs: fix the debugfs entry creation path f2fs: add global mutex_lock to protect f2fs_stat_list f2fs: remove the blk_plug usage in f2fs_write_data_pages f2fs: avoid redundant time update for parent directory in f2fs_delete_entry f2fs: remove redundant call to set_blocksize in f2fs_fill_super f2fs: move f2fs_balance_fs to punch_hole f2fs: add f2fs_balance_fs in several interfaces f2fs: revisit the f2fs_gc flow f2fs: check return value during recovery f2fs: avoid null dereference in f2fs_acl_from_disk f2fs: initialize newly allocated dnode structure f2fs: update f2fs partition info about SIT/NAT layout f2fs: update f2fs document to reflect SIT/NAT layout correctly f2fs: remove unneeded INIT_LIST_HEAD at few places ...
| * | | | f2fs: update f2fs document to reflect SIT/NAT layout correctlyHuajun Li2013-01-031-9/+9
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | document to reflect the layout generated by mkfs.f2fs . Signed-off-by: Huajun Li <huajun.li.lee@gmail.com> Signed-off-by: Jaegeuk Kim <jaegeuk.kim@samsung.com>
* | | | | Merge tag 'fixes' of git://git.kernel.org/pub/scm/linux/kernel/git/arm/arm-socLinus Torvalds2013-01-085-21/+17
|\ \ \ \ \ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Pull ARM SoC fixes from Olof Johansson: "People are back from the holiday breaks, and it shows. Here are a bunch of fixes for a number of platforms: - A couple of small fixes for Nomadik - A larger set of changes for kirkwood/mvebu - uart driver selection, dt clocks, gpio-poweroff fixups, a few __init annotation fixes and some error handling improvement in their xor dma driver. - i.MX had a couple of minor fixes (and a critical one for flexcan2 clock setup) - MXS has a small board fix and a framebuffer bugfix - A set of fixes for Samsung Exynos, fixing default bootargs and some Exynos5440 clock issues - A set of OMAP changes including PM fixes and a few sparse warning fixups All in all a bit more positive code delta than we'd ideally want to see here, mostly from the OMAP PM changes, but nothing overly crazy." * tag 'fixes' of git://git.kernel.org/pub/scm/linux/kernel/git/arm/arm-soc: (44 commits) ARM: clps711x: Fix bad merge of clockevents setup ARM: highbank: save and restore L2 cache and GIC on suspend ARM: highbank: add a power request clear ARM: highbank: fix secondary boot and hotplug ARM: highbank: fix typos with hignbank in power request functions ARM: dts: fix highbank cpu mpidr values ARM: dts: add device_type prop to cpu nodes on Calxeda platforms ARM: mx5: Fix MX53 flexcan2 clock ARM: OMAP2+: am33xx-hwmod: Fix wrongly terminated am33xx_usbss_mpu_irqs array pinctrl: mvebu: make pdma clock on dove mandatory ARM: Dove: Add pinctrl clock to DT dma: mv_xor: fix error handling for clocks dma: mv_xor: fix error handling of mv_xor_channel_add() arm: mvebu: Add missing ; for cpu node. arm: mvebu: Armada XP MV78230 has only three Ethernet interfaces arm: mvebu: Armada XP MV78230 has two cores, not one clk: mvebu: Remove inappropriate __init tagging ARM: Kirkwood: Use fixed-regulator instead of board gpio call ARM: Kirkwood: Fix missing sdio clock ARM: Kirkwood: Switch TWSI1 of 88f6282 to DT clock providers ...
| * \ \ \ \ Merge tag 'imx-fixes-3.8' of git://git.linaro.org/people/shawnguo/linux-2.6 ↵Olof Johansson2013-01-084-18/+0
| |\ \ \ \ \ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | into fixes From Shawn Guo: It includes one critical fix - wrong flexcan2 clock will hang system when the port gets brought up. The other two are non-critical fixes, which are sent together here, since it's still early -rc stage. * tag 'imx-fixes-3.8' of git://git.linaro.org/people/shawnguo/linux-2.6: ARM: mx5: Fix MX53 flexcan2 clock ARM: dts: imx31-bug: Fix manufacturer compatible string clk: imx: Remove 'clock-output-names' from the examples
| | * | | | | clk: imx: Remove 'clock-output-names' from the examplesFabio Estevam2013-01-034-18/+0
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | 'clock-output-names' is not used in any of the dts/dtsi files for i.mx. Remove it from the examples, so that the example and the real usage in the dtsi files can match. Signed-off-by: Fabio Estevam <fabio.estevam@freescale.com> Acked-by: Rob Herring <rob.herring@calxeda.com> Signed-off-by: Shawn Guo <shawn.guo@linaro.org>
| * | | | | | Power: gpio-poweroff: Fix documentation and gpio_is_validAndrew Lunn2013-01-061-3/+17
| | |_|_|_|/ | |/| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Improve the documentation to clarify level vs edge triggered power off. Improve the comments for level vs edge triggered power off. Make use of gpio_is_valid(). Reported-by: Stephen Warren <swarren@wwwdotorg.org> Signed-off-by: Andrew Lunn <andrew@lunn.ch> Signed-off-by: Jason Cooper <jason@lakedaemon.net>
* | | | | | Merge git://git.kernel.org/pub/scm/linux/kernel/git/davem/netLinus Torvalds2013-01-081-5/+11
|\ \ \ \ \ \ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Pull networking fixes from David Miller: 1) New sysctl ndisc_notify needs some documentation, from Hanns Frederic Sowa. 2) Netfilter REJECT target doesn't set transport header of SKB correctly, from Mukund Jampala. 3) Forcedeth driver needs to check for DMA mapping failures, from Larry Finger. 4) brcmsmac driver can't use usleep_range while holding locks, use udelay instead. From Niels Ole Salscheider. 5) Fix unregister of netlink bridge multicast database handlers, from Vlad Yasevich and Rami Rosen. 6) Fix checksum calculations in netfilter's ipv6 network prefix translation module. 7) Fix high order page allocation failures in netfilter xt_recent, from Eric Dumazet. 8) mac802154 needs to use netif_rx_ni() instead of netif_rx() because mac802154_process_data() can execute in process rather than interrupt context. From Alexander Aring. 9) Fix splice handling of MSG_SENDPAGE_NOTLAST, otherwise we elide one tcp_push() too many. From Eric Dumazet and Willy Tarreau. 10) Fix skb->truesize tracking in XEN netfront driver, from Ian Campbell. * git://git.kernel.org/pub/scm/linux/kernel/git/davem/net: (46 commits) xen/netfront: improve truesize tracking ipv4: fix NULL checking in devinet_ioctl() tcp: fix MSG_SENDPAGE_NOTLAST logic net/ipv4/ipconfig: really display the BOOTP/DHCP server's address. ip-sysctl: fix spelling errors mac802154: fix NOHZ local_softirq_pending 08 warning ipv6: document ndisc_notify in networking/ip-sysctl.txt ath9k: Fix Kconfig for ATH9K_HTC netfilter: xt_recent: avoid high order page allocations netfilter: fix missing dependencies for the NOTRACK target netfilter: ip6t_NPT: fix IPv6 NTP checksum calculation bridge: add empty br_mdb_init() and br_mdb_uninit() definitions. vxlan: allow live mac address change bridge: Correctly unregister MDB rtnetlink handlers brcmfmac: fix parsing rsn ie for ap mode. brcmsmac: add copyright information for Canonical rtlwifi: rtl8723ae: Fix warning for unchecked pci_map_single() call rtlwifi: rtl8192se: Fix warning for unchecked pci_map_single() call rtlwifi: rtl8192de: Fix warning for unchecked pci_map_single() call rtlwifi: rtl8192ce: Fix warning for unchecked pci_map_single() call ...
| * | | | | | ip-sysctl: fix spelling errorsstephen hemminger2013-01-041-5/+5
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Signed-off-by: Stephen Hemminger <shemminger@vyatta.com> Signed-off-by: David S. Miller <davem@davemloft.net>
| * | | | | | ipv6: document ndisc_notify in networking/ip-sysctl.txtHannes Frederic Sowa2013-01-041-0/+6
| | |/ / / / | |/| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | I slipped in a new sysctl without proper documentation. I would like to make up for this now. Signed-off-by: Hannes Frederic Sowa <hannes@stressinduktion.org> Signed-off-by: David S. Miller <davem@davemloft.net>
* | | | | | Merge tag 'pm+acpi-for-3.8-rc3' of ↵Linus Torvalds2013-01-071-4/+5
|\ \ \ \ \ \ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/rafael/linux-pm Pull ACPI and power management fixes from Rafael Wysocki: - Removal of some ACPICA code that the kernel will never use from Lv Zheng. - APEI fix from Adrian Huang. - Removal of unnecessary ACPI memory hotplug driver code from Liu Jinsong. - Minor ACPI power management fixes. - ACPI debug code fix from Joe Perches. - ACPI fix to make system bus device nodes get the right names. - PNP resources handling fixes from Witold Szczeponik. - cpuidle fix for a recent regression stalling boot on systems with great numbers of CPUs from Daniel Lezcano. - cpuidle fixes from Sivaram Nair. - intel_idle debug message fix from Youquan Song. - cpufreq build regression fix from Larry Finger. - cpufreq fix for an obscure initialization race related to statistics from Konstantin Khlebnikov. - cpufreq change disabling the Longhaul driver by default from Rafał Bilski. - PM core fix preventing device suspend errors from happening during system suspend due to obscure race conditions. - PM QoS local variable name cleanup. * tag 'pm+acpi-for-3.8-rc3' of git://git.kernel.org/pub/scm/linux/kernel/git/rafael/linux-pm: PM: Move disabling/enabling runtime PM to late suspend/early resume PM / QoS: Rename local variable in dev_pm_qos_add_ancestor_request() ACPI / scan: Do not use dummy HID for system bus ACPI nodes cpufreq / governor: Fix problem with cpufreq_ondemand or cpufreq_conservative cpufreq / Longhaul: Disable driver by default cpufreq / stats: fix race between stats allocation and first usage cpuidle: fix lock contention in the idle path intel_idle: pr_debug information need separated cpuidle / coupled: fix ready counter decrement cpuidle: Fix finding state with min power_usage PNP: Handle IORESOURCE_BITS in resource allocation PNP: Simplify setting of resources ACPI / power: Remove useless message from device registering routine ACPI / glue: Update DBG macro to include KERN_DEBUG ACPI / PM: Do not apply ACPI_SUCCESS() to acpi_bus_get_device() result ACPI / memhotplug: remove redundant logic of acpi memory hotadd ACPI / APEI: Fix the returned value in erst_dbg_read ACPICA: Remove useless mini-C library.
| * | | | | | PM: Move disabling/enabling runtime PM to late suspend/early resumeRafael J. Wysocki2013-01-051-4/+5
| | |/ / / / | |/| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Currently, the PM core disables runtime PM for all devices right after executing subsystem/driver .suspend() callbacks for them and re-enables it right before executing subsystem/driver .resume() callbacks for them. This may lead to problems when there are two devices such that the .suspend() callback executed for one of them depends on runtime PM working for the other. In that case, if runtime PM has already been disabled for the second device, the first one's .suspend() won't work correctly (and analogously for resume). To make those issues go away, make the PM core disable runtime PM for devices right before executing subsystem/driver .suspend_late() callbacks for them and enable runtime PM for them right after executing subsystem/driver .resume_early() callbacks for them. This way the potential conflitcs between .suspend_late()/.resume_early() and their runtime PM counterparts are still prevented from happening, but the subtle ordering issues related to disabling/enabling runtime PM for devices during system suspend/resume are much easier to avoid. Reported-and-tested-by: Jan-Matthias Braun <jan_braun@gmx.net> Signed-off-by: Rafael J. Wysocki <rafael.j.wysocki@intel.com> Reviewed-by: Ulf Hansson <ulf.hansson@linaro.org> Reviewed-by: Kevin Hilman <khilman@deeprootsystems.com> Cc: 3.4+ <stable@vger.kernel.org>
* | | | | | Documentation/sysctl/kernel.txt: document /proc/sys/shmallCarlos Alberto Lopez Perez2013-01-041-0/+13
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Signed-off-by: Carlos Alberto Lopez Perez <clopez@igalia.com> Cc: Rob Landley <rob@landley.net> Cc: Larry Finger <Larry.Finger@lwfinger.net> Cc: Neil Horman <nhorman@tuxdriver.com> Cc: Mitsuo Hayasaka <mitsuo.hayasaka.hu@hitachi.com> Cc: Tejun Heo <tj@kernel.org> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* | | | | | ipc: add sysctl to specify desired next object idStanislav Kinsbursky2013-01-041-0/+19
| |_|_|/ / |/| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Add 3 new variables and sysctls to tune them (by one "next_id" variable for messages, semaphores and shared memory respectively). This variable can be used to set desired id for next allocated IPC object. By default it's equal to -1 and old behaviour is preserved. If this variable is non-negative, then desired idr will be extracted from it and used as a start value to search for free IDR slot. Notes: 1) this patch doesn't guarantee that the new object will have desired id. So it's up to user space how to handle new object with wrong id. 2) After a sucessful id allocation attempt, "next_id" will be set back to -1 (if it was non-negative). [akpm@linux-foundation.org: checkpatch fixes] Signed-off-by: Stanislav Kinsbursky <skinsbursky@parallels.com> Cc: Serge Hallyn <serge.hallyn@canonical.com> Cc: "Eric W. Biederman" <ebiederm@xmission.com> Cc: Pavel Emelyanov <xemul@parallels.com> Cc: Al Viro <viro@zeniv.linux.org.uk> Cc: KOSAKI Motohiro <kosaki.motohiro@jp.fujitsu.com> Cc: Michael Kerrisk <mtk.manpages@gmail.com> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* | | | | Merge tag 'driver-core-3.8-rc2' of ↵Linus Torvalds2013-01-039-36/+14
|\ \ \ \ \ | |_|_|/ / |/| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/gregkh/driver-core Pull driver core __dev* removal patches - take 3 - from Greg Kroah-Hartman: "Here are the remaining __dev* removal patches against the 3.8-rc2 tree. All of these patches were previously sent to the subsystem maintainers, most of them were picked up and pushed to you, but there were a number that fell through the cracks, and new drivers were added during the merge window, so this series cleans up the rest of the instances of these markings. Third time's the charm... Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>" Fixed up trivial conflict with the pinctrl pull in pinctrl-sirf.c. * tag 'driver-core-3.8-rc2' of git://git.kernel.org/pub/scm/linux/kernel/git/gregkh/driver-core: (54 commits) misc: remove __dev* attributes. include: remove __dev* attributes. Documentation: remove __dev* attributes. Drivers: misc: remove __dev* attributes. Drivers: block: remove __dev* attributes. Drivers: bcma: remove __dev* attributes. Drivers: char: remove __dev* attributes. Drivers: clocksource: remove __dev* attributes. Drivers: ssb: remove __dev* attributes. Drivers: dma: remove __dev* attributes. Drivers: gpu: remove __dev* attributes. Drivers: infinband: remove __dev* attributes. Drivers: memory: remove __dev* attributes. Drivers: mmc: remove __dev* attributes. Drivers: iommu: remove __dev* attributes. Drivers: power: remove __dev* attributes. Drivers: message: remove __dev* attributes. Drivers: macintosh: remove __dev* attributes. Drivers: mfd: remove __dev* attributes. pstore: remove __dev* attributes. ...
| * | | | Documentation: remove __dev* attributes.Greg Kroah-Hartman2013-01-039-36/+14
| |/ / / | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | CONFIG_HOTPLUG is going away as an option. As a result, the __dev* markings need to be removed. This change removes the use of __devinit, __devexit_p, __devinitdata, __devinitconst, and __devexit from the kernel documentation. Based on patches originally written by Bill Pemberton, but redone by me in order to handle some of the coding style issues better, by hand. Cc: Bill Pemberton <wfp5p@virginia.edu> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* | | | Merge tag 'pinctrl-fixes' of ↵Linus Torvalds2013-01-031-0/+47
|\ \ \ \ | |/ / / |/| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/linusw/linux-pinctrl Pull pinctrl fixes from Linus Walleij: "A first round of pinctrl fixes for v3.8: - i.MX5 register configuration - Swap a kfree to devm_kfree() to avoid memory corruption in the at91 driver - Add the missing device tree binding doc for the SIRF pin controller - Enable the SIRF GPIO pull up/down configuration from the device tree, it was previously retired from the hard-coded approach. - NULL check for the prcm_base in the Nomadik pin controller. - Provide the prcm_base from the device tree in the DT boot path for the Nomadik pin controller." * tag 'pinctrl-fixes' of git://git.kernel.org/pub/scm/linux/kernel/git/linusw/linux-pinctrl: ARM: ux500: add pinctrl address resources pinctrl: nomadik: return if prcm_base is NULL pinctrl: sirf: enable GPIO pullup/down configuration from dts pinctrl: sirf: add missing DT-binding document pinctrl: fix comment mistake drivers/pinctrl/pinctrl-at91.c: convert kfree to devm_kfree pinctrl: imx5: fix GPIO_8 pad CAN1_RXCAN configuration
| * | | pinctrl: sirf: enable GPIO pullup/down configuration from dtsBarry Song2012-12-251-0/+3
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | commit 7bec207427c2efb794 remove sirfsoc_gpio_set_pull function, this patches takes the feature back by adding sirf,pullups and sirf,pulldowns prop in dts, and the driver will set the GPIO pull according to the dts. Cc: Arnd Bergmann <arnd@arndb.de> Signed-off-by: Barry Song <Baohua.Song@csr.com> Signed-off-by: Linus Walleij <linus.walleij@linaro.org>
| * | | pinctrl: sirf: add missing DT-binding documentBarry Song2012-12-251-0/+44
| |/ / | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | While sending email to Linus for reviewing: "pinctrl: sirf: add DT-binding pinmux mapping support" https://patchwork.kernel.org/patch/1364361/ i have included the devicetree/bindings/pinctrl/pinctrl-sirf.txt But while sending pull request with commit 056876f6c73406c, i missed the document. this patch takes the document back. Signed-off-by: Barry Song <Baohua.Song@csr.com> Signed-off-by: Linus Walleij <linus.walleij@linaro.org>
* / / watchdog: twl4030_wdt: add DT supportAaro Koskinen2013-01-021-0/+10
|/ / | | | | | | | | | | | | | | Add DT support for twl4030_wdt. This is needed to get twl4030_wdt to probe when booting with DT. Signed-off-by: Aaro Koskinen <aaro.koskinen@iki.fi> Signed-off-by: Wim Van Sebroeck <wim@iguana.be>
* | Merge git://www.linux-watchdog.org/linux-watchdogLinus Torvalds2012-12-211-0/+12
|\ \ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Pull watchdog updates from Wim Van Sebroeck: "This includes some fixes and code improvements (like clk_prepare_enable and clk_disable_unprepare), conversion from the omap_wdt and twl4030_wdt drivers to the watchdog framework, addition of the SB8x0 chipset support and the DA9055 Watchdog driver and some OF support for the davinci_wdt driver." * git://www.linux-watchdog.org/linux-watchdog: (22 commits) watchdog: mei: avoid oops in watchdog unregister code path watchdog: Orion: Fix possible null-deference in orion_wdt_probe watchdog: sp5100_tco: Add SB8x0 chipset support watchdog: davinci_wdt: add OF support watchdog: da9052: Fix invalid free of devm_ allocated data watchdog: twl4030_wdt: Change TWL4030_MODULE_PM_RECEIVER to TWL_MODULE_PM_RECEIVER watchdog: remove depends on CONFIG_EXPERIMENTAL watchdog: Convert dev_printk(KERN_<LEVEL> to dev_<level>( watchdog: DA9055 Watchdog driver watchdog: omap_wdt: eliminate goto watchdog: omap_wdt: delete redundant platform_set_drvdata() calls watchdog: omap_wdt: convert to devm_ functions watchdog: omap_wdt: convert to new watchdog core watchdog: WatchDog Timer Driver Core: fix comment watchdog: s3c2410_wdt: use clk_prepare_enable and clk_disable_unprepare watchdog: imx2_wdt: Select the driver via ARCH_MXC watchdog: cpu5wdt.c: add missing del_timer call watchdog: hpwdt.c: Increase version string watchdog: Convert twl4030_wdt to watchdog core davinci_wdt: preparation for switch to common clock framework ...
| * | watchdog: davinci_wdt: add OF supportMurali Karicheri2012-12-191-0/+12
| | | | | | | | | | | | | | | | | | | | | | | | This adds OF support for davinci_wdt driver. Signed-off-by: Murali Karicheri <m-karicheri2@ti.com> Acked-by: Grant Likely <grant.likely@secretlab.ca> Signed-off-by: Wim Van Sebroeck <wim@iguana.be>
* | | Merge branch 'akpm' (Andrew's patch-bomb)Linus Torvalds2012-12-202-13/+0
|\ \ \ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Merge the rest of Andrew's patches for -rc1: "A bunch of fixes and misc missed-out-on things. That'll do for -rc1. I still have a batch of IPC patches which still have a possible bug report which I'm chasing down." * emailed patches from Andrew Morton <akpm@linux-foundation.org>: (25 commits) keys: use keyring_alloc() to create module signing keyring keys: fix unreachable code sendfile: allows bypassing of notifier events SGI-XP: handle non-fatal traps fat: fix incorrect function comment Documentation: ABI: remove testing/sysfs-devices-node proc: fix inconsistent lock state linux/kernel.h: fix DIV_ROUND_CLOSEST with unsigned divisors memcg: don't register hotcpu notifier from ->css_alloc() checkpatch: warn on uapi #includes that #include <uapi/... revert "rtc: recycle id when unloading a rtc driver" mm: clean up transparent hugepage sysfs error messages hfsplus: add error message for the case of failure of sync fs in delayed_sync_fs() method hfsplus: rework processing of hfs_btree_write() returned error hfsplus: rework processing errors in hfsplus_free_extents() hfsplus: avoid crash on failed block map free kcmp: include linux/ptrace.h drivers/rtc/rtc-imxdi.c: must include <linux/spinlock.h> mm: cma: WARN if freed memory is still in use exec: do not leave bprm->interp on stack ...
| * | | Documentation: ABI: remove testing/sysfs-devices-nodeDavidlohr Bueso2012-12-201-7/+0
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | This file is already documented in the stable ABI (see commit 5bbe1ec11fcf). Signed-off-by: Davidlohr Bueso <davidlohr.bueso@hp.com> Cc: Greg KH <greg@kroah.com> Cc: Mel Gorman <mel@csn.ul.ie> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
| * | | Documentation: kernel-parameters.txt remove capability.disableJosh Boyer2012-12-201-6/+0
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Remove the documentation for capability.disable. The code supporting this parameter was removed with commit 5915eb53861c ("security: remove dummy module") Signed-off-by: Josh Boyer <jwboyer@redhat.com> Acked-by: Serge Hallyn <serge.hallyn@canonical.com> Cc: Rob Landley <rob@landley.net> Cc: Miklos Szeredi <mszeredi@suse.cz> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* | | | Merge branch 'for-linus' of ↵Linus Torvalds2012-12-207-36/+92
|\ \ \ \ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/viro/vfs Pull VFS update from Al Viro: "fscache fixes, ESTALE patchset, vmtruncate removal series, assorted misc stuff." * 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/viro/vfs: (79 commits) vfs: make lremovexattr retry once on ESTALE error vfs: make removexattr retry once on ESTALE vfs: make llistxattr retry once on ESTALE error vfs: make listxattr retry once on ESTALE error vfs: make lgetxattr retry once on ESTALE vfs: make getxattr retry once on an ESTALE error vfs: allow lsetxattr() to retry once on ESTALE errors vfs: allow setxattr to retry once on ESTALE errors vfs: allow utimensat() calls to retry once on an ESTALE error vfs: fix user_statfs to retry once on ESTALE errors vfs: make fchownat retry once on ESTALE errors vfs: make fchmodat retry once on ESTALE errors vfs: have chroot retry once on ESTALE error vfs: have chdir retry lookup and call once on ESTALE error vfs: have faccessat retry once on an ESTALE error vfs: have do_sys_truncate retry once on an ESTALE error vfs: fix renameat to retry on ESTALE errors vfs: make do_unlinkat retry once on ESTALE errors vfs: make do_rmdir retry once on ESTALE errors vfs: add a flags argument to user_path_parent ...
| * \ \ \ Merge branch 'fscache' of ↵Al Viro2012-12-205-18/+101
| |\ \ \ \ | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/dhowells/linux-fs into for-linus
| | * | | | FS-Cache: Provide proper invalidationDavid Howells2012-12-203-16/+65
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Provide a proper invalidation method rather than relying on the netfs retiring the cookie it has and getting a new one. The problem with this is that isn't easy for the netfs to make sure that it has completed/cancelled all its outstanding storage and retrieval operations on the cookie it is retiring. Instead, have the cache provide an invalidation method that will cancel or wait for all currently outstanding operations before invalidating the cache, and will cause new operations to queue up behind that. Whilst invalidation is in progress, some requests will be rejected until the cache can stack a barrier on the operation queue to cause new operations to be deferred behind it. Signed-off-by: David Howells <dhowells@redhat.com>
| | * | | | FS-Cache: Fix operation state management and accountingDavid Howells2012-12-202-2/+26
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Fix the state management of internal fscache operations and the accounting of what operations are in what states. This is done by: (1) Give struct fscache_operation a enum variable that directly represents the state it's currently in, rather than spreading this knowledge over a bunch of flags, who's processing the operation at the moment and whether it is queued or not. This makes it easier to write assertions to check the state at various points and to prevent invalid state transitions. (2) Add an 'operation complete' state and supply a function to indicate the completion of an operation (fscache_op_complete()) and make things call it. The final call to fscache_put_operation() can then check that an op in the appropriate state (complete or cancelled). (3) Adjust the use of object->n_ops, ->n_in_progress, ->n_exclusive to better govern the state of an object: (a) The ->n_ops is now the number of extant operations on the object and is now decremented by fscache_put_operation() only. (b) The ->n_in_progress is simply the number of objects that have been taken off of the object's pending queue for the purposes of being run. This is decremented by fscache_op_complete() only. (c) The ->n_exclusive is the number of exclusive ops that have been submitted and queued or are in progress. It is decremented by fscache_op_complete() and by fscache_cancel_op(). fscache_put_operation() and fscache_operation_gc() now no longer try to clean up ->n_exclusive and ->n_in_progress. That was leading to double decrements against fscache_cancel_op(). fscache_cancel_op() now no longer decrements ->n_ops. That was leading to double decrements against fscache_put_operation(). fscache_submit_exclusive_op() now decides whether it has to queue an op based on ->n_in_progress being > 0 rather than ->n_ops > 0 as the latter will persist in being true even after all preceding operations have been cancelled or completed. Furthermore, if an object is active and there are runnable ops against it, there must be at least one op running. (4) Add a remaining-pages counter (n_pages) to struct fscache_retrieval and provide a function to record completion of the pages as they complete. When n_pages reaches 0, the operation is deemed to be complete and fscache_op_complete() is called. Add calls to fscache_retrieval_complete() anywhere we've finished with a page we've been given to read or allocate for. This includes places where we just return pages to the netfs for reading from the server and where accessing the cache fails and we discard the proposed netfs page. The bugs in the unfixed state management manifest themselves as oopses like the following where the operation completion gets out of sync with return of the cookie by the netfs. This is possible because the cache unlocks and returns all the netfs pages before recording its completion - which means that there's nothing to stop the netfs discarding them and returning the cookie. FS-Cache: Cookie 'NFS.fh' still has outstanding reads ------------[ cut here ]------------ kernel BUG at fs/fscache/cookie.c:519! invalid opcode: 0000 [#1] SMP CPU 1 Modules linked in: cachefiles nfs fscache auth_rpcgss nfs_acl lockd sunrpc Pid: 400, comm: kswapd0 Not tainted 3.1.0-rc7-fsdevel+ #1090 /DG965RY RIP: 0010:[<ffffffffa007050a>] [<ffffffffa007050a>] __fscache_relinquish_cookie+0x170/0x343 [fscache] RSP: 0018:ffff8800368cfb00 EFLAGS: 00010282 RAX: 000000000000003c RBX: ffff880023cc8790 RCX: 0000000000000000 RDX: 0000000000002f2e RSI: 0000000000000001 RDI: ffffffff813ab86c RBP: ffff8800368cfb50 R08: 0000000000000002 R09: 0000000000000000 R10: ffff88003a1b7890 R11: ffff88001df6e488 R12: ffff880023d8ed98 R13: ffff880023cc8798 R14: 0000000000000004 R15: ffff88003b8bf370 FS: 0000000000000000(0000) GS:ffff88003bd00000(0000) knlGS:0000000000000000 CS: 0010 DS: 0000 ES: 0000 CR0: 000000008005003b CR2: 00000000008ba008 CR3: 0000000023d93000 CR4: 00000000000006e0 DR0: 0000000000000000 DR1: 0000000000000000 DR2: 0000000000000000 DR3: 0000000000000000 DR6: 00000000ffff0ff0 DR7: 0000000000000400 Process kswapd0 (pid: 400, threadinfo ffff8800368ce000, task ffff88003b8bf040) Stack: ffff88003b8bf040 ffff88001df6e528 ffff88001df6e528 ffffffffa00b46b0 ffff88003b8bf040 ffff88001df6e488 ffff88001df6e620 ffffffffa00b46b0 ffff88001ebd04c8 0000000000000004 ffff8800368cfb70 ffffffffa00b2c91 Call Trace: [<ffffffffa00b2c91>] nfs_fscache_release_inode_cookie+0x3b/0x47 [nfs] [<ffffffffa008f25f>] nfs_clear_inode+0x3c/0x41 [nfs] [<ffffffffa0090df1>] nfs4_evict_inode+0x2f/0x33 [nfs] [<ffffffff810d8d47>] evict+0xa1/0x15c [<ffffffff810d8e2e>] dispose_list+0x2c/0x38 [<ffffffff810d9ebd>] prune_icache_sb+0x28c/0x29b [<ffffffff810c56b7>] prune_super+0xd5/0x140 [<ffffffff8109b615>] shrink_slab+0x102/0x1ab [<ffffffff8109d690>] balance_pgdat+0x2f2/0x595 [<ffffffff8103e009>] ? process_timeout+0xb/0xb [<ffffffff8109dba3>] kswapd+0x270/0x289 [<ffffffff8104c5ea>] ? __init_waitqueue_head+0x46/0x46 [<ffffffff8109d933>] ? balance_pgdat+0x595/0x595 [<ffffffff8104bf7a>] kthread+0x7f/0x87 [<ffffffff813ad6b4>] kernel_thread_helper+0x4/0x10 [<ffffffff81026b98>] ? finish_task_switch+0x45/0xc0 [<ffffffff813abcdd>] ? retint_restore_args+0xe/0xe [<ffffffff8104befb>] ? __init_kthread_worker+0x53/0x53 [<ffffffff813ad6b0>] ? gs_change+0xb/0xb Signed-off-by: David Howells <dhowells@redhat.com>
| * | | | | documentation: drop vmtruncateMarco Stornelli2012-12-203-18/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Removed vmtruncate Signed-off-by: Marco Stornelli <marco.stornelli@gmail.com> Signed-off-by: Al Viro <viro@zeniv.linux.org.uk>
* | | | | | Merge branch 'for-3.8' of git://linux-nfs.org/~bfields/linuxLinus Torvalds2012-12-201-16/+4
|\ \ \ \ \ \ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Pull nfsd update from Bruce Fields: "Included this time: - more nfsd containerization work from Stanislav Kinsbursky: we're not quite there yet, but should be by 3.9. - NFSv4.1 progress: implementation of basic backchannel security negotiation and the mandatory BACKCHANNEL_CTL operation. See http://wiki.linux-nfs.org/wiki/index.php/Server_4.0_and_4.1_issues for remaining TODO's - Fixes for some bugs that could be triggered by unusual compounds. Our xdr code wasn't designed with v4 compounds in mind, and it shows. A more thorough rewrite is still a todo. - If you've ever seen "RPC: multiple fragments per record not supported" logged while using some sort of odd userland NFS client, that should now be fixed. - Further work from Jeff Layton on our mechanism for storing information about NFSv4 clients across reboots. - Further work from Bryan Schumaker on his fault-injection mechanism (which allows us to discard selective NFSv4 state, to excercise rarely-taken recovery code paths in the client.) - The usual mix of miscellaneous bugs and cleanup. Thanks to everyone who tested or contributed this cycle." * 'for-3.8' of git://linux-nfs.org/~bfields/linux: (111 commits) nfsd4: don't leave freed stateid hashed nfsd4: free_stateid can use the current stateid nfsd4: cleanup: replace rq_resused count by rq_next_page pointer nfsd: warn on odd reply state in nfsd_vfs_read nfsd4: fix oops on unusual readlike compound nfsd4: disable zero-copy on non-final read ops svcrpc: fix some printks NFSD: Correct the size calculation in fault_inject_write NFSD: Pass correct buffer size to rpc_ntop nfsd: pass proper net to nfsd_destroy() from NFSd kthreads nfsd: simplify service shutdown nfsd: replace boolean nfsd_up flag by users counter nfsd: simplify NFSv4 state init and shutdown nfsd: introduce helpers for generic resources init and shutdown nfsd: make NFSd service structure allocated per net nfsd: make NFSd service boot time per-net nfsd: per-net NFSd up flag introduced nfsd: move per-net startup code to separated function nfsd: pass net to __write_ports() and down nfsd: pass net to nfsd_set_nrthreads() ...
| * | | | | | nfsd4: delay filling in write iovec array till after xdr decodingJ. Bruce Fields2012-11-261-2/+2
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Our server rejects compounds containing more than one write operation. It's unclear whether this is really permitted by the spec; with 4.0, it's possibly OK, with 4.1 (which has clearer limits on compound parameters), it's probably not OK. No client that we're aware of has ever done this, but in theory it could be useful. The source of the limitation: we need an array of iovecs to pass to the write operation. In the worst case that array of iovecs could have hundreds of elements (the maximum rwsize divided by the page size), so it's too big to put on the stack, or in each compound op. So we instead keep a single such array in the compound argument. We fill in that array at the time we decode the xdr operation. But we decode every op in the compound before executing any of them. So once we've used that array we can't decode another write. If we instead delay filling in that array till the time we actually perform the write, we can reuse it. Another option might be to switch to decoding compound ops one at a time. I considered doing that, but it has a number of other side effects, and I'd rather fix just this one problem for now. Signed-off-by: J. Bruce Fields <bfields@redhat.com>
| * | | | | | nfsd4: update documentation on 4.1 progressJ. Bruce Fields2012-11-101-8/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | Signed-off-by: J. Bruce Fields <bfields@redhat.com>
| * | | | | | nfsd4: implement backchannel_ctl operationJ. Bruce Fields2012-11-071-6/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | This operation is mandatory for servers to implement. Signed-off-by: J. Bruce Fields <bfields@redhat.com>