aboutsummaryrefslogtreecommitdiffstats
Commit message (Collapse)AuthorAgeFilesLines
* tools: Define a Makefile function to do subdir processingDavid Howells2012-11-191-12/+12
| | | | | | | | | | | | | | | | | | Define a Makefile function that can be called with $(call ...) to wrap the subdir make invocations in tools/Makefile. This will allow us in the next patch to insert bits in there to honour O= flags when called from the top-level Makefile. Signed-off-by: David Howells <dhowells@redhat.com> Cc: Borislav Petkov <bp@amd64.org> Cc: Ingo Molnar <mingo@kernel.org> Cc: Linus Torvalds <torvalds@linux-foundation.org> Cc: Namhyung Kim <namhyung@gmail.com> Cc: Paul Mackerras <paulus@samba.org> Cc: Thomas Gleixner <tglx@linutronix.de> Link: http://lkml.kernel.org/r/1378.1352379110@warthog.procyon.org.uk Signed-off-by: Arnaldo Carvalho de Melo <acme@redhat.com>
* tools: Connect to the kernel build systemBorislav Petkov2012-04-111-0/+10
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Now you can do $ make tools/<toolname> from the toplevel kernel directory and have the respective tool built. If you want to build and install it, do $ make tools/<toolname>_install $ make tools/<toolname>_clean should clean the respective tool directories. If you want to clean all in tools, simply do $ make tools/clean Also, if you want to get what the possible targets are, simply calling $ make tools/ should give you the short help. $ make tools/install installs all tools, of course. Doh. Signed-off-by: Borislav Petkov <borislav.petkov@amd.com> Cc: Ingo Molnar <mingo@kernel.org> Cc: Michal Marek <mmarek@suse.cz> Cc: Sam Ravnborg <sam@ravnborg.org> Link: http://lkml.kernel.org/r/1334162178-17152-6-git-send-email-bp@amd64.org Signed-off-by: Arnaldo Carvalho de Melo <acme@redhat.com>
* tools: Add a help targetBorislav Petkov2012-04-111-0/+20
| | | | | | | | | | | | | ... and make it the default one so that calling 'make' without arguments in the tools/ directory gives you the possible targets to build along with a short description of what they are. Signed-off-by: Borislav Petkov <borislav.petkov@amd.com> Cc: Ingo Molnar <mingo@kernel.org> Cc: Michal Marek <mmarek@suse.cz> Cc: Sam Ravnborg <sam@ravnborg.org> Link: http://lkml.kernel.org/r/1334162178-17152-5-git-send-email-bp@amd64.org Signed-off-by: Arnaldo Carvalho de Melo <acme@redhat.com>
* tools: Add a toplevel MakefileBorislav Petkov2012-04-111-0/+47
Add a Makefile with all the targets under tools/. Signed-off-by: Borislav Petkov <borislav.petkov@amd.com> Cc: Ingo Molnar <mingo@kernel.org> Cc: Michal Marek <mmarek@suse.cz> Cc: Sam Ravnborg <sam@ravnborg.org> Link: http://lkml.kernel.org/r/1334162178-17152-4-git-send-email-bp@amd64.org Signed-off-by: Arnaldo Carvalho de Melo <acme@redhat.com>