aboutsummaryrefslogtreecommitdiffstats
Commit message (Collapse)AuthorAgeFilesLines
* USB: ffs-test: fix length argument of out function callMatthias Fend2012-05-071-1/+1
| | | | | | | | | | | The out functions should only handle actual available data instead of the complete buffer. Otherwise for example the ep0_consume function will report ghost events since it tries to decode the complete buffer - which may contain partly invalid data. Signed-off-by: Matthias Fend <matthias.fend@wolfvision.net> Cc: stable <stable@vger.kernel.org> Acked-by: Michal Nazarewicz <mina86@mina86.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* Merge branch 'x86-build-for-linus' of ↵Linus Torvalds2012-03-221-28/+1
|\ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/tip/tip Pull x86/build changes from Ingo Molnar. * 'x86-build-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/tip/tip: x86, build: Fix portability issues when cross-building x86, tools: Remove unneeded header files from tools/build.c USB: ffs-test: Don't duplicate {get,put}_unaligned*() functions x86, efi: Fix endian issues and unaligned accesses x86, boot: Restrict CFLAGS for hostprogs x86, mkpiggy: Don't open code put_unaligned_le32() x86, relocs: Don't open code put_unaligned_le32() tools/include: Add byteshift headers for endian access
| * USB: ffs-test: Don't duplicate {get,put}_unaligned*() functionsMatt Fleming2012-02-281-28/+1
| | | | | | | | | | | | | | | | | | | | | | Use the header file in tools/include instead of duplicating the endian functions. Cc: Davidlohr Bueso <dave@gnu.org> Acked-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org> Signed-off-by: Matt Fleming <matt.fleming@intel.com> Link: http://lkml.kernel.org/r/1330436245-24875-7-git-send-email-matt@console-pimps.org Signed-off-by: H. Peter Anvin <hpa@zytor.com>
* | usb: gadget: update Michal Nazarewicz's email addressMichal Nazarewicz2012-01-241-1/+1
|/ | | | | | | | | | The m.nazarewicz@samsung.com email address is no longer valid, so this commit replaces it with mina86@mina86.com which is employer-agnostic and thus should be valid for foreseeable feature. Signed-off-by: Michal Nazarewicz <mina86@mina86.com> Signed-off-by: Felipe Balbi <balbi@ti.com>
* USB: ffs-test: fix header pathDavidlohr Bueso2011-02-281-2/+2
| | | | | | | | | | | When compiling this program the functionfs.h header cannot be found, producing: ffs-test.c:40: fatal error: linux/usb/functionfs.h: No such file or directory This patch also fixes the following warning: ffs-test.c:453: warning: format ‘%4d’ expects type ‘int’, but argument 3 has type ‘size_t’ Signed-off-by: Davidlohr Bueso <dave@gnu.org> Signed-off-by: Greg Kroah-Hartman <gregkh@suse.de>
* USB: ffs-test: FunctionFS testing programMichal Nazarewicz2010-05-201-0/+554
This adds an example user-space FunctionFS driver which implements a source/sink interface used for testing. Signed-off-by: Michal Nazarewicz <m.nazarewicz@samsung.com> Cc: Kyungmin Park <kyungmin.park@samsung.com> Cc: Marek Szyprowski <m.szyprowski@samsung.com> Signed-off-by: Greg Kroah-Hartman <gregkh@suse.de>