aboutsummaryrefslogtreecommitdiffstats
path: root/tools/usb
Commit message (Collapse)AuthorAgeFilesLines
* tools: usb: ffs-test: Fix build failureMaxin B. John2013-03-201-1/+1
| | | | | | | | | | | | | | | | | | commit a0f11aceee531d444f58b939e6a537ee5e2b9cc5 upstream. Fixes this build failure: gcc -Wall -Wextra -g -lpthread -I../include -o testusb testusb.c gcc -Wall -Wextra -g -lpthread -I../include -o ffs-test ffs-test.c In file included from ffs-test.c:41:0: ../../include/linux/usb/functionfs.h:4:39: fatal error: uapi/linux/usb/functionfs.h: No such file or directory compilation terminated. make: *** [ffs-test] Error 1 Signed-off-by: Maxin B. John <maxin.john@enea.com> Acked-by: Michal Nazarewicz <mina86@mina86.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* tools/usb: remove last USBFS userSebastian Andrzej Siewior2012-09-101-24/+1
| | | | | | | | | In commit fb28d58b ("USB: remove CONFIG_USB_DEVICEFS") USBFS got removed. Since it is gone we can stop using it in testusb and try udev nodes right away. Signed-off-by: Sebastian Andrzej Siewior <bigeasy@linutronix.de> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* testusb: expose looping forever option "l" to userDu, ChangbinX2012-06-131-5/+16
| | | | | | | | | | | | | | | The testusb.c tool has support for looping forever implemented, which may be useful for stress test, yet it is not exposed to the user, so even though the code is there, it cannot be used. This commit adds "l" to the set of options handled by the application which enables the feature. Also, I collate help information for each command line option to make it easier to use for novice. Signed-off-by: Du Changbin <changbinx.du@intel.com> Acked-by: Michal Nazarewicz <mina86@mina86.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* USB: testusb: add path /dev/bus/usb to default search paths for usbfsDu, ChangbinX2012-05-151-0/+5
| | | | | | | | | As real device-nodes managed by udev whose nodes lived in /dev/bus/usb are mostly used today, let testusb tool use that directory as one default path make tool be more convenient to use. Signed-off-by: Du Changbin <changbinx.du@intel.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* USB: ffs-test: fix length argument of out function callMatthias Fend2012-05-071-1/+1
| | | | | | | | | | | The out functions should only handle actual available data instead of the complete buffer. Otherwise for example the ep0_consume function will report ghost events since it tries to decode the complete buffer - which may contain partly invalid data. Signed-off-by: Matthias Fend <matthias.fend@wolfvision.net> Cc: stable <stable@vger.kernel.org> Acked-by: Michal Nazarewicz <mina86@mina86.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* Merge branch 'x86-build-for-linus' of ↵Linus Torvalds2012-03-222-29/+2
|\ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/tip/tip Pull x86/build changes from Ingo Molnar. * 'x86-build-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/tip/tip: x86, build: Fix portability issues when cross-building x86, tools: Remove unneeded header files from tools/build.c USB: ffs-test: Don't duplicate {get,put}_unaligned*() functions x86, efi: Fix endian issues and unaligned accesses x86, boot: Restrict CFLAGS for hostprogs x86, mkpiggy: Don't open code put_unaligned_le32() x86, relocs: Don't open code put_unaligned_le32() tools/include: Add byteshift headers for endian access
| * USB: ffs-test: Don't duplicate {get,put}_unaligned*() functionsMatt Fleming2012-02-282-29/+2
| | | | | | | | | | | | | | | | | | | | | | Use the header file in tools/include instead of duplicating the endian functions. Cc: Davidlohr Bueso <dave@gnu.org> Acked-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org> Signed-off-by: Matt Fleming <matt.fleming@intel.com> Link: http://lkml.kernel.org/r/1330436245-24875-7-git-send-email-matt@console-pimps.org Signed-off-by: H. Peter Anvin <hpa@zytor.com>
* | usb: gadget: update Michal Nazarewicz's email addressMichal Nazarewicz2012-01-242-2/+2
|/ | | | | | | | | | The m.nazarewicz@samsung.com email address is no longer valid, so this commit replaces it with mina86@mina86.com which is employer-agnostic and thus should be valid for foreseeable feature. Signed-off-by: Michal Nazarewicz <mina86@mina86.com> Signed-off-by: Felipe Balbi <balbi@ti.com>
* USB: ffs-test: fix header pathDavidlohr Bueso2011-02-281-2/+2
| | | | | | | | | | | When compiling this program the functionfs.h header cannot be found, producing: ffs-test.c:40: fatal error: linux/usb/functionfs.h: No such file or directory This patch also fixes the following warning: ffs-test.c:453: warning: format ‘%4d’ expects type ‘int’, but argument 3 has type ‘size_t’ Signed-off-by: Davidlohr Bueso <dave@gnu.org> Signed-off-by: Greg Kroah-Hartman <gregkh@suse.de>
* USB: tools: Add a MakefileDavidlohr Bueso2011-02-171-0/+13
| | | | | | | Build USB tools easier. Signed-off-by: Davidlohr Bueso <dave@gnu.org> Signed-off-by: Greg Kroah-Hartman <gregkh@suse.de>
* USB: usbtest - add alignment tests to test scriptMartin Fuzzey2011-01-221-0/+26
| | | | | | | | | | | | | Enhance the test script to call the new tests added to usbtest in order to detect host controllers that don't accept byte aligned DMA. The unaligned tests are called after their aligned equivalents but for fewer iterations (since alignment failure is generally immediate). Signed-off-by: Martin Fuzzey <mfuzzey@gmail.com> Signed-off-by: Greg Kroah-Hartman <gregkh@suse.de>
* USB: usbtest - add shell script to test HCDsDavid Brownell2011-01-221-0/+249
| | | | | | | | This patch just adds the script available at http://www.linux-usb.org/usbtest/test.sh as is. Signed-off-by: Martin Fuzzey <mfuzzey@gmail.com> Signed-off-by: Greg Kroah-Hartman <gregkh@suse.de>
* USB: testusb: testusb compatibility with FunctionFS gadgetMichal Nazarewicz2010-05-201-70/+190
| | | | | | | | | | | | | | | | | | | The FunctionFS gadget may provide the source/sink interface not as the first interface (with id == 0) but some different interface hence a code to find the interface number is required. (Note that you will still configure the gadget to report idProduct == 0xa4a4 (an "echo 0xa4a4 >/sys/module/g_ffs/parameters/usb_product" should suffice) or configure host to handle 0x0525:0xa4ac devices using the usbtest driver.) Signed-off-by: Michal Nazarewicz <m.nazarewicz@samsung.com> Cc: Kyungmin Park <kyungmin.park@samsung.com> Cc: Marek Szyprowski <m.szyprowski@samsung.com> Signed-off-by: Greg Kroah-Hartman <gregkh@suse.de>
* USB: testusb: an USB testing applicationDavid Brownell2010-05-201-0/+427
| | | | | | | | | | | | | | | | The testusb program just issues ioctls to perform the tests implemented by the kernel driver. It can generate a variety of transfer patterns; you should make sure to test both regular streaming and mixes of transfer sizes (including short transfers). For more information on how this can be used and on USB testing refer to <URL:http://www.linux-usb.org/usbtest/>. Signed-off-by: Michal Nazarewicz <m.nazarewicz@samsung.com> Cc: Kyungmin Park <kyungmin.park@samsung.com> Cc: Marek Szyprowski <m.szyprowski@samsung.com> Signed-off-by: Greg Kroah-Hartman <gregkh@suse.de>
* USB: ffs-test: FunctionFS testing programMichal Nazarewicz2010-05-201-0/+554
This adds an example user-space FunctionFS driver which implements a source/sink interface used for testing. Signed-off-by: Michal Nazarewicz <m.nazarewicz@samsung.com> Cc: Kyungmin Park <kyungmin.park@samsung.com> Cc: Marek Szyprowski <m.szyprowski@samsung.com> Signed-off-by: Greg Kroah-Hartman <gregkh@suse.de>