aboutsummaryrefslogtreecommitdiffstats
path: root/tools/vm
Commit message (Collapse)AuthorAgeFilesLines
* tools/vm: add .gitignore to ignore built binariesJoonsoo Kim2013-02-051-0/+2
| | | | | | | | | There is no .gitignore in tools/vm, so 'git status' always show built binaries. To ignore this, add .gitignore. Signed-off-by: Joonsoo Kim <iamjoonsoo.kim@lge.com> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* UAPI: fix tools/vm/page-types.cDavid Howells2012-10-251-1/+1
| | | | | | | | | | | | | | | | Fix tools/vm/page-types.c to use the UAPI variant of linux/kernel-page-flags.h lest the following error appear: In file included from page-types.c:38:0: ../../include/linux/kernel-page-flags.h:4:42: fatal error: uapi/linux/kernel-page-flags.h: No such file or directory Reported-by: Daniel Hazelton <dshadowwolf@gmail.com> Signed-off-by: David Howells <dhowells@redhat.com> Reviewed-by: Fengguang Wu <fengguang.wu@intel.com> Tested-by: Daniel Hazelton <dshadowwolf@gmail.com> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* UAPI: (Scripted) Disintegrate include/linuxDavid Howells2012-10-131-1/+1
| | | | | | | | | Signed-off-by: David Howells <dhowells@redhat.com> Acked-by: Arnd Bergmann <arnd@arndb.de> Acked-by: Thomas Gleixner <tglx@linutronix.de> Acked-by: Michael Kerrisk <mtk.manpages@gmail.com> Acked-by: Paul E. McKenney <paulmck@linux.vnet.ibm.com> Acked-by: Dave Jones <davej@redhat.com>
* mm: Fix signal SIGFPE in slabinfo.c.majianpeng2012-07-021-7/+7
| | | | | | | | | In function slab_stats(), if total_free is equal zero, it will error. So fix it. Acked-by: Christoph Lameter <cl@linux.com> Signed-off-by: majianpeng <majianpeng@gmail.com> Signed-off-by: Pekka Enberg <penberg@kernel.org>
* tools/vm/page-types.c: cleanupsUlrich Drepper2012-05-291-11/+11
| | | | | | | | | | | | | | | | Compiling page-type.c with a recent compiler produces many warnings, mostly related to signed/unsigned comparisons. This patch cleans up most of them. One remaining warning is about an unused parameter. The <compiler.h> file doesn't define a __unused macro (or the like) yet. This can be addressed later. Signed-off-by: Ulrich Drepper <drepper@gmail.com> Acked-by: KOSAKI Motohiro <kosaki.motohiro@jp.fujitsu.com> Acked-by: Fengguang Wu <fengguang.wu@intel.com> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* kbuild: install kernel-page-flags.hUlrich Drepper2012-05-291-27/+1
| | | | | | | | | | | | | | | | Programs using /proc/kpageflags need to know about the various flags. The <linux/kernel-page-flags.h> provides them and the comments in the file indicate that it is supposed to be used by user-level code. But the file is not installed. Install the headers and mark the unstable flags as out-of-bounds. The page-type tool is also adjusted to not duplicate the definitions Signed-off-by: Ulrich Drepper <drepper@gmail.com> Acked-by: KOSAKI Motohiro <kosaki.motohiro@jp.fujitsu.com> Acked-by: Fengguang Wu <fengguang.wu@intel.com> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* mm: move slabinfo.c to tools/vmDave Young2012-03-282-2/+1395
| | | | | | | | | | | | | We have tools/vm/ folder for vm tools, so move slabinfo.c from tools/slub/ to tools/vm/ Signed-off-by: Dave Young <dyoung@redhat.com> Cc: Wu Fengguang <fengguang.wu@intel.com> Acked-by: Christoph Lameter <cl@linux.com> Cc: Pekka Enberg <penberg@cs.helsinki.fi> Cc: Frederic Weisbecker <fweisbec@gmail.com> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* mm: move page-types.c from Documentation to tools/vmDave Young2012-03-282-0/+1113
tools/ is the better place for vm tools which are used by many people. Moving them to tools also make them open to more users instead of hide in Documentation folder. This patch moves page-types.c to tools/vm/page-types.c. Also add a Makefile in tools/vm and fix two coding style problems: a) change const arrary to 'const char * const', b) change a space to tab for indent. Signed-off-by: Dave Young <dyoung@redhat.com> Acked-by: Wu Fengguang <fengguang.wu@intel.com> Cc: Christoph Lameter <cl@linux.com> Cc: Pekka Enberg <penberg@cs.helsinki.fi> Cc: Frederic Weisbecker <fweisbec@gmail.com> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>