aboutsummaryrefslogtreecommitdiffstats
path: root/tools
Commit message (Collapse)AuthorAgeFilesLines
* tools: usb: ffs-test: Fix build failureMaxin B. John2013-03-201-1/+1
| | | | | | | | | | | | | | | | | | commit a0f11aceee531d444f58b939e6a537ee5e2b9cc5 upstream. Fixes this build failure: gcc -Wall -Wextra -g -lpthread -I../include -o testusb testusb.c gcc -Wall -Wextra -g -lpthread -I../include -o ffs-test ffs-test.c In file included from ffs-test.c:41:0: ../../include/linux/usb/functionfs.h:4:39: fatal error: uapi/linux/usb/functionfs.h: No such file or directory compilation terminated. make: *** [ffs-test] Error 1 Signed-off-by: Maxin B. John <maxin.john@enea.com> Acked-by: Michal Nazarewicz <mina86@mina86.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* perf hists: Fix period symbol_conf.field_sep displayJiri Olsa2013-02-281-1/+5
| | | | | | | | | | | | | | | | | | | | | commit c0d246b85fc7d42688d7a5d999ea671777caf65b upstream. Currently we don't properly display hist data with symbol_conf.field_sep separator. We need to display either space or separator. Signed-off-by: Jiri Olsa <jolsa@redhat.com> Cc: Arnaldo Carvalho de Melo <acme@ghostprotocols.net> Cc: Peter Zijlstra <a.p.zijlstra@chello.nl> Cc: Ingo Molnar <mingo@elte.hu> Cc: Paul Mackerras <paulus@samba.org> Cc: Corey Ashford <cjashfor@linux.vnet.ibm.com> Cc: Frederic Weisbecker <fweisbec@gmail.com> Cc: Namhyung Kim <namhyung@kernel.org> Link: http://lkml.kernel.org/n/tip-cyggwys0bz5kqdowwvfd8h72@git.kernel.org Signed-off-by: Arnaldo Carvalho de Melo <acme@redhat.com> Cc: Josh Boyer <jwboyer@redhat.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* perf tools: Fix build with bison 2.3 and older.Vinson Lee2013-02-283-4/+2
| | | | | | | | | | | | | | | | | | | | | | | | | | | | commit 85df3b3769222894e9692b383c7af124b7721086 upstream. The %name-prefix "prefix" syntax is not available on bison 2.3 and older. Substitute with the -p "prefix" command-line option for compatibility with older versions of bison. This patch fixes this build error with older versions of bison. CC util/sysfs.o BISON util/pmu-bison.c util/pmu.y:2.14-24: syntax error, unexpected string, expecting = make: *** [util/pmu-bison.c] Error 1 Signed-off-by: Vinson Lee <vlee@twitter.com> Tested-by: Li Zefan <lizefan@huawei.com> Cc: Ingo Molnar <mingo@redhat.com> Cc: Jiri Olsa <jolsa@redhat.com> Cc: Li Zefan <lizefan@huawei.com> Cc: Namhyung Kim <namhyung@gmail.com> Cc: Paul Mackerras <paulus@samba.org> Cc: Pekka Enberg <penberg@kernel.org> Link: http://lkml.kernel.org/r/1360792138-29186-1-git-send-email-vlee@twitter.com Signed-off-by: Arnaldo Carvalho de Melo <acme@redhat.com> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* tools/vm: add .gitignore to ignore built binariesJoonsoo Kim2013-02-051-0/+2
| | | | | | | | | There is no .gitignore in tools/vm, so 'git status' always show built binaries. To ignore this, add .gitignore. Signed-off-by: Joonsoo Kim <iamjoonsoo.kim@lge.com> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* Merge tag 'arm64-fixes' of ↵Linus Torvalds2013-01-231-1/+1
|\ | | | | | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/cmarinas/linux-aarch64 Pull arm64 fixes from Catalin Marinas: - ELF coredump fix (more registers dumped than what user space expects) - SUBARCH name generation (s/aarch64/arm64/) * tag 'arm64-fixes' of git://git.kernel.org/pub/scm/linux/kernel/git/cmarinas/linux-aarch64: arm64: makefile: fix uname munging when setting ARCH on native machine arm64: elf: fix core dumping to match what glibc expects
| * arm64: makefile: fix uname munging when setting ARCH on native machineWill Deacon2013-01-221-1/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | By popular demand, arch/aarch64 is now known as arch/arm64. However, uname -m (and indeed the GNU triplet) still use aarch64 as the machine string. This patch fixes native builds of both the kernel and perf tools by updating the relevant Makefiles to munge the output of uname -m and set the ARCH variable appropriately. Cc: <stable@vger.kernel.org> Signed-off-by: Will Deacon <will.deacon@arm.com> Signed-off-by: Catalin Marinas <catalin.marinas@arm.com>
* | perf tools: Fix building from 'make perf-*-src-pkg' tarballsSebastian Andrzej Siewior2013-01-101-0/+10
|/ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Thanks (mostly) to uapi the package created from perf-*-src-pkg FTBFS: | CC perf.o |In file included from util/../perf.h:8:0, | from util/cache.h:7, | from perf.c:12: |arch/x86/include/asm/unistd.h:4:29: fatal error: uapi/asm/unistd.h: No such file or directory | | CC perf.o |In file included from util/../perf.h:106:0, | from util/cache.h:7, | from perf.c:12: |include/linux/perf_event.h:17:35: fatal error: uapi/linux/perf_event.h: No such file or directory | | CC perf.o |In file included from include/uapi/linux/perf_event.h:19:0, | from util/../perf.h:106, | from util/cache.h:7, | from perf.c:12: |util/include/asm/byteorder.h:2:49: fatal error: ../../../../include/uapi/linux/swab.h: No such file or directory | | CC perf.o |In file included from util/include/../../../../include/linux/list.h:7:0, | from util/include/linux/list.h:4, | from util/parse-events.h:7, | from perf.c:15: |util/include/linux/const.h:1:50: fatal error: ../../../../include/uapi/linux/const.h: No such file or directory | |In file included from builtin-kvm.c:26:0: |arch/x86/include/asm/svm.h:4:26: fatal error: uapi/asm/svm.h: No such file or directory | |In file included from util/evsel.c:21:0: |include/linux/hw_breakpoint.h:5:38: fatal error: uapi/linux/hw_breakpoint.h: No such file or directory | | CC util/evsel.o |In file included from util/perf_regs.h:5:0, | from util/evsel.c:23: |arch/x86/include/perf_regs.h:6:27: fatal error: asm/perf_regs.h: No such file or directory | | CC util/rbtree.o |In file included from ../../lib/rbtree.c:24:0: |util/include/linux/rbtree_augmented.h:2:56: fatal error: ../../../../include/linux/rbtree_augmented.h: No such file or directory This patch adds the missing files. Signed-off-by: Sebastian Andrzej Siewior <bigeasy@linutronix.de> Cc: Ingo Molnar <mingo@redhat.com> Cc: Paul Mackerras <paulus@samba.org> Cc: Peter Zijlstra <a.p.zijlstra@chello.nl> Link: http://lkml.kernel.org/r/1357654134-28538-1-git-send-email-bigeasy@linutronix.de Signed-off-by: Arnaldo Carvalho de Melo <acme@redhat.com>
* selftests: IPC message queue copy feature testStanislav Kinsbursky2013-01-042-0/+271
| | | | | | | | | | | | | | | This test can be used to check wheither kernel supports IPC message queue copy and restore features (required by CRIU project). Signed-off-by: Stanislav Kinsbursky <skinsbursky@parallels.com> Cc: Serge Hallyn <serge.hallyn@canonical.com> Cc: "Eric W. Biederman" <ebiederm@xmission.com> Cc: Pavel Emelyanov <xemul@parallels.com> Cc: Al Viro <viro@zeniv.linux.org.uk> Cc: KOSAKI Motohiro <kosaki.motohiro@jp.fujitsu.com> Cc: Michael Kerrisk <mtk.manpages@gmail.com> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* Merge tag 'virtio-next-for-linus' of ↵Linus Torvalds2012-12-202-51/+37
|\ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/rusty/linux Pull virtio update from Rusty Russell: "Some nice cleanups, and even a patch my wife did as a "live" demo for Latinoware 2012. There's a slightly non-trivial merge in virtio-net, as we cleaned up the virtio add_buf interface while DaveM accepted the mq virtio-net patches." * tag 'virtio-next-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/rusty/linux: (27 commits) virtio_console: Add support for remoteproc serial virtio_console: Merge struct buffer_token into struct port_buffer virtio: add drv_to_virtio to make code clearly virtio: use dev_to_virtio wrapper in virtio virtio-mmio: Fix irq parsing in command line parameter virtio_console: Free buffers from out-queue upon close virtio: Convert dev_printk(KERN_<LEVEL> to dev_<level>( virtio_console: Use kmalloc instead of kzalloc virtio_console: Free buffer if splice fails virtio: tools: make it clear that virtqueue_add_buf() no longer returns > 0 virtio: scsi: make it clear that virtqueue_add_buf() no longer returns > 0 virtio: rpmsg: make it clear that virtqueue_add_buf() no longer returns > 0 virtio: net: make it clear that virtqueue_add_buf() no longer returns > 0 virtio: console: make it clear that virtqueue_add_buf() no longer returns > 0 virtio: make virtqueue_add_buf() returning 0 on success, not capacity. virtio: console: don't rely on virtqueue_add_buf() returning capacity. virtio_net: don't rely on virtqueue_add_buf() returning capacity. virtio-net: remove unused skb_vnet_hdr->num_sg field virtio-net: correct capacity math on ring full virtio: move queue_index and num_free fields into core struct virtqueue. ...
| * virtio: tools: make it clear that virtqueue_add_buf() no longer returns > 0Rusty Russell2012-12-171-2/+2
| | | | | | | | | | | | We simplified virtqueue_add_buf(), make it clear in the callers. Signed-off-by: Rusty Russell <rusty@rustcorp.com.au>
| * lguest: fix block request handling in example launcher.Rusty Russell2012-10-221-49/+35
| | | | | | | | | | | | | | | | | | | | | | | | | | virtio requests are scatter-gather-style descriptors, but no assumptions should be made about the layout. lguest was lazy here, but saved by the fact that the network device hands all requests to tun (which does it correctly) and console and random devices simply use readv and writev. Block devices, however, are broken: we convert to iovecs internally, just make sure we handle the correctly. Signed-off-by: Rusty Russell <rusty@rustcorp.com.au>
* | Merge branch 'release' of ↵Linus Torvalds2012-12-185-81/+728
|\ \ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/lenb/linux Pull powertool update from Len Brown: "This updates the tree w/ the latest version of turbostat, which reports temperature and - on SNB and later - Watts." Fix up semantic merge conflict as per Len. * 'release' of git://git.kernel.org/pub/scm/linux/kernel/git/lenb/linux: tools: Allow tools to be installed in a user specified location tools/power: turbostat: make Makefile a bit more capable tools/power x86_energy_perf_policy: close /proc/stat in for_every_cpu() tools/power turbostat: v3.0: monitor Watts and Temperature tools/power turbostat: fix output buffering issue tools/power turbostat: prevent infinite loop on migration error path x86 power: define RAPL MSRs tools/power/x86/turbostat: share kernel MSR #defines
| * | tools: Allow tools to be installed in a user specified locationJosh Boyer2012-11-301-2/+4
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | When building x86_energy_perf_policy or turbostat within the confines of a packaging system such as RPM, we need to be able to have it install to the buildroot and not the root filesystem of the build machine. This adds a DESTDIR variable that when set will act as a prefix for the install location of these tools. Signed-off-by: Josh Boyer <jwboyer@redhat.com> Signed-off-by: Len Brown <len.brown@intel.com>
| * | tools/power: turbostat: make Makefile a bit more capableMark Asselstine2012-11-301-4/+16
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | The turbostat Makefile is pretty simple, its output is placed in the same directory as the source, the install rule has no concept of a prefix or sysroot, and you can set CC to use a specific compiler but not use the more familiar CROSS_COMPILE. By making a few minor changes these limitations are removed while leaving the default behavior matching what it used to be. Example build with these changes: make CROSS_COMPILE=i686-wrs-linux-gnu- DESTDIR=/tmp install or from the tools directory make CROSS_COMPILE=i686-wrs-linux-gnu- DESTDIR=/tmp turbostat_install Signed-off-by: Mark Asselstine <mark.asselstine@windriver.com> Signed-off-by: Len Brown <len.brown@intel.com>
| * | tools/power x86_energy_perf_policy: close /proc/stat in for_every_cpu()Colin Ian King2012-11-301-1/+1
| | | | | | | | | | | | | | | | | | | | | | | | Instead of returning out of for_every_cpu() we should break out of the loop= which will then tidy up correctly by closing the file /proc/stat. Signed-off-by: Colin Ian King <colin.king@canonical.com> Signed-off-by: Len Brown <len.brown@intel.com>
| * | tools/power turbostat: v3.0: monitor Watts and TemperatureLen Brown2012-11-302-56/+690
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Show power in Watts and temperature in Celsius when hardware support is present. Intel's Sandy Bridge and Ivy Bridge processor generations support RAPL (Run-Time-Average-Power-Limiting). Per the Intel SDM (Intel® 64 and IA-32 Architectures Software Developer Manual) RAPL provides hardware energy counters and power control MSRs (Model Specific Registers). RAPL MSRs are designed primarily as a method to implement power capping. However, they are useful for monitoring system power whether or not power capping is used. In addition, Turbostat now shows temperature from DTS (Digital Thermal Sensor) and PTM (Package Thermal Monitor) hardware, if present. As before, turbostat reads MSRs, and never writes MSRs. New columns are present in turbostat output: The Pkg_W column shows Watts for each package (socket) in the system. On multi-socket systems, the system summary on the 1st row shows the sum for all sockets together. The Cor_W column shows Watts due to processors cores. Note that Core_W is included in Pkg_W. The optional GFX_W column shows Watts due to the graphics "un-core". Note that GFX_W is included in Pkg_W. The optional RAM_W column on server processors shows Watts due to DRAM DIMMS. As DRAM DIMMs are outside the processor package, RAM_W is not included in Pkg_W. The optional PKG_% and RAM_% columns on server processors shows the % of time in the measurement interval that RAPL power limiting is in effect on the package and on DRAM. Note that the RAPL energy counters have some limitations. First, hardware updates the counters about once every milli-second. This is fine for typical turbostat measurement intervals > 1 sec. However, when turbostat is used to measure events that approach 1ms, the counters are less useful. Second, the 32-bit energy counters are subject to wrapping. For example, a counter incrementing 15 micro-Joule units on a 130 Watt TDP server processor could (in theory) roll over in about 9 minutes. Turbostat detects and handles up to 1 counter overflow per measurement interval. But when the measurement interval exceeds the guaranteed counter range, we can't detect if more than 1 overflow occured. So in this case turbostat indicates that the results are in question by replacing the fractional part of the Watts in the output with "**": Pkg_W Cor_W GFX_W 3** 0** 0** Third, the RAPL counters are energy (Joule) counters -- they sum up weighted events in the package to estimate energy consumed. They are not analong power (Watt) meters. In practice, they tend to under-count because they don't cover every possible use of energy in the package. The accuracy of the RAPL counters will vary between product generations, and between SKU's in the same product generation, and with temperature. turbostat's -v (verbose) option now displays more power and thermal configuration information -- as shown on the turbostat.8 manual page. For example, it now displays the Package and DRAM Thermal Design Power (TDP): cpu0: MSR_PKG_POWER_INFO: 0x2f064001980410 (130 W TDP, RAPL 51 - 200 W, 0.045898 sec.) cpu0: MSR_DRAM_POWER_INFO,: 0x28025800780118 (35 W TDP, RAPL 15 - 75 W, 0.039062 sec.) cpu8: MSR_PKG_POWER_INFO: 0x2f064001980410 (130 W TDP, RAPL 51 - 200 W, 0.045898 sec.) cpu8: MSR_DRAM_POWER_INFO,: 0x28025800780118 (35 W TDP, RAPL 15 - 75 W, 0.039062 sec.) Signed-off-by: Len Brown <len.brown@intel.com>
| * | tools/power turbostat: fix output buffering issueLen Brown2012-11-301-0/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | In periodic mode, turbostat writes to stdout, but users were un-able to re-direct stdout, eg. turbostat > outputfile would result in an empty outputfile. Signed-off-by: Len Brown <len.brown@intel.com>
| * | tools/power turbostat: prevent infinite loop on migration error pathLen Brown2012-11-261-1/+10
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Turbostat assumed if it can't migrate to a CPU, then the CPU must have gone off-line and turbostat should re-initialize with the new topology. But if turbostat can not migrate because it is restricted by a cpuset, then it will fail to migrate even after re-initialization, resulting in an infinite loop. Spit out a warning when we can't migrate and endure only 2 re-initialize cycles in a row before giving up and exiting. Signed-off-by: Len Brown <len.brown@intel.com>
| * | tools/power/x86/turbostat: share kernel MSR #definesLen Brown2012-11-232-19/+8
| | | | | | | | | | | | | | | | | | | | | | | | Now that turbostat is built in the kernel tree, it can share MSR #defines with the kernel. Signed-off-by: Len Brown <len.brown@intel.com> Cc: x86@kernel.org
* | | tools/testing/selftests/kcmp/kcmp_test.c: print reason for failure in kcmp_testDave Jones2012-12-171-2/+4
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | I was curious why sys_kcmp wasn't working, which led me to the testcase. It turned out I hadn't enabled CHECKPOINT_RESTORE in the kernel I was testing. Add a decoding of errno to the testcase to make that obvious. Signed-off-by: Dave Jones <davej@redhat.com> Acked-by: Cyrill Gorcunov <gorcunov@openvz.org> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* | | breakpoint selftests: print failure status instead of cause make errorDave Young2012-12-171-1/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | In case breakpoint test exit non zero value it will cause make error. Better way is just print the test failure status. Signed-off-by: Dave Young <dyoung@redhat.com> Reviewed-by: Pekka Enberg <penberg@kernel.org> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* | | kcmp selftests: print fail status instead of cause make errorDave Young2012-12-171-1/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | In case kcmp_test exit non zero value it will cause make error. Better way is just print the test failure status. Signed-off-by: Dave Young <dyoung@redhat.com> Reviewed-by: Pekka Enberg <penberg@kernel.org> Cc: Cyrill Gorcunov <gorcunov@openvz.org> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* | | kcmp selftests: make run_tests fixDave Young2012-12-171-2/+2
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | make run_tests need the target is run_tests instead of run-tests Also gcc output should be kcmp_test. Fix these two issues. Signed-off-by: Dave Young <dyoung@redhat.com> Cc: Pekka Enberg <penberg@kernel.org> Cc: Cyrill Gorcunov <gorcunov@openvz.org> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* | | mem-hotplug selftests: print failure status instead of cause make errorDave Young2012-12-171-1/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Original behavior: bash-4.1$ make -C memory-hotplug run_tests make: Entering directory `/home/dave/git/linux-2.6/tools/testing/selftests/memory-hotplug' ./on-off-test.sh make: execvp: ./on-off-test.sh: Permission denied make: *** [run_tests] Error 127 make: Leaving directory `/home/dave/git/linux-2.6/tools/testing/selftests/memory-hotplug' After applying the patch: bash-4.1$ make -C memory-hotplug run_tests make: Entering directory `/home/dave/git/linux-2.6/tools/testing/selftests/memory-hotplug' /bin/sh: ./on-off-test.sh: Permission denied memory-hotplug selftests: [FAIL] make: Leaving directory `/home/dave/git/linux-2.6/tools/testing/selftests/memory-hotplug' Signed-off-by: Dave Young <dyoung@redhat.com> Reviewed-by: Pekka Enberg <penberg@kernel.org> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* | | cpu-hotplug selftests: print failure status instead of cause make errorDave Young2012-12-171-1/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Original behavior: bash-4.1$ make -C cpu-hotplug run_tests make: Entering directory `/home/dave/git/linux-2.6/tools/testing/selftests/cpu-hotplug' ./on-off-test.sh make: execvp: ./on-off-test.sh: Permission denied make: *** [run_tests] Error 127 make: Leaving directory `/home/dave/git/linux-2.6/tools/testing/selftests/cpu-hotplug' After applying the patch: bash-4.1$ make -C cpu-hotplug run_tests make: Entering directory `/home/dave/git/linux-2.6/tools/testing/selftests/cpu-hotplug' /bin/sh: ./on-off-test.sh: Permission denied cpu-hotplug selftests: [FAIL] make: Leaving directory `/home/dave/git/linux-2.6/tools/testing/selftests/cpu-hotplug' Signed-off-by: Dave Young <dyoung@redhat.com> Reviewed-by: Pekka Enberg <penberg@kernel.org> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* | | mqueue selftests: print failure status instead of cause make errorDave Young2012-12-171-2/+2
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Original behavior: bash-4.1$ make -C mqueue run_tests make: Entering directory `/home/dave/git/linux-2.6/tools/testing/selftests/mqueue' ./mq_open_tests /test1 Not running as root, but almost all tests require root in order to modify system settings. Exiting. make: *** [run_tests] Error 1 make: Leaving directory `/home/dave/git/linux-2.6/tools/testing/selftests/mqueue' After applying the patch: bash-4.1$ make -C mqueue run_tests make: Entering directory `/home/dave/git/linux-2.6/tools/testing/selftests/mqueue' Not running as root, but almost all tests require root in order to modify system settings. Exiting. mq_open_tests: [FAIL] Not running as root, but almost all tests require root in order to modify system settings. Exiting. mq_perf_tests: [FAIL] make: Leaving directory `/home/dave/git/linux-2.6/tools/testing/selftests/mqueue' Signed-off-by: Dave Young <dyoung@redhat.com> Reviewed-by: Pekka Enberg <penberg@kernel.org> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* | | vm selftests: print failure status instead of cause make errorDave Young2012-12-171-1/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Original behavior: bash-4.1$ make -C vm run_tests make: Entering directory `/home/dave/git/linux-2.6/tools/testing/selftests/vm' /bin/sh ./run_vmtests ./run_vmtests: line 24: /proc/sys/vm/nr_hugepages: Permission denied Please run this test as root make: *** [run_tests] Error 1 make: Leaving directory `/home/dave/git/linux-2.6/tools/testing/selftests/vm' After applying the patch: bash-4.1$ make -C vm run_tests make: Entering directory `/home/dave/git/linux-2.6/tools/testing/selftests/vm' ./run_vmtests: line 24: /proc/sys/vm/nr_hugepages: Permission denied Please run this test as root vmtests: [FAIL] make: Leaving directory `/home/dave/git/linux-2.6/tools/testing/selftests/vm' Signed-off-by: Dave Young <dyoung@redhat.com> Cc: Pekka Enberg <penberg@kernel.org> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* | | Merge tag 'ktest-v3.8' of ↵Linus Torvalds2012-12-132-8/+158
|\ \ \ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/rostedt/linux-ktest Pull ktest update from Steven Rostedt: "fixes and updated for new boot loaders" * tag 'ktest-v3.8' of git://git.kernel.org/pub/scm/linux/kernel/git/rostedt/linux-ktest: ktest: Test if target machine is up before install ktest: Fix breakage from change of oldnoconfig to olddefconfig ktest: Add native support for syslinux boot loader ktest: Sync before reboot ktest: Add support for grub2
| * | | ktest: Test if target machine is up before installSteven Rostedt2012-12-111-0/+10
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Sometimes a test kernel will crash or hang on reboot (this is even more apparent when testing a config without CGROUPS on a box running systemd). When this happens, on the next iteration of installing a kernel, ktest will fail when it tries to install. Have ktest do a check to see if the target can be connected to via ssh before it tries to install. If it can't connect, then reboot again. This time the reboot will fail because it can't connect and will force a power cycle. Signed-off-by: Steven Rostedt <rostedt@goodmis.org>
| * | | ktest: Fix breakage from change of oldnoconfig to olddefconfigSteven Rostedt2012-12-111-4/+8
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Commit fb16d891 "kconfig: replace 'oldnoconfig' with 'olddefconfig', and keep the old name", changed ktest's default config update from oldnoconfig to olddefconfig without adding oldnoconfig as a backup. The make oldnoconfig works much better than its backup of: yes '' | make oldconfig But due to this change, and the fact that ktest is used to build lots of older kernels (and for bisects), it forgoes the oldnoconfig completely. Cc: Adam Lee <adam8157@gmail.com> Cc: Michal Marek <mmarek@suse.cz> Signed-off-by: Steven Rostedt <rostedt@goodmis.org>
| * | | ktest: Add native support for syslinux boot loaderSteven Rostedt2012-12-112-2/+48
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | I installed Fedora 17 which no longer supports grub v1. I worked with grub2 for a while, but there's so many issues with it and automated rebooting, that I decided to switch to syslinux. Instead of using the REBOOT_SCRIPT and add customized changes to get syslinux booted, I thought it better to make ktest aware of syslinux and add options to simplify the use of syslinux on a target test box. Acked-by: H. Peter Anvin <hpa@zytor.com> Cc: John 'Warthog9' Hawley <warthog9@kernel.org> Signed-off-by: Steven Rostedt <rostedt@goodmis.org>
| * | | ktest: Sync before rebootSteven Rostedt2012-12-111-0/+3
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Before rebooting the target, run the sync command, as it seems that either Grub2 or systemd gets screwed up if you update to reboot a kernel once and do a reboot without doing a sync. Signed-off-by: Steven Rostedt <rostedt@goodmis.org>
| * | | ktest: Add support for grub2Steven Rostedt2012-11-132-4/+91
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | As only grub or 'script' is supported for rebooting to a new kernel, and Fedora 17 has dropped support for grub, I decided to add grub2 support as well (I also plan on adding syslinux/extlinux support too). The options GRUB_FILE and GRUB_REBOOT were added to allow the user to specify where to find the grub.cfg and what tool to use to reboot into the next kernel respectively. Signed-off-by: Steven Rostedt <rostedt@goodmis.org>
* | | | Merge branch 'for-linus' of ↵Linus Torvalds2012-12-131-1/+1
|\ \ \ \ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/jikos/trivial Pull trivial branch from Jiri Kosina: "Usual stuff -- comment/printk typo fixes, documentation updates, dead code elimination." * 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/jikos/trivial: (39 commits) HOWTO: fix double words typo x86 mtrr: fix comment typo in mtrr_bp_init propagate name change to comments in kernel source doc: Update the name of profiling based on sysfs treewide: Fix typos in various drivers treewide: Fix typos in various Kconfig wireless: mwifiex: Fix typo in wireless/mwifiex driver messages: i2o: Fix typo in messages/i2o scripts/kernel-doc: check that non-void fcts describe their return value Kernel-doc: Convention: Use a "Return" section to describe return values radeon: Fix typo and copy/paste error in comments doc: Remove unnecessary declarations from Documentation/accounting/getdelays.c various: Fix spelling of "asynchronous" in comments. Fix misspellings of "whether" in comments. eisa: Fix spelling of "asynchronous". various: Fix spelling of "registered" in comments. doc: fix quite a few typos within Documentation target: iscsi: fix comment typos in target/iscsi drivers treewide: fix typo of "suport" in various comments and Kconfig treewide: fix typo of "suppport" in various comments ...
| * | | | treewide: Fix typos in various driversMasanari Iida2012-12-031-1/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Fix typos in printk within various drivers. Signed-off-by: Masanari Iida <standby24x7@gmail.com> Signed-off-by: Jiri Kosina <jkosina@suse.cz>
* | | | | Merge tag 'firewire-updates' of ↵Linus Torvalds2012-12-131-0/+4
|\ \ \ \ \ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/ieee1394/linux1394 Pull IEEE 1394 (FireWire) subsystem updates from Stefan Richter: - IPv4-over-1394: fixes for broadcast and multicast - SBP-2: allow thin-provisioning related commands - trivia * tag 'firewire-updates' of git://git.kernel.org/pub/scm/linux/kernel/git/ieee1394/linux1394: firewire: net: remove unused variable in fwnet_receive_broadcast() firewire: net: Fix handling of fragmented multicast/broadcast packets. firewire: sbp2: allow WRITE SAME and REPORT SUPPORTED OPERATION CODES tools/firewire: nosy-dump: check for allocation failure
| * | | | | tools/firewire: nosy-dump: check for allocation failureStefan Richter2012-12-021-0/+4
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Behavior of null pointer dereference is undefined in the C language. Portably implement the desired behavior. Reported-by: Yang Yeping <yangyeping_666@hotmail.com> Signed-off-by: Stefan Richter <stefanr@s5r6.in-berlin.de>
* | | | | | Merge git://git.kernel.org/pub/scm/linux/kernel/git/davem/net-nextLinus Torvalds2012-12-121-1/+1
|\ \ \ \ \ \ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Pull networking changes from David Miller: 1) Allow to dump, monitor, and change the bridge multicast database using netlink. From Cong Wang. 2) RFC 5961 TCP blind data injection attack mitigation, from Eric Dumazet. 3) Networking user namespace support from Eric W. Biederman. 4) tuntap/virtio-net multiqueue support by Jason Wang. 5) Support for checksum offload of encapsulated packets (basically, tunneled traffic can still be checksummed by HW). From Joseph Gasparakis. 6) Allow BPF filter access to VLAN tags, from Eric Dumazet and Daniel Borkmann. 7) Bridge port parameters over netlink and BPDU blocking support from Stephen Hemminger. 8) Improve data access patterns during inet socket demux by rearranging socket layout, from Eric Dumazet. 9) TIPC protocol updates and cleanups from Ying Xue, Paul Gortmaker, and Jon Maloy. 10) Update TCP socket hash sizing to be more in line with current day realities. The existing heurstics were choosen a decade ago. From Eric Dumazet. 11) Fix races, queue bloat, and excessive wakeups in ATM and associated drivers, from Krzysztof Mazur and David Woodhouse. 12) Support DOVE (Distributed Overlay Virtual Ethernet) extensions in VXLAN driver, from David Stevens. 13) Add "oops_only" mode to netconsole, from Amerigo Wang. 14) Support set and query of VEB/VEPA bridge mode via PF_BRIDGE, also allow DCB netlink to work on namespaces other than the initial namespace. From John Fastabend. 15) Support PTP in the Tigon3 driver, from Matt Carlson. 16) tun/vhost zero copy fixes and improvements, plus turn it on by default, from Michael S. Tsirkin. 17) Support per-association statistics in SCTP, from Michele Baldessari. And many, many, driver updates, cleanups, and improvements. Too numerous to mention individually. * git://git.kernel.org/pub/scm/linux/kernel/git/davem/net-next: (1722 commits) net/mlx4_en: Add support for destination MAC in steering rules net/mlx4_en: Use generic etherdevice.h functions. net: ethtool: Add destination MAC address to flow steering API bridge: add support of adding and deleting mdb entries bridge: notify mdb changes via netlink ndisc: Unexport ndisc_{build,send}_skb(). uapi: add missing netconf.h to export list pkt_sched: avoid requeues if possible solos-pci: fix double-free of TX skb in DMA mode bnx2: Fix accidental reversions. bna: Driver Version Updated to 3.1.2.1 bna: Firmware update bna: Add RX State bna: Rx Page Based Allocation bna: TX Intr Coalescing Fix bna: Tx and Rx Optimizations bna: Code Cleanup and Enhancements ath9k: check pdata variable before dereferencing it ath5k: RX timestamp is reported at end of frame ath9k_htc: RX timestamp is reported at end of frame ...
| * | | | | | tools:virtio: fix compilation warningCong Ding2012-12-061-1/+1
| |/ / / / / | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | We do not allow old-style function definition. Always spell foo(void) if a function does not take any parameters. Signed-off-by: Cong Ding <dinggnu@gmail.com> Signed-off-by: Michael S. Tsirkin <mst@redhat.com>
* | | | | | Merge branch 'perf-core-for-linus' of ↵Linus Torvalds2012-12-11141-3599/+7570
|\ \ \ \ \ \ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/tip/tip Pull perf updates from Ingo Molnar: "Lots of activity: 211 files changed, 8328 insertions(+), 4116 deletions(-) most of it on the tooling side. Main changes: * ftrace enhancements and fixes from Steve Rostedt. * uprobes fixes, cleanups and preparation for the ARM port from Oleg Nesterov. * UAPI fixes, from David Howels - prepares the arch/x86 UAPI transition * Separate perf tests into multiple objects, one per test, from Jiri Olsa. * Make hardware event translations available in sysfs, from Jiri Olsa. * Fixes to /proc/pid/maps parsing, preparatory to supporting data maps, from Namhyung Kim * Implement ui_progress for GTK, from Namhyung Kim * Add framework for automated perf_event_attr tests, where tools with different command line options will be run from a 'perf test', via python glue, and the perf syscall will be intercepted to verify that the perf_event_attr fields set by the tool are those expected, from Jiri Olsa * Add a 'link' method for hists, so that we can have the leader with buckets for all the entries in all the hists. This new method is now used in the default 'diff' output, making the sum of the 'baseline' column be 100%, eliminating blind spots. * libtraceevent fixes for compiler warnings trying to make perf it build on some distros, like fedora 14, 32-bit, some of the warnings really pointed to real bugs. * Add a browser for 'perf script' and make it available from the report and annotate browsers. It does filtering to find the scripts that handle events found in the perf.data file used. From Feng Tang * perf inject changes to allow showing where a task sleeps, from Andrew Vagin. * Makefile improvements from Namhyung Kim. * Add --pre and --post command hooks in 'stat', from Peter Zijlstra. * Don't stop synthesizing threads when one vanishes, this is for the existing threads when we start a tool like trace. * Use sched:sched_stat_runtime to provide a thread summary, this produces the same output as the 'trace summary' subcommand of tglx's original "trace" tool. * Support interrupted syscalls in 'trace' * Add an event duration column and filter in 'trace'. * There are references to the man pages in some tools, so try to build Documentation when installing, warning the user if that is not possible, from Borislav Petkov. * Give user better message if precise is not supported, from David Ahern. * Try to find cross-built objdump path by using the session environment information in the perf.data file header, from Irina Tirdea, original patch and idea by Namhyung Kim. * Diplays more output on features check for make V=1, so that one can figure out what is happening by looking at gcc output, etc. From Jiri Olsa. * Add on_exit implementation for systems without one, e.g. Android, from Bernhard Rosenkraenzer. * Only process events for vcpus of interest, helps handling large number of events, from David Ahern. * Cross compilation fixes for Android, from Irina Tirdea. * Add documentation on compiling for Android, from Irina Tirdea. * perf diff improvements from Jiri Olsa. * Target (task/user/cpu/syswide) handling improvements, from Namhyung Kim. * Add support in 'trace' for tracing workload given by command line, from Namhyung Kim. * ... and much more." * 'perf-core-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/tip/tip: (194 commits) uprobes: Use percpu_rw_semaphore to fix register/unregister vs dup_mmap() race perf evsel: Introduce is_group_member method perf powerpc: Use uapi/unistd.h to fix build error tools: Pass the target in descend tools: Honour the O= flag when tool build called from a higher Makefile tools: Define a Makefile function to do subdir processing perf ui: Always compile browser setup code perf ui: Add ui_progress__finish() perf ui gtk: Implement ui_progress functions perf ui: Introduce generic ui_progress helper perf ui tui: Move progress.c under ui/tui directory perf tools: Add basic event modifier sanity check perf tools: Omit group members from perf_evlist__disable/enable perf tools: Ensure single disable call per event in record comand perf tools: Fix 'disabled' attribute config for record command perf tools: Fix attributes for '{}' defined event groups perf tools: Use sscanf for parsing /proc/pid/maps perf tools: Add gtk.<command> config option for launching GTK browser perf tools: Fix compile error on NO_NEWT=1 build perf hists: Initialize all of he->stat with zeroes ...
| * \ \ \ \ \ Merge branch 'linus' into perf/coreIngo Molnar2012-12-0820-449/+140
| |\ \ \ \ \ \ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Conflicts: tools/perf/Makefile tools/perf/builtin-test.c tools/perf/perf.h tools/perf/tests/parse-events.c tools/perf/util/evsel.h Signed-off-by: Ingo Molnar <mingo@kernel.org>
| * | | | | | | perf evsel: Introduce is_group_member methodArnaldo Carvalho de Melo2012-11-145-16/+23
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | To clarify what is being tested, instead of assuming that evsel->leader == NULL means either an 'isolated' evsel or a 'group leader'. Cc: David Ahern <dsahern@gmail.com> Cc: Frederic Weisbecker <fweisbec@gmail.com> Cc: Jiri Olsa <jolsa@redhat.com> Cc: Mike Galbraith <efault@gmx.de> Cc: Namhyung Kim <namhyung@gmail.com> Cc: Paul Mackerras <paulus@samba.org> Cc: Peter Zijlstra <peterz@infradead.org> Cc: Stephane Eranian <eranian@google.com> Link: http://lkml.kernel.org/n/tip-lvdbvimaxw9nc5een5vmem0c@git.kernel.org Signed-off-by: Arnaldo Carvalho de Melo <acme@redhat.com>
| * | | | | | | perf powerpc: Use uapi/unistd.h to fix build errorSukadev Bhattiprolu2012-11-141-1/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Use the 'unistd.h' from arch/powerpc/include/uapi to build the perf tool. Signed-off-by: Sukadev Bhattiprolu <sukadev@linux.vnet.ibm.com> Acked-by: David Howells <dhowells@redhat.com> Cc: Anton Blanchard <anton@au1.ibm.com> Cc: Ingo Molnar <mingo@redhat.com> Cc: Paul Mackerras <paulus@samba.org> Cc: Peter Zijlstra <a.p.zijlstra@chello.nl> Cc: Robert Richter <robert.richter@amd.com> Cc: linuxppc-dev@ozlabs.org Link: http://lkml.kernel.org/r/20121107191818.GA16211@us.ibm.com Signed-off-by: Arnaldo Carvalho de Melo <acme@redhat.com>
| * | | | | | | tools: Pass the target in descendDavid Howells2012-11-141-2/+2
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Fixing: [acme@sandy linux]$ cd tools [acme@sandy tools]$ make clean DESCEND power/cpupower CC lib/cpufreq.o CC lib/sysfs.o LD libcpupower.so.0.0.0 CC utils/helpers/amd.o utils/helpers/amd.c:7:21: error: pci/pci.h: No such file or directory In file included from utils/helpers/amd.c:9: ./utils/helpers/helpers.h:137: warning: ‘struct pci_access’ declared inside parameter list ./utils/helpers/helpers.h:137: warning: its scope is only this definition or declaration, which is probably not what you want ./utils/helpers/helpers.h:139: warning: ‘struct pci_access’ declared inside parameter list utils/helpers/amd.c: In function ‘amd_pci_get_num_boost_states’: utils/helpers/amd.c:120: warning: passing argument 1 of ‘pci_slot_func_init’ from incompatible pointer type ./utils/helpers/helpers.h:138: note: expected ‘struct pci_access **’ but argument is of type ‘struct pci_access **’ utils/helpers/amd.c:125: warning: implicit declaration of function ‘pci_read_byte’ utils/helpers/amd.c:132: warning: implicit declaration of function ‘pci_cleanup’ make[1]: *** [utils/helpers/amd.o] Error 1 make: *** [cpupower_clean] Error 2 [acme@sandy tools]$ Reported-by: Arnaldo Carvalho de Melo <acme@ghostprotocols.net> Signed-off-by: David Howells <dhowells@redhat.com> Cc: Borislav Petkov <bp@amd64.org> Cc: Ingo Molnar <mingo@kernel.org> Cc: Linus Torvalds <torvalds@linux-foundation.org> Cc: Namhyung Kim <namhyung@gmail.com> Cc: Paul Mackerras <paulus@samba.org> Cc: Thomas Gleixner <tglx@linutronix.de> Link: http://lkml.kernel.org/n/tip-tviyimq6x6nm77sj5lt4t19f@git.kernel.org Signed-off-by: Arnaldo Carvalho de Melo <acme@redhat.com>
| * | | | | | | tools: Honour the O= flag when tool build called from a higher MakefileDavid Howells2012-11-141-4/+13
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Honour the O= flag that was passed to a higher level Makefile and then passed down as part of a tool build. To make this work, the top-level Makefile passes the original O= flag and subdir=tools to the tools/Makefile, and that in turn passes subdir=$(O)/$(subdir)/foodir when building tool foo in directory $(O)/$(subdir)/foodir (where the intervening slashes aren't added if an element is missing). For example, take perf. This is found in tools/perf/. Assume we're building into directory ~/zebra/, so we pass O=~/zebra to make. Dependening on where we run the build from, we see: make run in dir $(OUTPUT) dir ======================= ================== linux ~/zebra/tools/perf/ linux/tools ~/zebra/perf/ linux/tools/perf ~/zebra/ and if O= is not set, we get: make run in dir $(OUTPUT) dir ======================= ================== linux linux/tools/perf/ linux/tools linux/tools/perf/ linux/tools/perf linux/tools/perf/ The output directories are created by the descend function if they don't already exist. Signed-off-by: David Howells <dhowells@redhat.com> Cc: Borislav Petkov <bp@amd64.org> Cc: Ingo Molnar <mingo@kernel.org> Cc: Linus Torvalds <torvalds@linux-foundation.org> Cc: Namhyung Kim <namhyung@gmail.com> Cc: Paul Mackerras <paulus@samba.org> Cc: Thomas Gleixner <tglx@linutronix.de> Link: http://lkml.kernel.org/r/1378.1352379110@warthog.procyon.org.uk Signed-off-by: Arnaldo Carvalho de Melo <acme@redhat.com>
| * | | | | | | tools: Define a Makefile function to do subdir processingDavid Howells2012-11-142-12/+20
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Define a Makefile function that can be called with $(call ...) to wrap the subdir make invocations in tools/Makefile. This will allow us in the next patch to insert bits in there to honour O= flags when called from the top-level Makefile. Signed-off-by: David Howells <dhowells@redhat.com> Cc: Borislav Petkov <bp@amd64.org> Cc: Ingo Molnar <mingo@kernel.org> Cc: Linus Torvalds <torvalds@linux-foundation.org> Cc: Namhyung Kim <namhyung@gmail.com> Cc: Paul Mackerras <paulus@samba.org> Cc: Thomas Gleixner <tglx@linutronix.de> Link: http://lkml.kernel.org/r/1378.1352379110@warthog.procyon.org.uk Signed-off-by: Arnaldo Carvalho de Melo <acme@redhat.com>
| * | | | | | | perf ui: Always compile browser setup codeNamhyung Kim2012-11-143-40/+30
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | We now have proper fallback logic, so always build it regardless of TUI or GTK setting. Signed-off-by: Namhyung Kim <namhyung@kernel.org> Cc: Ingo Molnar <mingo@kernel.org> Cc: Pekka Enberg <penberg@kernel.org> Cc: Peter Zijlstra <peterz@infradead.org> Link: http://lkml.kernel.org/r/1352813436-14173-5-git-send-email-namhyung@kernel.org Signed-off-by: Arnaldo Carvalho de Melo <acme@redhat.com>
| * | | | | | | perf ui: Add ui_progress__finish()Namhyung Kim2012-11-145-0/+19
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Sometimes we need to know when the progress bar should disappear. Checking curr >= total wasn't enough since there're cases not met that condition for the last call. So add a new ->finish callback to identify this explicitly. Currently only GTK frontend needs it. Signed-off-by: Namhyung Kim <namhyung@kernel.org> Cc: Ingo Molnar <mingo@kernel.org> Cc: Pekka Enberg <penberg@kernel.org> Cc: Peter Zijlstra <peterz@infradead.org> Link: http://lkml.kernel.org/r/1352813436-14173-4-git-send-email-namhyung@kernel.org Signed-off-by: Arnaldo Carvalho de Melo <acme@redhat.com>
| * | | | | | | perf ui gtk: Implement ui_progress functionsNamhyung Kim2012-11-144-0/+54
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Implement progress update function for GTK2 front end. Note that since it will be called before gtk main loop so that we should call gtk event loop handler directly. Signed-off-by: Namhyung Kim <namhyung@kernel.org> Cc: Ingo Molnar <mingo@kernel.org> Cc: Pekka Enberg <penberg@kernel.org> Cc: Peter Zijlstra <peterz@infradead.org> Link: http://lkml.kernel.org/r/1352813436-14173-3-git-send-email-namhyung@kernel.org Signed-off-by: Arnaldo Carvalho de Melo <acme@redhat.com>
| * | | | | | | perf ui: Introduce generic ui_progress helperNamhyung Kim2012-11-146-12/+41
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Make ui_progress functions generic so that UI frontend code will add its callbacks. Signed-off-by: Namhyung Kim <namhyung@kernel.org> Cc: Ingo Molnar <mingo@kernel.org> Cc: Pekka Enberg <penberg@kernel.org> Cc: Peter Zijlstra <peterz@infradead.org> Link: http://lkml.kernel.org/r/1352813436-14173-2-git-send-email-namhyung@kernel.org Signed-off-by: Arnaldo Carvalho de Melo <acme@redhat.com>