From 4e53f78e5b06c073a5c10814c72e98c1ca8a9f10 Mon Sep 17 00:00:00 2001 From: Michael S. Tsirkin Date: Mon, 29 Nov 2010 19:16:37 +0200 Subject: tools/virtio: virtio_test tool This is the userspace part of the tool: it includes a bunch of stubs for linux APIs, somewhat simular to linuxsched. This makes it possible to recompile the ring code in userspace. A small test example is implemented combining this with vhost_test module. Signed-off-by: Michael S. Tsirkin --- tools/virtio/linux/virtio.h | 223 ++++++++++++++++++++++++++++++++++++++++++++ 1 file changed, 223 insertions(+) create mode 100644 tools/virtio/linux/virtio.h (limited to 'tools/virtio/linux/virtio.h') diff --git a/tools/virtio/linux/virtio.h b/tools/virtio/linux/virtio.h new file mode 100644 index 000000000000..669bcdd45805 --- /dev/null +++ b/tools/virtio/linux/virtio.h @@ -0,0 +1,223 @@ +#ifndef LINUX_VIRTIO_H +#define LINUX_VIRTIO_H + +#include +#include +#include +#include +#include +#include + +#include +#include + +typedef unsigned long long dma_addr_t; + +struct scatterlist { + unsigned long page_link; + unsigned int offset; + unsigned int length; + dma_addr_t dma_address; +}; + +struct page { + unsigned long long dummy; +}; + +#define BUG_ON(__BUG_ON_cond) assert(!(__BUG_ON_cond)) + +/* Physical == Virtual */ +#define virt_to_phys(p) ((unsigned long)p) +#define phys_to_virt(a) ((void *)(unsigned long)(a)) +/* Page address: Virtual / 4K */ +#define virt_to_page(p) ((struct page*)((virt_to_phys(p) / 4096) * \ + sizeof(struct page))) +#define offset_in_page(p) (((unsigned long)p) % 4096) +#define sg_phys(sg) ((sg->page_link & ~0x3) / sizeof(struct page) * 4096 + \ + sg->offset) +static inline void sg_mark_end(struct scatterlist *sg) +{ + /* + * Set termination bit, clear potential chain bit + */ + sg->page_link |= 0x02; + sg->page_link &= ~0x01; +} +static inline void sg_init_table(struct scatterlist *sgl, unsigned int nents) +{ + memset(sgl, 0, sizeof(*sgl) * nents); + sg_mark_end(&sgl[nents - 1]); +} +static inline void sg_assign_page(struct scatterlist *sg, struct page *page) +{ + unsigned long page_link = sg->page_link & 0x3; + + /* + * In order for the low bit stealing approach to work, pages + * must be aligned at a 32-bit boundary as a minimum. + */ + BUG_ON((unsigned long) page & 0x03); + sg->page_link = page_link | (unsigned long) page; +} + +static inline void sg_set_page(struct scatterlist *sg, struct page *page, + unsigned int len, unsigned int offset) +{ + sg_assign_page(sg, page); + sg->offset = offset; + sg->length = len; +} + +static inline void sg_set_buf(struct scatterlist *sg, const void *buf, + unsigned int buflen) +{ + sg_set_page(sg, virt_to_page(buf), buflen, offset_in_page(buf)); +} + +static inline void sg_init_one(struct scatterlist *sg, const void *buf, unsigned int buflen) +{ + sg_init_table(sg, 1); + sg_set_buf(sg, buf, buflen); +} + +typedef __u16 u16; + +typedef enum { + GFP_KERNEL, + GFP_ATOMIC, +} gfp_t; +typedef enum { + IRQ_NONE, + IRQ_HANDLED +} irqreturn_t; + +static inline void *kmalloc(size_t s, gfp_t gfp) +{ + return malloc(s); +} + +static inline void kfree(void *p) +{ + free(p); +} + +#define container_of(ptr, type, member) ({ \ + const typeof( ((type *)0)->member ) *__mptr = (ptr); \ + (type *)( (char *)__mptr - offsetof(type,member) );}) + +#define uninitialized_var(x) x = x + +# ifndef likely +# define likely(x) (__builtin_expect(!!(x), 1)) +# endif +# ifndef unlikely +# define unlikely(x) (__builtin_expect(!!(x), 0)) +# endif + +#define pr_err(format, ...) fprintf (stderr, format, ## __VA_ARGS__) +#ifdef DEBUG +#define pr_debug(format, ...) fprintf (stderr, format, ## __VA_ARGS__) +#else +#define pr_debug(format, ...) do {} while (0) +#endif +#define dev_err(dev, format, ...) fprintf (stderr, format, ## __VA_ARGS__) +#define dev_warn(dev, format, ...) fprintf (stderr, format, ## __VA_ARGS__) + +/* TODO: empty stubs for now. Broken but enough for virtio_ring.c */ +#define list_add_tail(a, b) do {} while (0) +#define list_del(a) do {} while (0) + +#define BIT_WORD(nr) ((nr) / BITS_PER_LONG) +#define BITS_PER_BYTE 8 +#define BITS_PER_LONG (sizeof(long) * BITS_PER_BYTE) +#define BIT_MASK(nr) (1UL << ((nr) % BITS_PER_LONG)) +/* TODO: Not atomic as it should be: + * we don't use this for anything important. */ +static inline void clear_bit(int nr, volatile unsigned long *addr) +{ + unsigned long mask = BIT_MASK(nr); + unsigned long *p = ((unsigned long *)addr) + BIT_WORD(nr); + + *p &= ~mask; +} + +static inline int test_bit(int nr, const volatile unsigned long *addr) +{ + return 1UL & (addr[BIT_WORD(nr)] >> (nr & (BITS_PER_LONG-1))); +} + +/* The only feature we care to support */ +#define virtio_has_feature(dev, feature) \ + test_bit((feature), (dev)->features) +/* end of stubs */ + +struct virtio_device { + void *dev; + unsigned long features[1]; +}; + +struct virtqueue { + /* TODO: commented as list macros are empty stubs for now. + * Broken but enough for virtio_ring.c + * struct list_head list; */ + void (*callback)(struct virtqueue *vq); + const char *name; + struct virtio_device *vdev; + void *priv; +}; + +#define EXPORT_SYMBOL_GPL(__EXPORT_SYMBOL_GPL_name) \ + void __EXPORT_SYMBOL_GPL##__EXPORT_SYMBOL_GPL_name() { \ +} +#define MODULE_LICENSE(__MODULE_LICENSE_value) \ + const char *__MODULE_LICENSE_name = __MODULE_LICENSE_value + +#define CONFIG_SMP + +#if defined(__i386__) || defined(__x86_64__) +#define barrier() asm volatile("" ::: "memory") +#define mb() __sync_synchronize() + +#define smp_mb() mb() +# define smp_rmb() barrier() +# define smp_wmb() barrier() +#else +#error Please fill in barrier macros +#endif + +/* Interfaces exported by virtio_ring. */ +int virtqueue_add_buf_gfp(struct virtqueue *vq, + struct scatterlist sg[], + unsigned int out_num, + unsigned int in_num, + void *data, + gfp_t gfp); + +static inline int virtqueue_add_buf(struct virtqueue *vq, + struct scatterlist sg[], + unsigned int out_num, + unsigned int in_num, + void *data) +{ + return virtqueue_add_buf_gfp(vq, sg, out_num, in_num, data, GFP_ATOMIC); +} + +void virtqueue_kick(struct virtqueue *vq); + +void *virtqueue_get_buf(struct virtqueue *vq, unsigned int *len); + +void virtqueue_disable_cb(struct virtqueue *vq); + +bool virtqueue_enable_cb(struct virtqueue *vq); + +void *virtqueue_detach_unused_buf(struct virtqueue *vq); +struct virtqueue *vring_new_virtqueue(unsigned int num, + unsigned int vring_align, + struct virtio_device *vdev, + void *pages, + void (*notify)(struct virtqueue *vq), + void (*callback)(struct virtqueue *vq), + const char *name); +void vring_del_virtqueue(struct virtqueue *vq); + +#endif -- cgit v1.2.3-54-g00ecf