# =========================================================================== # Module versions # =========================================================================== # # Stage one of module building created the following: # a) The individual .o files used for the module # b) A .o file which is the .o files above linked together # c) A .mod file in $(MODVERDIR)/, listing the name of the # the preliminary .o file, plus all .o files # Stage 2 is handled by this file and does the following # 1) Find all modules from the files listed in $(MODVERDIR)/ # 2) modpost is then used to # 3) create one .mod.c file pr. module # 4) create one Module.symvers file with CRC for all exported symbols # 5) compile all .mod.c files # 6) final link of the module to a file # Step 3 is used to place certain information in the module's ELF # section, including information such as: # Version magic (see include/linux/vermagic.h for full details) # - Kernel release # - SMP is CONFIG_SMP # - PREEMPT is CONFIG_PREEMPT # - GCC Version # Module info # - Module version (MODULE_VERSION) # - Module alias'es (MODULE_ALIAS) # - Module license (MODULE_LICENSE) # - See include/linux/module.h for more details # Step 4 is solely used to allow module versioning in external modules, # where the CRC of each module is retrieved from the Module.symvers file. # KBUILD_MODPOST_WARN can be set to avoid error out in case of undefined # symbols in the final module linking stage # KBUILD_MODPOST_NOFINAL can be set to skip the final link of modules. # This is solely useful to speed up test compiles PHONY := _modpost _modpost: __modpost include include/config/auto.conf include scripts/Kbuild.include # When building external modules load the Kbuild file to retrieve EXTRA_SYMBOLS info ifneq ($(KBUILD_EXTMOD),) # set src + obj - they may be used when building the .mod.c file obj := $(KBUILD_EXTMOD) src := $(obj) # Include the module's Makefile to find KBUILD_EXTRA_SYMBOLS include $(if $(wildcard $(KBUILD_EXTMOD)/Kbuild), \ $(KBUILD_EXTMOD)/Kbuild, $(KBUILD_EXTMOD)/Makefile) endif include scripts/Makefile.lib kernelsymfile := $(objtree)/Module.symvers modulesymfile := $(firstword $(KBUILD_EXTMOD))/Module.symvers # Step 1), find all modules listed in $(MODVERDIR)/ __modules := $(sort $(shell grep -h '\.ko$$' /dev/null $(wildcard $(MODVERDIR)/*.mod))) modules := $(patsubst %.o,%.ko, $(wildcard $(__modules:.ko=.o))) # Stop after building .o files if NOFINAL is set. Makes compile tests quicker _modpost: $(if $(KBUILD_MODPOST_NOFINAL), $(modules:.ko:.o),$(modules)) ifneq ($(KBUILD_BUILDHOST),$(ARCH)) cross_build := 1 endif # Step 2), invoke modpost # Includes step 3,4 modpost = scripts/mod/modpost \ $(if $(CONFIG_MODVERSIONS),-m) \ $(if $(CONFIG_MODULE_SRCVERSION_ALL),-a,) \ $(if $(KBUILD_EXTMOD),-i,-o) $(kernelsymfile) \ $(if $(KBUILD_EXTMOD),-I $(modulesymfile)) \ $(if $(KBUILD_EXTRA_SYMBOLS), $(patsubst %, -e %,$(KBUILD_EXTRA_SYMBOLS))) \ $(if $(KBUILD_EXTMOD),-o $(modulesymfile)) \ $(if $(CONFIG_DEBUG_SECTION_MISMATCH),,-S) \ $(if $(KBUILD_EXTMOD)$(KBUILD_MODPOST_WARN),-w) \ $(if $(cross_build),-c) quiet_cmd_modpost = MODPOST $(words $(filter-out vmlinux FORCE, $^)) modules cmd_modpost = $(modpost) -s PHONY += __modpost __modpost: $(modules:.ko=.o) FORCE $(call cmd,modpost) $(wildcard vmlinux) $(filter-out FORCE,$^) quiet_cmd_kernel-mod = MODPOST $@ cmd_kernel-mod = $(modpost) $@ vmlinux.o: FORCE $(call cmd,kernel-mod) # Declare generated files as targets for modpost $(symverfile): __modpost ; $(modules:.ko=.mod.c): __modpost ; # Step 5), compile all *.mod.c files # modname is set to make c_flags define KBUILD_MODNAME modname = $(notdir $(@:.mod.o=)) quiet_cmd_cc_o_c = CC $@ cmd_cc_o_c = $(CC) $(c_flags) $(KBUILD_CFLAGS_MODULE) $(CFLAGS_MODULE) \ -c -o $@ $< $(modules:.ko=.mod.o): %.mod.o: %.mod.c FORCE $(call if_changed_dep,cc_o_c) targets += $(modules:.ko=.mod.o) # Step 6), final link of the modules quiet_cmd_ld_ko_o = LD [M] $@ cmd_ld_ko_o = $(LD) -r $(LDFLAGS) \ $(KBUILD_LDFLAGS_MODULE) $(LDFLAGS_MODULE) \ -o $@ $(filter-out FORCE,$^) $(modules): %.ko :%.o %.mod.o FORCE $(call if_changed,ld_ko_o) targets += $(modules) # Add FORCE to the prequisites of a target to force it to be always rebuilt. # --------------------------------------------------------------------------- PHONY += FORCE FORCE: # Read all saved command lines and dependencies for the $(targets) we # may be building above, using $(if_changed{,_dep}). As an # optimization, we don't need to read them if the target does not # exist, we will rebuild anyway in that case. targets := $(wildcard $(sort $(targets))) cmd_files := $(wildcard $(foreach f,$(targets),$(dir $(f)).$(notdir $(f)).cmd)) ifneq ($(cmd_files),) include $(cmd_files) endif # Declare the contents of the .PHONY variable as phony. We keep that # information in a variable se we can use it in if_changed and friends. .PHONY: $(PHONY)