/* * builtin-probe.c * * Builtin probe command: Set up probe events by C expression * * Written by Masami Hiramatsu * * This program is free software; you can redistribute it and/or modify * it under the terms of the GNU General Public License as published by * the Free Software Foundation; either version 2 of the License, or * (at your option) any later version. * * This program is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the * GNU General Public License for more details. * * You should have received a copy of the GNU General Public License * along with this program; if not, write to the Free Software * Foundation, Inc., 59 Temple Place - Suite 330, Boston, MA 02111-1307, USA. * */ #include #include #include #include #include #include #include #include #include #include "perf.h" #include "builtin.h" #include "util/util.h" #include "util/strlist.h" #include "util/strfilter.h" #include "util/symbol.h" #include "util/debug.h" #include "util/debugfs.h" #include "util/parse-options.h" #include "util/probe-finder.h" #include "util/probe-event.h" #define DEFAULT_VAR_FILTER "!__k???tab_* & !__crc_*" #define DEFAULT_FUNC_FILTER "!_*" /* Session management structure */ static struct { bool list_events; bool force_add; bool show_lines; bool show_vars; bool show_ext_vars; bool show_funcs; bool mod_events; bool uprobes; int nevents; struct perf_probe_event events[MAX_PROBES]; struct strlist *dellist; struct line_range line_range; const char *target; int max_probe_points; struct strfilter *filter; } params; /* Parse an event definition. Note that any error must die. */ static int parse_probe_event(const char *str) { struct perf_probe_event *pev = ¶ms.events[params.nevents]; int ret; pr_debug("probe-definition(%d): %s\n", params.nevents, str); if (++params.nevents == MAX_PROBES) { pr_err("Too many probes (> %d) were specified.", MAX_PROBES); return -1; } pev->uprobes = params.uprobes; /* Parse a perf-probe command into event */ ret = parse_perf_probe_command(str, pev); pr_debug("%d arguments\n", pev->nargs); return ret; } static int set_target(const char *ptr) { int found = 0; const char *buf; /* * The first argument after options can be an absolute path * to an executable / library or kernel module. * * TODO: Support relative path, and $PATH, $LD_LIBRARY_PATH, * short module name. */ if (!params.target && ptr && *ptr == '/') { params.target = ptr; found = 1; buf = ptr + (strlen(ptr) - 3); if (strcmp(buf, ".ko")) params.uprobes = true; } return found; } static int parse_probe_event_argv(int argc, const char **argv) { int i, len, ret, found_target; char *buf; found_target = set_target(argv[0]); if (found_target && argc == 1) return 0; /* Bind up rest arguments */ len = 0; for (i = 0; i < argc; i++) { if (i == 0 && found_target) continue; len += strlen(argv[i]) + 1; } buf = zalloc(len + 1); if (buf == NULL) return -ENOMEM; len = 0; for (i = 0; i < argc; i++) { if (i == 0 && found_target) continue; len += sprintf(&buf[len], "%s ", argv[i]); } params.mod_events = true; ret = parse_probe_event(buf); free(buf); return ret; } static int opt_add_probe_event(const struct option *opt __maybe_unused, const char *str, int unset __maybe_unused) { if (str) { params.mod_events = true; return parse_probe_event(str); } else return 0; } static int opt_del_probe_event(const struct option *opt __maybe_unused, const char *str, int unset __maybe_unused) { if (str) { params.mod_events = true; if (!params.dellist) params.dellist = strlist__new(true, NULL); strlist__add(params.dellist, str); } return 0; } static int opt_set_target(const struct option *opt, const char *str, int unset __maybe_unused) { int ret = -ENOENT; if (str && !params.target) { if (!strcmp(opt->long_name, "exec")) params.uprobes = true; #ifdef DWARF_SUPPORT else if (!strcmp(opt->long_name, "module")) params.uprobes = false; #endif else return ret; params.target = str; ret = 0; } return ret; } #ifdef DWARF_SUPPORT static int opt_show_lines(const struct option *opt __maybe_unused, const char *str, int unset __maybe_unused) { int ret = 0; if (!str) return 0; if (params.show_lines) { pr_warning("Warning: more than one --line options are" " detected. Only the first one is valid.\n"); return 0; } params.show_lines = true; ret = parse_line_range_desc(str, ¶ms.line_range); INIT_LIST_HEAD(¶ms.line_range.line_list); return ret; } static int opt_show_vars(const struct option *opt __maybe_unused, const char *str, int unset __maybe_unused) { struct perf_probe_event *pev = ¶ms.events[params.nevents]; int ret; if (!str) return 0; ret = parse_probe_event(str); if (!ret && pev->nargs != 0) { pr_err(" Error: '--vars' doesn't accept arguments.\n"); return -EINVAL; } params.show_vars = true; return ret; } #endif static int opt_set_filter(const struct option *opt __maybe_unused, const char *str, int unset __maybe_unused) { const char *err; if (str) { pr_debug2("Set filter: %s\n", str); if (params.filter) strfilter__delete(params.filter); params.filter = strfilter__new(str, &err); if (!params.filter) { pr_err("Filter parse error at %td.\n", err - str + 1); pr_err("Source: \"%s\"\n", str); pr_err(" %*c\n", (int)(err - str + 1), '^'); return -EINVAL; } } return 0; } int cmd_probe(int argc, const char **argv, const char *prefix __maybe_unused) { const char * const probe_usage[] = { "perf probe [] 'PROBEDEF' ['PROBEDEF' ...]", "perf probe [] --add 'PROBEDEF' [--add 'PROBEDEF' ...]", "perf probe [] --del '[GROUP:]EVENT' ...", "perf probe --list", #ifdef DWARF_SUPPORT "perf probe [] --line 'LINEDESC'", "perf probe [] --vars 'PROBEPOINT'", #endif NULL }; const struct option options[] = { OPT_INCR('v', "verbose", &verbose, "be more verbose (show parsed arguments, etc)"), OPT_BOOLEAN('l', "list", ¶ms.list_events, "list up current probe events"), OPT_CALLBACK('d', "del", NULL, "[GROUP:]EVENT", "delete a probe event.", opt_del_probe_event), OPT_CALLBACK('a', "add", NULL, #ifdef DWARF_SUPPORT "[EVENT=]FUNC[@SRC][+OFF|%return|:RL|;PT]|SRC:AL|SRC;PT" " [[NAME=]ARG ...]", #else "[EVENT=]FUNC[+OFF|%return] [[NAME=]ARG ...]", #endif "probe point definition, where\n" "\t\tGROUP:\tGroup name (optional)\n" "\t\tEVENT:\tEvent name\n" "\t\tFUNC:\tFunction name\n" "\t\tOFF:\tOffset from function entry (in byte)\n" "\t\t%return:\tPut the probe at function return\n" #ifdef DWARF_SUPPORT "\t\tSRC:\tSource code path\n" "\t\tRL:\tRelative line number from function entry.\n" "\t\tAL:\tAbsolute line number in file.\n" "\t\tPT:\tLazy expression of line code.\n" "\t\tARG:\tProbe argument (local variable name or\n" "\t\t\tkprobe-tracer argument format.)\n", #else "\t\tARG:\tProbe argument (kprobe-tracer argument format.)\n", #endif opt_add_probe_event), OPT_BOOLEAN('f', "force", ¶ms.force_add, "forcibly add events" " with existing name"), #ifdef DWARF_SUPPORT OPT_CALLBACK('L', "line", NULL, "FUNC[:RLN[+NUM|-RLN2]]|SRC:ALN[+NUM|-ALN2]", "Show source code lines.", opt_show_lines), OPT_CALLBACK('V', "vars", NULL, "FUNC[@SRC][+OFF|%return|:RL|;PT]|SRC:AL|SRC;PT", "Show accessible variables on PROBEDEF", opt_show_vars), OPT_BOOLEAN('\0', "externs", ¶ms.show_ext_vars, "Show external variables too (with --vars only)"), OPT_STRING('k', "vmlinux", &symbol_conf.vmlinux_name, "file", "vmlinux pathname"), OPT_STRING('s', "source", &symbol_conf.source_prefix, "directory", "path to kernel source"), OPT_CALLBACK('m', "module", NULL, "modname|path", "target module name (for online) or path (for offline)", opt_set_target), #endif OPT__DRY_RUN(&probe_event_dry_run), OPT_INTEGER('\0', "max-probes", ¶ms.max_probe_points, "Set how many probe points can be found for a probe."), OPT_BOOLEAN('F', "funcs", ¶ms.show_funcs, "Show potential probe-able functions."), OPT_CALLBACK('\0', "filter", NULL, "[!]FILTER", "Set a filter (with --vars/funcs only)\n" "\t\t\t(default: \"" DEFAULT_VAR_FILTER "\" for --vars,\n" "\t\t\t \"" DEFAULT_FUNC_FILTER "\" for --funcs)", opt_set_filter), OPT_CALLBACK('x', "exec", NULL, "executable|path", "target executable name or path", opt_set_target), OPT_END() }; int ret; argc = parse_options(argc, argv, options, probe_usage, PARSE_OPT_STOP_AT_NON_OPTION); if (argc > 0) { if (strcmp(argv[0], "-") == 0) { pr_warning(" Error: '-' is not supported.\n"); usage_with_options(probe_usage, options); } ret = parse_probe_event_argv(argc, argv); if (ret < 0) { pr_err(" Error: Parse Error. (%d)\n", ret); return ret; } } if (params.max_probe_points == 0) params.max_probe_points = MAX_PROBES; if ((!params.nevents && !params.dellist && !params.list_events && !params.show_lines && !params.show_funcs)) usage_with_options(probe_usage, options); /* * Only consider the user's kernel image path if given. */ symbol_conf.try_vmlinux_path = (symbol_conf.vmlinux_name == NULL); if (params.list_events) { if (params.mod_events) { pr_err(" Error: Don't use --list with --add/--del.\n"); usage_with_options(probe_usage, options); } if (params.show_lines) { pr_err(" Error: Don't use --list with --line.\n"); usage_with_options(probe_usage, options); } if (params.show_vars) { pr_err(" Error: Don't use --list with --vars.\n"); usage_with_options(probe_usage, options); } if (params.show_funcs) { pr_err(" Error: Don't use --list with --funcs.\n"); usage_with_options(probe_usage, options); } if (params.uprobes) { pr_warning(" Error: Don't use --list with --exec.\n"); usage_with_options(probe_usage, options); } ret = show_perf_probe_events(); if (ret < 0) pr_err(" Error: Failed to show event list. (%d)\n", ret); return ret; } if (params.show_funcs) { if (params.nevents != 0 || params.dellist) { pr_err(" Error: Don't use --funcs with" " --add/--del.\n"); usage_with_options(probe_usage, options); } if (params.show_lines) { pr_err(" Error: Don't use --funcs with --line.\n"); usage_with_options(probe_usage, options); } if (params.show_vars) { pr_err(" Error: Don't use --funcs with --vars.\n"); usage_with_options(probe_usage, options); } if (!params.filter) params.filter = strfilter__new(DEFAULT_FUNC_FILTER, NULL); ret = show_available_funcs(params.target, params.filter, params.uprobes); strfilter__delete(params.filter); if (ret < 0) pr_err(" Error: Failed to show functions." " (%d)\n", ret); return ret; } #ifdef DWARF_SUPPORT if (params.show_lines && !params.uprobes) { if (params.mod_events) { pr_err(" Error: Don't use --line with" " --add/--del.\n"); usage_with_options(probe_usage, options); } if (params.show_vars) { pr_err(" Error: Don't use --line with --vars.\n"); usage_with_options(probe_usage, options); } ret = show_line_range(¶ms.line_range, params.target); if (ret < 0) pr_err(" Error: Failed to show lines. (%d)\n", ret); return ret; } if (params.show_vars) { if (params.mod_events) { pr_err(" Error: Don't use --vars with" " --add/--del.\n"); usage_with_options(probe_usage, options); } if (!params.filter) params.filter = strfilter__new(DEFAULT_VAR_FILTER, NULL); ret = show_available_vars(params.events, params.nevents, params.max_probe_points, params.target, params.filter, params.show_ext_vars); strfilter__delete(params.filter); if (ret < 0) pr_err(" Error: Failed to show vars. (%d)\n", ret); return ret; } #endif if (params.dellist) { ret = del_perf_probe_events(params.dellist); strlist__delete(params.dellist); if (ret < 0) { pr_err(" Error: Failed to delete events. (%d)\n", ret); return ret; } } if (params.nevents) { ret = add_perf_probe_events(params.events, params.nevents, params.max_probe_points, params.target, params.force_add); if (ret < 0) { pr_err(" Error: Failed to add events. (%d)\n", ret); return ret; } } return 0; }