#ifndef LINUX_VIRTIO_H #define LINUX_VIRTIO_H #include #include #include #include #include #include #include #include typedef unsigned long long dma_addr_t; struct scatterlist { unsigned long page_link; unsigned int offset; unsigned int length; dma_addr_t dma_address; }; struct page { unsigned long long dummy; }; #define BUG_ON(__BUG_ON_cond) assert(!(__BUG_ON_cond)) /* Physical == Virtual */ #define virt_to_phys(p) ((unsigned long)p) #define phys_to_virt(a) ((void *)(unsigned long)(a)) /* Page address: Virtual / 4K */ #define virt_to_page(p) ((struct page*)((virt_to_phys(p) / 4096) * \ sizeof(struct page))) #define offset_in_page(p) (((unsigned long)p) % 4096) #define sg_phys(sg) ((sg->page_link & ~0x3) / sizeof(struct page) * 4096 + \ sg->offset) static inline void sg_mark_end(struct scatterlist *sg) { /* * Set termination bit, clear potential chain bit */ sg->page_link |= 0x02; sg->page_link &= ~0x01; } static inline void sg_init_table(struct scatterlist *sgl, unsigned int nents) { memset(sgl, 0, sizeof(*sgl) * nents); sg_mark_end(&sgl[nents - 1]); } static inline void sg_assign_page(struct scatterlist *sg, struct page *page) { unsigned long page_link = sg->page_link & 0x3; /* * In order for the low bit stealing approach to work, pages * must be aligned at a 32-bit boundary as a minimum. */ BUG_ON((unsigned long) page & 0x03); sg->page_link = page_link | (unsigned long) page; } static inline void sg_set_page(struct scatterlist *sg, struct page *page, unsigned int len, unsigned int offset) { sg_assign_page(sg, page); sg->offset = offset; sg->length = len; } static inline void sg_set_buf(struct scatterlist *sg, const void *buf, unsigned int buflen) { sg_set_page(sg, virt_to_page(buf), buflen, offset_in_page(buf)); } static inline void sg_init_one(struct scatterlist *sg, const void *buf, unsigned int buflen) { sg_init_table(sg, 1); sg_set_buf(sg, buf, buflen); } typedef __u16 u16; typedef enum { GFP_KERNEL, GFP_ATOMIC, } gfp_t; typedef enum { IRQ_NONE, IRQ_HANDLED } irqreturn_t; static inline void *kmalloc(size_t s, gfp_t gfp) { return malloc(s); } static inline void kfree(void *p) { free(p); } #define container_of(ptr, type, member) ({ \ const typeof( ((type *)0)->member ) *__mptr = (ptr); \ (type *)( (char *)__mptr - offsetof(type,member) );}) #define uninitialized_var(x) x = x # ifndef likely # define likely(x) (__builtin_expect(!!(x), 1)) # endif # ifndef unlikely # define unlikely(x) (__builtin_expect(!!(x), 0)) # endif #define pr_err(format, ...) fprintf (stderr, format, ## __VA_ARGS__) #ifdef DEBUG #define pr_debug(format, ...) fprintf (stderr, format, ## __VA_ARGS__) #else #define pr_debug(format, ...) do {} while (0) #endif #define dev_err(dev, format, ...) fprintf (stderr, format, ## __VA_ARGS__) #define dev_warn(dev, format, ...) fprintf (stderr, format, ## __VA_ARGS__) /* TODO: empty stubs for now. Broken but enough for virtio_ring.c */ #define list_add_tail(a, b) do {} while (0) #define list_del(a) do {} while (0) #define BIT_WORD(nr) ((nr) / BITS_PER_LONG) #define BITS_PER_BYTE 8 #define BITS_PER_LONG (sizeof(long) * BITS_PER_BYTE) #define BIT_MASK(nr) (1UL << ((nr) % BITS_PER_LONG)) /* TODO: Not atomic as it should be: * we don't use this for anything important. */ static inline void clear_bit(int nr, volatile unsigned long *addr) { unsigned long mask = BIT_MASK(nr); unsigned long *p = ((unsigned long *)addr) + BIT_WORD(nr); *p &= ~mask; } static inline int test_bit(int nr, const volatile unsigned long *addr) { return 1UL & (addr[BIT_WORD(nr)] >> (nr & (BITS_PER_LONG-1))); } /* The only feature we care to support */ #define virtio_has_feature(dev, feature) \ test_bit((feature), (dev)->features) /* end of stubs */ struct virtio_device { void *dev; unsigned long features[1]; }; struct virtqueue { /* TODO: commented as list macros are empty stubs for now. * Broken but enough for virtio_ring.c * struct list_head list; */ void (*callback)(struct virtqueue *vq); const char *name; struct virtio_device *vdev; void *priv; }; #define EXPORT_SYMBOL_GPL(__EXPORT_SYMBOL_GPL_name) \ void __EXPORT_SYMBOL_GPL##__EXPORT_SYMBOL_GPL_name() { \ } #define MODULE_LICENSE(__MODULE_LICENSE_value) \ const char *__MODULE_LICENSE_name = __MODULE_LICENSE_value #define CONFIG_SMP #if defined(__i386__) || defined(__x86_64__) #define barrier() asm volatile("" ::: "memory") #define mb() __sync_synchronize() #define smp_mb() mb() # define smp_rmb() barrier() # define smp_wmb() barrier() /* Weak barriers should be used. If not - it's a bug */ # define rmb() abort() # define wmb() abort() #else #error Please fill in barrier macros #endif /* Interfaces exported by virtio_ring. */ int virtqueue_add_buf(struct virtqueue *vq, struct scatterlist sg[], unsigned int out_num, unsigned int in_num, void *data, gfp_t gfp); void virtqueue_kick(struct virtqueue *vq); void *virtqueue_get_buf(struct virtqueue *vq, unsigned int *len); void virtqueue_disable_cb(struct virtqueue *vq); bool virtqueue_enable_cb(struct virtqueue *vq); bool virtqueue_enable_cb_delayed(struct virtqueue *vq); void *virtqueue_detach_unused_buf(struct virtqueue *vq); struct virtqueue *vring_new_virtqueue(unsigned int num, unsigned int vring_align, struct virtio_device *vdev, bool weak_barriers, void *pages, void (*notify)(struct virtqueue *vq), void (*callback)(struct virtqueue *vq), const char *name); void vring_del_virtqueue(struct virtqueue *vq); #endif