aboutsummaryrefslogtreecommitdiffstats
blob: 7bd776f9c3c70cc2f92290cbae254a9858c41daf (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
What:		/sys/bus/usb/devices/<busnum>-<devnum>:<config num>.<interface num>/<hid-bus>:<vendor-id>:<product-id>.<num>/koneplus/roccatkoneplus<minor>/actual_profile
Date:		October 2010
Contact:	Stefan Achatz <erazor_de@users.sourceforge.net>
Description:	The integer value of this attribute ranges from 0-4.
                When read, this attribute returns the number of the actual
                profile. This value is persistent, so its equivalent to the
                profile that's active when the mouse is powered on next time.
		When written, this file sets the number of the startup profile
		and the mouse activates this profile immediately.
Users:		http://roccat.sourceforge.net

What:		/sys/bus/usb/devices/<busnum>-<devnum>:<config num>.<interface num>/<hid-bus>:<vendor-id>:<product-id>.<num>/koneplus/roccatkoneplus<minor>/info
Date:		November 2012
Contact:	Stefan Achatz <erazor_de@users.sourceforge.net>
Description:	When read, this file returns general data like firmware version.
		When written, the device can be reset.
		The data is 8 bytes long.
Users:		http://roccat.sourceforge.net

What:		/sys/bus/usb/devices/<busnum>-<devnum>:<config num>.<interface num>/<hid-bus>:<vendor-id>:<product-id>.<num>/koneplus/roccatkoneplus<minor>/macro
Date:		October 2010
Contact:	Stefan Achatz <erazor_de@users.sourceforge.net>
Description:	The mouse can store a macro with max 500 key/button strokes
		internally.
		When written, this file lets one set the sequence for a specific
		button for a specific profile. Button and profile numbers are
		included in written data. The data has to be 2082 bytes long.
		This file is writeonly.
Users:		http://roccat.sourceforge.net

What:		/sys/bus/usb/devices/<busnum>-<devnum>:<config num>.<interface num>/<hid-bus>:<vendor-id>:<product-id>.<num>/koneplus/roccatkoneplus<minor>/profile_buttons
Date:		August 2010
Contact:	Stefan Achatz <erazor_de@users.sourceforge.net>
Description:	The mouse can store 5 profiles which can be switched by the
		press of a button. A profile is split in settings and buttons.
		profile_buttons holds information about button layout.
		When written, this file lets one write the respective profile
		buttons back to the mouse. The data has to be 77 bytes long.
		The mouse will reject invalid data.
		Which profile to write is determined by the profile number
		contained in the data.
		Before reading this file, control has to be written to select
		which profile to read.
Users:		http://roccat.sourceforge.net

What:		/sys/bus/usb/devices/<busnum>-<devnum>:<config num>.<interface num>/<hid-bus>:<vendor-id>:<product-id>.<num>/koneplus/roccatkoneplus<minor>/profile_settings
Date:		October 2010
Contact:	Stefan Achatz <erazor_de@users.sourceforge.net>
Description:	The mouse can store 5 profiles which can be switched by the
		press of a button. A profile is split in settings and buttons.
		profile_settings holds information like resolution, sensitivity
		and light effects.
		When written, this file lets one write the respective profile
		settings back to the mouse. The data has to be 43 bytes long.
		The mouse will reject invalid data.
		Which profile to write is determined by the profile number
		contained in the data.
		Before reading this file, control has to be written to select
		which profile to read.
Users:		http://roccat.sourceforge.net

What:		/sys/bus/usb/devices/<busnum>-<devnum>:<config num>.<interface num>/<hid-bus>:<vendor-id>:<product-id>.<num>/koneplus/roccatkoneplus<minor>/sensor
Date:		October 2010
Contact:	Stefan Achatz <erazor_de@users.sourceforge.net>
Description:	The mouse has a tracking- and a distance-control-unit. These
		can be activated/deactivated and the lift-off distance can be
		set. The data has to be 6 bytes long.
		This file is writeonly.
Users:		http://roccat.sourceforge.net

What:		/sys/bus/usb/devices/<busnum>-<devnum>:<config num>.<interface num>/<hid-bus>:<vendor-id>:<product-id>.<num>/koneplus/roccatkoneplus<minor>/talk
Date:		May 2011
Contact:	Stefan Achatz <erazor_de@users.sourceforge.net>
Description:	Used to active some easy* functions of the mouse from outside.
		The data has to be 16 bytes long.
		This file is writeonly.
Users:		http://roccat.sourceforge.net

What:		/sys/bus/usb/devices/<busnum>-<devnum>:<config num>.<interface num>/<hid-bus>:<vendor-id>:<product-id>.<num>/koneplus/roccatkoneplus<minor>/tcu
Date:		October 2010
Contact:	Stefan Achatz <erazor_de@users.sourceforge.net>
Description:	When written a calibration process for the tracking control unit
		can be initiated/cancelled. Also lets one read/write sensor
		registers.
		The data has to be 4 bytes long.
Users:		http://roccat.sourceforge.net

What:		/sys/bus/usb/devices/<busnum>-<devnum>:<config num>.<interface num>/<hid-bus>:<vendor-id>:<product-id>.<num>/koneplus/roccatkoneplus<minor>/tcu_image
Date:		October 2010
Contact:	Stefan Achatz <erazor_de@users.sourceforge.net>
Description:	When read the mouse returns a 30x30 pixel image of the
		sampled underground. This works only in the course of a
		calibration process initiated with tcu.
		The returned data is 1028 bytes in size.
		This file is readonly.
Users:		http://roccat.sourceforge.net