aboutsummaryrefslogtreecommitdiffstats
blob: 74be14679ed891820cd9c3a7393007f8dd21d07d (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
Linux 2.4.2 Secure Attention Key (SAK) handling
18 March 2001, Andrew Morton

An operating system's Secure Attention Key is a security tool which is
provided as protection against trojan password capturing programs.  It
is an undefeatable way of killing all programs which could be
masquerading as login applications.  Users need to be taught to enter
this key sequence before they log in to the system.

From the PC keyboard, Linux has two similar but different ways of
providing SAK.  One is the ALT-SYSRQ-K sequence.  You shouldn't use
this sequence.  It is only available if the kernel was compiled with
sysrq support.

The proper way of generating a SAK is to define the key sequence using
`loadkeys'.  This will work whether or not sysrq support is compiled
into the kernel.

SAK works correctly when the keyboard is in raw mode.  This means that
once defined, SAK will kill a running X server.  If the system is in
run level 5, the X server will restart.  This is what you want to
happen.

What key sequence should you use? Well, CTRL-ALT-DEL is used to reboot
the machine.  CTRL-ALT-BACKSPACE is magical to the X server.  We'll
choose CTRL-ALT-PAUSE.

In your rc.sysinit (or rc.local) file, add the command

	echo "control alt keycode 101 = SAK" | /bin/loadkeys

And that's it!  Only the superuser may reprogram the SAK key.


NOTES
=====

1: Linux SAK is said to be not a "true SAK" as is required by
   systems which implement C2 level security.  This author does not
   know why.


2: On the PC keyboard, SAK kills all applications which have
   /dev/console opened.

   Unfortunately this includes a number of things which you don't
   actually want killed.  This is because these applications are
   incorrectly holding /dev/console open.  Be sure to complain to your
   Linux distributor about this!

   You can identify processes which will be killed by SAK with the
   command

	# ls -l /proc/[0-9]*/fd/* | grep console
	l-wx------    1 root     root           64 Mar 18 00:46 /proc/579/fd/0 -> /dev/console

   Then:

	# ps aux|grep 579
	root       579  0.0  0.1  1088  436 ?        S    00:43   0:00 gpm -t ps/2

   So `gpm' will be killed by SAK.  This is a bug in gpm.  It should
   be closing standard input.  You can work around this by finding the
   initscript which launches gpm and changing it thusly:

   Old:

	daemon gpm

   New:

	daemon gpm < /dev/null

   Vixie cron also seems to have this problem, and needs the same treatment.

   Also, one prominent Linux distribution has the following three
   lines in its rc.sysinit and rc scripts:

	exec 3<&0
	exec 4>&1
	exec 5>&2

   These commands cause *all* daemons which are launched by the
   initscripts to have file descriptors 3, 4 and 5 attached to
   /dev/console.  So SAK kills them all.  A workaround is to simply
   delete these lines, but this may cause system management
   applications to malfunction - test everything well.