aboutsummaryrefslogtreecommitdiffstats
blob: 4f27785ca0c87f8cf0ab4c28c9566595b032ed64 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
ACPI based device enumeration
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
ACPI 5 introduced a set of new resources (UartTSerialBus, I2cSerialBus,
SpiSerialBus, GpioIo and GpioInt) which can be used in enumerating slave
devices behind serial bus controllers.

In addition we are starting to see peripherals integrated in the
SoC/Chipset to appear only in ACPI namespace. These are typically devices
that are accessed through memory-mapped registers.

In order to support this and re-use the existing drivers as much as
possible we decided to do following:

	o Devices that have no bus connector resource are represented as
	  platform devices.

	o Devices behind real busses where there is a connector resource
	  are represented as struct spi_device or struct i2c_device
	  (standard UARTs are not busses so there is no struct uart_device).

As both ACPI and Device Tree represent a tree of devices (and their
resources) this implementation follows the Device Tree way as much as
possible.

The ACPI implementation enumerates devices behind busses (platform, SPI and
I2C), creates the physical devices and binds them to their ACPI handle in
the ACPI namespace.

This means that when ACPI_HANDLE(dev) returns non-NULL the device was
enumerated from ACPI namespace. This handle can be used to extract other
device-specific configuration. There is an example of this below.

Platform bus support
~~~~~~~~~~~~~~~~~~~~
Since we are using platform devices to represent devices that are not
connected to any physical bus we only need to implement a platform driver
for the device and add supported ACPI IDs. If this same IP-block is used on
some other non-ACPI platform, the driver might work out of the box or needs
some minor changes.

Adding ACPI support for an existing driver should be pretty
straightforward. Here is the simplest example:

	#ifdef CONFIG_ACPI
	static struct acpi_device_id mydrv_acpi_match[] = {
		/* ACPI IDs here */
		{ }
	};
	MODULE_DEVICE_TABLE(acpi, mydrv_acpi_match);
	#endif

	static struct platform_driver my_driver = {
		...
		.driver = {
			.acpi_match_table = ACPI_PTR(mydrv_acpi_match),
		},
	};

If the driver needs to perform more complex initialization like getting and
configuring GPIOs it can get its ACPI handle and extract this information
from ACPI tables.

Currently the kernel is not able to automatically determine from which ACPI
device it should make the corresponding platform device so we need to add
the ACPI device explicitly to acpi_platform_device_ids list defined in
drivers/acpi/scan.c. This limitation is only for the platform devices, SPI
and I2C devices are created automatically as described below.

SPI serial bus support
~~~~~~~~~~~~~~~~~~~~~~
Slave devices behind SPI bus have SpiSerialBus resource attached to them.
This is extracted automatically by the SPI core and the slave devices are
enumerated once spi_register_master() is called by the bus driver.

Here is what the ACPI namespace for a SPI slave might look like:

	Device (EEP0)
	{
		Name (_ADR, 1)
		Name (_CID, Package() {
			"ATML0025",
			"AT25",
		})
		...
		Method (_CRS, 0, NotSerialized)
		{
			SPISerialBus(1, PolarityLow, FourWireMode, 8,
				ControllerInitiated, 1000000, ClockPolarityLow,
				ClockPhaseFirst, "\\_SB.PCI0.SPI1",)
		}
		...

The SPI device drivers only need to add ACPI IDs in a similar way than with
the platform device drivers. Below is an example where we add ACPI support
to at25 SPI eeprom driver (this is meant for the above ACPI snippet):

	#ifdef CONFIG_ACPI
	static struct acpi_device_id at25_acpi_match[] = {
		{ "AT25", 0 },
		{ },
	};
	MODULE_DEVICE_TABLE(acpi, at25_acpi_match);
	#endif

	static struct spi_driver at25_driver = {
		.driver = {
			...
			.acpi_match_table = ACPI_PTR(at25_acpi_match),
		},
	};

Note that this driver actually needs more information like page size of the
eeprom etc. but at the time writing this there is no standard way of
passing those. One idea is to return this in _DSM method like:

	Device (EEP0)
	{
		...
		Method (_DSM, 4, NotSerialized)
		{
			Store (Package (6)
			{
				"byte-len", 1024,
				"addr-mode", 2,
				"page-size, 32
			}, Local0)

			// Check UUIDs etc.

			Return (Local0)
		}

Then the at25 SPI driver can get this configation by calling _DSM on its
ACPI handle like:

	struct acpi_buffer output = { ACPI_ALLOCATE_BUFFER, NULL };
	struct acpi_object_list input;
	acpi_status status;

	/* Fill in the input buffer */

	status = acpi_evaluate_object(ACPI_HANDLE(&spi->dev), "_DSM",
				      &input, &output);
	if (ACPI_FAILURE(status))
		/* Handle the error */

	/* Extract the data here */

	kfree(output.pointer);

I2C serial bus support
~~~~~~~~~~~~~~~~~~~~~~
The slaves behind I2C bus controller only need to add the ACPI IDs like
with the platform and SPI drivers. However the I2C bus controller driver
needs to call acpi_i2c_register_devices() after it has added the adapter.

An I2C bus (controller) driver does:

	...
	ret = i2c_add_numbered_adapter(adapter);
	if (ret)
		/* handle error */

	of_i2c_register_devices(adapter);
	/* Enumerate the slave devices behind this bus via ACPI */
	acpi_i2c_register_devices(adapter);

Below is an example of how to add ACPI support to the existing mpu3050
input driver:

	#ifdef CONFIG_ACPI
	static struct acpi_device_id mpu3050_acpi_match[] = {
		{ "MPU3050", 0 },
		{ },
	};
	MODULE_DEVICE_TABLE(acpi, mpu3050_acpi_match);
	#endif

	static struct i2c_driver mpu3050_i2c_driver = {
		.driver	= {
			.name	= "mpu3050",
			.owner	= THIS_MODULE,
			.pm	= &mpu3050_pm,
			.of_match_table = mpu3050_of_match,
			.acpi_match_table  ACPI_PTR(mpu3050_acpi_match),
		},
		.probe		= mpu3050_probe,
		.remove		= __devexit_p(mpu3050_remove),
		.id_table	= mpu3050_ids,
	};

GPIO support
~~~~~~~~~~~~
ACPI 5 introduced two new resources to describe GPIO connections: GpioIo
and GpioInt. These resources are used be used to pass GPIO numbers used by
the device to the driver. For example:

	Method (_CRS, 0, NotSerialized)
	{
		Name (SBUF, ResourceTemplate()
		{
			GpioIo (Exclusive, PullDefault, 0x0000, 0x0000,
				IoRestrictionOutputOnly, "\\_SB.PCI0.GPI0",
				0x00, ResourceConsumer,,)
			{
				// Pin List
				0x0055
			}
			...

			Return (SBUF)
		}
	}

These GPIO numbers are controller relative and path "\\_SB.PCI0.GPI0"
specifies the path to the controller. In order to use these GPIOs in Linux
we need to translate them to the Linux GPIO numbers.

The driver can do this by including <linux/acpi_gpio.h> and then calling
acpi_get_gpio(path, gpio). This will return the Linux GPIO number or
negative errno if there was no translation found.

Other GpioIo parameters must be converted first by the driver to be
suitable to the gpiolib before passing them.

In case of GpioInt resource an additional call to gpio_to_irq() must be
done before calling request_irq().