aboutsummaryrefslogtreecommitdiffstats
blob: 1943fae014fd8a7d98a6af898558535556ffaaf3 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
		The Common Clk Framework
		Mike Turquette <mturquette@ti.com>

This document endeavours to explain the common clk framework details,
and how to port a platform over to this framework.  It is not yet a
detailed explanation of the clock api in include/linux/clk.h, but
perhaps someday it will include that information.

	Part 1 - introduction and interface split

The common clk framework is an interface to control the clock nodes
available on various devices today.  This may come in the form of clock
gating, rate adjustment, muxing or other operations.  This framework is
enabled with the CONFIG_COMMON_CLK option.

The interface itself is divided into two halves, each shielded from the
details of its counterpart.  First is the common definition of struct
clk which unifies the framework-level accounting and infrastructure that
has traditionally been duplicated across a variety of platforms.  Second
is a common implementation of the clk.h api, defined in
drivers/clk/clk.c.  Finally there is struct clk_ops, whose operations
are invoked by the clk api implementation.

The second half of the interface is comprised of the hardware-specific
callbacks registered with struct clk_ops and the corresponding
hardware-specific structures needed to model a particular clock.  For
the remainder of this document any reference to a callback in struct
clk_ops, such as .enable or .set_rate, implies the hardware-specific
implementation of that code.  Likewise, references to struct clk_foo
serve as a convenient shorthand for the implementation of the
hardware-specific bits for the hypothetical "foo" hardware.

Tying the two halves of this interface together is struct clk_hw, which
is defined in struct clk_foo and pointed to within struct clk.  This
allows easy for navigation between the two discrete halves of the common
clock interface.

	Part 2 - common data structures and api

Below is the common struct clk definition from
include/linux/clk-private.h, modified for brevity:

	struct clk {
		const char		*name;
		const struct clk_ops	*ops;
		struct clk_hw		*hw;
		char			**parent_names;
		struct clk		**parents;
		struct clk		*parent;
		struct hlist_head	children;
		struct hlist_node	child_node;
		...
	};

The members above make up the core of the clk tree topology.  The clk
api itself defines several driver-facing functions which operate on
struct clk.  That api is documented in include/linux/clk.h.

Platforms and devices utilizing the common struct clk use the struct
clk_ops pointer in struct clk to perform the hardware-specific parts of
the operations defined in clk.h:

	struct clk_ops {
		int		(*prepare)(struct clk_hw *hw);
		void		(*unprepare)(struct clk_hw *hw);
		int		(*enable)(struct clk_hw *hw);
		void		(*disable)(struct clk_hw *hw);
		int		(*is_enabled)(struct clk_hw *hw);
		unsigned long	(*recalc_rate)(struct clk_hw *hw,
						unsigned long parent_rate);
		long		(*round_rate)(struct clk_hw *hw, unsigned long,
						unsigned long *);
		int		(*set_parent)(struct clk_hw *hw, u8 index);
		u8		(*get_parent)(struct clk_hw *hw);
		int		(*set_rate)(struct clk_hw *hw, unsigned long);
		void		(*init)(struct clk_hw *hw);
	};

	Part 3 - hardware clk implementations

The strength of the common struct clk comes from its .ops and .hw pointers
which abstract the details of struct clk from the hardware-specific bits, and
vice versa.  To illustrate consider the simple gateable clk implementation in
drivers/clk/clk-gate.c:

struct clk_gate {
	struct clk_hw	hw;
	void __iomem    *reg;
	u8              bit_idx;
	...
};

struct clk_gate contains struct clk_hw hw as well as hardware-specific
knowledge about which register and bit controls this clk's gating.
Nothing about clock topology or accounting, such as enable_count or
notifier_count, is needed here.  That is all handled by the common
framework code and struct clk.

Let's walk through enabling this clk from driver code:

	struct clk *clk;
	clk = clk_get(NULL, "my_gateable_clk");

	clk_prepare(clk);
	clk_enable(clk);

The call graph for clk_enable is very simple:

clk_enable(clk);
	clk->ops->enable(clk->hw);
	[resolves to...]
		clk_gate_enable(hw);
		[resolves struct clk gate with to_clk_gate(hw)]
			clk_gate_set_bit(gate);

And the definition of clk_gate_set_bit:

static void clk_gate_set_bit(struct clk_gate *gate)
{
	u32 reg;

	reg = __raw_readl(gate->reg);
	reg |= BIT(gate->bit_idx);
	writel(reg, gate->reg);
}

Note that to_clk_gate is defined as:

#define to_clk_gate(_hw) container_of(_hw, struct clk_gate, clk)

This pattern of abstraction is used for every clock hardware
representation.

	Part 4 - supporting your own clk hardware

When implementing support for a new type of clock it only necessary to
include the following header:

#include <linux/clk-provider.h>

include/linux/clk.h is included within that header and clk-private.h
must never be included from the code which implements the operations for
a clock.  More on that below in Part 5.

To construct a clk hardware structure for your platform you must define
the following:

struct clk_foo {
	struct clk_hw hw;
	... hardware specific data goes here ...
};

To take advantage of your data you'll need to support valid operations
for your clk:

struct clk_ops clk_foo_ops {
	.enable		= &clk_foo_enable;
	.disable	= &clk_foo_disable;
};

Implement the above functions using container_of:

#define to_clk_foo(_hw) container_of(_hw, struct clk_foo, hw)

int clk_foo_enable(struct clk_hw *hw)
{
	struct clk_foo *foo;

	foo = to_clk_foo(hw);

	... perform magic on foo ...

	return 0;
};

Below is a matrix detailing which clk_ops are mandatory based upon the
hardware capbilities of that clock.  A cell marked as "y" means
mandatory, a cell marked as "n" implies that either including that
callback is invalid or otherwise uneccesary.  Empty cells are either
optional or must be evaluated on a case-by-case basis.

                           clock hardware characteristics
	     -----------------------------------------------------------
             | gate | change rate | single parent | multiplexer | root |
             |------|-------------|---------------|-------------|------|
.prepare     |      |             |               |             |      |
.unprepare   |      |             |               |             |      |
             |      |             |               |             |      |
.enable      | y    |             |               |             |      |
.disable     | y    |             |               |             |      |
.is_enabled  | y    |             |               |             |      |
             |      |             |               |             |      |
.recalc_rate |      | y           |               |             |      |
.round_rate  |      | y           |               |             |      |
.set_rate    |      | y           |               |             |      |
             |      |             |               |             |      |
.set_parent  |      |             | n             | y           | n    |
.get_parent  |      |             | n             | y           | n    |
             |      |             |               |             |      |
.init        |      |             |               |             |      |
	     -----------------------------------------------------------

Finally, register your clock at run-time with a hardware-specific
registration function.  This function simply populates struct clk_foo's
data and then passes the common struct clk parameters to the framework
with a call to:

clk_register(...)

See the basic clock types in drivers/clk/clk-*.c for examples.

	Part 5 - static initialization of clock data

For platforms with many clocks (often numbering into the hundreds) it
may be desirable to statically initialize some clock data.  This
presents a problem since the definition of struct clk should be hidden
from everyone except for the clock core in drivers/clk/clk.c.

To get around this problem struct clk's definition is exposed in
include/linux/clk-private.h along with some macros for more easily
initializing instances of the basic clock types.  These clocks must
still be initialized with the common clock framework via a call to
__clk_init.

clk-private.h must NEVER be included by code which implements struct
clk_ops callbacks, nor must it be included by any logic which pokes
around inside of struct clk at run-time.  To do so is a layering
violation.

To better enforce this policy, always follow this simple rule: any
statically initialized clock data MUST be defined in a separate file
from the logic that implements its ops.  Basically separate the logic
from the data and all is well.