1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
|
Texas instruments video serializer de serializer
================================================
See Documentation/video-serdes.txt for generic information about
video serializer / de serializers.
FPDlink3 video serdes devices are I2C slave devices. They are always
used in pairs where one device is connected to the CPU/SoC which is
called local device and the other one is called remote device.
FPDlink3 video serdes devices have some gpios which can be controlled
over I2C. Also, the FPDlink supports gpio forwarding. Which means that
the remote device can copy the gpio values from it's remote device.
Also, each of the remote device is an I2C master itself, so it can
interface some I2C slaves at remote end. For e.g, a backlight LCD chip
connected to the de serializer or the camera connected to a serializer.
So these slaves can be accessed from local devices via I2C aliases.
A pair of serializer/deserializer can be used for tunneling the i2c
transactions over LVDS channel. The one of the device is connected to
the system i2c bus in slave mode and the other one acts as a master
at the remote end. But, the slave device can register dummy aliases
remote master and for each of the remote slaves.
As this is acting like a i2c bridge driver, we need a method for
configuring the address translations.
Required Properties:
- compatible: should be one of the following.
- "ti,ds90ub913aq": For TI FPDlink3 12bit video serializer
- "ti,ds90ub914aq": For TI FPDlink3 12bit video de serializer
- "ti,ds90uh925q": For TI FPDlink3 24bit video serializer
- "ti,ds90uh928q": For TI FPDlink3 24bit video de serializer
- reg: I2C slave address
This would be the alias adress for remote device. The CPU side
ser/des would address the remote device using this address.
Optional Properties:
- gpio-controller: Marks the device node as a gpio controller.
- #gpio-cells: Should be 1. The first cell is the GPIO number.
- ranges: This is the address translation table for mapping i2c devices
on the remote bus to the i2c address(alias) on parent bus.
The first entry in the ranges property has to of the corresponding
remote ser/des device.
For dynamic address mapping, keep the remote slave address as 0x0
The corresponding alias would be used if the remote slave doesn't
have an address already mapped.
- slave-mode: This property marks the ser/des as remote device.
For a device where 'slave-mode' property is absent, it is considered
as master device and 'ranges' and 'i2c-bus-num' properties are
compulsory.
Example:
Following example demonstrates device node structure for a camera connected
using FPDlink3 ser/des. Here the deserializer and serializer are connected
only via the LVDS link. The camera is connected on the serializer i2c bus.
Here, serializer and camera are not connected to the system i2c bus, but it
can be accessed from the system i2c bus. The deserializer maps each of the
remote slave onto the system i2c bus and acts as a bridge to transfer any
messages addressed to the remote devices.
=======================================
+-------+
|I2C bus|
+-------+
|
|0x60<real> +------------+
+-----------|Deserializer|0x60
| +------------+
| X
| X
| X <LVDS link>
| X
| X
| +----------+
| | Remote |
| | i2c bus |
| +----------+
| |
|0x74<alias> | +----------+
| <- - - - +------|Serializer| 0x58
| | +----------+
| |
|0x38<alias> | +---------+
| <- - - - +------|OV Camera| 0x30
| | +---------+
|
|
=======================================
i2cbus {
lvds_des: deserializer@60 {
compatible = "ti,ds90ub914aq";
reg = <0x60>;
gpio-controller;
#gpio-cells=1;
i2c-bus-num = <5>;
};
};
&lvds_des {
ranges = <0x58 0x74>,
<0x38 0x30>;
lvds_ser: serializer@58 {
compatible = "ti,ds90ub913aq";
reg = <0x58>;
remote-device = <&lvds_des>;
gpio-controller;
#gpio-cells=1;
slave-mode;
};
lvds_cam: camera@30 {
compatible = "ov10635"
reg = <0x30>;
gpios = <&lvds_ser 0>;
/* power pin controlled by serializer local gpio */
};
};
|