aboutsummaryrefslogtreecommitdiffstats
blob: f4769b9399df7d2950508797a78faf16e5f9512b (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
402
403
404
405
406
407
408
409
410
411
412
413
414
415
416
417
418
419
420
421
422
423
424
425
426
427
428
429
430
431
432
433
434
435
436
437
438
439
440
441
442
443
444
445
446
447
448
449
450
451
452
453
454
455
456
457
458
459
460
461
462
463
464
465
466
467
468
469
470
471
472
473
474
475
476
477
478
479
480
481
482
483
484
485
486
487
488
489
490
491
492
493
494
495
496
497
498
499
500
501
502
503
504
505
506
507
508
509
510
511
512
513
514
515
516
517
518
519
520
521
522
523
524
525
526
527
528
529
530
531
532
533
534
535
536
537
538
539
540
541
542
543
544
545
546
547
548
549
550
551
552
553
554
555
556
557
558
559
560
561
562
563
564
565
566
567
568
569
570
571
572
573
574
575
576
577
578
579
580
581
582
583
584
585
586
587
588
589
590
591
592
593
594
595
596
597
598
599
600
601
602
603
604
605
606
607
608
609
610
611
612
613
614
615
616
617
618
619
620
621
622
623
624
625
626
627
628
629
630
631
632
633
634
635
636
637
638
639
640
641
642
643
644
645
646
647
648
649
650
651
652
653
654
655
656
657
658
659
660
661
662
663
664
665
666
667
668
669
670
671
672
673
674
675
676
677
678
679
680
681
682
			  ==========================
			  FS-CACHE CACHE BACKEND API
			  ==========================

The FS-Cache system provides an API by which actual caches can be supplied to
FS-Cache for it to then serve out to network filesystems and other interested
parties.

This API is declared in <linux/fscache-cache.h>.


====================================
INITIALISING AND REGISTERING A CACHE
====================================

To start off, a cache definition must be initialised and registered for each
cache the backend wants to make available.  For instance, CacheFS does this in
the fill_super() operation on mounting.

The cache definition (struct fscache_cache) should be initialised by calling:

	void fscache_init_cache(struct fscache_cache *cache,
				struct fscache_cache_ops *ops,
				const char *idfmt,
				...);

Where:

 (*) "cache" is a pointer to the cache definition;

 (*) "ops" is a pointer to the table of operations that the backend supports on
     this cache; and

 (*) "idfmt" is a format and printf-style arguments for constructing a label
     for the cache.


The cache should then be registered with FS-Cache by passing a pointer to the
previously initialised cache definition to:

	int fscache_add_cache(struct fscache_cache *cache,
			      struct fscache_object *fsdef,
			      const char *tagname);

Two extra arguments should also be supplied:

 (*) "fsdef" which should point to the object representation for the FS-Cache
     master index in this cache.  Netfs primary index entries will be created
     here.  FS-Cache keeps the caller's reference to the index object if
     successful and will release it upon withdrawal of the cache.

 (*) "tagname" which, if given, should be a text string naming this cache.  If
     this is NULL, the identifier will be used instead.  For CacheFS, the
     identifier is set to name the underlying block device and the tag can be
     supplied by mount.

This function may return -ENOMEM if it ran out of memory or -EEXIST if the tag
is already in use.  0 will be returned on success.


=====================
UNREGISTERING A CACHE
=====================

A cache can be withdrawn from the system by calling this function with a
pointer to the cache definition:

	void fscache_withdraw_cache(struct fscache_cache *cache);

In CacheFS's case, this is called by put_super().


========
SECURITY
========

The cache methods are executed one of two contexts:

 (1) that of the userspace process that issued the netfs operation that caused
     the cache method to be invoked, or

 (2) that of one of the processes in the FS-Cache thread pool.

In either case, this may not be an appropriate context in which to access the
cache.

The calling process's fsuid, fsgid and SELinux security identities may need to
be masqueraded for the duration of the cache driver's access to the cache.
This is left to the cache to handle; FS-Cache makes no effort in this regard.


===================================
CONTROL AND STATISTICS PRESENTATION
===================================

The cache may present data to the outside world through FS-Cache's interfaces
in sysfs and procfs - the former for control and the latter for statistics.

A sysfs directory called /sys/fs/fscache/<cachetag>/ is created if CONFIG_SYSFS
is enabled.  This is accessible through the kobject struct fscache_cache::kobj
and is for use by the cache as it sees fit.


========================
RELEVANT DATA STRUCTURES
========================

 (*) Index/Data file FS-Cache representation cookie:

	struct fscache_cookie {
		struct fscache_object_def	*def;
		struct fscache_netfs		*netfs;
		void				*netfs_data;
		...
	};

     The fields that might be of use to the backend describe the object
     definition, the netfs definition and the netfs's data for this cookie.
     The object definition contain functions supplied by the netfs for loading
     and matching index entries; these are required to provide some of the
     cache operations.


 (*) In-cache object representation:

	struct fscache_object {
		int				debug_id;
		enum {
			FSCACHE_OBJECT_RECYCLING,
			...
		}				state;
		spinlock_t			lock
		struct fscache_cache		*cache;
		struct fscache_cookie		*cookie;
		...
	};

     Structures of this type should be allocated by the cache backend and
     passed to FS-Cache when requested by the appropriate cache operation.  In
     the case of CacheFS, they're embedded in CacheFS's internal object
     structures.

     The debug_id is a simple integer that can be used in debugging messages
     that refer to a particular object.  In such a case it should be printed
     using "OBJ%x" to be consistent with FS-Cache.

     Each object contains a pointer to the cookie that represents the object it
     is backing.  An object should retired when put_object() is called if it is
     in state FSCACHE_OBJECT_RECYCLING.  The fscache_object struct should be
     initialised by calling fscache_object_init(object).


 (*) FS-Cache operation record:

	struct fscache_operation {
		atomic_t		usage;
		struct fscache_object	*object;
		unsigned long		flags;
	#define FSCACHE_OP_EXCLUSIVE
		void (*processor)(struct fscache_operation *op);
		void (*release)(struct fscache_operation *op);
		...
	};

     FS-Cache has a pool of threads that it uses to give CPU time to the
     various asynchronous operations that need to be done as part of driving
     the cache.  These are represented by the above structure.  The processor
     method is called to give the op CPU time, and the release method to get
     rid of it when its usage count reaches 0.

     An operation can be made exclusive upon an object by setting the
     appropriate flag before enqueuing it with fscache_enqueue_operation().  If
     an operation needs more processing time, it should be enqueued again.


 (*) FS-Cache retrieval operation record:

	struct fscache_retrieval {
		struct fscache_operation op;
		struct address_space	*mapping;
		struct list_head	*to_do;
		...
	};

     A structure of this type is allocated by FS-Cache to record retrieval and
     allocation requests made by the netfs.  This struct is then passed to the
     backend to do the operation.  The backend may get extra refs to it by
     calling fscache_get_retrieval() and refs may be discarded by calling
     fscache_put_retrieval().

     A retrieval operation can be used by the backend to do retrieval work.  To
     do this, the retrieval->op.processor method pointer should be set
     appropriately by the backend and fscache_enqueue_retrieval() called to
     submit it to the thread pool.  CacheFiles, for example, uses this to queue
     page examination when it detects PG_lock being cleared.

     The to_do field is an empty list available for the cache backend to use as
     it sees fit.


 (*) FS-Cache storage operation record:

	struct fscache_storage {
		struct fscache_operation op;
		pgoff_t			store_limit;
		...
	};

     A structure of this type is allocated by FS-Cache to record outstanding
     writes to be made.  FS-Cache itself enqueues this operation and invokes
     the write_page() method on the object at appropriate times to effect
     storage.


================
CACHE OPERATIONS
================

The cache backend provides FS-Cache with a table of operations that can be
performed on the denizens of the cache.  These are held in a structure of type:

	struct fscache_cache_ops

 (*) Name of cache provider [mandatory]:

	const char *name

     This isn't strictly an operation, but should be pointed at a string naming
     the backend.


 (*) Allocate a new object [mandatory]:

	struct fscache_object *(*alloc_object)(struct fscache_cache *cache,
					       struct fscache_cookie *cookie)

     This method is used to allocate a cache object representation to back a
     cookie in a particular cache.  fscache_object_init() should be called on
     the object to initialise it prior to returning.

     This function may also be used to parse the index key to be used for
     multiple lookup calls to turn it into a more convenient form.  FS-Cache
     will call the lookup_complete() method to allow the cache to release the
     form once lookup is complete or aborted.


 (*) Look up and create object [mandatory]:

	void (*lookup_object)(struct fscache_object *object)

     This method is used to look up an object, given that the object is already
     allocated and attached to the cookie.  This should instantiate that object
     in the cache if it can.

     The method should call fscache_object_lookup_negative() as soon as
     possible if it determines the object doesn't exist in the cache.  If the
     object is found to exist and the netfs indicates that it is valid then
     fscache_obtained_object() should be called once the object is in a
     position to have data stored in it.  Similarly, fscache_obtained_object()
     should also be called once a non-present object has been created.

     If a lookup error occurs, fscache_object_lookup_error() should be called
     to abort the lookup of that object.


 (*) Release lookup data [mandatory]:

	void (*lookup_complete)(struct fscache_object *object)

     This method is called to ask the cache to release any resources it was
     using to perform a lookup.


 (*) Increment object refcount [mandatory]:

	struct fscache_object *(*grab_object)(struct fscache_object *object)

     This method is called to increment the reference count on an object.  It
     may fail (for instance if the cache is being withdrawn) by returning NULL.
     It should return the object pointer if successful.


 (*) Lock/Unlock object [mandatory]:

	void (*lock_object)(struct fscache_object *object)
	void (*unlock_object)(struct fscache_object *object)

     These methods are used to exclusively lock an object.  It must be possible
     to schedule with the lock held, so a spinlock isn't sufficient.


 (*) Pin/Unpin object [optional]:

	int (*pin_object)(struct fscache_object *object)
	void (*unpin_object)(struct fscache_object *object)

     These methods are used to pin an object into the cache.  Once pinned an
     object cannot be reclaimed to make space.  Return -ENOSPC if there's not
     enough space in the cache to permit this.


 (*) Update object [mandatory]:

	int (*update_object)(struct fscache_object *object)

     This is called to update the index entry for the specified object.  The
     new information should be in object->cookie->netfs_data.  This can be
     obtained by calling object->cookie->def->get_aux()/get_attr().


 (*) Discard object [mandatory]:

	void (*drop_object)(struct fscache_object *object)

     This method is called to indicate that an object has been unbound from its
     cookie, and that the cache should release the object's resources and
     retire it if it's in state FSCACHE_OBJECT_RECYCLING.

     This method should not attempt to release any references held by the
     caller.  The caller will invoke the put_object() method as appropriate.


 (*) Release object reference [mandatory]:

	void (*put_object)(struct fscache_object *object)

     This method is used to discard a reference to an object.  The object may
     be freed when all the references to it are released.


 (*) Synchronise a cache [mandatory]:

	void (*sync)(struct fscache_cache *cache)

     This is called to ask the backend to synchronise a cache with its backing
     device.


 (*) Dissociate a cache [mandatory]:

	void (*dissociate_pages)(struct fscache_cache *cache)

     This is called to ask a cache to perform any page dissociations as part of
     cache withdrawal.


 (*) Notification that the attributes on a netfs file changed [mandatory]:

	int (*attr_changed)(struct fscache_object *object);

     This is called to indicate to the cache that certain attributes on a netfs
     file have changed (for example the maximum size a file may reach).  The
     cache can read these from the netfs by calling the cookie's get_attr()
     method.

     The cache may use the file size information to reserve space on the cache.
     It should also call fscache_set_store_limit() to indicate to FS-Cache the
     highest byte it's willing to store for an object.

     This method may return -ve if an error occurred or the cache object cannot
     be expanded.  In such a case, the object will be withdrawn from service.

     This operation is run asynchronously from FS-Cache's thread pool, and
     storage and retrieval operations from the netfs are excluded during the
     execution of this operation.


 (*) Reserve cache space for an object's data [optional]:

	int (*reserve_space)(struct fscache_object *object, loff_t size);

     This is called to request that cache space be reserved to hold the data
     for an object and the metadata used to track it.  Zero size should be
     taken as request to cancel a reservation.

     This should return 0 if successful, -ENOSPC if there isn't enough space
     available, or -ENOMEM or -EIO on other errors.

     The reservation may exceed the current size of the object, thus permitting
     future expansion.  If the amount of space consumed by an object would
     exceed the reservation, it's permitted to refuse requests to allocate
     pages, but not required.  An object may be pruned down to its reservation
     size if larger than that already.


 (*) Request page be read from cache [mandatory]:

	int (*read_or_alloc_page)(struct fscache_retrieval *op,
				  struct page *page,
				  gfp_t gfp)

     This is called to attempt to read a netfs page from the cache, or to
     reserve a backing block if not.  FS-Cache will have done as much checking
     as it can before calling, but most of the work belongs to the backend.

     If there's no page in the cache, then -ENODATA should be returned if the
     backend managed to reserve a backing block; -ENOBUFS or -ENOMEM if it
     didn't.

     If there is suitable data in the cache, then a read operation should be
     queued and 0 returned.  When the read finishes, fscache_end_io() should be
     called.

     The fscache_mark_pages_cached() should be called for the page if any cache
     metadata is retained.  This will indicate to the netfs that the page needs
     explicit uncaching.  This operation takes a pagevec, thus allowing several
     pages to be marked at once.

     The retrieval record pointed to by op should be retained for each page
     queued and released when I/O on the page has been formally ended.
     fscache_get/put_retrieval() are available for this purpose.

     The retrieval record may be used to get CPU time via the FS-Cache thread
     pool.  If this is desired, the op->op.processor should be set to point to
     the appropriate processing routine, and fscache_enqueue_retrieval() should
     be called at an appropriate point to request CPU time.  For instance, the
     retrieval routine could be enqueued upon the completion of a disk read.
     The to_do field in the retrieval record is provided to aid in this.

     If an I/O error occurs, fscache_io_error() should be called and -ENOBUFS
     returned if possible or fscache_end_io() called with a suitable error
     code.

     fscache_put_retrieval() should be called after a page or pages are dealt
     with.  This will complete the operation when all pages are dealt with.


 (*) Request pages be read from cache [mandatory]:

	int (*read_or_alloc_pages)(struct fscache_retrieval *op,
				   struct list_head *pages,
				   unsigned *nr_pages,
				   gfp_t gfp)

     This is like the read_or_alloc_page() method, except it is handed a list
     of pages instead of one page.  Any pages on which a read operation is
     started must be added to the page cache for the specified mapping and also
     to the LRU.  Such pages must also be removed from the pages list and
     *nr_pages decremented per page.

     If there was an error such as -ENOMEM, then that should be returned; else
     if one or more pages couldn't be read or allocated, then -ENOBUFS should
     be returned; else if one or more pages couldn't be read, then -ENODATA
     should be returned.  If all the pages are dispatched then 0 should be
     returned.


 (*) Request page be allocated in the cache [mandatory]:

	int (*allocate_page)(struct fscache_retrieval *op,
			     struct page *page,
			     gfp_t gfp)

     This is like the read_or_alloc_page() method, except that it shouldn't
     read from the cache, even if there's data there that could be retrieved.
     It should, however, set up any internal metadata required such that
     the write_page() method can write to the cache.

     If there's no backing block available, then -ENOBUFS should be returned
     (or -ENOMEM if there were other problems).  If a block is successfully
     allocated, then the netfs page should be marked and 0 returned.


 (*) Request pages be allocated in the cache [mandatory]:

	int (*allocate_pages)(struct fscache_retrieval *op,
			      struct list_head *pages,
			      unsigned *nr_pages,
			      gfp_t gfp)

     This is an multiple page version of the allocate_page() method.  pages and
     nr_pages should be treated as for the read_or_alloc_pages() method.


 (*) Request page be written to cache [mandatory]:

	int (*write_page)(struct fscache_storage *op,
			  struct page *page);

     This is called to write from a page on which there was a previously
     successful read_or_alloc_page() call or similar.  FS-Cache filters out
     pages that don't have mappings.

     This method is called asynchronously from the FS-Cache thread pool.  It is
     not required to actually store anything, provided -ENODATA is then
     returned to the next read of this page.

     If an error occurred, then a negative error code should be returned,
     otherwise zero should be returned.  FS-Cache will take appropriate action
     in response to an error, such as withdrawing this object.

     If this method returns success then FS-Cache will inform the netfs
     appropriately.


 (*) Discard retained per-page metadata [mandatory]:

	void (*uncache_page)(struct fscache_object *object, struct page *page)

     This is called when a netfs page is being evicted from the pagecache.  The
     cache backend should tear down any internal representation or tracking it
     maintains for this page.


==================
FS-CACHE UTILITIES
==================

FS-Cache provides some utilities that a cache backend may make use of:

 (*) Note occurrence of an I/O error in a cache:

	void fscache_io_error(struct fscache_cache *cache)

     This tells FS-Cache that an I/O error occurred in the cache.  After this
     has been called, only resource dissociation operations (object and page
     release) will be passed from the netfs to the cache backend for the
     specified cache.

     This does not actually withdraw the cache.  That must be done separately.


 (*) Invoke the retrieval I/O completion function:

	void fscache_end_io(struct fscache_retrieval *op, struct page *page,
			    int error);

     This is called to note the end of an attempt to retrieve a page.  The
     error value should be 0 if successful and an error otherwise.


 (*) Record that one or more pages being retrieved or allocated have been dealt
     with:

	void fscache_retrieval_complete(struct fscache_retrieval *op,
					int n_pages);

     This is called to record the fact that one or more pages have been dealt
     with and are no longer the concern of this operation.  When the number of
     pages remaining in the operation reaches 0, the operation will be
     completed.


 (*) Record operation completion:

	void fscache_op_complete(struct fscache_operation *op);

     This is called to record the completion of an operation.  This deducts
     this operation from the parent object's run state, potentially permitting
     one or more pending operations to start running.


 (*) Set highest store limit:

	void fscache_set_store_limit(struct fscache_object *object,
				     loff_t i_size);

     This sets the limit FS-Cache imposes on the highest byte it's willing to
     try and store for a netfs.  Any page over this limit is automatically
     rejected by fscache_read_alloc_page() and co with -ENOBUFS.


 (*) Mark pages as being cached:

	void fscache_mark_pages_cached(struct fscache_retrieval *op,
				       struct pagevec *pagevec);

     This marks a set of pages as being cached.  After this has been called,
     the netfs must call fscache_uncache_page() to unmark the pages.


 (*) Perform coherency check on an object:

	enum fscache_checkaux fscache_check_aux(struct fscache_object *object,
						const void *data,
						uint16_t datalen);

     This asks the netfs to perform a coherency check on an object that has
     just been looked up.  The cookie attached to the object will determine the
     netfs to use.  data and datalen should specify where the auxiliary data
     retrieved from the cache can be found.

     One of three values will be returned:

	(*) FSCACHE_CHECKAUX_OKAY

	    The coherency data indicates the object is valid as is.

	(*) FSCACHE_CHECKAUX_NEEDS_UPDATE

	    The coherency data needs updating, but otherwise the object is
	    valid.

	(*) FSCACHE_CHECKAUX_OBSOLETE

	    The coherency data indicates that the object is obsolete and should
	    be discarded.


 (*) Initialise a freshly allocated object:

	void fscache_object_init(struct fscache_object *object);

     This initialises all the fields in an object representation.


 (*) Indicate the destruction of an object:

	void fscache_object_destroyed(struct fscache_cache *cache);

     This must be called to inform FS-Cache that an object that belonged to a
     cache has been destroyed and deallocated.  This will allow continuation
     of the cache withdrawal process when it is stopped pending destruction of
     all the objects.


 (*) Indicate negative lookup on an object:

	void fscache_object_lookup_negative(struct fscache_object *object);

     This is called to indicate to FS-Cache that a lookup process for an object
     found a negative result.

     This changes the state of an object to permit reads pending on lookup
     completion to go off and start fetching data from the netfs server as it's
     known at this point that there can't be any data in the cache.

     This may be called multiple times on an object.  Only the first call is
     significant - all subsequent calls are ignored.


 (*) Indicate an object has been obtained:

	void fscache_obtained_object(struct fscache_object *object);

     This is called to indicate to FS-Cache that a lookup process for an object
     produced a positive result, or that an object was created.  This should
     only be called once for any particular object.

     This changes the state of an object to indicate:

	(1) if no call to fscache_object_lookup_negative() has been made on
	    this object, that there may be data available, and that reads can
	    now go and look for it; and

        (2) that writes may now proceed against this object.


 (*) Indicate that object lookup failed:

	void fscache_object_lookup_error(struct fscache_object *object);

     This marks an object as having encountered a fatal error (usually EIO)
     and causes it to move into a state whereby it will be withdrawn as soon
     as possible.


 (*) Get and release references on a retrieval record:

	void fscache_get_retrieval(struct fscache_retrieval *op);
	void fscache_put_retrieval(struct fscache_retrieval *op);

     These two functions are used to retain a retrieval record whilst doing
     asynchronous data retrieval and block allocation.


 (*) Enqueue a retrieval record for processing.

	void fscache_enqueue_retrieval(struct fscache_retrieval *op);

     This enqueues a retrieval record for processing by the FS-Cache thread
     pool.  One of the threads in the pool will invoke the retrieval record's
     op->op.processor callback function.  This function may be called from
     within the callback function.


 (*) List of object state names:

	const char *fscache_object_states[];

     For debugging purposes, this may be used to turn the state that an object
     is in into a text string for display purposes.