aboutsummaryrefslogtreecommitdiffstats
blob: 99b57abddf8a186e2dcb399e167778c3605147df (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
kernel-doc nano-HOWTO
=====================

How to format kernel-doc comments
---------------------------------

In order to provide embedded, 'C' friendly, easy to maintain,
but consistent and extractable documentation of the functions and
data structures in the Linux kernel, the Linux kernel has adopted
a consistent style for documenting functions and their parameters,
and structures and their members.

The format for this documentation is called the kernel-doc format.
It is documented in this Documentation/kernel-doc-nano-HOWTO.txt file.

This style embeds the documentation within the source files, using
a few simple conventions.  The scripts/kernel-doc perl script, some
SGML templates in Documentation/DocBook, and other tools understand
these conventions, and are used to extract this embedded documentation
into various documents.

In order to provide good documentation of kernel functions and data
structures, please use the following conventions to format your
kernel-doc comments in Linux kernel source.

We definitely need kernel-doc formatted documentation for functions
that are exported to loadable modules using EXPORT_SYMBOL.

We also look to provide kernel-doc formatted documentation for
functions externally visible to other kernel files (not marked
"static").

We also recommend providing kernel-doc formatted documentation
for private (file "static") routines, for consistency of kernel
source code layout.  But this is lower priority and at the
discretion of the MAINTAINER of that kernel source file.

Data structures visible in kernel include files should also be
documented using kernel-doc formatted comments.

The opening comment mark "/**" is reserved for kernel-doc comments.
Only comments so marked will be considered by the kernel-doc scripts,
and any comment so marked must be in kernel-doc format.  Do not use
"/**" to be begin a comment block unless the comment block contains
kernel-doc formatted comments.  The closing comment marker for
kernel-doc comments can be either "*/" or "**/", but "*/" is
preferred in the Linux kernel tree.

Kernel-doc comments should be placed just before the function
or data structure being described.

Example kernel-doc function comment:

/**
 * foobar() - short function description of foobar
 * @arg1:	Describe the first argument to foobar.
 * @arg2:	Describe the second argument to foobar.
 *		One can provide multiple line descriptions
 *		for arguments.
 *
 * A longer description, with more discussion of the function foobar()
 * that might be useful to those using or modifying it.  Begins with
 * empty comment line, and may include additional embedded empty
 * comment lines.
 *
 * The longer description can have multiple paragraphs.
 *
 * Return: Describe the return value of foobar.
 */

The short description following the subject can span multiple lines
and ends with an @argument description, an empty line or the end of
the comment block.

The @argument descriptions must begin on the very next line following
this opening short function description line, with no intervening
empty comment lines.

If a function parameter is "..." (varargs), it should be listed in
kernel-doc notation as:
 * @...: description

The return value, if any, should be described in a dedicated section
named "Return".

Example kernel-doc data structure comment.

/**
 * struct blah - the basic blah structure
 * @mem1:	describe the first member of struct blah
 * @mem2:	describe the second member of struct blah,
 *		perhaps with more lines and words.
 *
 * Longer description of this structure.
 */

The kernel-doc function comments describe each parameter to the
function, in order, with the @name lines.

The kernel-doc data structure comments describe each structure member
in the data structure, with the @name lines.

The longer description formatting is "reflowed", losing your line
breaks.  So presenting carefully formatted lists within these
descriptions won't work so well; derived documentation will lose
the formatting.

See the section below "How to add extractable documentation to your
source files" for more details and notes on how to format kernel-doc
comments.

Components of the kernel-doc system
-----------------------------------

Many places in the source tree have extractable documentation in the
form of block comments above functions.  The components of this system
are:

- scripts/kernel-doc

  This is a perl script that hunts for the block comments and can mark
  them up directly into DocBook, man, text, and HTML. (No, not
  texinfo.)

- Documentation/DocBook/*.tmpl

  These are SGML template files, which are normal SGML files with
  special place-holders for where the extracted documentation should
  go.

- scripts/basic/docproc.c

  This is a program for converting SGML template files into SGML
  files. When a file is referenced it is searched for symbols
  exported (EXPORT_SYMBOL), to be able to distinguish between internal
  and external functions.
  It invokes kernel-doc, giving it the list of functions that
  are to be documented.
  Additionally it is used to scan the SGML template files to locate
  all the files referenced herein. This is used to generate dependency
  information as used by make.

- Makefile

  The targets 'sgmldocs', 'psdocs', 'pdfdocs', and 'htmldocs' are used
  to build DocBook files, PostScript files, PDF files, and html files
  in Documentation/DocBook.

- Documentation/DocBook/Makefile

  This is where C files are associated with SGML templates.


How to extract the documentation
--------------------------------

If you just want to read the ready-made books on the various
subsystems (see Documentation/DocBook/*.tmpl), just type 'make
psdocs', or 'make pdfdocs', or 'make htmldocs', depending on your
preference.  If you would rather read a different format, you can type
'make sgmldocs' and then use DocBook tools to convert
Documentation/DocBook/*.sgml to a format of your choice (for example,
'db2html ...' if 'make htmldocs' was not defined).

If you want to see man pages instead, you can do this:

$ cd linux
$ scripts/kernel-doc -man $(find -name '*.c') | split-man.pl /tmp/man
$ scripts/kernel-doc -man $(find -name '*.h') | split-man.pl /tmp/man

Here is split-man.pl:

-->
#!/usr/bin/perl

if ($#ARGV < 0) {
   die "where do I put the results?\n";
}

mkdir $ARGV[0],0777;
$state = 0;
while (<STDIN>) {
    if (/^\.TH \"[^\"]*\" 9 \"([^\"]*)\"/) {
	if ($state == 1) { close OUT }
	$state = 1;
	$fn = "$ARGV[0]/$1.9";
	print STDERR "Creating $fn\n";
	open OUT, ">$fn" or die "can't open $fn: $!\n";
	print OUT $_;
    } elsif ($state != 0) {
	print OUT $_;
    }
}

close OUT;
<--

If you just want to view the documentation for one function in one
file, you can do this:

$ scripts/kernel-doc -man -function fn file | nroff -man | less

or this:

$ scripts/kernel-doc -text -function fn file


How to add extractable documentation to your source files
---------------------------------------------------------

The format of the block comment is like this:

/**
 * function_name(:)? (- short description)?
(* @parameterx(space)*: (description of parameter x)?)*
(* a blank line)?
 * (Description:)? (Description of function)?
 * (section header: (section description)? )*
(*)?*/

All "description" text can span multiple lines, although the
function_name & its short description are traditionally on a single line.
Description text may also contain blank lines (i.e., lines that contain
only a "*").

"section header:" names must be unique per function (or struct,
union, typedef, enum).

Use the section header "Return" for sections describing the return value
of a function.

Avoid putting a spurious blank line after the function name, or else the
description will be repeated!

All descriptive text is further processed, scanning for the following special
patterns, which are highlighted appropriately.

'funcname()' - function
'$ENVVAR' - environment variable
'&struct_name' - name of a structure (up to two words including 'struct')
'@parameter' - name of a parameter
'%CONST' - name of a constant.

NOTE 1:  The multi-line descriptive text you provide does *not* recognize
line breaks, so if you try to format some text nicely, as in:

  Return:
    0 - cool
    1 - invalid arg
    2 - out of memory

this will all run together and produce:

  Return: 0 - cool 1 - invalid arg 2 - out of memory

NOTE 2:  If the descriptive text you provide has lines that begin with
some phrase followed by a colon, each of those phrases will be taken as
a new section heading, which means you should similarly try to avoid text
like:

  Return:
    0: cool
    1: invalid arg
    2: out of memory

every line of which would start a new section.  Again, probably not
what you were after.

Take a look around the source tree for examples.


kernel-doc for structs, unions, enums, and typedefs
---------------------------------------------------

Beside functions you can also write documentation for structs, unions,
enums and typedefs. Instead of the function name you must write the name
of the declaration;  the struct/union/enum/typedef must always precede
the name. Nesting of declarations is not supported.
Use the argument mechanism to document members or constants.

Inside a struct description, you can use the "private:" and "public:"
comment tags.  Structure fields that are inside a "private:" area
are not listed in the generated output documentation.  The "private:"
and "public:" tags must begin immediately following a "/*" comment
marker.  They may optionally include comments between the ":" and the
ending "*/" marker.

Example:

/**
 * struct my_struct - short description
 * @a: first member
 * @b: second member
 *
 * Longer description
 */
struct my_struct {
    int a;
    int b;
/* private: internal use only */
    int c;
};


Including documentation blocks in source files
----------------------------------------------

To facilitate having source code and comments close together, you can
include kernel-doc documentation blocks that are free-form comments
instead of being kernel-doc for functions, structures, unions,
enums, or typedefs.  This could be used for something like a
theory of operation for a driver or library code, for example.

This is done by using a DOC: section keyword with a section title.  E.g.:

/**
 * DOC: Theory of Operation
 *
 * The whizbang foobar is a dilly of a gizmo.  It can do whatever you
 * want it to do, at any time.  It reads your mind.  Here's how it works.
 *
 * foo bar splat
 *
 * The only drawback to this gizmo is that is can sometimes damage
 * hardware, software, or its subject(s).
 */

DOC: sections are used in SGML templates files as indicated below.


How to make new SGML template files
-----------------------------------

SGML template files (*.tmpl) are like normal SGML files, except that
they can contain escape sequences where extracted documentation should
be inserted.

!E<filename> is replaced by the documentation, in <filename>, for
functions that are exported using EXPORT_SYMBOL: the function list is
collected from files listed in Documentation/DocBook/Makefile.

!I<filename> is replaced by the documentation for functions that are
_not_ exported using EXPORT_SYMBOL.

!D<filename> is used to name additional files to search for functions
exported using EXPORT_SYMBOL.

!F<filename> <function [functions...]> is replaced by the
documentation, in <filename>, for the functions listed.

!P<filename> <section title> is replaced by the contents of the DOC:
section titled <section title> from <filename>.
Spaces are allowed in <section title>; do not quote the <section title>.

!C<filename> is replaced by nothing, but makes the tools check that
all DOC: sections and documented functions, symbols, etc. are used.
This makes sense to use when you use !F/!P only and want to verify
that all documentation is included.

Tim.
*/ <twaugh@redhat.com>