aboutsummaryrefslogtreecommitdiffstats
blob: 54f10478e8e30ccda77da9d345c01b9ace781e07 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
This file documents how to use memory mapped I/O with netlink.

Author: Patrick McHardy <kaber@trash.net>

Overview
--------

Memory mapped netlink I/O can be used to increase throughput and decrease
overhead of unicast receive and transmit operations. Some netlink subsystems
require high throughput, these are mainly the netfilter subsystems
nfnetlink_queue and nfnetlink_log, but it can also help speed up large
dump operations of f.i. the routing database.

Memory mapped netlink I/O used two circular ring buffers for RX and TX which
are mapped into the processes address space.

The RX ring is used by the kernel to directly construct netlink messages into
user-space memory without copying them as done with regular socket I/O,
additionally as long as the ring contains messages no recvmsg() or poll()
syscalls have to be issued by user-space to get more message.

The TX ring is used to process messages directly from user-space memory, the
kernel processes all messages contained in the ring using a single sendmsg()
call.

Usage overview
--------------

In order to use memory mapped netlink I/O, user-space needs three main changes:

- ring setup
- conversion of the RX path to get messages from the ring instead of recvmsg()
- conversion of the TX path to construct messages into the ring

Ring setup is done using setsockopt() to provide the ring parameters to the
kernel, then a call to mmap() to map the ring into the processes address space:

- setsockopt(fd, SOL_NETLINK, NETLINK_RX_RING, &params, sizeof(params));
- setsockopt(fd, SOL_NETLINK, NETLINK_TX_RING, &params, sizeof(params));
- ring = mmap(NULL, size, PROT_READ | PROT_WRITE, MAP_SHARED, fd, 0)

Usage of either ring is optional, but even if only the RX ring is used the
mapping still needs to be writable in order to update the frame status after
processing.

Conversion of the reception path involves calling poll() on the file
descriptor, once the socket is readable the frames from the ring are
processed in order until no more messages are available, as indicated by
a status word in the frame header.

On kernel side, in order to make use of memory mapped I/O on receive, the
originating netlink subsystem needs to support memory mapped I/O, otherwise
it will use an allocated socket buffer as usual and the contents will be
 copied to the ring on transmission, nullifying most of the performance gains.
Dumps of kernel databases automatically support memory mapped I/O.

Conversion of the transmit path involves changing message construction to
use memory from the TX ring instead of (usually) a buffer declared on the
stack and setting up the frame header appropriately. Optionally poll() can
be used to wait for free frames in the TX ring.

Structured and definitions for using memory mapped I/O are contained in
<linux/netlink.h>.

RX and TX rings
----------------

Each ring contains a number of continuous memory blocks, containing frames of
fixed size dependent on the parameters used for ring setup.

Ring:	[ block 0 ]
		[ frame 0 ]
		[ frame 1 ]
	[ block 1 ]
		[ frame 2 ]
		[ frame 3 ]
	...
	[ block n ]
		[ frame 2 * n ]
		[ frame 2 * n + 1 ]

The blocks are only visible to the kernel, from the point of view of user-space
the ring just contains the frames in a continuous memory zone.

The ring parameters used for setting up the ring are defined as follows:

struct nl_mmap_req {
	unsigned int	nm_block_size;
	unsigned int	nm_block_nr;
	unsigned int	nm_frame_size;
	unsigned int	nm_frame_nr;
};

Frames are grouped into blocks, where each block is a continuous region of memory
and holds nm_block_size / nm_frame_size frames. The total number of frames in
the ring is nm_frame_nr. The following invariants hold:

- frames_per_block = nm_block_size / nm_frame_size

- nm_frame_nr = frames_per_block * nm_block_nr

Some parameters are constrained, specifically:

- nm_block_size must be a multiple of the architectures memory page size.
  The getpagesize() function can be used to get the page size.

- nm_frame_size must be equal or larger to NL_MMAP_HDRLEN, IOW a frame must be
  able to hold at least the frame header

- nm_frame_size must be smaller or equal to nm_block_size

- nm_frame_size must be a multiple of NL_MMAP_MSG_ALIGNMENT

- nm_frame_nr must equal the actual number of frames as specified above.

When the kernel can't allocate physically continuous memory for a ring block,
it will fall back to use physically discontinuous memory. This might affect
performance negatively, in order to avoid this the nm_frame_size parameter
should be chosen to be as small as possible for the required frame size and
the number of blocks should be increased instead.

Ring frames
------------

Each frames contain a frame header, consisting of a synchronization word and some
meta-data, and the message itself.

Frame:	[ header message ]

The frame header is defined as follows:

struct nl_mmap_hdr {
	unsigned int	nm_status;
	unsigned int	nm_len;
	__u32		nm_group;
	/* credentials */
	__u32		nm_pid;
	__u32		nm_uid;
	__u32		nm_gid;
};

- nm_status is used for synchronizing processing between the kernel and user-
  space and specifies ownership of the frame as well as the operation to perform

- nm_len contains the length of the message contained in the data area

- nm_group specified the destination multicast group of message

- nm_pid, nm_uid and nm_gid contain the netlink pid, UID and GID of the sending
  process. These values correspond to the data available using SOCK_PASSCRED in
  the SCM_CREDENTIALS cmsg.

The possible values in the status word are:

- NL_MMAP_STATUS_UNUSED:
	RX ring:	frame belongs to the kernel and contains no message
			for user-space. Approriate action is to invoke poll()
			to wait for new messages.

	TX ring:	frame belongs to user-space and can be used for
			message construction.

- NL_MMAP_STATUS_RESERVED:
	RX ring only:	frame is currently used by the kernel for message
			construction and contains no valid message yet.
			Appropriate action is to invoke poll() to wait for
			new messages.

- NL_MMAP_STATUS_VALID:
	RX ring:	frame contains a valid message. Approriate action is
			to process the message and release the frame back to
			the kernel by setting the status to
			NL_MMAP_STATUS_UNUSED or queue the frame by setting the
			status to NL_MMAP_STATUS_SKIP.

	TX ring:	the frame contains a valid message from user-space to
			be processed by the kernel. After completing processing
			the kernel will release the frame back to user-space by
			setting the status to NL_MMAP_STATUS_UNUSED.

- NL_MMAP_STATUS_COPY:
	RX ring only:	a message is ready to be processed but could not be
			stored in the ring, either because it exceeded the
			frame size or because the originating subsystem does
			not support memory mapped I/O. Appropriate action is
			to invoke recvmsg() to receive the message and release
			the frame back to the kernel by setting the status to
			NL_MMAP_STATUS_UNUSED.

- NL_MMAP_STATUS_SKIP:
	RX ring only:	user-space queued the message for later processing, but
			processed some messages following it in the ring. The
			kernel should skip this frame when looking for unused
			frames.

The data area of a frame begins at a offset of NL_MMAP_HDRLEN relative to the
frame header.

TX limitations
--------------

As of Jan 2015 the message is always copied from the ring frame to an
allocated buffer due to unresolved security concerns.
See commit 4682a0358639b29cf ("netlink: Always copy on mmap TX.").

Example
-------

Ring setup:

	unsigned int block_size = 16 * getpagesize();
	struct nl_mmap_req req = {
		.nm_block_size		= block_size,
		.nm_block_nr		= 64,
		.nm_frame_size		= 16384,
		.nm_frame_nr		= 64 * block_size / 16384,
	};
	unsigned int ring_size;
	void *rx_ring, *tx_ring;

	/* Configure ring parameters */
	if (setsockopt(fd, SOL_NETLINK, NETLINK_RX_RING, &req, sizeof(req)) < 0)
		exit(1);
	if (setsockopt(fd, SOL_NETLINK, NETLINK_TX_RING, &req, sizeof(req)) < 0)
		exit(1)

	/* Calculate size of each individual ring */
	ring_size = req.nm_block_nr * req.nm_block_size;

	/* Map RX/TX rings. The TX ring is located after the RX ring */
	rx_ring = mmap(NULL, 2 * ring_size, PROT_READ | PROT_WRITE,
		       MAP_SHARED, fd, 0);
	if ((long)rx_ring == -1L)
		exit(1);
	tx_ring = rx_ring + ring_size:

Message reception:

This example assumes some ring parameters of the ring setup are available.

	unsigned int frame_offset = 0;
	struct nl_mmap_hdr *hdr;
	struct nlmsghdr *nlh;
	unsigned char buf[16384];
	ssize_t len;

	while (1) {
		struct pollfd pfds[1];

		pfds[0].fd	= fd;
		pfds[0].events	= POLLIN | POLLERR;
		pfds[0].revents	= 0;

		if (poll(pfds, 1, -1) < 0 && errno != -EINTR)
			exit(1);

		/* Check for errors. Error handling omitted */
		if (pfds[0].revents & POLLERR)
			<handle error>

		/* If no new messages, poll again */
		if (!(pfds[0].revents & POLLIN))
			continue;

		/* Process all frames */
		while (1) {
			/* Get next frame header */
			hdr = rx_ring + frame_offset;

			if (hdr->nm_status == NL_MMAP_STATUS_VALID) {
				/* Regular memory mapped frame */
				nlh = (void *)hdr + NL_MMAP_HDRLEN;
				len = hdr->nm_len;

				/* Release empty message immediately. May happen
				 * on error during message construction.
				 */
				if (len == 0)
					goto release;
			} else if (hdr->nm_status == NL_MMAP_STATUS_COPY) {
				/* Frame queued to socket receive queue */
				len = recv(fd, buf, sizeof(buf), MSG_DONTWAIT);
				if (len <= 0)
					break;
				nlh = buf;
			} else
				/* No more messages to process, continue polling */
				break;

			process_msg(nlh);
release:
			/* Release frame back to the kernel */
			hdr->nm_status = NL_MMAP_STATUS_UNUSED;

			/* Advance frame offset to next frame */
			frame_offset = (frame_offset + frame_size) % ring_size;
		}
	}

Message transmission:

This example assumes some ring parameters of the ring setup are available.
A single message is constructed and transmitted, to send multiple messages
at once they would be constructed in consecutive frames before a final call
to sendto().

	unsigned int frame_offset = 0;
	struct nl_mmap_hdr *hdr;
	struct nlmsghdr *nlh;
	struct sockaddr_nl addr = {
		.nl_family	= AF_NETLINK,
	};

	hdr = tx_ring + frame_offset;
	if (hdr->nm_status != NL_MMAP_STATUS_UNUSED)
		/* No frame available. Use poll() to avoid. */
		exit(1);

	nlh = (void *)hdr + NL_MMAP_HDRLEN;

	/* Build message */
	build_message(nlh);

	/* Fill frame header: length and status need to be set */
	hdr->nm_len	= nlh->nlmsg_len;
	hdr->nm_status	= NL_MMAP_STATUS_VALID;

	if (sendto(fd, NULL, 0, 0, &addr, sizeof(addr)) < 0)
		exit(1);

	/* Advance frame offset to next frame */
	frame_offset = (frame_offset + frame_size) % ring_size;