aboutsummaryrefslogtreecommitdiffstats
blob: 4abe83e1045a4b38e85b05ebfeb3e8e62841a7f6 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
402
403
404
405
406
407
408
409
410
411
412
413
414
415
416
417
418
419
420
421
422
423
424
425
426
427
428
429
430
431
432
433
434
435
436
437
438
439
440
441
442
443
444
445
446
447
448
449
450
451
452
453
454
455
456
457
458
459
460
461
462
463
464
465
466
467
468
469
470
471
472
473
474
475
476
477
478
479
480
481
482
483
484
485
486
487
488
489
490
491
492
493
494
495
496
497
498
499
500
501
502
503
504
505
506
507
508
509
510
511
512
513
514
515
516
517
518
519
520
521
522
523
524
525
526
527
528
529
530
531
532
533
534
535
536
537
538
539
540
541
542
543
544
545
546
547
548
549
550
551
552
553
554
555
556
557
558
559
560
561
562
563
564
565
566
567
568
569
570
571
572
573
574
575
576
577
578
579
580
581
582
583
584
585
586
587
588
589
590
591
592
593
594
595
596
597
598
599
600
601
602
603
604
605
606
607
608
609
610
611
612
613
614
615
616
617
618
619
620
621
622
623
624
625
626
627
628
629
630
631
632
633
634
635
636
637
638
639
640
641
642
643
644
645
646
647
648
649
650
651
652
653
654
655
656
657
658
659
660
661
662
663
664
665
666
667
668
669
670
671
672
673
674
675
676
677
678
679
680
681
682
683
684
685
686
687
688
689
690
691
692
693
694
695
696
697
698
699
700
701
702
703
704
705
706
707
708
709
710
711
712
713
714
715
716
717
718
719
720
721
722
723
724
725
726
727
728
729
730
731
732
733
734
735
736
737
738
739
740
741
742
743
744
745
746
747
748
749
750
751
752
753
754
755
756
757
758
759
760
761
762
763
764
765
766
767
768
769
770
771
772
773
774
775
776
777
778
779
780
781
782
783
784
785
786
787
788
789
790
791
792
793
794
795
796
797
798
799
800
801
802
803
804
805
806
807
808
809
810
811
812
813
814
815
816
817
818
819
820
821
822
823
824
825
826
827
828
829
830
831
832
833
834
835
836
837
838
839
840
841
842
843
844
845
846
847
848
849
850
851
852
853
854
855
856
857
858
859
860
861
862
863
864
865
866
867
868
869
870
871
872
873
874
875
876
877
878
879
880
881
882
883
884
885
886
887
Runtime Power Management Framework for I/O Devices

(C) 2009-2011 Rafael J. Wysocki <rjw@sisk.pl>, Novell Inc.
(C) 2010 Alan Stern <stern@rowland.harvard.edu>

1. Introduction

Support for runtime power management (runtime PM) of I/O devices is provided
at the power management core (PM core) level by means of:

* The power management workqueue pm_wq in which bus types and device drivers can
  put their PM-related work items.  It is strongly recommended that pm_wq be
  used for queuing all work items related to runtime PM, because this allows
  them to be synchronized with system-wide power transitions (suspend to RAM,
  hibernation and resume from system sleep states).  pm_wq is declared in
  include/linux/pm_runtime.h and defined in kernel/power/main.c.

* A number of runtime PM fields in the 'power' member of 'struct device' (which
  is of the type 'struct dev_pm_info', defined in include/linux/pm.h) that can
  be used for synchronizing runtime PM operations with one another.

* Three device runtime PM callbacks in 'struct dev_pm_ops' (defined in
  include/linux/pm.h).

* A set of helper functions defined in drivers/base/power/runtime.c that can be
  used for carrying out runtime PM operations in such a way that the
  synchronization between them is taken care of by the PM core.  Bus types and
  device drivers are encouraged to use these functions.

The runtime PM callbacks present in 'struct dev_pm_ops', the device runtime PM
fields of 'struct dev_pm_info' and the core helper functions provided for
runtime PM are described below.

2. Device Runtime PM Callbacks

There are three device runtime PM callbacks defined in 'struct dev_pm_ops':

struct dev_pm_ops {
	...
	int (*runtime_suspend)(struct device *dev);
	int (*runtime_resume)(struct device *dev);
	int (*runtime_idle)(struct device *dev);
	...
};

The ->runtime_suspend(), ->runtime_resume() and ->runtime_idle() callbacks
are executed by the PM core for the device's subsystem that may be either of
the following:

  1. PM domain of the device, if the device's PM domain object, dev->pm_domain,
     is present.

  2. Device type of the device, if both dev->type and dev->type->pm are present.

  3. Device class of the device, if both dev->class and dev->class->pm are
     present.

  4. Bus type of the device, if both dev->bus and dev->bus->pm are present.

If the subsystem chosen by applying the above rules doesn't provide the relevant
callback, the PM core will invoke the corresponding driver callback stored in
dev->driver->pm directly (if present).

The PM core always checks which callback to use in the order given above, so the
priority order of callbacks from high to low is: PM domain, device type, class
and bus type.  Moreover, the high-priority one will always take precedence over
a low-priority one.  The PM domain, bus type, device type and class callbacks
are referred to as subsystem-level callbacks in what follows.

By default, the callbacks are always invoked in process context with interrupts
enabled.  However, the pm_runtime_irq_safe() helper function can be used to tell
the PM core that it is safe to run the ->runtime_suspend(), ->runtime_resume()
and ->runtime_idle() callbacks for the given device in atomic context with
interrupts disabled.  This implies that the callback routines in question must
not block or sleep, but it also means that the synchronous helper functions
listed at the end of Section 4 may be used for that device within an interrupt
handler or generally in an atomic context.

The subsystem-level suspend callback, if present, is _entirely_ _responsible_
for handling the suspend of the device as appropriate, which may, but need not
include executing the device driver's own ->runtime_suspend() callback (from the
PM core's point of view it is not necessary to implement a ->runtime_suspend()
callback in a device driver as long as the subsystem-level suspend callback
knows what to do to handle the device).

  * Once the subsystem-level suspend callback (or the driver suspend callback,
    if invoked directly) has completed successfully for the given device, the PM
    core regards the device as suspended, which need not mean that it has been
    put into a low power state.  It is supposed to mean, however, that the
    device will not process data and will not communicate with the CPU(s) and
    RAM until the appropriate resume callback is executed for it.  The runtime
    PM status of a device after successful execution of the suspend callback is
    'suspended'.

  * If the suspend callback returns -EBUSY or -EAGAIN, the device's runtime PM
    status remains 'active', which means that the device _must_ be fully
    operational afterwards.

  * If the suspend callback returns an error code different from -EBUSY and
    -EAGAIN, the PM core regards this as a fatal error and will refuse to run
    the helper functions described in Section 4 for the device until its status
    is directly set to  either'active', or 'suspended' (the PM core provides
    special helper functions for this purpose).

In particular, if the driver requires remote wakeup capability (i.e. hardware
mechanism allowing the device to request a change of its power state, such as
PCI PME) for proper functioning and device_run_wake() returns 'false' for the
device, then ->runtime_suspend() should return -EBUSY.  On the other hand, if
device_run_wake() returns 'true' for the device and the device is put into a
low-power state during the execution of the suspend callback, it is expected
that remote wakeup will be enabled for the device.  Generally, remote wakeup
should be enabled for all input devices put into low-power states at run time.

The subsystem-level resume callback, if present, is _entirely_ _responsible_ for
handling the resume of the device as appropriate, which may, but need not
include executing the device driver's own ->runtime_resume() callback (from the
PM core's point of view it is not necessary to implement a ->runtime_resume()
callback in a device driver as long as the subsystem-level resume callback knows
what to do to handle the device).

  * Once the subsystem-level resume callback (or the driver resume callback, if
    invoked directly) has completed successfully, the PM core regards the device
    as fully operational, which means that the device _must_ be able to complete
    I/O operations as needed.  The runtime PM status of the device is then
    'active'.

  * If the resume callback returns an error code, the PM core regards this as a
    fatal error and will refuse to run the helper functions described in Section
    4 for the device, until its status is directly set to either 'active', or
    'suspended' (by means of special helper functions provided by the PM core
    for this purpose).

The idle callback (a subsystem-level one, if present, or the driver one) is
executed by the PM core whenever the device appears to be idle, which is
indicated to the PM core by two counters, the device's usage counter and the
counter of 'active' children of the device.

  * If any of these counters is decreased using a helper function provided by
    the PM core and it turns out to be equal to zero, the other counter is
    checked.  If that counter also is equal to zero, the PM core executes the
    idle callback with the device as its argument.

The action performed by the idle callback is totally dependent on the subsystem
(or driver) in question, but the expected and recommended action is to check
if the device can be suspended (i.e. if all of the conditions necessary for
suspending the device are satisfied) and to queue up a suspend request for the
device in that case.  The value returned by this callback is ignored by the PM
core.

The helper functions provided by the PM core, described in Section 4, guarantee
that the following constraints are met with respect to runtime PM callbacks for
one device:

(1) The callbacks are mutually exclusive (e.g. it is forbidden to execute
    ->runtime_suspend() in parallel with ->runtime_resume() or with another
    instance of ->runtime_suspend() for the same device) with the exception that
    ->runtime_suspend() or ->runtime_resume() can be executed in parallel with
    ->runtime_idle() (although ->runtime_idle() will not be started while any
    of the other callbacks is being executed for the same device).

(2) ->runtime_idle() and ->runtime_suspend() can only be executed for 'active'
    devices (i.e. the PM core will only execute ->runtime_idle() or
    ->runtime_suspend() for the devices the runtime PM status of which is
    'active').

(3) ->runtime_idle() and ->runtime_suspend() can only be executed for a device
    the usage counter of which is equal to zero _and_ either the counter of
    'active' children of which is equal to zero, or the 'power.ignore_children'
    flag of which is set.

(4) ->runtime_resume() can only be executed for 'suspended' devices  (i.e. the
    PM core will only execute ->runtime_resume() for the devices the runtime
    PM status of which is 'suspended').

Additionally, the helper functions provided by the PM core obey the following
rules:

  * If ->runtime_suspend() is about to be executed or there's a pending request
    to execute it, ->runtime_idle() will not be executed for the same device.

  * A request to execute or to schedule the execution of ->runtime_suspend()
    will cancel any pending requests to execute ->runtime_idle() for the same
    device.

  * If ->runtime_resume() is about to be executed or there's a pending request
    to execute it, the other callbacks will not be executed for the same device.

  * A request to execute ->runtime_resume() will cancel any pending or
    scheduled requests to execute the other callbacks for the same device,
    except for scheduled autosuspends.

3. Runtime PM Device Fields

The following device runtime PM fields are present in 'struct dev_pm_info', as
defined in include/linux/pm.h:

  struct timer_list suspend_timer;
    - timer used for scheduling (delayed) suspend and autosuspend requests

  unsigned long timer_expires;
    - timer expiration time, in jiffies (if this is different from zero, the
      timer is running and will expire at that time, otherwise the timer is not
      running)

  struct work_struct work;
    - work structure used for queuing up requests (i.e. work items in pm_wq)

  wait_queue_head_t wait_queue;
    - wait queue used if any of the helper functions needs to wait for another
      one to complete

  spinlock_t lock;
    - lock used for synchronisation

  atomic_t usage_count;
    - the usage counter of the device

  atomic_t child_count;
    - the count of 'active' children of the device

  unsigned int ignore_children;
    - if set, the value of child_count is ignored (but still updated)

  unsigned int disable_depth;
    - used for disabling the helper funcions (they work normally if this is
      equal to zero); the initial value of it is 1 (i.e. runtime PM is
      initially disabled for all devices)

  unsigned int runtime_error;
    - if set, there was a fatal error (one of the callbacks returned error code
      as described in Section 2), so the helper funtions will not work until
      this flag is cleared; this is the error code returned by the failing
      callback

  unsigned int idle_notification;
    - if set, ->runtime_idle() is being executed

  unsigned int request_pending;
    - if set, there's a pending request (i.e. a work item queued up into pm_wq)

  enum rpm_request request;
    - type of request that's pending (valid if request_pending is set)

  unsigned int deferred_resume;
    - set if ->runtime_resume() is about to be run while ->runtime_suspend() is
      being executed for that device and it is not practical to wait for the
      suspend to complete; means "start a resume as soon as you've suspended"

  unsigned int run_wake;
    - set if the device is capable of generating runtime wake-up events

  enum rpm_status runtime_status;
    - the runtime PM status of the device; this field's initial value is
      RPM_SUSPENDED, which means that each device is initially regarded by the
      PM core as 'suspended', regardless of its real hardware status

  unsigned int runtime_auto;
    - if set, indicates that the user space has allowed the device driver to
      power manage the device at run time via the /sys/devices/.../power/control
      interface; it may only be modified with the help of the pm_runtime_allow()
      and pm_runtime_forbid() helper functions

  unsigned int no_callbacks;
    - indicates that the device does not use the runtime PM callbacks (see
      Section 8); it may be modified only by the pm_runtime_no_callbacks()
      helper function

  unsigned int irq_safe;
    - indicates that the ->runtime_suspend() and ->runtime_resume() callbacks
      will be invoked with the spinlock held and interrupts disabled

  unsigned int use_autosuspend;
    - indicates that the device's driver supports delayed autosuspend (see
      Section 9); it may be modified only by the
      pm_runtime{_dont}_use_autosuspend() helper functions

  unsigned int timer_autosuspends;
    - indicates that the PM core should attempt to carry out an autosuspend
      when the timer expires rather than a normal suspend

  int autosuspend_delay;
    - the delay time (in milliseconds) to be used for autosuspend

  unsigned long last_busy;
    - the time (in jiffies) when the pm_runtime_mark_last_busy() helper
      function was last called for this device; used in calculating inactivity
      periods for autosuspend

All of the above fields are members of the 'power' member of 'struct device'.

4. Runtime PM Device Helper Functions

The following runtime PM helper functions are defined in
drivers/base/power/runtime.c and include/linux/pm_runtime.h:

  void pm_runtime_init(struct device *dev);
    - initialize the device runtime PM fields in 'struct dev_pm_info'

  void pm_runtime_remove(struct device *dev);
    - make sure that the runtime PM of the device will be disabled after
      removing the device from device hierarchy

  int pm_runtime_idle(struct device *dev);
    - execute the subsystem-level idle callback for the device; returns 0 on
      success or error code on failure, where -EINPROGRESS means that
      ->runtime_idle() is already being executed

  int pm_runtime_suspend(struct device *dev);
    - execute the subsystem-level suspend callback for the device; returns 0 on
      success, 1 if the device's runtime PM status was already 'suspended', or
      error code on failure, where -EAGAIN or -EBUSY means it is safe to attempt
      to suspend the device again in future and -EACCES means that
      'power.disable_depth' is different from 0

  int pm_runtime_autosuspend(struct device *dev);
    - same as pm_runtime_suspend() except that the autosuspend delay is taken
      into account; if pm_runtime_autosuspend_expiration() says the delay has
      not yet expired then an autosuspend is scheduled for the appropriate time
      and 0 is returned

  int pm_runtime_resume(struct device *dev);
    - execute the subsystem-level resume callback for the device; returns 0 on
      success, 1 if the device's runtime PM status was already 'active' or
      error code on failure, where -EAGAIN means it may be safe to attempt to
      resume the device again in future, but 'power.runtime_error' should be
      checked additionally, and -EACCES means that 'power.disable_depth' is
      different from 0

  int pm_request_idle(struct device *dev);
    - submit a request to execute the subsystem-level idle callback for the
      device (the request is represented by a work item in pm_wq); returns 0 on
      success or error code if the request has not been queued up

  int pm_request_autosuspend(struct device *dev);
    - schedule the execution of the subsystem-level suspend callback for the
      device when the autosuspend delay has expired; if the delay has already
      expired then the work item is queued up immediately

  int pm_schedule_suspend(struct device *dev, unsigned int delay);
    - schedule the execution of the subsystem-level suspend callback for the
      device in future, where 'delay' is the time to wait before queuing up a
      suspend work item in pm_wq, in milliseconds (if 'delay' is zero, the work
      item is queued up immediately); returns 0 on success, 1 if the device's PM
      runtime status was already 'suspended', or error code if the request
      hasn't been scheduled (or queued up if 'delay' is 0); if the execution of
      ->runtime_suspend() is already scheduled and not yet expired, the new
      value of 'delay' will be used as the time to wait

  int pm_request_resume(struct device *dev);
    - submit a request to execute the subsystem-level resume callback for the
      device (the request is represented by a work item in pm_wq); returns 0 on
      success, 1 if the device's runtime PM status was already 'active', or
      error code if the request hasn't been queued up

  void pm_runtime_get_noresume(struct device *dev);
    - increment the device's usage counter

  int pm_runtime_get(struct device *dev);
    - increment the device's usage counter, run pm_request_resume(dev) and
      return its result

  int pm_runtime_get_sync(struct device *dev);
    - increment the device's usage counter, run pm_runtime_resume(dev) and
      return its result

  void pm_runtime_put_noidle(struct device *dev);
    - decrement the device's usage counter

  int pm_runtime_put(struct device *dev);
    - decrement the device's usage counter; if the result is 0 then run
      pm_request_idle(dev) and return its result

  int pm_runtime_put_autosuspend(struct device *dev);
    - decrement the device's usage counter; if the result is 0 then run
      pm_request_autosuspend(dev) and return its result

  int pm_runtime_put_sync(struct device *dev);
    - decrement the device's usage counter; if the result is 0 then run
      pm_runtime_idle(dev) and return its result

  int pm_runtime_put_sync_suspend(struct device *dev);
    - decrement the device's usage counter; if the result is 0 then run
      pm_runtime_suspend(dev) and return its result

  int pm_runtime_put_sync_autosuspend(struct device *dev);
    - decrement the device's usage counter; if the result is 0 then run
      pm_runtime_autosuspend(dev) and return its result

  void pm_runtime_enable(struct device *dev);
    - decrement the device's 'power.disable_depth' field; if that field is equal
      to zero, the runtime PM helper functions can execute subsystem-level
      callbacks described in Section 2 for the device

  int pm_runtime_disable(struct device *dev);
    - increment the device's 'power.disable_depth' field (if the value of that
      field was previously zero, this prevents subsystem-level runtime PM
      callbacks from being run for the device), make sure that all of the pending
      runtime PM operations on the device are either completed or canceled;
      returns 1 if there was a resume request pending and it was necessary to
      execute the subsystem-level resume callback for the device to satisfy that
      request, otherwise 0 is returned

  int pm_runtime_barrier(struct device *dev);
    - check if there's a resume request pending for the device and resume it
      (synchronously) in that case, cancel any other pending runtime PM requests
      regarding it and wait for all runtime PM operations on it in progress to
      complete; returns 1 if there was a resume request pending and it was
      necessary to execute the subsystem-level resume callback for the device to
      satisfy that request, otherwise 0 is returned

  void pm_suspend_ignore_children(struct device *dev, bool enable);
    - set/unset the power.ignore_children flag of the device

  int pm_runtime_set_active(struct device *dev);
    - clear the device's 'power.runtime_error' flag, set the device's runtime
      PM status to 'active' and update its parent's counter of 'active'
      children as appropriate (it is only valid to use this function if
      'power.runtime_error' is set or 'power.disable_depth' is greater than
      zero); it will fail and return error code if the device has a parent
      which is not active and the 'power.ignore_children' flag of which is unset

  void pm_runtime_set_suspended(struct device *dev);
    - clear the device's 'power.runtime_error' flag, set the device's runtime
      PM status to 'suspended' and update its parent's counter of 'active'
      children as appropriate (it is only valid to use this function if
      'power.runtime_error' is set or 'power.disable_depth' is greater than
      zero)

  bool pm_runtime_suspended(struct device *dev);
    - return true if the device's runtime PM status is 'suspended' and its
      'power.disable_depth' field is equal to zero, or false otherwise

  bool pm_runtime_status_suspended(struct device *dev);
    - return true if the device's runtime PM status is 'suspended'

  void pm_runtime_allow(struct device *dev);
    - set the power.runtime_auto flag for the device and decrease its usage
      counter (used by the /sys/devices/.../power/control interface to
      effectively allow the device to be power managed at run time)

  void pm_runtime_forbid(struct device *dev);
    - unset the power.runtime_auto flag for the device and increase its usage
      counter (used by the /sys/devices/.../power/control interface to
      effectively prevent the device from being power managed at run time)

  void pm_runtime_no_callbacks(struct device *dev);
    - set the power.no_callbacks flag for the device and remove the runtime
      PM attributes from /sys/devices/.../power (or prevent them from being
      added when the device is registered)

  void pm_runtime_irq_safe(struct device *dev);
    - set the power.irq_safe flag for the device, causing the runtime-PM
      callbacks to be invoked with interrupts off

  void pm_runtime_mark_last_busy(struct device *dev);
    - set the power.last_busy field to the current time

  void pm_runtime_use_autosuspend(struct device *dev);
    - set the power.use_autosuspend flag, enabling autosuspend delays

  void pm_runtime_dont_use_autosuspend(struct device *dev);
    - clear the power.use_autosuspend flag, disabling autosuspend delays

  void pm_runtime_set_autosuspend_delay(struct device *dev, int delay);
    - set the power.autosuspend_delay value to 'delay' (expressed in
      milliseconds); if 'delay' is negative then runtime suspends are
      prevented

  unsigned long pm_runtime_autosuspend_expiration(struct device *dev);
    - calculate the time when the current autosuspend delay period will expire,
      based on power.last_busy and power.autosuspend_delay; if the delay time
      is 1000 ms or larger then the expiration time is rounded up to the
      nearest second; returns 0 if the delay period has already expired or
      power.use_autosuspend isn't set, otherwise returns the expiration time
      in jiffies

It is safe to execute the following helper functions from interrupt context:

pm_request_idle()
pm_request_autosuspend()
pm_schedule_suspend()
pm_request_resume()
pm_runtime_get_noresume()
pm_runtime_get()
pm_runtime_put_noidle()
pm_runtime_put()
pm_runtime_put_autosuspend()
pm_runtime_enable()
pm_suspend_ignore_children()
pm_runtime_set_active()
pm_runtime_set_suspended()
pm_runtime_suspended()
pm_runtime_mark_last_busy()
pm_runtime_autosuspend_expiration()

If pm_runtime_irq_safe() has been called for a device then the following helper
functions may also be used in interrupt context:

pm_runtime_idle()
pm_runtime_suspend()
pm_runtime_autosuspend()
pm_runtime_resume()
pm_runtime_get_sync()
pm_runtime_put_sync()
pm_runtime_put_sync_suspend()
pm_runtime_put_sync_autosuspend()

5. Runtime PM Initialization, Device Probing and Removal

Initially, the runtime PM is disabled for all devices, which means that the
majority of the runtime PM helper funtions described in Section 4 will return
-EAGAIN until pm_runtime_enable() is called for the device.

In addition to that, the initial runtime PM status of all devices is
'suspended', but it need not reflect the actual physical state of the device.
Thus, if the device is initially active (i.e. it is able to process I/O), its
runtime PM status must be changed to 'active', with the help of
pm_runtime_set_active(), before pm_runtime_enable() is called for the device.

However, if the device has a parent and the parent's runtime PM is enabled,
calling pm_runtime_set_active() for the device will affect the parent, unless
the parent's 'power.ignore_children' flag is set.  Namely, in that case the
parent won't be able to suspend at run time, using the PM core's helper
functions, as long as the child's status is 'active', even if the child's
runtime PM is still disabled (i.e. pm_runtime_enable() hasn't been called for
the child yet or pm_runtime_disable() has been called for it).  For this reason,
once pm_runtime_set_active() has been called for the device, pm_runtime_enable()
should be called for it too as soon as reasonably possible or its runtime PM
status should be changed back to 'suspended' with the help of
pm_runtime_set_suspended().

If the default initial runtime PM status of the device (i.e. 'suspended')
reflects the actual state of the device, its bus type's or its driver's
->probe() callback will likely need to wake it up using one of the PM core's
helper functions described in Section 4.  In that case, pm_runtime_resume()
should be used.  Of course, for this purpose the device's runtime PM has to be
enabled earlier by calling pm_runtime_enable().

If the device bus type's or driver's ->probe() callback runs
pm_runtime_suspend() or pm_runtime_idle() or their asynchronous counterparts,
they will fail returning -EAGAIN, because the device's usage counter is
incremented by the driver core before executing ->probe().  Still, it may be
desirable to suspend the device as soon as ->probe() has finished, so the driver
core uses pm_runtime_put_sync() to invoke the subsystem-level idle callback for
the device at that time.

Moreover, the driver core prevents runtime PM callbacks from racing with the bus
notifier callback in __device_release_driver(), which is necessary, because the
notifier is used by some subsystems to carry out operations affecting the
runtime PM functionality.  It does so by calling pm_runtime_get_sync() before
driver_sysfs_remove() and the BUS_NOTIFY_UNBIND_DRIVER notifications.  This
resumes the device if it's in the suspended state and prevents it from
being suspended again while those routines are being executed.

To allow bus types and drivers to put devices into the suspended state by
calling pm_runtime_suspend() from their ->remove() routines, the driver core
executes pm_runtime_put_sync() after running the BUS_NOTIFY_UNBIND_DRIVER
notifications in __device_release_driver().  This requires bus types and
drivers to make their ->remove() callbacks avoid races with runtime PM directly,
but also it allows of more flexibility in the handling of devices during the
removal of their drivers.

The user space can effectively disallow the driver of the device to power manage
it at run time by changing the value of its /sys/devices/.../power/control
attribute to "on", which causes pm_runtime_forbid() to be called.  In principle,
this mechanism may also be used by the driver to effectively turn off the
runtime power management of the device until the user space turns it on.
Namely, during the initialization the driver can make sure that the runtime PM
status of the device is 'active' and call pm_runtime_forbid().  It should be
noted, however, that if the user space has already intentionally changed the
value of /sys/devices/.../power/control to "auto" to allow the driver to power
manage the device at run time, the driver may confuse it by using
pm_runtime_forbid() this way.

6. Runtime PM and System Sleep

Runtime PM and system sleep (i.e., system suspend and hibernation, also known
as suspend-to-RAM and suspend-to-disk) interact with each other in a couple of
ways.  If a device is active when a system sleep starts, everything is
straightforward.  But what should happen if the device is already suspended?

The device may have different wake-up settings for runtime PM and system sleep.
For example, remote wake-up may be enabled for runtime suspend but disallowed
for system sleep (device_may_wakeup(dev) returns 'false').  When this happens,
the subsystem-level system suspend callback is responsible for changing the
device's wake-up setting (it may leave that to the device driver's system
suspend routine).  It may be necessary to resume the device and suspend it again
in order to do so.  The same is true if the driver uses different power levels
or other settings for runtime suspend and system sleep.

During system resume, the simplest approach is to bring all devices back to full
power, even if they had been suspended before the system suspend began.  There
are several reasons for this, including:

  * The device might need to switch power levels, wake-up settings, etc.

  * Remote wake-up events might have been lost by the firmware.

  * The device's children may need the device to be at full power in order
    to resume themselves.

  * The driver's idea of the device state may not agree with the device's
    physical state.  This can happen during resume from hibernation.

  * The device might need to be reset.

  * Even though the device was suspended, if its usage counter was > 0 then most
    likely it would need a runtime resume in the near future anyway.

If the device had been suspended before the system suspend began and it's
brought back to full power during resume, then its runtime PM status will have
to be updated to reflect the actual post-system sleep status.  The way to do
this is:

	pm_runtime_disable(dev);
	pm_runtime_set_active(dev);
	pm_runtime_enable(dev);

The PM core always increments the runtime usage counter before calling the
->suspend() callback and decrements it after calling the ->resume() callback.
Hence disabling runtime PM temporarily like this will not cause any runtime
suspend attempts to be permanently lost.  If the usage count goes to zero
following the return of the ->resume() callback, the ->runtime_idle() callback
will be invoked as usual.

On some systems, however, system sleep is not entered through a global firmware
or hardware operation.  Instead, all hardware components are put into low-power
states directly by the kernel in a coordinated way.  Then, the system sleep
state effectively follows from the states the hardware components end up in
and the system is woken up from that state by a hardware interrupt or a similar
mechanism entirely under the kernel's control.  As a result, the kernel never
gives control away and the states of all devices during resume are precisely
known to it.  If that is the case and none of the situations listed above takes
place (in particular, if the system is not waking up from hibernation), it may
be more efficient to leave the devices that had been suspended before the system
suspend began in the suspended state.

The PM core does its best to reduce the probability of race conditions between
the runtime PM and system suspend/resume (and hibernation) callbacks by carrying
out the following operations:

  * During system suspend it calls pm_runtime_get_noresume() and
    pm_runtime_barrier() for every device right before executing the
    subsystem-level .suspend() callback for it.  In addition to that it calls
    pm_runtime_disable() for every device right after executing the
    subsystem-level .suspend() callback for it.

  * During system resume it calls pm_runtime_enable() and pm_runtime_put_sync()
    for every device right before and right after executing the subsystem-level
    .resume() callback for it, respectively.

7. Generic subsystem callbacks

Subsystems may wish to conserve code space by using the set of generic power
management callbacks provided by the PM core, defined in
driver/base/power/generic_ops.c:

  int pm_generic_runtime_idle(struct device *dev);
    - invoke the ->runtime_idle() callback provided by the driver of this
      device, if defined, and call pm_runtime_suspend() for this device if the
      return value is 0 or the callback is not defined

  int pm_generic_runtime_suspend(struct device *dev);
    - invoke the ->runtime_suspend() callback provided by the driver of this
      device and return its result, or return -EINVAL if not defined

  int pm_generic_runtime_resume(struct device *dev);
    - invoke the ->runtime_resume() callback provided by the driver of this
      device and return its result, or return -EINVAL if not defined

  int pm_generic_suspend(struct device *dev);
    - if the device has not been suspended at run time, invoke the ->suspend()
      callback provided by its driver and return its result, or return 0 if not
      defined

  int pm_generic_suspend_noirq(struct device *dev);
    - if pm_runtime_suspended(dev) returns "false", invoke the ->suspend_noirq()
      callback provided by the device's driver and return its result, or return
      0 if not defined

  int pm_generic_resume(struct device *dev);
    - invoke the ->resume() callback provided by the driver of this device and,
      if successful, change the device's runtime PM status to 'active'

  int pm_generic_resume_noirq(struct device *dev);
    - invoke the ->resume_noirq() callback provided by the driver of this device

  int pm_generic_freeze(struct device *dev);
    - if the device has not been suspended at run time, invoke the ->freeze()
      callback provided by its driver and return its result, or return 0 if not
      defined

  int pm_generic_freeze_noirq(struct device *dev);
    - if pm_runtime_suspended(dev) returns "false", invoke the ->freeze_noirq()
      callback provided by the device's driver and return its result, or return
      0 if not defined

  int pm_generic_thaw(struct device *dev);
    - if the device has not been suspended at run time, invoke the ->thaw()
      callback provided by its driver and return its result, or return 0 if not
      defined

  int pm_generic_thaw_noirq(struct device *dev);
    - if pm_runtime_suspended(dev) returns "false", invoke the ->thaw_noirq()
      callback provided by the device's driver and return its result, or return
      0 if not defined

  int pm_generic_poweroff(struct device *dev);
    - if the device has not been suspended at run time, invoke the ->poweroff()
      callback provided by its driver and return its result, or return 0 if not
      defined

  int pm_generic_poweroff_noirq(struct device *dev);
    - if pm_runtime_suspended(dev) returns "false", run the ->poweroff_noirq()
      callback provided by the device's driver and return its result, or return
      0 if not defined

  int pm_generic_restore(struct device *dev);
    - invoke the ->restore() callback provided by the driver of this device and,
      if successful, change the device's runtime PM status to 'active'

  int pm_generic_restore_noirq(struct device *dev);
    - invoke the ->restore_noirq() callback provided by the device's driver

These functions can be assigned to the ->runtime_idle(), ->runtime_suspend(),
->runtime_resume(), ->suspend(), ->suspend_noirq(), ->resume(),
->resume_noirq(), ->freeze(), ->freeze_noirq(), ->thaw(), ->thaw_noirq(),
->poweroff(), ->poweroff_noirq(), ->restore(), ->restore_noirq() callback
pointers in the subsystem-level dev_pm_ops structures.

If a subsystem wishes to use all of them at the same time, it can simply assign
the GENERIC_SUBSYS_PM_OPS macro, defined in include/linux/pm.h, to its
dev_pm_ops structure pointer.

Device drivers that wish to use the same function as a system suspend, freeze,
poweroff and runtime suspend callback, and similarly for system resume, thaw,
restore, and runtime resume, can achieve this with the help of the
UNIVERSAL_DEV_PM_OPS macro defined in include/linux/pm.h (possibly setting its
last argument to NULL).

8. "No-Callback" Devices

Some "devices" are only logical sub-devices of their parent and cannot be
power-managed on their own.  (The prototype example is a USB interface.  Entire
USB devices can go into low-power mode or send wake-up requests, but neither is
possible for individual interfaces.)  The drivers for these devices have no
need of runtime PM callbacks; if the callbacks did exist, ->runtime_suspend()
and ->runtime_resume() would always return 0 without doing anything else and
->runtime_idle() would always call pm_runtime_suspend().

Subsystems can tell the PM core about these devices by calling
pm_runtime_no_callbacks().  This should be done after the device structure is
initialized and before it is registered (although after device registration is
also okay).  The routine will set the device's power.no_callbacks flag and
prevent the non-debugging runtime PM sysfs attributes from being created.

When power.no_callbacks is set, the PM core will not invoke the
->runtime_idle(), ->runtime_suspend(), or ->runtime_resume() callbacks.
Instead it will assume that suspends and resumes always succeed and that idle
devices should be suspended.

As a consequence, the PM core will never directly inform the device's subsystem
or driver about runtime power changes.  Instead, the driver for the device's
parent must take responsibility for telling the device's driver when the
parent's power state changes.

9. Autosuspend, or automatically-delayed suspends

Changing a device's power state isn't free; it requires both time and energy.
A device should be put in a low-power state only when there's some reason to
think it will remain in that state for a substantial time.  A common heuristic
says that a device which hasn't been used for a while is liable to remain
unused; following this advice, drivers should not allow devices to be suspended
at runtime until they have been inactive for some minimum period.  Even when
the heuristic ends up being non-optimal, it will still prevent devices from
"bouncing" too rapidly between low-power and full-power states.

The term "autosuspend" is an historical remnant.  It doesn't mean that the
device is automatically suspended (the subsystem or driver still has to call
the appropriate PM routines); rather it means that runtime suspends will
automatically be delayed until the desired period of inactivity has elapsed.

Inactivity is determined based on the power.last_busy field.  Drivers should
call pm_runtime_mark_last_busy() to update this field after carrying out I/O,
typically just before calling pm_runtime_put_autosuspend().  The desired length
of the inactivity period is a matter of policy.  Subsystems can set this length
initially by calling pm_runtime_set_autosuspend_delay(), but after device
registration the length should be controlled by user space, using the
/sys/devices/.../power/autosuspend_delay_ms attribute.

In order to use autosuspend, subsystems or drivers must call
pm_runtime_use_autosuspend() (preferably before registering the device), and
thereafter they should use the various *_autosuspend() helper functions instead
of the non-autosuspend counterparts:

	Instead of: pm_runtime_suspend    use: pm_runtime_autosuspend;
	Instead of: pm_schedule_suspend   use: pm_request_autosuspend;
	Instead of: pm_runtime_put        use: pm_runtime_put_autosuspend;
	Instead of: pm_runtime_put_sync   use: pm_runtime_put_sync_autosuspend.

Drivers may also continue to use the non-autosuspend helper functions; they
will behave normally, not taking the autosuspend delay into account.
Similarly, if the power.use_autosuspend field isn't set then the autosuspend
helper functions will behave just like the non-autosuspend counterparts.

Under some circumstances a driver or subsystem may want to prevent a device
from autosuspending immediately, even though the usage counter is zero and the
autosuspend delay time has expired.  If the ->runtime_suspend() callback
returns -EAGAIN or -EBUSY, and if the next autosuspend delay expiration time is
in the future (as it normally would be if the callback invoked
pm_runtime_mark_last_busy()), the PM core will automatically reschedule the
autosuspend.  The ->runtime_suspend() callback can't do this rescheduling
itself because no suspend requests of any kind are accepted while the device is
suspending (i.e., while the callback is running).

The implementation is well suited for asynchronous use in interrupt contexts.
However such use inevitably involves races, because the PM core can't
synchronize ->runtime_suspend() callbacks with the arrival of I/O requests.
This synchronization must be handled by the driver, using its private lock.
Here is a schematic pseudo-code example:

	foo_read_or_write(struct foo_priv *foo, void *data)
	{
		lock(&foo->private_lock);
		add_request_to_io_queue(foo, data);
		if (foo->num_pending_requests++ == 0)
			pm_runtime_get(&foo->dev);
		if (!foo->is_suspended)
			foo_process_next_request(foo);
		unlock(&foo->private_lock);
	}

	foo_io_completion(struct foo_priv *foo, void *req)
	{
		lock(&foo->private_lock);
		if (--foo->num_pending_requests == 0) {
			pm_runtime_mark_last_busy(&foo->dev);
			pm_runtime_put_autosuspend(&foo->dev);
		} else {
			foo_process_next_request(foo);
		}
		unlock(&foo->private_lock);
		/* Send req result back to the user ... */
	}

	int foo_runtime_suspend(struct device *dev)
	{
		struct foo_priv foo = container_of(dev, ...);
		int ret = 0;

		lock(&foo->private_lock);
		if (foo->num_pending_requests > 0) {
			ret = -EBUSY;
		} else {
			/* ... suspend the device ... */
			foo->is_suspended = 1;
		}
		unlock(&foo->private_lock);
		return ret;
	}

	int foo_runtime_resume(struct device *dev)
	{
		struct foo_priv foo = container_of(dev, ...);

		lock(&foo->private_lock);
		/* ... resume the device ... */
		foo->is_suspended = 0;
		pm_runtime_mark_last_busy(&foo->dev);
		if (foo->num_pending_requests > 0)
			foo_process_requests(foo);
		unlock(&foo->private_lock);
		return 0;
	}

The important point is that after foo_io_completion() asks for an autosuspend,
the foo_runtime_suspend() callback may race with foo_read_or_write().
Therefore foo_runtime_suspend() has to check whether there are any pending I/O
requests (while holding the private lock) before allowing the suspend to
proceed.

In addition, the power.autosuspend_delay field can be changed by user space at
any time.  If a driver cares about this, it can call
pm_runtime_autosuspend_expiration() from within the ->runtime_suspend()
callback while holding its private lock.  If the function returns a nonzero
value then the delay has not yet expired and the callback should return
-EAGAIN.