aboutsummaryrefslogtreecommitdiffstats
blob: 33ed8007a8458893572046e3d5acf2248ca39e8e (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
402
403
404
405
406
407
408
409
410
411
412
413
414
415
416
417
418
419
420
421
422
423
424
425
426
427
428
429
430
431
432
433
434
435
436
437
438
439
440
441
442
443
444
445
446
447
448
449
450
451
452
453
454
455
456
457
458
459
460
461
462
463
464
465
466
467
468
469
470
471
472
473
474
475
476
477
478
479
480
481
482
483
484
485
486
487
488
489
490
491
492
493
494
495
496
497
498
499
500
501
502
503
504
505
506
507
508
509
510
511
512
513
514
515
516
517
518
519
520
521
522
523
524
525
526
527
528
529
530
531
532
533
534
535
536
537
538
539
540
541
542
543
544
545
546
547
548
549
550
551
552
553
554
555
556
557
558
559
560
561
562
563
564
565
566
567
568
569
570
571
572
573
574
575
576
577
578
579
580
581
582
583
584
585
586
587
588
589
590
591
592
593
594
595
596
597
598
599
600
601
602
603
604
605
606
607
608
609
610
611
612
613
614
615
616
617
618
619
620
621
622
623
624
625
626
627
628
629
630
631
632
633
634
635
636
637
638
639
640
641
642
643
644
645
646
647
648
649
650
651
652
653
654
655
656
657
658
659
660
661
662
663
664
665
666
667
668
669
670
671
672
673
674
675
676
677
678
679
680
681
682
683
684
685
686
687
688
689
690
691
692
693
694
695
696
697
698
699
700
701
702
703
704
705
706
707
708
709
710
711
712
713
714
715
716
717
718
719
720
721
722
723
724
725
726
727
728
729
730
731
732
733
734
735
736
737
738
739
740
741
742
743
744
745
746
747
748
749
750
751
752
753
754
755
756
757
758
759
760
761
762
763
764
765
766
767
768
769
770
771
772
773
774
775
776
777
778
779
780
781
#
# Copyright (c) 2006 Steven Rostedt
# Licensed under the GNU Free Documentation License, Version 1.2
#

RT-mutex implementation design
------------------------------

This document tries to describe the design of the rtmutex.c implementation.
It doesn't describe the reasons why rtmutex.c exists. For that please see
Documentation/rt-mutex.txt.  Although this document does explain problems
that happen without this code, but that is in the concept to understand
what the code actually is doing.

The goal of this document is to help others understand the priority
inheritance (PI) algorithm that is used, as well as reasons for the
decisions that were made to implement PI in the manner that was done.


Unbounded Priority Inversion
----------------------------

Priority inversion is when a lower priority process executes while a higher
priority process wants to run.  This happens for several reasons, and
most of the time it can't be helped.  Anytime a high priority process wants
to use a resource that a lower priority process has (a mutex for example),
the high priority process must wait until the lower priority process is done
with the resource.  This is a priority inversion.  What we want to prevent
is something called unbounded priority inversion.  That is when the high
priority process is prevented from running by a lower priority process for
an undetermined amount of time.

The classic example of unbounded priority inversion is were you have three
processes, let's call them processes A, B, and C, where A is the highest
priority process, C is the lowest, and B is in between. A tries to grab a lock
that C owns and must wait and lets C run to release the lock. But in the
meantime, B executes, and since B is of a higher priority than C, it preempts C,
but by doing so, it is in fact preempting A which is a higher priority process.
Now there's no way of knowing how long A will be sleeping waiting for C
to release the lock, because for all we know, B is a CPU hog and will
never give C a chance to release the lock.  This is called unbounded priority
inversion.

Here's a little ASCII art to show the problem.

   grab lock L1 (owned by C)
     |
A ---+
        C preempted by B
          |
C    +----+

B         +-------->
                B now keeps A from running.


Priority Inheritance (PI)
-------------------------

There are several ways to solve this issue, but other ways are out of scope
for this document.  Here we only discuss PI.

PI is where a process inherits the priority of another process if the other
process blocks on a lock owned by the current process.  To make this easier
to understand, let's use the previous example, with processes A, B, and C again.

This time, when A blocks on the lock owned by C, C would inherit the priority
of A.  So now if B becomes runnable, it would not preempt C, since C now has
the high priority of A.  As soon as C releases the lock, it loses its
inherited priority, and A then can continue with the resource that C had.

Terminology
-----------

Here I explain some terminology that is used in this document to help describe
the design that is used to implement PI.

PI chain - The PI chain is an ordered series of locks and processes that cause
           processes to inherit priorities from a previous process that is
           blocked on one of its locks.  This is described in more detail
           later in this document.

mutex    - In this document, to differentiate from locks that implement
           PI and spin locks that are used in the PI code, from now on
           the PI locks will be called a mutex.

lock     - In this document from now on, I will use the term lock when
           referring to spin locks that are used to protect parts of the PI
           algorithm.  These locks disable preemption for UP (when
           CONFIG_PREEMPT is enabled) and on SMP prevents multiple CPUs from
           entering critical sections simultaneously.

spin lock - Same as lock above.

waiter   - A waiter is a struct that is stored on the stack of a blocked
           process.  Since the scope of the waiter is within the code for
           a process being blocked on the mutex, it is fine to allocate
           the waiter on the process's stack (local variable).  This
           structure holds a pointer to the task, as well as the mutex that
           the task is blocked on.  It also has the plist node structures to
           place the task in the waiter_list of a mutex as well as the
           pi_list of a mutex owner task (described below).

           waiter is sometimes used in reference to the task that is waiting
           on a mutex. This is the same as waiter->task.

waiters  - A list of processes that are blocked on a mutex.

top waiter - The highest priority process waiting on a specific mutex.

top pi waiter - The highest priority process waiting on one of the mutexes
                that a specific process owns.

Note:  task and process are used interchangeably in this document, mostly to
       differentiate between two processes that are being described together.


PI chain
--------

The PI chain is a list of processes and mutexes that may cause priority
inheritance to take place.  Multiple chains may converge, but a chain
would never diverge, since a process can't be blocked on more than one
mutex at a time.

Example:

   Process:  A, B, C, D, E
   Mutexes:  L1, L2, L3, L4

   A owns: L1
           B blocked on L1
           B owns L2
                  C blocked on L2
                  C owns L3
                         D blocked on L3
                         D owns L4
                                E blocked on L4

The chain would be:

   E->L4->D->L3->C->L2->B->L1->A

To show where two chains merge, we could add another process F and
another mutex L5 where B owns L5 and F is blocked on mutex L5.

The chain for F would be:

   F->L5->B->L1->A

Since a process may own more than one mutex, but never be blocked on more than
one, the chains merge.

Here we show both chains:

   E->L4->D->L3->C->L2-+
                       |
                       +->B->L1->A
                       |
                 F->L5-+

For PI to work, the processes at the right end of these chains (or we may
also call it the Top of the chain) must be equal to or higher in priority
than the processes to the left or below in the chain.

Also since a mutex may have more than one process blocked on it, we can
have multiple chains merge at mutexes.  If we add another process G that is
blocked on mutex L2:

  G->L2->B->L1->A

And once again, to show how this can grow I will show the merging chains
again.

   E->L4->D->L3->C-+
                   +->L2-+
                   |     |
                 G-+     +->B->L1->A
                         |
                   F->L5-+


Plist
-----

Before I go further and talk about how the PI chain is stored through lists
on both mutexes and processes, I'll explain the plist.  This is similar to
the struct list_head functionality that is already in the kernel.
The implementation of plist is out of scope for this document, but it is
very important to understand what it does.

There are a few differences between plist and list, the most important one
being that plist is a priority sorted linked list.  This means that the
priorities of the plist are sorted, such that it takes O(1) to retrieve the
highest priority item in the list.  Obviously this is useful to store processes
based on their priorities.

Another difference, which is important for implementation, is that, unlike
list, the head of the list is a different element than the nodes of a list.
So the head of the list is declared as struct plist_head and nodes that will
be added to the list are declared as struct plist_node.


Mutex Waiter List
-----------------

Every mutex keeps track of all the waiters that are blocked on itself. The mutex
has a plist to store these waiters by priority.  This list is protected by
a spin lock that is located in the struct of the mutex. This lock is called
wait_lock.  Since the modification of the waiter list is never done in
interrupt context, the wait_lock can be taken without disabling interrupts.


Task PI List
------------

To keep track of the PI chains, each process has its own PI list.  This is
a list of all top waiters of the mutexes that are owned by the process.
Note that this list only holds the top waiters and not all waiters that are
blocked on mutexes owned by the process.

The top of the task's PI list is always the highest priority task that
is waiting on a mutex that is owned by the task.  So if the task has
inherited a priority, it will always be the priority of the task that is
at the top of this list.

This list is stored in the task structure of a process as a plist called
pi_list.  This list is protected by a spin lock also in the task structure,
called pi_lock.  This lock may also be taken in interrupt context, so when
locking the pi_lock, interrupts must be disabled.


Depth of the PI Chain
---------------------

The maximum depth of the PI chain is not dynamic, and could actually be
defined.  But is very complex to figure it out, since it depends on all
the nesting of mutexes.  Let's look at the example where we have 3 mutexes,
L1, L2, and L3, and four separate functions func1, func2, func3 and func4.
The following shows a locking order of L1->L2->L3, but may not actually
be directly nested that way.

void func1(void)
{
	mutex_lock(L1);

	/* do anything */

	mutex_unlock(L1);
}

void func2(void)
{
	mutex_lock(L1);
	mutex_lock(L2);

	/* do something */

	mutex_unlock(L2);
	mutex_unlock(L1);
}

void func3(void)
{
	mutex_lock(L2);
	mutex_lock(L3);

	/* do something else */

	mutex_unlock(L3);
	mutex_unlock(L2);
}

void func4(void)
{
	mutex_lock(L3);

	/* do something again */

	mutex_unlock(L3);
}

Now we add 4 processes that run each of these functions separately.
Processes A, B, C, and D which run functions func1, func2, func3 and func4
respectively, and such that D runs first and A last.  With D being preempted
in func4 in the "do something again" area, we have a locking that follows:

D owns L3
       C blocked on L3
       C owns L2
              B blocked on L2
              B owns L1
                     A blocked on L1

And thus we have the chain A->L1->B->L2->C->L3->D.

This gives us a PI depth of 4 (four processes), but looking at any of the
functions individually, it seems as though they only have at most a locking
depth of two.  So, although the locking depth is defined at compile time,
it still is very difficult to find the possibilities of that depth.

Now since mutexes can be defined by user-land applications, we don't want a DOS
type of application that nests large amounts of mutexes to create a large
PI chain, and have the code holding spin locks while looking at a large
amount of data.  So to prevent this, the implementation not only implements
a maximum lock depth, but also only holds at most two different locks at a
time, as it walks the PI chain.  More about this below.


Mutex owner and flags
---------------------

The mutex structure contains a pointer to the owner of the mutex.  If the
mutex is not owned, this owner is set to NULL.  Since all architectures
have the task structure on at least a four byte alignment (and if this is
not true, the rtmutex.c code will be broken!), this allows for the two
least significant bits to be used as flags.  This part is also described
in Documentation/rt-mutex.txt, but will also be briefly described here.

Bit 0 is used as the "Pending Owner" flag.  This is described later.
Bit 1 is used as the "Has Waiters" flags.  This is also described later
  in more detail, but is set whenever there are waiters on a mutex.


cmpxchg Tricks
--------------

Some architectures implement an atomic cmpxchg (Compare and Exchange).  This
is used (when applicable) to keep the fast path of grabbing and releasing
mutexes short.

cmpxchg is basically the following function performed atomically:

unsigned long _cmpxchg(unsigned long *A, unsigned long *B, unsigned long *C)
{
	unsigned long T = *A;
	if (*A == *B) {
		*A = *C;
	}
	return T;
}
#define cmpxchg(a,b,c) _cmpxchg(&a,&b,&c)

This is really nice to have, since it allows you to only update a variable
if the variable is what you expect it to be.  You know if it succeeded if
the return value (the old value of A) is equal to B.

The macro rt_mutex_cmpxchg is used to try to lock and unlock mutexes. If
the architecture does not support CMPXCHG, then this macro is simply set
to fail every time.  But if CMPXCHG is supported, then this will
help out extremely to keep the fast path short.

The use of rt_mutex_cmpxchg with the flags in the owner field help optimize
the system for architectures that support it.  This will also be explained
later in this document.


Priority adjustments
--------------------

The implementation of the PI code in rtmutex.c has several places that a
process must adjust its priority.  With the help of the pi_list of a
process this is rather easy to know what needs to be adjusted.

The functions implementing the task adjustments are rt_mutex_adjust_prio,
__rt_mutex_adjust_prio (same as the former, but expects the task pi_lock
to already be taken), rt_mutex_getprio, and rt_mutex_setprio.

rt_mutex_getprio and rt_mutex_setprio are only used in __rt_mutex_adjust_prio.

rt_mutex_getprio returns the priority that the task should have.  Either the
task's own normal priority, or if a process of a higher priority is waiting on
a mutex owned by the task, then that higher priority should be returned.
Since the pi_list of a task holds an order by priority list of all the top
waiters of all the mutexes that the task owns, rt_mutex_getprio simply needs
to compare the top pi waiter to its own normal priority, and return the higher
priority back.

(Note:  if looking at the code, you will notice that the lower number of
        prio is returned.  This is because the prio field in the task structure
        is an inverse order of the actual priority.  So a "prio" of 5 is
        of higher priority than a "prio" of 10.)

__rt_mutex_adjust_prio examines the result of rt_mutex_getprio, and if the
result does not equal the task's current priority, then rt_mutex_setprio
is called to adjust the priority of the task to the new priority.
Note that rt_mutex_setprio is defined in kernel/sched.c to implement the
actual change in priority.

It is interesting to note that __rt_mutex_adjust_prio can either increase
or decrease the priority of the task.  In the case that a higher priority
process has just blocked on a mutex owned by the task, __rt_mutex_adjust_prio
would increase/boost the task's priority.  But if a higher priority task
were for some reason to leave the mutex (timeout or signal), this same function
would decrease/unboost the priority of the task.  That is because the pi_list
always contains the highest priority task that is waiting on a mutex owned
by the task, so we only need to compare the priority of that top pi waiter
to the normal priority of the given task.


High level overview of the PI chain walk
----------------------------------------

The PI chain walk is implemented by the function rt_mutex_adjust_prio_chain.

The implementation has gone through several iterations, and has ended up
with what we believe is the best.  It walks the PI chain by only grabbing
at most two locks at a time, and is very efficient.

The rt_mutex_adjust_prio_chain can be used either to boost or lower process
priorities.

rt_mutex_adjust_prio_chain is called with a task to be checked for PI
(de)boosting (the owner of a mutex that a process is blocking on), a flag to
check for deadlocking, the mutex that the task owns, and a pointer to a waiter
that is the process's waiter struct that is blocked on the mutex (although this
parameter may be NULL for deboosting).

For this explanation, I will not mention deadlock detection. This explanation
will try to stay at a high level.

When this function is called, there are no locks held.  That also means
that the state of the owner and lock can change when entered into this function.

Before this function is called, the task has already had rt_mutex_adjust_prio
performed on it.  This means that the task is set to the priority that it
should be at, but the plist nodes of the task's waiter have not been updated
with the new priorities, and that this task may not be in the proper locations
in the pi_lists and wait_lists that the task is blocked on.  This function
solves all that.

A loop is entered, where task is the owner to be checked for PI changes that
was passed by parameter (for the first iteration).  The pi_lock of this task is
taken to prevent any more changes to the pi_list of the task.  This also
prevents new tasks from completing the blocking on a mutex that is owned by this
task.

If the task is not blocked on a mutex then the loop is exited.  We are at
the top of the PI chain.

A check is now done to see if the original waiter (the process that is blocked
on the current mutex) is the top pi waiter of the task.  That is, is this
waiter on the top of the task's pi_list.  If it is not, it either means that
there is another process higher in priority that is blocked on one of the
mutexes that the task owns, or that the waiter has just woken up via a signal
or timeout and has left the PI chain.  In either case, the loop is exited, since
we don't need to do any more changes to the priority of the current task, or any
task that owns a mutex that this current task is waiting on.  A priority chain
walk is only needed when a new top pi waiter is made to a task.

The next check sees if the task's waiter plist node has the priority equal to
the priority the task is set at.  If they are equal, then we are done with
the loop.  Remember that the function started with the priority of the
task adjusted, but the plist nodes that hold the task in other processes
pi_lists have not been adjusted.

Next, we look at the mutex that the task is blocked on. The mutex's wait_lock
is taken.  This is done by a spin_trylock, because the locking order of the
pi_lock and wait_lock goes in the opposite direction. If we fail to grab the
lock, the pi_lock is released, and we restart the loop.

Now that we have both the pi_lock of the task as well as the wait_lock of
the mutex the task is blocked on, we update the task's waiter's plist node
that is located on the mutex's wait_list.

Now we release the pi_lock of the task.

Next the owner of the mutex has its pi_lock taken, so we can update the
task's entry in the owner's pi_list.  If the task is the highest priority
process on the mutex's wait_list, then we remove the previous top waiter
from the owner's pi_list, and replace it with the task.

Note: It is possible that the task was the current top waiter on the mutex,
      in which case the task is not yet on the pi_list of the waiter.  This
      is OK, since plist_del does nothing if the plist node is not on any
      list.

If the task was not the top waiter of the mutex, but it was before we
did the priority updates, that means we are deboosting/lowering the
task.  In this case, the task is removed from the pi_list of the owner,
and the new top waiter is added.

Lastly, we unlock both the pi_lock of the task, as well as the mutex's
wait_lock, and continue the loop again.  On the next iteration of the
loop, the previous owner of the mutex will be the task that will be
processed.

Note: One might think that the owner of this mutex might have changed
      since we just grab the mutex's wait_lock. And one could be right.
      The important thing to remember is that the owner could not have
      become the task that is being processed in the PI chain, since
      we have taken that task's pi_lock at the beginning of the loop.
      So as long as there is an owner of this mutex that is not the same
      process as the tasked being worked on, we are OK.

      Looking closely at the code, one might be confused.  The check for the
      end of the PI chain is when the task isn't blocked on anything or the
      task's waiter structure "task" element is NULL.  This check is
      protected only by the task's pi_lock.  But the code to unlock the mutex
      sets the task's waiter structure "task" element to NULL with only
      the protection of the mutex's wait_lock, which was not taken yet.
      Isn't this a race condition if the task becomes the new owner?

      The answer is No!  The trick is the spin_trylock of the mutex's
      wait_lock.  If we fail that lock, we release the pi_lock of the
      task and continue the loop, doing the end of PI chain check again.

      In the code to release the lock, the wait_lock of the mutex is held
      the entire time, and it is not let go when we grab the pi_lock of the
      new owner of the mutex.  So if the switch of a new owner were to happen
      after the check for end of the PI chain and the grabbing of the
      wait_lock, the unlocking code would spin on the new owner's pi_lock
      but never give up the wait_lock.  So the PI chain loop is guaranteed to
      fail the spin_trylock on the wait_lock, release the pi_lock, and
      try again.

      If you don't quite understand the above, that's OK. You don't have to,
      unless you really want to make a proof out of it ;)


Pending Owners and Lock stealing
--------------------------------

One of the flags in the owner field of the mutex structure is "Pending Owner".
What this means is that an owner was chosen by the process releasing the
mutex, but that owner has yet to wake up and actually take the mutex.

Why is this important?  Why can't we just give the mutex to another process
and be done with it?

The PI code is to help with real-time processes, and to let the highest
priority process run as long as possible with little latencies and delays.
If a high priority process owns a mutex that a lower priority process is
blocked on, when the mutex is released it would be given to the lower priority
process.  What if the higher priority process wants to take that mutex again.
The high priority process would fail to take that mutex that it just gave up
and it would need to boost the lower priority process to run with full
latency of that critical section (since the low priority process just entered
it).

There's no reason a high priority process that gives up a mutex should be
penalized if it tries to take that mutex again.  If the new owner of the
mutex has not woken up yet, there's no reason that the higher priority process
could not take that mutex away.

To solve this, we introduced Pending Ownership and Lock Stealing.  When a
new process is given a mutex that it was blocked on, it is only given
pending ownership.  This means that it's the new owner, unless a higher
priority process comes in and tries to grab that mutex.  If a higher priority
process does come along and wants that mutex, we let the higher priority
process "steal" the mutex from the pending owner (only if it is still pending)
and continue with the mutex.


Taking of a mutex (The walk through)
------------------------------------

OK, now let's take a look at the detailed walk through of what happens when
taking a mutex.

The first thing that is tried is the fast taking of the mutex.  This is
done when we have CMPXCHG enabled (otherwise the fast taking automatically
fails).  Only when the owner field of the mutex is NULL can the lock be
taken with the CMPXCHG and nothing else needs to be done.

If there is contention on the lock, whether it is owned or pending owner
we go about the slow path (rt_mutex_slowlock).

The slow path function is where the task's waiter structure is created on
the stack.  This is because the waiter structure is only needed for the
scope of this function.  The waiter structure holds the nodes to store
the task on the wait_list of the mutex, and if need be, the pi_list of
the owner.

The wait_lock of the mutex is taken since the slow path of unlocking the
mutex also takes this lock.

We then call try_to_take_rt_mutex.  This is where the architecture that
does not implement CMPXCHG would always grab the lock (if there's no
contention).

try_to_take_rt_mutex is used every time the task tries to grab a mutex in the
slow path.  The first thing that is done here is an atomic setting of
the "Has Waiters" flag of the mutex's owner field.  Yes, this could really
be false, because if the mutex has no owner, there are no waiters and
the current task also won't have any waiters.  But we don't have the lock
yet, so we assume we are going to be a waiter.  The reason for this is to
play nice for those architectures that do have CMPXCHG.  By setting this flag
now, the owner of the mutex can't release the mutex without going into the
slow unlock path, and it would then need to grab the wait_lock, which this
code currently holds.  So setting the "Has Waiters" flag forces the owner
to synchronize with this code.

Now that we know that we can't have any races with the owner releasing the
mutex, we check to see if we can take the ownership.  This is done if the
mutex doesn't have a owner, or if we can steal the mutex from a pending
owner.  Let's look at the situations we have here.

  1) Has owner that is pending
  ----------------------------

  The mutex has a owner, but it hasn't woken up and the mutex flag
  "Pending Owner" is set.  The first check is to see if the owner isn't the
  current task.  This is because this function is also used for the pending
  owner to grab the mutex.  When a pending owner wakes up, it checks to see
  if it can take the mutex, and this is done if the owner is already set to
  itself.  If so, we succeed and leave the function, clearing the "Pending
  Owner" bit.

  If the pending owner is not current, we check to see if the current priority is
  higher than the pending owner.  If not, we fail the function and return.

  There's also something special about a pending owner.  That is a pending owner
  is never blocked on a mutex.  So there is no PI chain to worry about.  It also
  means that if the mutex doesn't have any waiters, there's no accounting needed
  to update the pending owner's pi_list, since we only worry about processes
  blocked on the current mutex.

  If there are waiters on this mutex, and we just stole the ownership, we need
  to take the top waiter, remove it from the pi_list of the pending owner, and
  add it to the current pi_list.  Note that at this moment, the pending owner
  is no longer on the list of waiters.  This is fine, since the pending owner
  would add itself back when it realizes that it had the ownership stolen
  from itself.  When the pending owner tries to grab the mutex, it will fail
  in try_to_take_rt_mutex if the owner field points to another process.

  2) No owner
  -----------

  If there is no owner (or we successfully stole the lock), we set the owner
  of the mutex to current, and set the flag of "Has Waiters" if the current
  mutex actually has waiters, or we clear the flag if it doesn't.  See, it was
  OK that we set that flag early, since now it is cleared.

  3) Failed to grab ownership
  ---------------------------

  The most interesting case is when we fail to take ownership. This means that
  there exists an owner, or there's a pending owner with equal or higher
  priority than the current task.

We'll continue on the failed case.

If the mutex has a timeout, we set up a timer to go off to break us out
of this mutex if we failed to get it after a specified amount of time.

Now we enter a loop that will continue to try to take ownership of the mutex, or
fail from a timeout or signal.

Once again we try to take the mutex.  This will usually fail the first time
in the loop, since it had just failed to get the mutex.  But the second time
in the loop, this would likely succeed, since the task would likely be
the pending owner.

If the mutex is TASK_INTERRUPTIBLE a check for signals and timeout is done
here.

The waiter structure has a "task" field that points to the task that is blocked
on the mutex.  This field can be NULL the first time it goes through the loop
or if the task is a pending owner and had its mutex stolen.  If the "task"
field is NULL then we need to set up the accounting for it.

Task blocks on mutex
--------------------

The accounting of a mutex and process is done with the waiter structure of
the process.  The "task" field is set to the process, and the "lock" field
to the mutex.  The plist nodes are initialized to the processes current
priority.

Since the wait_lock was taken at the entry of the slow lock, we can safely
add the waiter to the wait_list.  If the current process is the highest
priority process currently waiting on this mutex, then we remove the
previous top waiter process (if it exists) from the pi_list of the owner,
and add the current process to that list.  Since the pi_list of the owner
has changed, we call rt_mutex_adjust_prio on the owner to see if the owner
should adjust its priority accordingly.

If the owner is also blocked on a lock, and had its pi_list changed
(or deadlock checking is on), we unlock the wait_lock of the mutex and go ahead
and run rt_mutex_adjust_prio_chain on the owner, as described earlier.

Now all locks are released, and if the current process is still blocked on a
mutex (waiter "task" field is not NULL), then we go to sleep (call schedule).

Waking up in the loop
---------------------

The schedule can then wake up for a few reasons.
  1) we were given pending ownership of the mutex.
  2) we received a signal and was TASK_INTERRUPTIBLE
  3) we had a timeout and was TASK_INTERRUPTIBLE

In any of these cases, we continue the loop and once again try to grab the
ownership of the mutex.  If we succeed, we exit the loop, otherwise we continue
and on signal and timeout, will exit the loop, or if we had the mutex stolen
we just simply add ourselves back on the lists and go back to sleep.

Note: For various reasons, because of timeout and signals, the steal mutex
      algorithm needs to be careful. This is because the current process is
      still on the wait_list. And because of dynamic changing of priorities,
      especially on SCHED_OTHER tasks, the current process can be the
      highest priority task on the wait_list.

Failed to get mutex on Timeout or Signal
----------------------------------------

If a timeout or signal occurred, the waiter's "task" field would not be
NULL and the task needs to be taken off the wait_list of the mutex and perhaps
pi_list of the owner.  If this process was a high priority process, then
the rt_mutex_adjust_prio_chain needs to be executed again on the owner,
but this time it will be lowering the priorities.


Unlocking the Mutex
-------------------

The unlocking of a mutex also has a fast path for those architectures with
CMPXCHG.  Since the taking of a mutex on contention always sets the
"Has Waiters" flag of the mutex's owner, we use this to know if we need to
take the slow path when unlocking the mutex.  If the mutex doesn't have any
waiters, the owner field of the mutex would equal the current process and
the mutex can be unlocked by just replacing the owner field with NULL.

If the owner field has the "Has Waiters" bit set (or CMPXCHG is not available),
the slow unlock path is taken.

The first thing done in the slow unlock path is to take the wait_lock of the
mutex.  This synchronizes the locking and unlocking of the mutex.

A check is made to see if the mutex has waiters or not.  On architectures that
do not have CMPXCHG, this is the location that the owner of the mutex will
determine if a waiter needs to be awoken or not.  On architectures that
do have CMPXCHG, that check is done in the fast path, but it is still needed
in the slow path too.  If a waiter of a mutex woke up because of a signal
or timeout between the time the owner failed the fast path CMPXCHG check and
the grabbing of the wait_lock, the mutex may not have any waiters, thus the
owner still needs to make this check. If there are no waiters then the mutex
owner field is set to NULL, the wait_lock is released and nothing more is
needed.

If there are waiters, then we need to wake one up and give that waiter
pending ownership.

On the wake up code, the pi_lock of the current owner is taken.  The top
waiter of the lock is found and removed from the wait_list of the mutex
as well as the pi_list of the current owner.  The task field of the new
pending owner's waiter structure is set to NULL, and the owner field of the
mutex is set to the new owner with the "Pending Owner" bit set, as well
as the "Has Waiters" bit if there still are other processes blocked on the
mutex.

The pi_lock of the previous owner is released, and the new pending owner's
pi_lock is taken.  Remember that this is the trick to prevent the race
condition in rt_mutex_adjust_prio_chain from adding itself as a waiter
on the mutex.

We now clear the "pi_blocked_on" field of the new pending owner, and if
the mutex still has waiters pending, we add the new top waiter to the pi_list
of the pending owner.

Finally we unlock the pi_lock of the pending owner and wake it up.


Contact
-------

For updates on this document, please email Steven Rostedt <rostedt@goodmis.org>


Credits
-------

Author:  Steven Rostedt <rostedt@goodmis.org>

Reviewers:  Ingo Molnar, Thomas Gleixner, Thomas Duetsch, and Randy Dunlap

Updates
-------

This document was originally written for 2.6.17-rc3-mm1