aboutsummaryrefslogtreecommitdiffstats
blob: a6ae3c9d9c4077f213243f3ae54e6df044ebb793 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
/*
 *  Port on Texas Instruments TMS320C6x architecture
 *
 *  Copyright (C) 2004, 2006, 2009, 2010, 2011 Texas Instruments Incorporated
 *  Author: Aurelien Jacquiot (aurelien.jacquiot@jaluna.com)
 *
 *  Large parts taken directly from powerpc.
 *
 *  This program is free software; you can redistribute it and/or modify
 *  it under the terms of the GNU General Public License version 2 as
 *  published by the Free Software Foundation.
 */
#ifndef _ASM_C6X_IRQ_H
#define _ASM_C6X_IRQ_H

#include <linux/threads.h>
#include <linux/list.h>
#include <linux/radix-tree.h>
#include <asm/percpu.h>

#define irq_canonicalize(irq)  (irq)

/*
 * The C64X+ core has 16 IRQ vectors. One each is used by Reset and NMI. Two
 * are reserved. The remaining 12 vectors are used to route SoC interrupts.
 * These interrupt vectors are prioritized with IRQ 4 having the highest
 * priority and IRQ 15 having the lowest.
 *
 * The C64x+ megamodule provides a PIC which combines SoC IRQ sources into a
 * single core IRQ vector. There are four combined sources, each of which
 * feed into one of the 12 general interrupt vectors. The remaining 8 vectors
 * can each route a single SoC interrupt directly.
 */
#define NR_PRIORITY_IRQS 16

#define NR_IRQS_LEGACY	NR_PRIORITY_IRQS

/* Total number of virq in the platform */
#define NR_IRQS		256

/* This number is used when no interrupt has been assigned */
#define NO_IRQ		0

/* This type is the placeholder for a hardware interrupt number. It has to
 * be big enough to enclose whatever representation is used by a given
 * platform.
 */
typedef unsigned long irq_hw_number_t;

/* Interrupt controller "host" data structure. This could be defined as a
 * irq domain controller. That is, it handles the mapping between hardware
 * and virtual interrupt numbers for a given interrupt domain. The host
 * structure is generally created by the PIC code for a given PIC instance
 * (though a host can cover more than one PIC if they have a flat number
 * model). It's the host callbacks that are responsible for setting the
 * irq_chip on a given irq_desc after it's been mapped.
 *
 * The host code and data structures are fairly agnostic to the fact that
 * we use an open firmware device-tree. We do have references to struct
 * device_node in two places: in irq_find_host() to find the host matching
 * a given interrupt controller node, and of course as an argument to its
 * counterpart host->ops->match() callback. However, those are treated as
 * generic pointers by the core and the fact that it's actually a device-node
 * pointer is purely a convention between callers and implementation. This
 * code could thus be used on other architectures by replacing those two
 * by some sort of arch-specific void * "token" used to identify interrupt
 * controllers.
 */
struct irq_host;
struct radix_tree_root;
struct device_node;

/* Functions below are provided by the host and called whenever a new mapping
 * is created or an old mapping is disposed. The host can then proceed to
 * whatever internal data structures management is required. It also needs
 * to setup the irq_desc when returning from map().
 */
struct irq_host_ops {
	/* Match an interrupt controller device node to a host, returns
	 * 1 on a match
	 */
	int (*match)(struct irq_host *h, struct device_node *node);

	/* Create or update a mapping between a virtual irq number and a hw
	 * irq number. This is called only once for a given mapping.
	 */
	int (*map)(struct irq_host *h, unsigned int virq, irq_hw_number_t hw);

	/* Dispose of such a mapping */
	void (*unmap)(struct irq_host *h, unsigned int virq);

	/* Translate device-tree interrupt specifier from raw format coming
	 * from the firmware to a irq_hw_number_t (interrupt line number) and
	 * type (sense) that can be passed to set_irq_type(). In the absence
	 * of this callback, irq_create_of_mapping() and irq_of_parse_and_map()
	 * will return the hw number in the first cell and IRQ_TYPE_NONE for
	 * the type (which amount to keeping whatever default value the
	 * interrupt controller has for that line)
	 */
	int (*xlate)(struct irq_host *h, struct device_node *ctrler,
		     const u32 *intspec, unsigned int intsize,
		     irq_hw_number_t *out_hwirq, unsigned int *out_type);
};

struct irq_host {
	struct list_head	link;

	/* type of reverse mapping technique */
	unsigned int		revmap_type;
#define IRQ_HOST_MAP_PRIORITY   0 /* core priority irqs, get irqs 1..15 */
#define IRQ_HOST_MAP_NOMAP	1 /* no fast reverse mapping */
#define IRQ_HOST_MAP_LINEAR	2 /* linear map of interrupts */
#define IRQ_HOST_MAP_TREE	3 /* radix tree */
	union {
		struct {
			unsigned int size;
			unsigned int *revmap;
		} linear;
		struct radix_tree_root tree;
	} revmap_data;
	struct irq_host_ops	*ops;
	void			*host_data;
	irq_hw_number_t		inval_irq;

	/* Optional device node pointer */
	struct device_node	*of_node;
};

struct irq_data;
extern irq_hw_number_t irqd_to_hwirq(struct irq_data *d);
extern irq_hw_number_t virq_to_hw(unsigned int virq);
extern bool virq_is_host(unsigned int virq, struct irq_host *host);

/**
 * irq_alloc_host - Allocate a new irq_host data structure
 * @of_node: optional device-tree node of the interrupt controller
 * @revmap_type: type of reverse mapping to use
 * @revmap_arg: for IRQ_HOST_MAP_LINEAR linear only: size of the map
 * @ops: map/unmap host callbacks
 * @inval_irq: provide a hw number in that host space that is always invalid
 *
 * Allocates and initialize and irq_host structure. Note that in the case of
 * IRQ_HOST_MAP_LEGACY, the map() callback will be called before this returns
 * for all legacy interrupts except 0 (which is always the invalid irq for
 * a legacy controller). For a IRQ_HOST_MAP_LINEAR, the map is allocated by
 * this call as well. For a IRQ_HOST_MAP_TREE, the radix tree will be allocated
 * later during boot automatically (the reverse mapping will use the slow path
 * until that happens).
 */
extern struct irq_host *irq_alloc_host(struct device_node *of_node,
				       unsigned int revmap_type,
				       unsigned int revmap_arg,
				       struct irq_host_ops *ops,
				       irq_hw_number_t inval_irq);


/**
 * irq_find_host - Locates a host for a given device node
 * @node: device-tree node of the interrupt controller
 */
extern struct irq_host *irq_find_host(struct device_node *node);


/**
 * irq_set_default_host - Set a "default" host
 * @host: default host pointer
 *
 * For convenience, it's possible to set a "default" host that will be used
 * whenever NULL is passed to irq_create_mapping(). It makes life easier for
 * platforms that want to manipulate a few hard coded interrupt numbers that
 * aren't properly represented in the device-tree.
 */
extern void irq_set_default_host(struct irq_host *host);


/**
 * irq_set_virq_count - Set the maximum number of virt irqs
 * @count: number of linux virtual irqs, capped with NR_IRQS
 *
 * This is mainly for use by platforms like iSeries who want to program
 * the virtual irq number in the controller to avoid the reverse mapping
 */
extern void irq_set_virq_count(unsigned int count);


/**
 * irq_create_mapping - Map a hardware interrupt into linux virq space
 * @host: host owning this hardware interrupt or NULL for default host
 * @hwirq: hardware irq number in that host space
 *
 * Only one mapping per hardware interrupt is permitted. Returns a linux
 * virq number.
 * If the sense/trigger is to be specified, set_irq_type() should be called
 * on the number returned from that call.
 */
extern unsigned int irq_create_mapping(struct irq_host *host,
				       irq_hw_number_t hwirq);


/**
 * irq_dispose_mapping - Unmap an interrupt
 * @virq: linux virq number of the interrupt to unmap
 */
extern void irq_dispose_mapping(unsigned int virq);

/**
 * irq_find_mapping - Find a linux virq from an hw irq number.
 * @host: host owning this hardware interrupt
 * @hwirq: hardware irq number in that host space
 *
 * This is a slow path, for use by generic code. It's expected that an
 * irq controller implementation directly calls the appropriate low level
 * mapping function.
 */
extern unsigned int irq_find_mapping(struct irq_host *host,
				     irq_hw_number_t hwirq);

/**
 * irq_create_direct_mapping - Allocate a virq for direct mapping
 * @host: host to allocate the virq for or NULL for default host
 *
 * This routine is used for irq controllers which can choose the hardware
 * interrupt numbers they generate. In such a case it's simplest to use
 * the linux virq as the hardware interrupt number.
 */
extern unsigned int irq_create_direct_mapping(struct irq_host *host);

/**
 * irq_radix_revmap_insert - Insert a hw irq to linux virq number mapping.
 * @host: host owning this hardware interrupt
 * @virq: linux irq number
 * @hwirq: hardware irq number in that host space
 *
 * This is for use by irq controllers that use a radix tree reverse
 * mapping for fast lookup.
 */
extern void irq_radix_revmap_insert(struct irq_host *host, unsigned int virq,
				    irq_hw_number_t hwirq);

/**
 * irq_radix_revmap_lookup - Find a linux virq from a hw irq number.
 * @host: host owning this hardware interrupt
 * @hwirq: hardware irq number in that host space
 *
 * This is a fast path, for use by irq controller code that uses radix tree
 * revmaps
 */
extern unsigned int irq_radix_revmap_lookup(struct irq_host *host,
					    irq_hw_number_t hwirq);

/**
 * irq_linear_revmap - Find a linux virq from a hw irq number.
 * @host: host owning this hardware interrupt
 * @hwirq: hardware irq number in that host space
 *
 * This is a fast path, for use by irq controller code that uses linear
 * revmaps. It does fallback to the slow path if the revmap doesn't exist
 * yet and will create the revmap entry with appropriate locking
 */

extern unsigned int irq_linear_revmap(struct irq_host *host,
				      irq_hw_number_t hwirq);



/**
 * irq_alloc_virt - Allocate virtual irq numbers
 * @host: host owning these new virtual irqs
 * @count: number of consecutive numbers to allocate
 * @hint: pass a hint number, the allocator will try to use a 1:1 mapping
 *
 * This is a low level function that is used internally by irq_create_mapping()
 * and that can be used by some irq controllers implementations for things
 * like allocating ranges of numbers for MSIs. The revmaps are left untouched.
 */
extern unsigned int irq_alloc_virt(struct irq_host *host,
				   unsigned int count,
				   unsigned int hint);

/**
 * irq_free_virt - Free virtual irq numbers
 * @virq: virtual irq number of the first interrupt to free
 * @count: number of interrupts to free
 *
 * This function is the opposite of irq_alloc_virt. It will not clear reverse
 * maps, this should be done previously by unmap'ing the interrupt. In fact,
 * all interrupts covered by the range being freed should have been unmapped
 * prior to calling this.
 */
extern void irq_free_virt(unsigned int virq, unsigned int count);

extern void __init init_pic_c64xplus(void);

extern void init_IRQ(void);

struct pt_regs;

extern asmlinkage void c6x_do_IRQ(unsigned int prio, struct pt_regs *regs);

extern unsigned long irq_err_count;

#endif /* _ASM_C6X_IRQ_H */