aboutsummaryrefslogtreecommitdiffstats
blob: 07cf288b692ed42bee86c3026247508b170d87ad (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
#ifndef _ASM_X86_ELF_H
#define _ASM_X86_ELF_H

/*
 * ELF register definitions..
 */
#include <linux/thread_info.h>

#include <asm/ptrace.h>
#include <asm/user.h>
#include <asm/auxvec.h>

typedef unsigned long elf_greg_t;

#define ELF_NGREG (sizeof(struct user_regs_struct) / sizeof(elf_greg_t))
typedef elf_greg_t elf_gregset_t[ELF_NGREG];

typedef struct user_i387_struct elf_fpregset_t;

#ifdef __i386__

typedef struct user_fxsr_struct elf_fpxregset_t;

#define R_386_NONE	0
#define R_386_32	1
#define R_386_PC32	2
#define R_386_GOT32	3
#define R_386_PLT32	4
#define R_386_COPY	5
#define R_386_GLOB_DAT	6
#define R_386_JMP_SLOT	7
#define R_386_RELATIVE	8
#define R_386_GOTOFF	9
#define R_386_GOTPC	10
#define R_386_NUM	11

/*
 * These are used to set parameters in the core dumps.
 */
#define ELF_CLASS	ELFCLASS32
#define ELF_DATA	ELFDATA2LSB
#define ELF_ARCH	EM_386

#else

/* x86-64 relocation types */
#define R_X86_64_NONE		0	/* No reloc */
#define R_X86_64_64		1	/* Direct 64 bit  */
#define R_X86_64_PC32		2	/* PC relative 32 bit signed */
#define R_X86_64_GOT32		3	/* 32 bit GOT entry */
#define R_X86_64_PLT32		4	/* 32 bit PLT address */
#define R_X86_64_COPY		5	/* Copy symbol at runtime */
#define R_X86_64_GLOB_DAT	6	/* Create GOT entry */
#define R_X86_64_JUMP_SLOT	7	/* Create PLT entry */
#define R_X86_64_RELATIVE	8	/* Adjust by program base */
#define R_X86_64_GOTPCREL	9	/* 32 bit signed pc relative
					   offset to GOT */
#define R_X86_64_32		10	/* Direct 32 bit zero extended */
#define R_X86_64_32S		11	/* Direct 32 bit sign extended */
#define R_X86_64_16		12	/* Direct 16 bit zero extended */
#define R_X86_64_PC16		13	/* 16 bit sign extended pc relative */
#define R_X86_64_8		14	/* Direct 8 bit sign extended  */
#define R_X86_64_PC8		15	/* 8 bit sign extended pc relative */

#define R_X86_64_NUM		16

/*
 * These are used to set parameters in the core dumps.
 */
#define ELF_CLASS	ELFCLASS64
#define ELF_DATA	ELFDATA2LSB
#define ELF_ARCH	EM_X86_64

#endif

#include <asm/vdso.h>

#ifdef CONFIG_X86_64
extern unsigned int vdso64_enabled;
#endif
#if defined(CONFIG_X86_32) || defined(CONFIG_IA32_EMULATION)
extern unsigned int vdso32_enabled;
#endif

/*
 * This is used to ensure we don't load something for the wrong architecture.
 */
#define elf_check_arch_ia32(x) \
	(((x)->e_machine == EM_386) || ((x)->e_machine == EM_486))

#include <asm/processor.h>

#ifdef CONFIG_X86_32
#include <asm/desc.h>

#define elf_check_arch(x)	elf_check_arch_ia32(x)

/* SVR4/i386 ABI (pages 3-31, 3-32) says that when the program starts %edx
   contains a pointer to a function which might be registered using `atexit'.
   This provides a mean for the dynamic linker to call DT_FINI functions for
   shared libraries that have been loaded before the code runs.

   A value of 0 tells we have no such handler.

   We might as well make sure everything else is cleared too (except for %esp),
   just to make things more deterministic.
 */
#define ELF_PLAT_INIT(_r, load_addr)		\
	do {					\
	_r->bx = 0; _r->cx = 0; _r->dx = 0;	\
	_r->si = 0; _r->di = 0; _r->bp = 0;	\
	_r->ax = 0;				\
} while (0)

/*
 * regs is struct pt_regs, pr_reg is elf_gregset_t (which is
 * now struct_user_regs, they are different)
 */

#define ELF_CORE_COPY_REGS_COMMON(pr_reg, regs)	\
do {						\
	pr_reg[0] = regs->bx;			\
	pr_reg[1] = regs->cx;			\
	pr_reg[2] = regs->dx;			\
	pr_reg[3] = regs->si;			\
	pr_reg[4] = regs->di;			\
	pr_reg[5] = regs->bp;			\
	pr_reg[6] = regs->ax;			\
	pr_reg[7] = regs->ds & 0xffff;		\
	pr_reg[8] = regs->es & 0xffff;		\
	pr_reg[9] = regs->fs & 0xffff;		\
	pr_reg[11] = regs->orig_ax;		\
	pr_reg[12] = regs->ip;			\
	pr_reg[13] = regs->cs & 0xffff;		\
	pr_reg[14] = regs->flags;		\
	pr_reg[15] = regs->sp;			\
	pr_reg[16] = regs->ss & 0xffff;		\
} while (0);

#define ELF_CORE_COPY_REGS(pr_reg, regs)	\
do {						\
	ELF_CORE_COPY_REGS_COMMON(pr_reg, regs);\
	pr_reg[10] = get_user_gs(regs);		\
} while (0);

#define ELF_CORE_COPY_KERNEL_REGS(pr_reg, regs)	\
do {						\
	ELF_CORE_COPY_REGS_COMMON(pr_reg, regs);\
	savesegment(gs, pr_reg[10]);		\
} while (0);

#define ELF_PLATFORM	(utsname()->machine)
#define set_personality_64bit()	do { } while (0)

#else /* CONFIG_X86_32 */

/*
 * This is used to ensure we don't load something for the wrong architecture.
 */
#define elf_check_arch(x)			\
	((x)->e_machine == EM_X86_64)

#define compat_elf_check_arch(x)					\
	(elf_check_arch_ia32(x) ||					\
	 (IS_ENABLED(CONFIG_X86_X32_ABI) && (x)->e_machine == EM_X86_64))

#if __USER32_DS != __USER_DS
# error "The following code assumes __USER32_DS == __USER_DS"
#endif

static inline void elf_common_init(struct thread_struct *t,
				   struct pt_regs *regs, const u16 ds)
{
	/* ax gets execve's return value. */
	/*regs->ax = */ regs->bx = regs->cx = regs->dx = 0;
	regs->si = regs->di = regs->bp = 0;
	regs->r8 = regs->r9 = regs->r10 = regs->r11 = 0;
	regs->r12 = regs->r13 = regs->r14 = regs->r15 = 0;
	t->fs = t->gs = 0;
	t->fsindex = t->gsindex = 0;
	t->ds = t->es = ds;
}

#define ELF_PLAT_INIT(_r, load_addr)			\
	elf_common_init(&current->thread, _r, 0)

#define	COMPAT_ELF_PLAT_INIT(regs, load_addr)		\
	elf_common_init(&current->thread, regs, __USER_DS)

void compat_start_thread(struct pt_regs *regs, u32 new_ip, u32 new_sp);
#define compat_start_thread compat_start_thread

void set_personality_ia32(bool);
#define COMPAT_SET_PERSONALITY(ex)			\
	set_personality_ia32((ex).e_machine == EM_X86_64)

#define COMPAT_ELF_PLATFORM			("i686")

/*
 * regs is struct pt_regs, pr_reg is elf_gregset_t (which is
 * now struct_user_regs, they are different). Assumes current is the process
 * getting dumped.
 */

#define ELF_CORE_COPY_REGS(pr_reg, regs)			\
do {								\
	unsigned v;						\
	(pr_reg)[0] = (regs)->r15;				\
	(pr_reg)[1] = (regs)->r14;				\
	(pr_reg)[2] = (regs)->r13;				\
	(pr_reg)[3] = (regs)->r12;				\
	(pr_reg)[4] = (regs)->bp;				\
	(pr_reg)[5] = (regs)->bx;				\
	(pr_reg)[6] = (regs)->r11;				\
	(pr_reg)[7] = (regs)->r10;				\
	(pr_reg)[8] = (regs)->r9;				\
	(pr_reg)[9] = (regs)->r8;				\
	(pr_reg)[10] = (regs)->ax;				\
	(pr_reg)[11] = (regs)->cx;				\
	(pr_reg)[12] = (regs)->dx;				\
	(pr_reg)[13] = (regs)->si;				\
	(pr_reg)[14] = (regs)->di;				\
	(pr_reg)[15] = (regs)->orig_ax;				\
	(pr_reg)[16] = (regs)->ip;				\
	(pr_reg)[17] = (regs)->cs;				\
	(pr_reg)[18] = (regs)->flags;				\
	(pr_reg)[19] = (regs)->sp;				\
	(pr_reg)[20] = (regs)->ss;				\
	(pr_reg)[21] = current->thread.fs;			\
	(pr_reg)[22] = current->thread.gs;			\
	asm("movl %%ds,%0" : "=r" (v)); (pr_reg)[23] = v;	\
	asm("movl %%es,%0" : "=r" (v)); (pr_reg)[24] = v;	\
	asm("movl %%fs,%0" : "=r" (v)); (pr_reg)[25] = v;	\
	asm("movl %%gs,%0" : "=r" (v)); (pr_reg)[26] = v;	\
} while (0);

/* I'm not sure if we can use '-' here */
#define ELF_PLATFORM       ("x86_64")
extern void set_personality_64bit(void);
extern unsigned int sysctl_vsyscall32;
extern int force_personality32;

#endif /* !CONFIG_X86_32 */

#define CORE_DUMP_USE_REGSET
#define ELF_EXEC_PAGESIZE	4096

/*
 * This is the base location for PIE (ET_DYN with INTERP) loads. On
 * 64-bit, this is raised to 4GB to leave the entire 32-bit address
 * space open for things that want to use the area for 32-bit pointers.
 */
#define ELF_ET_DYN_BASE		(mmap_is_ia32() ? 0x000400000UL : \
						  0x100000000UL)

/* This yields a mask that user programs can use to figure out what
   instruction set this CPU supports.  This could be done in user space,
   but it's not easy, and we've already done it here.  */

#define ELF_HWCAP		(boot_cpu_data.x86_capability[0])

/* This yields a string that ld.so will use to load implementation
   specific libraries for optimization.  This is more specific in
   intent than poking at uname or /proc/cpuinfo.

   For the moment, we have only optimizations for the Intel generations,
   but that could change... */

#define SET_PERSONALITY(ex) set_personality_64bit()

/*
 * An executable for which elf_read_implies_exec() returns TRUE will
 * have the READ_IMPLIES_EXEC personality flag set automatically.
 */
#define elf_read_implies_exec(ex, executable_stack)	\
	(executable_stack != EXSTACK_DISABLE_X)

struct task_struct;

#define	ARCH_DLINFO_IA32						\
do {									\
	if (VDSO_CURRENT_BASE) {					\
		NEW_AUX_ENT(AT_SYSINFO,	VDSO_ENTRY);			\
		NEW_AUX_ENT(AT_SYSINFO_EHDR, VDSO_CURRENT_BASE);	\
	}								\
} while (0)

#ifdef CONFIG_X86_32

#define STACK_RND_MASK (0x7ff)

#define ARCH_DLINFO		ARCH_DLINFO_IA32

/* update AT_VECTOR_SIZE_ARCH if the number of NEW_AUX_ENT entries changes */

#else /* CONFIG_X86_32 */

/* 1GB for 64bit, 8MB for 32bit */
#define STACK_RND_MASK (test_thread_flag(TIF_ADDR32) ? 0x7ff : 0x3fffff)

#define ARCH_DLINFO							\
do {									\
	if (vdso64_enabled)						\
		NEW_AUX_ENT(AT_SYSINFO_EHDR,				\
			    (unsigned long __force)current->mm->context.vdso); \
} while (0)

/* As a historical oddity, the x32 and x86_64 vDSOs are controlled together. */
#define ARCH_DLINFO_X32							\
do {									\
	if (vdso64_enabled)						\
		NEW_AUX_ENT(AT_SYSINFO_EHDR,				\
			    (unsigned long __force)current->mm->context.vdso); \
} while (0)

#define AT_SYSINFO		32

#define COMPAT_ARCH_DLINFO						\
if (test_thread_flag(TIF_X32))						\
	ARCH_DLINFO_X32;						\
else									\
	ARCH_DLINFO_IA32

#define COMPAT_ELF_ET_DYN_BASE	(TASK_UNMAPPED_BASE + 0x1000000)

#endif /* !CONFIG_X86_32 */

#define VDSO_CURRENT_BASE	((unsigned long)current->mm->context.vdso)

#define VDSO_ENTRY							\
	((unsigned long)current->mm->context.vdso +			\
	 vdso_image_32.sym___kernel_vsyscall)

struct linux_binprm;

#define ARCH_HAS_SETUP_ADDITIONAL_PAGES 1
extern int arch_setup_additional_pages(struct linux_binprm *bprm,
				       int uses_interp);
extern int compat_arch_setup_additional_pages(struct linux_binprm *bprm,
					      int uses_interp);
#define compat_arch_setup_additional_pages compat_arch_setup_additional_pages

/*
 * True on X86_32 or when emulating IA32 on X86_64
 */
static inline int mmap_is_ia32(void)
{
	return config_enabled(CONFIG_X86_32) ||
	       (config_enabled(CONFIG_COMPAT) &&
		test_thread_flag(TIF_ADDR32));
}

/* Do not change the values. See get_align_mask() */
enum align_flags {
	ALIGN_VA_32	= BIT(0),
	ALIGN_VA_64	= BIT(1),
};

struct va_alignment {
	int flags;
	unsigned long mask;
	unsigned long bits;
} ____cacheline_aligned;

extern struct va_alignment va_align;
extern unsigned long align_vdso_addr(unsigned long);
#endif /* _ASM_X86_ELF_H */