aboutsummaryrefslogtreecommitdiffstats
blob: 3c782d025c36c9673dc45e3f5603d69a660352ba (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
#
# Makefile for the linux kernel signature checking certificates.
#

obj-$(CONFIG_SYSTEM_TRUSTED_KEYRING) += system_keyring.o system_certificates.o

###############################################################################
#
# When a Kconfig string contains a filename, it is suitable for
# passing to shell commands. It is surrounded by double-quotes, and
# any double-quotes or backslashes within it are escaped by
# backslashes.
#
# This is no use for dependencies or $(wildcard). We need to strip the
# surrounding quotes and the escaping from quotes and backslashes, and
# we *do* need to escape any spaces in the string. So, for example:
#
# Usage: $(eval $(call config_filename,FOO))
#
# Defines FOO_FILENAME based on the contents of the CONFIG_FOO option,
# transformed as described above to be suitable for use within the
# makefile.
#
# Also, if the filename is a relative filename and exists in the source
# tree but not the build tree, define FOO_SRCPREFIX as $(srctree)/ to
# be prefixed to *both* command invocation and dependencies.
#
# Note: We also print the filenames in the quiet_cmd_foo text, and
# perhaps ought to have a version specially escaped for that purpose.
# But it's only cosmetic, and $(patsubst "%",%,$(CONFIG_FOO)) is good
# enough.  It'll strip the quotes in the common case where there's no
# space and it's a simple filename, and it'll retain the quotes when
# there's a space. There are some esoteric cases in which it'll print
# the wrong thing, but we don't really care. The actual dependencies
# and commands *do* get it right, with various combinations of single
# and double quotes, backslashes and spaces in the filenames.
#
###############################################################################
#
quote := $(firstword " ")
space :=
space +=
space_escape := %%%SPACE%%%
#
define config_filename
ifneq ($$(CONFIG_$(1)),"")
$(1)_FILENAME := $$(subst \\,\,$$(subst \$$(quote),$$(quote),$$(subst $$(space_escape),\$$(space),$$(patsubst "%",%,$$(subst $$(space),$$(space_escape),$$(CONFIG_$(1)))))))
ifneq ($$(patsubst /%,%,$$(firstword $$($(1)_FILENAME))),$$(firstword $$($(1)_FILENAME)))
else
ifeq ($$(wildcard $$($(1)_FILENAME)),)
ifneq ($$(wildcard $$(srctree)/$$($(1)_FILENAME)),)
$(1)_SRCPREFIX := $(srctree)/
endif
endif
endif
endif
endef
#
###############################################################################

ifeq ($(CONFIG_SYSTEM_TRUSTED_KEYRING),y)

$(eval $(call config_filename,SYSTEM_TRUSTED_KEYS))

# GCC doesn't include .incbin files in -MD generated dependencies (PR#66871)
$(obj)/system_certificates.o: $(obj)/x509_certificate_list

# Cope with signing_key.x509 existing in $(srctree) not $(objtree)
AFLAGS_system_certificates.o := -I$(srctree)

quiet_cmd_extract_certs  = EXTRACT_CERTS   $(patsubst "%",%,$(2))
      cmd_extract_certs  = scripts/extract-cert $(2) $@ || ( rm $@; exit 1)

targets += x509_certificate_list
$(obj)/x509_certificate_list: scripts/extract-cert $(SYSTEM_TRUSTED_KEYS_SRCPREFIX)$(SYSTEM_TRUSTED_KEYS_FILENAME) FORCE
	$(call if_changed,extract_certs,$(SYSTEM_TRUSTED_KEYS_SRCPREFIX)$(CONFIG_SYSTEM_TRUSTED_KEYS))
endif

clean-files := x509_certificate_list .x509.list

ifeq ($(CONFIG_MODULE_SIG),y)
###############################################################################
#
# If module signing is requested, say by allyesconfig, but a key has not been
# supplied, then one will need to be generated to make sure the build does not
# fail and that the kernel may be used afterwards.
#
###############################################################################
ifndef CONFIG_MODULE_SIG_HASH
$(error Could not determine digest type to use from kernel config)
endif

# We do it this way rather than having a boolean option for enabling an
# external private key, because 'make randconfig' might enable such a
# boolean option and we unfortunately can't make it depend on !RANDCONFIG.
ifeq ($(CONFIG_MODULE_SIG_KEY),"certs/signing_key.pem")
$(obj)/signing_key.pem: $(obj)/x509.genkey
	@echo "###"
	@echo "### Now generating an X.509 key pair to be used for signing modules."
	@echo "###"
	@echo "### If this takes a long time, you might wish to run rngd in the"
	@echo "### background to keep the supply of entropy topped up.  It"
	@echo "### needs to be run as root, and uses a hardware random"
	@echo "### number generator if one is available."
	@echo "###"
	openssl req -new -nodes -utf8 -$(CONFIG_MODULE_SIG_HASH) -days 36500 \
		-batch -x509 -config $(obj)/x509.genkey \
		-outform PEM -out $(obj)/signing_key.pem \
		-keyout $(obj)/signing_key.pem 2>&1
	@echo "###"
	@echo "### Key pair generated."
	@echo "###"

$(obj)/x509.genkey:
	@echo Generating X.509 key generation config
	@echo  >$@ "[ req ]"
	@echo >>$@ "default_bits = 4096"
	@echo >>$@ "distinguished_name = req_distinguished_name"
	@echo >>$@ "prompt = no"
	@echo >>$@ "string_mask = utf8only"
	@echo >>$@ "x509_extensions = myexts"
	@echo >>$@
	@echo >>$@ "[ req_distinguished_name ]"
	@echo >>$@ "#O = Unspecified company"
	@echo >>$@ "CN = Build time autogenerated kernel key"
	@echo >>$@ "#emailAddress = unspecified.user@unspecified.company"
	@echo >>$@
	@echo >>$@ "[ myexts ]"
	@echo >>$@ "basicConstraints=critical,CA:FALSE"
	@echo >>$@ "keyUsage=digitalSignature"
	@echo >>$@ "subjectKeyIdentifier=hash"
	@echo >>$@ "authorityKeyIdentifier=keyid"
endif

$(eval $(call config_filename,MODULE_SIG_KEY))

# If CONFIG_MODULE_SIG_KEY isn't a PKCS#11 URI, depend on it
ifeq ($(patsubst pkcs11:%,%,$(firstword $(MODULE_SIG_KEY_FILENAME))),$(firstword $(MODULE_SIG_KEY_FILENAME)))
X509_DEP := $(MODULE_SIG_KEY_SRCPREFIX)$(MODULE_SIG_KEY_FILENAME)
endif

# GCC PR#66871 again.
$(obj)/system_certificates.o: $(obj)/signing_key.x509

targets += signing_key.x509
$(obj)/signing_key.x509: scripts/extract-cert $(X509_DEP) FORCE
	$(call if_changed,extract_certs,$(MODULE_SIG_KEY_SRCPREFIX)$(CONFIG_MODULE_SIG_KEY))
endif