aboutsummaryrefslogtreecommitdiffstats
blob: 7b02b652e267e016a60c69f1c47e31689332a07b (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
/*
 *  Copyright (c) 2000-2001 Vojtech Pavlik
 *
 *  Based on the work of:
 *	Alan Cox	Robin O'Leary
 */

/*
 * IBM PC110 touchpad driver for Linux
 */

/*
 * This program is free software; you can redistribute it and/or modify
 * it under the terms of the GNU General Public License as published by
 * the Free Software Foundation; either version 2 of the License, or
 * (at your option) any later version.
 *
 * This program is distributed in the hope that it will be useful,
 * but WITHOUT ANY WARRANTY; without even the implied warranty of
 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
 * GNU General Public License for more details.
 *
 * You should have received a copy of the GNU General Public License
 * along with this program; if not, write to the Free Software
 * Foundation, Inc., 59 Temple Place, Suite 330, Boston, MA 02111-1307 USA
 *
 * Should you need to contact me, the author, you can do so either by
 * e-mail - mail your message to <vojtech@ucw.cz>, or by paper mail:
 * Vojtech Pavlik, Simunkova 1594, Prague 8, 182 00 Czech Republic
 */

#include <linux/module.h>
#include <linux/kernel.h>
#include <linux/errno.h>
#include <linux/ioport.h>
#include <linux/input.h>
#include <linux/init.h>
#include <linux/interrupt.h>
#include <linux/pci.h>
#include <linux/delay.h>

#include <asm/io.h>
#include <asm/irq.h>

MODULE_AUTHOR("Vojtech Pavlik <vojtech@ucw.cz>");
MODULE_DESCRIPTION("IBM PC110 touchpad driver");
MODULE_LICENSE("GPL");

#define PC110PAD_OFF	0x30
#define PC110PAD_ON	0x38

static int pc110pad_irq = 10;
static int pc110pad_io = 0x15e0;

static struct input_dev *pc110pad_dev;
static int pc110pad_data[3];
static int pc110pad_count;

static irqreturn_t pc110pad_interrupt(int irq, void *ptr)
{
	int value     = inb_p(pc110pad_io);
	int handshake = inb_p(pc110pad_io + 2);

	outb(handshake |  1, pc110pad_io + 2);
	udelay(2);
	outb(handshake & ~1, pc110pad_io + 2);
	udelay(2);
	inb_p(0x64);

	pc110pad_data[pc110pad_count++] = value;

	if (pc110pad_count < 3)
		return IRQ_HANDLED;

	input_report_key(pc110pad_dev, BTN_TOUCH,
		pc110pad_data[0] & 0x01);
	input_report_abs(pc110pad_dev, ABS_X,
		pc110pad_data[1] | ((pc110pad_data[0] << 3) & 0x80) | ((pc110pad_data[0] << 1) & 0x100));
	input_report_abs(pc110pad_dev, ABS_Y,
		pc110pad_data[2] | ((pc110pad_data[0] << 4) & 0x80));
	input_sync(pc110pad_dev);

	pc110pad_count = 0;
	return IRQ_HANDLED;
}

static void pc110pad_close(struct input_dev *dev)
{
	outb(PC110PAD_OFF, pc110pad_io + 2);
}

static int pc110pad_open(struct input_dev *dev)
{
	pc110pad_interrupt(0, NULL);
	pc110pad_interrupt(0, NULL);
	pc110pad_interrupt(0, NULL);
	outb(PC110PAD_ON, pc110pad_io + 2);
	pc110pad_count = 0;

	return 0;
}

/*
 * We try to avoid enabling the hardware if it's not
 * there, but we don't know how to test. But we do know
 * that the PC110 is not a PCI system. So if we find any
 * PCI devices in the machine, we don't have a PC110.
 */
static int __init pc110pad_init(void)
{
	int err;

	if (!no_pci_devices())
		return -ENODEV;

	if (!request_region(pc110pad_io, 4, "pc110pad")) {
		printk(KERN_ERR "pc110pad: I/O area %#x-%#x in use.\n",
				pc110pad_io, pc110pad_io + 4);
		return -EBUSY;
	}

	outb(PC110PAD_OFF, pc110pad_io + 2);

	if (request_irq(pc110pad_irq, pc110pad_interrupt, 0, "pc110pad", NULL)) {
		printk(KERN_ERR "pc110pad: Unable to get irq %d.\n", pc110pad_irq);
		err = -EBUSY;
		goto err_release_region;
	}

	pc110pad_dev = input_allocate_device();
	if (!pc110pad_dev) {
		printk(KERN_ERR "pc110pad: Not enough memory.\n");
		err = -ENOMEM;
		goto err_free_irq;
	}

	pc110pad_dev->name = "IBM PC110 TouchPad";
	pc110pad_dev->phys = "isa15e0/input0";
	pc110pad_dev->id.bustype = BUS_ISA;
	pc110pad_dev->id.vendor = 0x0003;
	pc110pad_dev->id.product = 0x0001;
	pc110pad_dev->id.version = 0x0100;

	pc110pad_dev->evbit[0] = BIT_MASK(EV_KEY) | BIT_MASK(EV_ABS);
	pc110pad_dev->absbit[0] = BIT_MASK(ABS_X) | BIT_MASK(ABS_Y);
	pc110pad_dev->keybit[BIT_WORD(BTN_TOUCH)] = BIT_MASK(BTN_TOUCH);

	input_abs_set_max(pc110pad_dev, ABS_X, 0x1ff);
	input_abs_set_max(pc110pad_dev, ABS_Y, 0x0ff);

	pc110pad_dev->open = pc110pad_open;
	pc110pad_dev->close = pc110pad_close;

	err = input_register_device(pc110pad_dev);
	if (err)
		goto err_free_dev;

	return 0;

 err_free_dev:
	input_free_device(pc110pad_dev);
 err_free_irq:
	free_irq(pc110pad_irq, NULL);
 err_release_region:
	release_region(pc110pad_io, 4);

	return err;
}

static void __exit pc110pad_exit(void)
{
	outb(PC110PAD_OFF, pc110pad_io + 2);
	free_irq(pc110pad_irq, NULL);
	input_unregister_device(pc110pad_dev);
	release_region(pc110pad_io, 4);
}

module_init(pc110pad_init);
module_exit(pc110pad_exit);