aboutsummaryrefslogtreecommitdiffstats
blob: 6a1d6447b864d527ed0db5d5aca6ce67703ac227 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
402
403
404
405
406
407
408
409
410
411
412
413
414
415
416
417
418
419
420
421
422
423
424
425
426
427
428
429
430
431
432
433
434
435
436
437
438
439
440
441
442
443
444
445
446
447
448
449
450
451
452
453
454
455
456
457
458
459
460
461
462
463
464
465
466
467
468
469
470
471
472
473
474
475
476
477
478
479
480
481
482
483
484
485
486
487
488
489
490
491
492
493
494
495
496
497
498
499
500
501
502
503
504
505
506
507
508
509
510
511
512
513
514
515
516
517
518
519
520
521
522
523
524
525
526
527
/*P:050
 * Lguest guests use a very simple method to describe devices.  It's a
 * series of device descriptors contained just above the top of normal Guest
 * memory.
 *
 * We use the standard "virtio" device infrastructure, which provides us with a
 * console, a network and a block driver.  Each one expects some configuration
 * information and a "virtqueue" or two to send and receive data.
:*/
#include <linux/init.h>
#include <linux/bootmem.h>
#include <linux/lguest_launcher.h>
#include <linux/virtio.h>
#include <linux/virtio_config.h>
#include <linux/interrupt.h>
#include <linux/virtio_ring.h>
#include <linux/err.h>
#include <linux/export.h>
#include <linux/slab.h>
#include <asm/io.h>
#include <asm/paravirt.h>
#include <asm/lguest_hcall.h>

/* The pointer to our (page) of device descriptions. */
static void *lguest_devices;

/*
 * For Guests, device memory can be used as normal memory, so we cast away the
 * __iomem to quieten sparse.
 */
static inline void *lguest_map(unsigned long phys_addr, unsigned long pages)
{
	return (__force void *)ioremap_cache(phys_addr, PAGE_SIZE*pages);
}

static inline void lguest_unmap(void *addr)
{
	iounmap((__force void __iomem *)addr);
}

/*D:100
 * Each lguest device is just a virtio device plus a pointer to its entry
 * in the lguest_devices page.
 */
struct lguest_device {
	struct virtio_device vdev;

	/* The entry in the lguest_devices page for this device. */
	struct lguest_device_desc *desc;
};

/*
 * Since the virtio infrastructure hands us a pointer to the virtio_device all
 * the time, it helps to have a curt macro to get a pointer to the struct
 * lguest_device it's enclosed in.
 */
#define to_lgdev(vd) container_of(vd, struct lguest_device, vdev)

/*D:130
 * Device configurations
 *
 * The configuration information for a device consists of one or more
 * virtqueues, a feature bitmap, and some configuration bytes.  The
 * configuration bytes don't really matter to us: the Launcher sets them up, and
 * the driver will look at them during setup.
 *
 * A convenient routine to return the device's virtqueue config array:
 * immediately after the descriptor.
 */
static struct lguest_vqconfig *lg_vq(const struct lguest_device_desc *desc)
{
	return (void *)(desc + 1);
}

/* The features come immediately after the virtqueues. */
static u8 *lg_features(const struct lguest_device_desc *desc)
{
	return (void *)(lg_vq(desc) + desc->num_vq);
}

/* The config space comes after the two feature bitmasks. */
static u8 *lg_config(const struct lguest_device_desc *desc)
{
	return lg_features(desc) + desc->feature_len * 2;
}

/* The total size of the config page used by this device (incl. desc) */
static unsigned desc_size(const struct lguest_device_desc *desc)
{
	return sizeof(*desc)
		+ desc->num_vq * sizeof(struct lguest_vqconfig)
		+ desc->feature_len * 2
		+ desc->config_len;
}

/* This gets the device's feature bits. */
static u32 lg_get_features(struct virtio_device *vdev)
{
	unsigned int i;
	u32 features = 0;
	struct lguest_device_desc *desc = to_lgdev(vdev)->desc;
	u8 *in_features = lg_features(desc);

	/* We do this the slow but generic way. */
	for (i = 0; i < min(desc->feature_len * 8, 32); i++)
		if (in_features[i / 8] & (1 << (i % 8)))
			features |= (1 << i);

	return features;
}

/*
 * To notify on reset or feature finalization, we (ab)use the NOTIFY
 * hypercall, with the descriptor address of the device.
 */
static void status_notify(struct virtio_device *vdev)
{
	unsigned long offset = (void *)to_lgdev(vdev)->desc - lguest_devices;

	hcall(LHCALL_NOTIFY, (max_pfn << PAGE_SHIFT) + offset, 0, 0, 0);
}

/*
 * The virtio core takes the features the Host offers, and copies the ones
 * supported by the driver into the vdev->features array.  Once that's all
 * sorted out, this routine is called so we can tell the Host which features we
 * understand and accept.
 */
static void lg_finalize_features(struct virtio_device *vdev)
{
	unsigned int i, bits;
	struct lguest_device_desc *desc = to_lgdev(vdev)->desc;
	/* Second half of bitmap is features we accept. */
	u8 *out_features = lg_features(desc) + desc->feature_len;

	/* Give virtio_ring a chance to accept features. */
	vring_transport_features(vdev);

	/*
	 * The vdev->feature array is a Linux bitmask: this isn't the same as a
	 * the simple array of bits used by lguest devices for features.  So we
	 * do this slow, manual conversion which is completely general.
	 */
	memset(out_features, 0, desc->feature_len);
	bits = min_t(unsigned, desc->feature_len, sizeof(vdev->features)) * 8;
	for (i = 0; i < bits; i++) {
		if (test_bit(i, vdev->features))
			out_features[i / 8] |= (1 << (i % 8));
	}

	/* Tell Host we've finished with this device's feature negotiation */
	status_notify(vdev);
}

/* Once they've found a field, getting a copy of it is easy. */
static void lg_get(struct virtio_device *vdev, unsigned int offset,
		   void *buf, unsigned len)
{
	struct lguest_device_desc *desc = to_lgdev(vdev)->desc;

	/* Check they didn't ask for more than the length of the config! */
	BUG_ON(offset + len > desc->config_len);
	memcpy(buf, lg_config(desc) + offset, len);
}

/* Setting the contents is also trivial. */
static void lg_set(struct virtio_device *vdev, unsigned int offset,
		   const void *buf, unsigned len)
{
	struct lguest_device_desc *desc = to_lgdev(vdev)->desc;

	/* Check they didn't ask for more than the length of the config! */
	BUG_ON(offset + len > desc->config_len);
	memcpy(lg_config(desc) + offset, buf, len);
}

/*
 * The operations to get and set the status word just access the status field
 * of the device descriptor.
 */
static u8 lg_get_status(struct virtio_device *vdev)
{
	return to_lgdev(vdev)->desc->status;
}

static void lg_set_status(struct virtio_device *vdev, u8 status)
{
	BUG_ON(!status);
	to_lgdev(vdev)->desc->status = status;

	/* Tell Host immediately if we failed. */
	if (status & VIRTIO_CONFIG_S_FAILED)
		status_notify(vdev);
}

static void lg_reset(struct virtio_device *vdev)
{
	/* 0 status means "reset" */
	to_lgdev(vdev)->desc->status = 0;
	status_notify(vdev);
}

/*
 * Virtqueues
 *
 * The other piece of infrastructure virtio needs is a "virtqueue": a way of
 * the Guest device registering buffers for the other side to read from or
 * write into (ie. send and receive buffers).  Each device can have multiple
 * virtqueues: for example the console driver uses one queue for sending and
 * another for receiving.
 *
 * Fortunately for us, a very fast shared-memory-plus-descriptors virtqueue
 * already exists in virtio_ring.c.  We just need to connect it up.
 *
 * We start with the information we need to keep about each virtqueue.
 */

/*D:140 This is the information we remember about each virtqueue. */
struct lguest_vq_info {
	/* A copy of the information contained in the device config. */
	struct lguest_vqconfig config;

	/* The address where we mapped the virtio ring, so we can unmap it. */
	void *pages;
};

/*
 * When the virtio_ring code wants to prod the Host, it calls us here and we
 * make a hypercall.  We hand the physical address of the virtqueue so the Host
 * knows which virtqueue we're talking about.
 */
static void lg_notify(struct virtqueue *vq)
{
	/*
	 * We store our virtqueue information in the "priv" pointer of the
	 * virtqueue structure.
	 */
	struct lguest_vq_info *lvq = vq->priv;

	hcall(LHCALL_NOTIFY, lvq->config.pfn << PAGE_SHIFT, 0, 0, 0);
}

/* An extern declaration inside a C file is bad form.  Don't do it. */
extern void lguest_setup_irq(unsigned int irq);

/*
 * This routine finds the Nth virtqueue described in the configuration of
 * this device and sets it up.
 *
 * This is kind of an ugly duckling.  It'd be nicer to have a standard
 * representation of a virtqueue in the configuration space, but it seems that
 * everyone wants to do it differently.  The KVM coders want the Guest to
 * allocate its own pages and tell the Host where they are, but for lguest it's
 * simpler for the Host to simply tell us where the pages are.
 */
static struct virtqueue *lg_find_vq(struct virtio_device *vdev,
				    unsigned index,
				    void (*callback)(struct virtqueue *vq),
				    const char *name)
{
	struct lguest_device *ldev = to_lgdev(vdev);
	struct lguest_vq_info *lvq;
	struct virtqueue *vq;
	int err;

	/* We must have this many virtqueues. */
	if (index >= ldev->desc->num_vq)
		return ERR_PTR(-ENOENT);

	lvq = kmalloc(sizeof(*lvq), GFP_KERNEL);
	if (!lvq)
		return ERR_PTR(-ENOMEM);

	/*
	 * Make a copy of the "struct lguest_vqconfig" entry, which sits after
	 * the descriptor.  We need a copy because the config space might not
	 * be aligned correctly.
	 */
	memcpy(&lvq->config, lg_vq(ldev->desc)+index, sizeof(lvq->config));

	printk("Mapping virtqueue %i addr %lx\n", index,
	       (unsigned long)lvq->config.pfn << PAGE_SHIFT);
	/* Figure out how many pages the ring will take, and map that memory */
	lvq->pages = lguest_map((unsigned long)lvq->config.pfn << PAGE_SHIFT,
				DIV_ROUND_UP(vring_size(lvq->config.num,
							LGUEST_VRING_ALIGN),
					     PAGE_SIZE));
	if (!lvq->pages) {
		err = -ENOMEM;
		goto free_lvq;
	}

	/*
	 * OK, tell virtio_ring.c to set up a virtqueue now we know its size
	 * and we've got a pointer to its pages.  Note that we set weak_barriers
	 * to 'true': the host just a(nother) SMP CPU, so we only need inter-cpu
	 * barriers.
	 */
	vq = vring_new_virtqueue(lvq->config.num, LGUEST_VRING_ALIGN, vdev,
				 true, lvq->pages, lg_notify, callback, name);
	if (!vq) {
		err = -ENOMEM;
		goto unmap;
	}

	/* Make sure the interrupt is allocated. */
	lguest_setup_irq(lvq->config.irq);

	/*
	 * Tell the interrupt for this virtqueue to go to the virtio_ring
	 * interrupt handler.
	 *
	 * FIXME: We used to have a flag for the Host to tell us we could use
	 * the interrupt as a source of randomness: it'd be nice to have that
	 * back.
	 */
	err = request_irq(lvq->config.irq, vring_interrupt, IRQF_SHARED,
			  dev_name(&vdev->dev), vq);
	if (err)
		goto destroy_vring;

	/*
	 * Last of all we hook up our 'struct lguest_vq_info" to the
	 * virtqueue's priv pointer.
	 */
	vq->priv = lvq;
	return vq;

destroy_vring:
	vring_del_virtqueue(vq);
unmap:
	lguest_unmap(lvq->pages);
free_lvq:
	kfree(lvq);
	return ERR_PTR(err);
}
/*:*/

/* Cleaning up a virtqueue is easy */
static void lg_del_vq(struct virtqueue *vq)
{
	struct lguest_vq_info *lvq = vq->priv;

	/* Release the interrupt */
	free_irq(lvq->config.irq, vq);
	/* Tell virtio_ring.c to free the virtqueue. */
	vring_del_virtqueue(vq);
	/* Unmap the pages containing the ring. */
	lguest_unmap(lvq->pages);
	/* Free our own queue information. */
	kfree(lvq);
}

static void lg_del_vqs(struct virtio_device *vdev)
{
	struct virtqueue *vq, *n;

	list_for_each_entry_safe(vq, n, &vdev->vqs, list)
		lg_del_vq(vq);
}

static int lg_find_vqs(struct virtio_device *vdev, unsigned nvqs,
		       struct virtqueue *vqs[],
		       vq_callback_t *callbacks[],
		       const char *names[])
{
	struct lguest_device *ldev = to_lgdev(vdev);
	int i;

	/* We must have this many virtqueues. */
	if (nvqs > ldev->desc->num_vq)
		return -ENOENT;

	for (i = 0; i < nvqs; ++i) {
		vqs[i] = lg_find_vq(vdev, i, callbacks[i], names[i]);
		if (IS_ERR(vqs[i]))
			goto error;
	}
	return 0;

error:
	lg_del_vqs(vdev);
	return PTR_ERR(vqs[i]);
}

static const char *lg_bus_name(struct virtio_device *vdev)
{
	return "";
}

/* The ops structure which hooks everything together. */
static struct virtio_config_ops lguest_config_ops = {
	.get_features = lg_get_features,
	.finalize_features = lg_finalize_features,
	.get = lg_get,
	.set = lg_set,
	.get_status = lg_get_status,
	.set_status = lg_set_status,
	.reset = lg_reset,
	.find_vqs = lg_find_vqs,
	.del_vqs = lg_del_vqs,
	.bus_name = lg_bus_name,
};

/*
 * The root device for the lguest virtio devices.  This makes them appear as
 * /sys/devices/lguest/0,1,2 not /sys/devices/0,1,2.
 */
static struct device *lguest_root;

/*D:120
 * This is the core of the lguest bus: actually adding a new device.
 * It's a separate function because it's neater that way, and because an
 * earlier version of the code supported hotplug and unplug.  They were removed
 * early on because they were never used.
 *
 * As Andrew Tridgell says, "Untested code is buggy code".
 *
 * It's worth reading this carefully: we start with a pointer to the new device
 * descriptor in the "lguest_devices" page, and the offset into the device
 * descriptor page so we can uniquely identify it if things go badly wrong.
 */
static void add_lguest_device(struct lguest_device_desc *d,
			      unsigned int offset)
{
	struct lguest_device *ldev;

	/* Start with zeroed memory; Linux's device layer counts on it. */
	ldev = kzalloc(sizeof(*ldev), GFP_KERNEL);
	if (!ldev) {
		printk(KERN_EMERG "Cannot allocate lguest dev %u type %u\n",
		       offset, d->type);
		return;
	}

	/* This devices' parent is the lguest/ dir. */
	ldev->vdev.dev.parent = lguest_root;
	/*
	 * The device type comes straight from the descriptor.  There's also a
	 * device vendor field in the virtio_device struct, which we leave as
	 * 0.
	 */
	ldev->vdev.id.device = d->type;
	/*
	 * We have a simple set of routines for querying the device's
	 * configuration information and setting its status.
	 */
	ldev->vdev.config = &lguest_config_ops;
	/* And we remember the device's descriptor for lguest_config_ops. */
	ldev->desc = d;

	/*
	 * register_virtio_device() sets up the generic fields for the struct
	 * virtio_device and calls device_register().  This makes the bus
	 * infrastructure look for a matching driver.
	 */
	if (register_virtio_device(&ldev->vdev) != 0) {
		printk(KERN_ERR "Failed to register lguest dev %u type %u\n",
		       offset, d->type);
		kfree(ldev);
	}
}

/*D:110
 * scan_devices() simply iterates through the device page.  The type 0 is
 * reserved to mean "end of devices".
 */
static void scan_devices(void)
{
	unsigned int i;
	struct lguest_device_desc *d;

	/* We start at the page beginning, and skip over each entry. */
	for (i = 0; i < PAGE_SIZE; i += desc_size(d)) {
		d = lguest_devices + i;

		/* Once we hit a zero, stop. */
		if (d->type == 0)
			break;

		printk("Device at %i has size %u\n", i, desc_size(d));
		add_lguest_device(d, i);
	}
}

/*D:105
 * Fairly early in boot, lguest_devices_init() is called to set up the
 * lguest device infrastructure.  We check that we are a Guest by checking
 * pv_info.name: there are other ways of checking, but this seems most
 * obvious to me.
 *
 * So we can access the "struct lguest_device_desc"s easily, we map that memory
 * and store the pointer in the global "lguest_devices".  Then we register a
 * root device from which all our devices will hang (this seems to be the
 * correct sysfs incantation).
 *
 * Finally we call scan_devices() which adds all the devices found in the
 * lguest_devices page.
 */
static int __init lguest_devices_init(void)
{
	if (strcmp(pv_info.name, "lguest") != 0)
		return 0;

	lguest_root = root_device_register("lguest");
	if (IS_ERR(lguest_root))
		panic("Could not register lguest root");

	/* Devices are in a single page above top of "normal" mem */
	lguest_devices = lguest_map(max_pfn<<PAGE_SHIFT, 1);

	scan_devices();
	return 0;
}
/* We do this after core stuff, but before the drivers. */
postcore_initcall(lguest_devices_init);

/*D:150
 * At this point in the journey we used to now wade through the lguest
 * devices themselves: net, block and console.  Since they're all now virtio
 * devices rather than lguest-specific, I've decided to ignore them.  Mostly,
 * they're kind of boring.  But this does mean you'll never experience the
 * thrill of reading the forbidden love scene buried deep in the block driver.
 *
 * "make Launcher" beckons, where we answer questions like "Where do Guests
 * come from?", and "What do you do when someone asks for optimization?".
 */