aboutsummaryrefslogtreecommitdiffstats
blob: da165f6adcbfa67a12f9f19363692ab6c5d00d19 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
/*
 *  linux/fs/filesystems.c
 *
 *  Copyright (C) 1991, 1992  Linus Torvalds
 *
 *  table of configured filesystems
 */

#include <linux/syscalls.h>
#include <linux/fs.h>
#include <linux/proc_fs.h>
#include <linux/seq_file.h>
#include <linux/kmod.h>
#include <linux/init.h>
#include <linux/module.h>
#include <linux/slab.h>
#include <asm/uaccess.h>

/*
 * Handling of filesystem drivers list.
 * Rules:
 *	Inclusion to/removals from/scanning of list are protected by spinlock.
 *	During the unload module must call unregister_filesystem().
 *	We can access the fields of list element if:
 *		1) spinlock is held or
 *		2) we hold the reference to the module.
 *	The latter can be guaranteed by call of try_module_get(); if it
 *	returned 0 we must skip the element, otherwise we got the reference.
 *	Once the reference is obtained we can drop the spinlock.
 */

static struct file_system_type *file_systems;
static DEFINE_RWLOCK(file_systems_lock);

/* WARNING: This can be used only if we _already_ own a reference */
void get_filesystem(struct file_system_type *fs)
{
	__module_get(fs->owner);
}

void put_filesystem(struct file_system_type *fs)
{
	module_put(fs->owner);
}

static struct file_system_type **find_filesystem(const char *name, unsigned len)
{
	struct file_system_type **p;
	for (p=&file_systems; *p; p=&(*p)->next)
		if (strlen((*p)->name) == len &&
		    strncmp((*p)->name, name, len) == 0)
			break;
	return p;
}

/**
 *	register_filesystem - register a new filesystem
 *	@fs: the file system structure
 *
 *	Adds the file system passed to the list of file systems the kernel
 *	is aware of for mount and other syscalls. Returns 0 on success,
 *	or a negative errno code on an error.
 *
 *	The &struct file_system_type that is passed is linked into the kernel 
 *	structures and must not be freed until the file system has been
 *	unregistered.
 */
 
int register_filesystem(struct file_system_type * fs)
{
	int res = 0;
	struct file_system_type ** p;

	BUG_ON(strchr(fs->name, '.'));
	if (fs->next)
		return -EBUSY;
	write_lock(&file_systems_lock);
	p = find_filesystem(fs->name, strlen(fs->name));
	if (*p)
		res = -EBUSY;
	else
		*p = fs;
	write_unlock(&file_systems_lock);
	return res;
}

EXPORT_SYMBOL(register_filesystem);

/**
 *	unregister_filesystem - unregister a file system
 *	@fs: filesystem to unregister
 *
 *	Remove a file system that was previously successfully registered
 *	with the kernel. An error is returned if the file system is not found.
 *	Zero is returned on a success.
 *	
 *	Once this function has returned the &struct file_system_type structure
 *	may be freed or reused.
 */
 
int unregister_filesystem(struct file_system_type * fs)
{
	struct file_system_type ** tmp;

	write_lock(&file_systems_lock);
	tmp = &file_systems;
	while (*tmp) {
		if (fs == *tmp) {
			*tmp = fs->next;
			fs->next = NULL;
			write_unlock(&file_systems_lock);
			synchronize_rcu();
			return 0;
		}
		tmp = &(*tmp)->next;
	}
	write_unlock(&file_systems_lock);

	return -EINVAL;
}

EXPORT_SYMBOL(unregister_filesystem);

static int fs_index(const char __user * __name)
{
	struct file_system_type * tmp;
	struct filename *name;
	int err, index;

	name = getname(__name);
	err = PTR_ERR(name);
	if (IS_ERR(name))
		return err;

	err = -EINVAL;
	read_lock(&file_systems_lock);
	for (tmp=file_systems, index=0 ; tmp ; tmp=tmp->next, index++) {
		if (strcmp(tmp->name, name->name) == 0) {
			err = index;
			break;
		}
	}
	read_unlock(&file_systems_lock);
	putname(name);
	return err;
}

static int fs_name(unsigned int index, char __user * buf)
{
	struct file_system_type * tmp;
	int len, res;

	read_lock(&file_systems_lock);
	for (tmp = file_systems; tmp; tmp = tmp->next, index--)
		if (index <= 0 && try_module_get(tmp->owner))
			break;
	read_unlock(&file_systems_lock);
	if (!tmp)
		return -EINVAL;

	/* OK, we got the reference, so we can safely block */
	len = strlen(tmp->name) + 1;
	res = copy_to_user(buf, tmp->name, len) ? -EFAULT : 0;
	put_filesystem(tmp);
	return res;
}

static int fs_maxindex(void)
{
	struct file_system_type * tmp;
	int index;

	read_lock(&file_systems_lock);
	for (tmp = file_systems, index = 0 ; tmp ; tmp = tmp->next, index++)
		;
	read_unlock(&file_systems_lock);
	return index;
}

/*
 * Whee.. Weird sysv syscall. 
 */
SYSCALL_DEFINE3(sysfs, int, option, unsigned long, arg1, unsigned long, arg2)
{
	int retval = -EINVAL;

	switch (option) {
		case 1:
			retval = fs_index((const char __user *) arg1);
			break;

		case 2:
			retval = fs_name(arg1, (char __user *) arg2);
			break;

		case 3:
			retval = fs_maxindex();
			break;
	}
	return retval;
}

int __init get_filesystem_list(char *buf)
{
	int len = 0;
	struct file_system_type * tmp;

	read_lock(&file_systems_lock);
	tmp = file_systems;
	while (tmp && len < PAGE_SIZE - 80) {
		len += sprintf(buf+len, "%s\t%s\n",
			(tmp->fs_flags & FS_REQUIRES_DEV) ? "" : "nodev",
			tmp->name);
		tmp = tmp->next;
	}
	read_unlock(&file_systems_lock);
	return len;
}

#ifdef CONFIG_PROC_FS
static int filesystems_proc_show(struct seq_file *m, void *v)
{
	struct file_system_type * tmp;

	read_lock(&file_systems_lock);
	tmp = file_systems;
	while (tmp) {
		seq_printf(m, "%s\t%s\n",
			(tmp->fs_flags & FS_REQUIRES_DEV) ? "" : "nodev",
			tmp->name);
		tmp = tmp->next;
	}
	read_unlock(&file_systems_lock);
	return 0;
}

static int filesystems_proc_open(struct inode *inode, struct file *file)
{
	return single_open(file, filesystems_proc_show, NULL);
}

static const struct file_operations filesystems_proc_fops = {
	.open		= filesystems_proc_open,
	.read		= seq_read,
	.llseek		= seq_lseek,
	.release	= single_release,
};

static int __init proc_filesystems_init(void)
{
	proc_create("filesystems", 0, NULL, &filesystems_proc_fops);
	return 0;
}
module_init(proc_filesystems_init);
#endif

static struct file_system_type *__get_fs_type(const char *name, int len)
{
	struct file_system_type *fs;

	read_lock(&file_systems_lock);
	fs = *(find_filesystem(name, len));
	if (fs && !try_module_get(fs->owner))
		fs = NULL;
	read_unlock(&file_systems_lock);
	return fs;
}

struct file_system_type *get_fs_type(const char *name)
{
	struct file_system_type *fs;
	const char *dot = strchr(name, '.');
	int len = dot ? dot - name : strlen(name);

	fs = __get_fs_type(name, len);
	if (!fs && (request_module("%.*s", len, name) == 0))
		fs = __get_fs_type(name, len);

	if (dot && fs && !(fs->fs_flags & FS_HAS_SUBTYPE)) {
		put_filesystem(fs);
		fs = NULL;
	}
	return fs;
}

EXPORT_SYMBOL(get_fs_type);