aboutsummaryrefslogtreecommitdiffstats
blob: b91f3e34d44d5d39907b8bbef3de4fb6f37fbb69 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
#!/usr/bin/python
#
# diffconfig - a tool to compare .config files.
#
# originally written in 2006 by Matt Mackall
#  (at least, this was in his bloatwatch source code)
# last worked on 2008 by Tim Bird
#

import sys, os

def usage():
    print """Usage: diffconfig [-h] [-m] [<config1> <config2>]

Diffconfig is a simple utility for comparing two .config files.
Using standard diff to compare .config files often includes extraneous and
distracting information.  This utility produces sorted output with only the
changes in configuration values between the two files.

Added and removed items are shown with a leading plus or minus, respectively.
Changed items show the old and new values on a single line.

If -m is specified, then output will be in "merge" style, which has the
changed and new values in kernel config option format.

If no config files are specified, .config and .config.old are used.

Example usage:
 $ diffconfig .config config-with-some-changes
-EXT2_FS_XATTR  n
-EXT2_FS_XIP  n
 CRAMFS  n -> y
 EXT2_FS  y -> n
 LOG_BUF_SHIFT  14 -> 16
 PRINTK_TIME  n -> y
"""
    sys.exit(0)

# returns a dictionary of name/value pairs for config items in the file
def readconfig(config_file):
    d = {}
    for line in config_file:
        line = line[:-1]
        if line[:7] == "CONFIG_":
            name, val = line[7:].split("=", 1)
            d[name] = val
        if line[-11:] == " is not set":
            d[line[9:-11]] = "n"
    return d

def print_config(op, config, value, new_value):
    global merge_style

    if merge_style:
        if new_value:
            if new_value=="n":
                print "# CONFIG_%s is not set" % config
            else:
                print "CONFIG_%s=%s" % (config, new_value)
    else:
        if op=="-":
            print "-%s %s" % (config, value)
        elif op=="+":
            print "+%s %s" % (config, new_value)
        else:
            print " %s %s -> %s" % (config, value, new_value)

def main():
    global merge_style

    # parse command line args
    if ("-h" in sys.argv or "--help" in sys.argv):
	usage()

    merge_style = 0
    if "-m" in sys.argv:
        merge_style = 1
        sys.argv.remove("-m")

    argc = len(sys.argv)
    if not (argc==1 or argc == 3):
        print "Error: incorrect number of arguments or unrecognized option"
        usage()

    if argc == 1:
        # if no filenames given, assume .config and .config.old
        build_dir=""
        if os.environ.has_key("KBUILD_OUTPUT"):
            build_dir = os.environ["KBUILD_OUTPUT"]+"/"

        configa_filename = build_dir + ".config.old"
        configb_filename = build_dir + ".config"
    else:
        configa_filename = sys.argv[1]
        configb_filename = sys.argv[2]

    a = readconfig(file(configa_filename))
    b = readconfig(file(configb_filename))

    # print items in a but not b (accumulate, sort and print)
    old = []
    for config in a:
        if config not in b:
            old.append(config)
    old.sort()
    for config in old:
        print_config("-", config, a[config], None)
        del a[config]

    # print items that changed (accumulate, sort, and print)
    changed = []
    for config in a:
        if a[config] != b[config]:
            changed.append(config)
        else:
            del b[config]
    changed.sort()
    for config in changed:
        print_config("->", config, a[config], b[config])
        del b[config]

    # now print items in b but not in a
    # (items from b that were in a were removed above)
    new = b.keys()
    new.sort()
    for config in new:
        print_config("+", config, None, b[config])

main()