aboutsummaryrefslogtreecommitdiffstats
blob: b482f162a18af48e6e83f6097581a317d64b194f (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
#!/bin/sh
# Copyright (C) Martin Schlemmer <azarah@nosferatu.za.org>
# Copyright (C) 2006 Sam Ravnborg <sam@ravnborg.org>
#
# Released under the terms of the GNU GPL
#
# Generate a cpio packed initramfs. It uses gen_init_cpio to generate
# the cpio archive, and then compresses it.
# The script may also be used to generate the inputfile used for gen_init_cpio
# This script assumes that gen_init_cpio is located in usr/ directory

# error out on errors
set -e

usage() {
cat << EOF
Usage:
$0 [-o <file>] [-u <uid>] [-g <gid>] {-d | <cpio_source>} ...
	-o <file>      Create compressed initramfs file named <file> using
		       gen_init_cpio and compressor depending on the extension
	-u <uid>       User ID to map to user ID 0 (root).
		       <uid> is only meaningful if <cpio_source> is a
		       directory.  "squash" forces all files to uid 0.
	-g <gid>       Group ID to map to group ID 0 (root).
		       <gid> is only meaningful if <cpio_source> is a
		       directory.  "squash" forces all files to gid 0.
	<cpio_source>  File list or directory for cpio archive.
		       If <cpio_source> is a .cpio file it will be used
		       as direct input to initramfs.
	-d             Output the default cpio list.

All options except -o and -l may be repeated and are interpreted
sequentially and immediately.  -u and -g states are preserved across
<cpio_source> options so an explicit "-u 0 -g 0" is required
to reset the root/group mapping.
EOF
}

# awk style field access
# $1 - field number; rest is argument string
field() {
	shift $1 ; echo $1
}

list_default_initramfs() {
	# echo usr/kinit/kinit
	:
}

default_initramfs() {
	cat <<-EOF >> ${output}
		# This is a very simple, default initramfs

		dir /dev 0755 0 0
		nod /dev/console 0600 0 0 c 5 1
		dir /root 0700 0 0
		# file /kinit usr/kinit/kinit 0755 0 0
		# slink /init kinit 0755 0 0
	EOF
}

filetype() {
	local argv1="$1"

	# symlink test must come before file test
	if [ -L "${argv1}" ]; then
		echo "slink"
	elif [ -f "${argv1}" ]; then
		echo "file"
	elif [ -d "${argv1}" ]; then
		echo "dir"
	elif [ -b "${argv1}" -o -c "${argv1}" ]; then
		echo "nod"
	elif [ -p "${argv1}" ]; then
		echo "pipe"
	elif [ -S "${argv1}" ]; then
		echo "sock"
	else
		echo "invalid"
	fi
	return 0
}

list_print_mtime() {
	:
}

print_mtime() {
	local my_mtime="0"

	if [ -e "$1" ]; then
		my_mtime=$(find "$1" -printf "%T@\n" | sort -r | head -n 1)
	fi

	echo "# Last modified: ${my_mtime}" >> ${output}
	echo "" >> ${output}
}

list_parse() {
	[ ! -L "$1" ] && echo "$1 \\" || :
}

# for each file print a line in following format
# <filetype> <name> <path to file> <octal mode> <uid> <gid>
# for links, devices etc the format differs. See gen_init_cpio for details
parse() {
	local location="$1"
	local name="/${location#${srcdir}}"
	# change '//' into '/'
	name=$(echo "$name" | sed -e 's://*:/:g')
	local mode="$2"
	local uid="$3"
	local gid="$4"
	local ftype=$(filetype "${location}")
	# remap uid/gid to 0 if necessary
	[ "$root_uid" = "squash" ] && uid=0 || [ "$uid" -eq "$root_uid" ] && uid=0
	[ "$root_gid" = "squash" ] && gid=0 || [ "$gid" -eq "$root_gid" ] && gid=0
	local str="${mode} ${uid} ${gid}"

	[ "${ftype}" = "invalid" ] && return 0
	[ "${location}" = "${srcdir}" ] && return 0

	case "${ftype}" in
		"file")
			str="${ftype} ${name} ${location} ${str}"
			;;
		"nod")
			local dev=`LC_ALL=C ls -l "${location}"`
			local maj=`field 5 ${dev}`
			local min=`field 6 ${dev}`
			maj=${maj%,}

			[ -b "${location}" ] && dev="b" || dev="c"

			str="${ftype} ${name} ${str} ${dev} ${maj} ${min}"
			;;
		"slink")
			local target=`readlink "${location}"`
			str="${ftype} ${name} ${target} ${str}"
			;;
		*)
			str="${ftype} ${name} ${str}"
			;;
	esac

	echo "${str}" >> ${output}

	return 0
}

unknown_option() {
	printf "ERROR: unknown option \"$arg\"\n" >&2
	printf "If the filename validly begins with '-', " >&2
	printf "then it must be prefixed\n" >&2
	printf "by './' so that it won't be interpreted as an option." >&2
	printf "\n" >&2
	usage >&2
	exit 1
}

list_header() {
	:
}

header() {
	printf "\n#####################\n# $1\n" >> ${output}
}

# process one directory (incl sub-directories)
dir_filelist() {
	${dep_list}header "$1"

	srcdir=$(echo "$1" | sed -e 's://*:/:g')
	dirlist=$(find "${srcdir}" -printf "%p %m %U %G\n")

	# If $dirlist is only one line, then the directory is empty
	if [  "$(echo "${dirlist}" | wc -l)" -gt 1 ]; then
		${dep_list}print_mtime "$1"

		echo "${dirlist}" | \
		while read x; do
			${dep_list}parse ${x}
		done
	fi
}

# if only one file is specified and it is .cpio file then use it direct as fs
# if a directory is specified then add all files in given direcotry to fs
# if a regular file is specified assume it is in gen_initramfs format
input_file() {
	source="$1"
	if [ -f "$1" ]; then
		${dep_list}header "$1"
		is_cpio="$(echo "$1" | sed 's/^.*\.cpio\(\..*\)\?/cpio/')"
		if [ $2 -eq 0 -a ${is_cpio} = "cpio" ]; then
			cpio_file=$1
			echo "$1" | grep -q '^.*\.cpio\..*' && is_cpio_compressed="compressed"
			[ ! -z ${dep_list} ] && echo "$1"
			return 0
		fi
		if [ -z ${dep_list} ]; then
			print_mtime "$1" >> ${output}
			cat "$1"         >> ${output}
		else
		        echo "$1 \\"
			cat "$1" | while read type dir file perm ; do
				if [ "$type" = "file" ]; then
					echo "$file \\";
				fi
			done
		fi
	elif [ -d "$1" ]; then
		dir_filelist "$1"
	else
		echo "  ${prog}: Cannot open '$1'" >&2
		exit 1
	fi
}

prog=$0
root_uid=0
root_gid=0
dep_list=
cpio_file=
cpio_list=
output="/dev/stdout"
output_file=""
is_cpio_compressed=
compr="gzip -n -9 -f"

arg="$1"
case "$arg" in
	"-l")	# files included in initramfs - used by kbuild
		dep_list="list_"
		echo "deps_initramfs := $0 \\"
		shift
		;;
	"-o")	# generate compressed cpio image named $1
		shift
		output_file="$1"
		cpio_list="$(mktemp ${TMPDIR:-/tmp}/cpiolist.XXXXXX)"
		output=${cpio_list}
		echo "$output_file" | grep -q "\.gz$" && compr="gzip -n -9 -f"
		echo "$output_file" | grep -q "\.bz2$" && compr="bzip2 -9 -f"
		echo "$output_file" | grep -q "\.lzma$" && compr="lzma -9 -f"
		echo "$output_file" | grep -q "\.xz$" && \
				compr="xz --check=crc32 --lzma2=dict=1MiB"
		echo "$output_file" | grep -q "\.lzo$" && compr="lzop -9 -f"
		echo "$output_file" | grep -q "\.cpio$" && compr="cat"
		shift
		;;
esac
while [ $# -gt 0 ]; do
	arg="$1"
	shift
	case "$arg" in
		"-u")	# map $1 to uid=0 (root)
			root_uid="$1"
			shift
			;;
		"-g")	# map $1 to gid=0 (root)
			root_gid="$1"
			shift
			;;
		"-d")	# display default initramfs list
			default_list="$arg"
			${dep_list}default_initramfs
			;;
		"-h")
			usage
			exit 0
			;;
		*)
			case "$arg" in
				"-"*)
					unknown_option
					;;
				*)	# input file/dir - process it
					input_file "$arg" "$#"
					;;
			esac
			;;
	esac
done

# If output_file is set we will generate cpio archive and compress it
# we are careful to delete tmp files
if [ ! -z ${output_file} ]; then
	if [ -z ${cpio_file} ]; then
		timestamp=
		if test -n "$KBUILD_BUILD_TIMESTAMP"; then
			timestamp="$(date -d"$KBUILD_BUILD_TIMESTAMP" +%s || :)"
			if test -n "$timestamp"; then
				timestamp="-t $timestamp"
			fi
		fi
		cpio_tfile="$(mktemp ${TMPDIR:-/tmp}/cpiofile.XXXXXX)"
		usr/gen_init_cpio $timestamp ${cpio_list} > ${cpio_tfile}
	else
		cpio_tfile=${cpio_file}
	fi
	rm ${cpio_list}
	if [ "${is_cpio_compressed}" = "compressed" ]; then
		cat ${cpio_tfile} > ${output_file}
	else
		(cat ${cpio_tfile} | ${compr}  - > ${output_file}) \
		|| (rm -f ${output_file} ; false)
	fi
	[ -z ${cpio_file} ] && rm ${cpio_tfile}
fi
exit 0