aboutsummaryrefslogtreecommitdiffstats
blob: 11224eddcdc22ebcb40e20d77774e2a1834cb8fb (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
402
403
404
405
406
407
408
409
410
411
412
413
414
415
416
417
418
419
420
421
422
423
424
425
426
427
428
429
430
431
432
433
434
435
436
437
438
439
440
441
442
443
444
445
446
447
448
449
450
451
452
453
454
455
456
457
458
459
460
461
462
463
464
465
466
467
468
469
470
471
472
473
474
475
476
477
478
479
480
481
482
483
484
485
486
487
488
489
490
491
492
493
494
495
496
497
498
499
500
/*
 * An implementation of key value pair (KVP) functionality for Linux.
 *
 *
 * Copyright (C) 2010, Novell, Inc.
 * Author : K. Y. Srinivasan <ksrinivasan@novell.com>
 *
 * This program is free software; you can redistribute it and/or modify it
 * under the terms of the GNU General Public License version 2 as published
 * by the Free Software Foundation.
 *
 * This program is distributed in the hope that it will be useful, but
 * WITHOUT ANY WARRANTY; without even the implied warranty of
 * MERCHANTABILITY OR FITNESS FOR A PARTICULAR PURPOSE, GOOD TITLE or
 * NON INFRINGEMENT.  See the GNU General Public License for more
 * details.
 *
 * You should have received a copy of the GNU General Public License
 * along with this program; if not, write to the Free Software
 * Foundation, Inc., 51 Franklin St, Fifth Floor, Boston, MA 02110-1301 USA.
 *
 */


#include <sys/types.h>
#include <sys/socket.h>
#include <sys/poll.h>
#include <sys/utsname.h>
#include <linux/types.h>
#include <stdio.h>
#include <stdlib.h>
#include <unistd.h>
#include <string.h>
#include <errno.h>
#include <arpa/inet.h>
#include <linux/connector.h>
#include <linux/netlink.h>
#include <ifaddrs.h>
#include <netdb.h>
#include <syslog.h>

/*
 * KYS: TODO. Need to register these in the kernel.
 *
 * The following definitions are shared with the in-kernel component; do not
 * change any of this without making the corresponding changes in
 * the KVP kernel component.
 */
#define CN_KVP_IDX		0x9     /* MSFT KVP functionality */
#define CN_KVP_VAL		0x1 /* This supports queries from the kernel */
#define CN_KVP_USER_VAL		0x2 /* This supports queries from the user  */

/*
 * KVP protocol: The user mode component first registers with the
 * the kernel component. Subsequently, the kernel component requests, data
 * for the specified keys. In response to this message the user mode component
 * fills in the value corresponding to the specified key. We overload the
 * sequence field in the cn_msg header to define our KVP message types.
 *
 * We use this infrastructure for also supporting queries from user mode
 * application for state that may be maintained in the KVP kernel component.
 *
 * XXXKYS: Have a shared header file between the user and kernel (TODO)
 */

enum kvp_op {
	KVP_REGISTER = 0, /* Register the user mode component*/
	KVP_KERNEL_GET, /*Kernel is requesting the value for the specified key*/
	KVP_KERNEL_SET, /*Kernel is providing the value for the specified key*/
	KVP_USER_GET, /*User is requesting the value for the specified key*/
	KVP_USER_SET /*User is providing the value for the specified key*/
};

#define HV_KVP_EXCHANGE_MAX_KEY_SIZE	512
#define HV_KVP_EXCHANGE_MAX_VALUE_SIZE	2048

struct hv_ku_msg {
	__u32	kvp_index;
	__u8  kvp_key[HV_KVP_EXCHANGE_MAX_KEY_SIZE]; /* Key name */
	__u8  kvp_value[HV_KVP_EXCHANGE_MAX_VALUE_SIZE]; /* Key  value */
};

enum key_index {
	FullyQualifiedDomainName = 0,
	IntegrationServicesVersion, /*This key is serviced in the kernel*/
	NetworkAddressIPv4,
	NetworkAddressIPv6,
	OSBuildNumber,
	OSName,
	OSMajorVersion,
	OSMinorVersion,
	OSVersion,
	ProcessorArchitecture
};

/*
 * End of shared definitions.
 */

static char kvp_send_buffer[4096];
static char kvp_recv_buffer[4096];
static struct sockaddr_nl addr;

static char *os_name = "";
static char *os_major = "";
static char *os_minor = "";
static char *processor_arch;
static char *os_build;
static char *lic_version;
static struct utsname uts_buf;

void kvp_get_os_info(void)
{
	FILE	*file;
	char	*p, buf[512];

	uname(&uts_buf);
	os_build = uts_buf.release;
	processor_arch = uts_buf.machine;

	/*
	 * The current windows host (win7) expects the build
	 * string to be of the form: x.y.z
	 * Strip additional information we may have.
	 */
	p = strchr(os_build, '-');
	if (p)
		*p = '\0';

	file = fopen("/etc/SuSE-release", "r");
	if (file != NULL)
		goto kvp_osinfo_found;
	file  = fopen("/etc/redhat-release", "r");
	if (file != NULL)
		goto kvp_osinfo_found;
	/*
	 * Add code for other supported platforms.
	 */

	/*
	 * We don't have information about the os.
	 */
	os_name = uts_buf.sysname;
	return;

kvp_osinfo_found:
	/* up to three lines */
	p = fgets(buf, sizeof(buf), file);
	if (p) {
		p = strchr(buf, '\n');
		if (p)
			*p = '\0';
		p = strdup(buf);
		if (!p)
			goto done;
		os_name = p;

		/* second line */
		p = fgets(buf, sizeof(buf), file);
		if (p) {
			p = strchr(buf, '\n');
			if (p)
				*p = '\0';
			p = strdup(buf);
			if (!p)
				goto done;
			os_major = p;

			/* third line */
			p = fgets(buf, sizeof(buf), file);
			if (p)  {
				p = strchr(buf, '\n');
				if (p)
					*p = '\0';
				p = strdup(buf);
				if (p)
					os_minor = p;
			}
		}
	}

done:
	fclose(file);
	return;
}

static int
kvp_get_ip_address(int family, char *buffer, int length)
{
	struct ifaddrs *ifap;
	struct ifaddrs *curp;
	int ipv4_len = strlen("255.255.255.255") + 1;
	int ipv6_len = strlen("ffff:ffff:ffff:ffff:ffff:ffff:ffff:ffff")+1;
	int offset = 0;
	const char *str;
	char tmp[50];
	int error = 0;

	/*
	 * On entry into this function, the buffer is capable of holding the
	 * maximum key value (2048 bytes).
	 */

	if (getifaddrs(&ifap)) {
		strcpy(buffer, "getifaddrs failed\n");
		return 1;
	}

	curp = ifap;
	while (curp != NULL) {
		if ((curp->ifa_addr != NULL) &&
		   (curp->ifa_addr->sa_family == family)) {
			if (family == AF_INET) {
				struct sockaddr_in *addr =
				(struct sockaddr_in *) curp->ifa_addr;

				str = inet_ntop(family, &addr->sin_addr,
						tmp, 50);
				if (str == NULL) {
					strcpy(buffer, "inet_ntop failed\n");
					error = 1;
					goto getaddr_done;
				}
				if (offset == 0)
					strcpy(buffer, tmp);
				else
					strcat(buffer, tmp);
				strcat(buffer, ";");

				offset += strlen(str) + 1;
				if ((length - offset) < (ipv4_len + 1))
					goto getaddr_done;

			} else {

			/*
			 * We only support AF_INET and AF_INET6
			 * and the list of addresses is separated by a ";".
			 */
				struct sockaddr_in6 *addr =
				(struct sockaddr_in6 *) curp->ifa_addr;

				str = inet_ntop(family,
					&addr->sin6_addr.s6_addr,
					tmp, 50);
				if (str == NULL) {
					strcpy(buffer, "inet_ntop failed\n");
					error = 1;
					goto getaddr_done;
				}
				if (offset == 0)
					strcpy(buffer, tmp);
				else
					strcat(buffer, tmp);
				strcat(buffer, ";");
				offset += strlen(str) + 1;
				if ((length - offset) < (ipv6_len + 1))
					goto getaddr_done;

			}

		}
		curp = curp->ifa_next;
	}

getaddr_done:
	freeifaddrs(ifap);
	return error;
}


static int
kvp_get_domain_name(char *buffer, int length)
{
	struct addrinfo	hints, *info ;
	int error = 0;

	gethostname(buffer, length);
	memset(&hints, 0, sizeof(hints));
	hints.ai_family = AF_INET; /*Get only ipv4 addrinfo. */
	hints.ai_socktype = SOCK_STREAM;
	hints.ai_flags = AI_CANONNAME;

	error = getaddrinfo(buffer, NULL, &hints, &info);
	if (error != 0) {
		strcpy(buffer, "getaddrinfo failed\n");
		return error;
	}
	strcpy(buffer, info->ai_canonname);
	freeaddrinfo(info);
	return error;
}

static int
netlink_send(int fd, struct cn_msg *msg)
{
	struct nlmsghdr *nlh;
	unsigned int size;
	struct msghdr message;
	char buffer[64];
	struct iovec iov[2];

	size = NLMSG_SPACE(sizeof(struct cn_msg) + msg->len);

	nlh = (struct nlmsghdr *)buffer;
	nlh->nlmsg_seq = 0;
	nlh->nlmsg_pid = getpid();
	nlh->nlmsg_type = NLMSG_DONE;
	nlh->nlmsg_len = NLMSG_LENGTH(size - sizeof(*nlh));
	nlh->nlmsg_flags = 0;

	iov[0].iov_base = nlh;
	iov[0].iov_len = sizeof(*nlh);

	iov[1].iov_base = msg;
	iov[1].iov_len = size;

	memset(&message, 0, sizeof(message));
	message.msg_name = &addr;
	message.msg_namelen = sizeof(addr);
	message.msg_iov = iov;
	message.msg_iovlen = 2;

	return sendmsg(fd, &message, 0);
}

int main(void)
{
	int fd, len, sock_opt;
	int error;
	struct cn_msg *message;
	struct pollfd pfd;
	struct nlmsghdr *incoming_msg;
	struct cn_msg	*incoming_cn_msg;
	struct hv_ku_msg *hv_msg;
	char	*p;
	char	*key_value;
	char	*key_name;

	daemon(1, 0);
	openlog("KVP", 0, LOG_USER);
	syslog(LOG_INFO, "KVP starting; pid is:%d", getpid());
	/*
	 * Retrieve OS release information.
	 */
	kvp_get_os_info();

	fd = socket(AF_NETLINK, SOCK_DGRAM, NETLINK_CONNECTOR);
	if (fd < 0) {
		syslog(LOG_ERR, "netlink socket creation failed; error:%d", fd);
		exit(-1);
	}
	addr.nl_family = AF_NETLINK;
	addr.nl_pad = 0;
	addr.nl_pid = 0;
	addr.nl_groups = CN_KVP_IDX;


	error = bind(fd, (struct sockaddr *)&addr, sizeof(addr));
	if (error < 0) {
		syslog(LOG_ERR, "bind failed; error:%d", error);
		close(fd);
		exit(-1);
	}
	sock_opt = addr.nl_groups;
	setsockopt(fd, 270, 1, &sock_opt, sizeof(sock_opt));
	/*
	 * Register ourselves with the kernel.
	 */
	message = (struct cn_msg *)kvp_send_buffer;
	message->id.idx = CN_KVP_IDX;
	message->id.val = CN_KVP_VAL;
	message->seq = KVP_REGISTER;
	message->ack = 0;
	message->len = 0;

	len = netlink_send(fd, message);
	if (len < 0) {
		syslog(LOG_ERR, "netlink_send failed; error:%d", len);
		close(fd);
		exit(-1);
	}

	pfd.fd = fd;

	while (1) {
		pfd.events = POLLIN;
		pfd.revents = 0;
		poll(&pfd, 1, -1);

		len = recv(fd, kvp_recv_buffer, sizeof(kvp_recv_buffer), 0);

		if (len < 0) {
			syslog(LOG_ERR, "recv failed; error:%d", len);
			close(fd);
			return -1;
		}

		incoming_msg = (struct nlmsghdr *)kvp_recv_buffer;
		incoming_cn_msg = (struct cn_msg *)NLMSG_DATA(incoming_msg);

		switch (incoming_cn_msg->seq) {
		case KVP_REGISTER:
			/*
			 * Driver is registering with us; stash away the version
			 * information.
			 */
			p = (char *)incoming_cn_msg->data;
			lic_version = malloc(strlen(p) + 1);
			if (lic_version) {
				strcpy(lic_version, p);
				syslog(LOG_INFO, "KVP LIC Version: %s",
					lic_version);
			} else {
				syslog(LOG_ERR, "malloc failed");
			}
			continue;

		case KVP_KERNEL_GET:
			break;
		default:
			continue;
		}

		hv_msg = (struct hv_ku_msg *)incoming_cn_msg->data;
		key_name = (char *)hv_msg->kvp_key;
		key_value = (char *)hv_msg->kvp_value;

		switch (hv_msg->kvp_index) {
		case FullyQualifiedDomainName:
			kvp_get_domain_name(key_value,
					HV_KVP_EXCHANGE_MAX_VALUE_SIZE);
			strcpy(key_name, "FullyQualifiedDomainName");
			break;
		case IntegrationServicesVersion:
			strcpy(key_name, "IntegrationServicesVersion");
			strcpy(key_value, lic_version);
			break;
		case NetworkAddressIPv4:
			kvp_get_ip_address(AF_INET, key_value,
					HV_KVP_EXCHANGE_MAX_VALUE_SIZE);
			strcpy(key_name, "NetworkAddressIPv4");
			break;
		case NetworkAddressIPv6:
			kvp_get_ip_address(AF_INET6, key_value,
					HV_KVP_EXCHANGE_MAX_VALUE_SIZE);
			strcpy(key_name, "NetworkAddressIPv6");
			break;
		case OSBuildNumber:
			strcpy(key_value, os_build);
			strcpy(key_name, "OSBuildNumber");
			break;
		case OSName:
			strcpy(key_value, os_name);
			strcpy(key_name, "OSName");
			break;
		case OSMajorVersion:
			strcpy(key_value, os_major);
			strcpy(key_name, "OSMajorVersion");
			break;
		case OSMinorVersion:
			strcpy(key_value, os_minor);
			strcpy(key_name, "OSMinorVersion");
			break;
		case OSVersion:
			strcpy(key_value, os_build);
			strcpy(key_name, "OSVersion");
			break;
		case ProcessorArchitecture:
			strcpy(key_value, processor_arch);
			strcpy(key_name, "ProcessorArchitecture");
			break;
		default:
			strcpy(key_value, "Unknown Key");
			/*
			 * We use a null key name to terminate enumeration.
			 */
			strcpy(key_name, "");
			break;
		}
		/*
		 * Send the value back to the kernel. The response is
		 * already in the receive buffer. Update the cn_msg header to
		 * reflect the key value that has been added to the message
		 */

		incoming_cn_msg->id.idx = CN_KVP_IDX;
		incoming_cn_msg->id.val = CN_KVP_VAL;
		incoming_cn_msg->seq = KVP_USER_SET;
		incoming_cn_msg->ack = 0;
		incoming_cn_msg->len = sizeof(struct hv_ku_msg);

		len = netlink_send(fd, incoming_cn_msg);
		if (len < 0) {
			syslog(LOG_ERR, "net_link send failed; error:%d", len);
			exit(-1);
		}
	}

}