aboutsummaryrefslogtreecommitdiffstats
blob: b38a1f9ad4606db6e8544ee5908789eaae0ac0f0 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
perf-record(1)
==============

NAME
----
perf-record - Run a command and record its profile into perf.data

SYNOPSIS
--------
[verse]
'perf record' [-e <EVENT> | --event=EVENT] [-l] [-a] <command>
'perf record' [-e <EVENT> | --event=EVENT] [-l] [-a] -- <command> [<options>]

DESCRIPTION
-----------
This command runs a command and gathers a performance counter profile
from it, into perf.data - without displaying anything.

This file can then be inspected later on, using 'perf report'.


OPTIONS
-------
<command>...::
	Any command you can specify in a shell.

-e::
--event=::
	Select the PMU event. Selection can be:

        - a symbolic event name	(use 'perf list' to list all events)

        - a raw PMU event (eventsel+umask) in the form of rNNN where NNN is a
	  hexadecimal event descriptor.

        - a hardware breakpoint event in the form of '\mem:addr[:access]'
          where addr is the address in memory you want to break in.
          Access is the memory access type (read, write, execute) it can
          be passed as follows: '\mem:addr[:[r][w][x]]'.
          If you want to profile read-write accesses in 0x1000, just set
          'mem:0x1000:rw'.

--filter=<filter>::
        Event filter.

-a::
--all-cpus::
        System-wide collection from all CPUs.

-l::
        Scale counter values.

-p::
--pid=::
	Record events on existing process ID (comma separated list).

-t::
--tid=::
        Record events on existing thread ID (comma separated list).

-u::
--uid=::
        Record events in threads owned by uid. Name or number.

-r::
--realtime=::
	Collect data with this RT SCHED_FIFO priority.
-D::
--no-delay::
	Collect data without buffering.
-A::
--append::
	Append to the output file to do incremental profiling.

-f::
--force::
	Overwrite existing data file. (deprecated)

-c::
--count=::
	Event period to sample.

-o::
--output=::
	Output file name.

-i::
--no-inherit::
	Child tasks do not inherit counters.
-F::
--freq=::
	Profile at this frequency.

-m::
--mmap-pages=::
	Number of mmap data pages. Must be a power of two.

-g::
--call-graph::
	Do call-graph (stack chain/backtrace) recording.

-q::
--quiet::
	Don't print any message, useful for scripting.

-v::
--verbose::
	Be more verbose (show counter open errors, etc).

-s::
--stat::
	Per thread counts.

-d::
--data::
	Sample addresses.

-T::
--timestamp::
	Sample timestamps. Use it with 'perf report -D' to see the timestamps,
	for instance.

-n::
--no-samples::
	Don't sample.

-R::
--raw-samples::
Collect raw sample records from all opened counters (default for tracepoint counters).

-C::
--cpu::
Collect samples only on the list of CPUs provided. Multiple CPUs can be provided as a
comma-separated list with no space: 0,1. Ranges of CPUs are specified with -: 0-2.
In per-thread mode with inheritance mode on (default), samples are captured only when
the thread executes on the designated CPUs. Default is to monitor all CPUs.

-N::
--no-buildid-cache::
Do not update the builid cache. This saves some overhead in situations
where the information in the perf.data file (which includes buildids)
is sufficient.

-G name,...::
--cgroup name,...::
monitor only in the container (cgroup) called "name". This option is available only
in per-cpu mode. The cgroup filesystem must be mounted. All threads belonging to
container "name" are monitored when they run on the monitored CPUs. Multiple cgroups
can be provided. Each cgroup is applied to the corresponding event, i.e., first cgroup
to first event, second cgroup to second event and so on. It is possible to provide
an empty cgroup (monitor all the time) using, e.g., -G foo,,bar. Cgroups must have
corresponding events, i.e., they always refer to events defined earlier on the command
line.

-b::
--branch-any::
Enable taken branch stack sampling. Any type of taken branch may be sampled.
This is a shortcut for --branch-filter any. See --branch-filter for more infos.

-j::
--branch-filter::
Enable taken branch stack sampling. Each sample captures a series of consecutive
taken branches. The number of branches captured with each sample depends on the
underlying hardware, the type of branches of interest, and the executed code.
It is possible to select the types of branches captured by enabling filters. The
following filters are defined:

        - any:  any type of branches
        - any_call: any function call or system call
        - any_ret: any function return or system call return
        - ind_call: any indirect branch
        - u:  only when the branch target is at the user level
        - k: only when the branch target is in the kernel
        - hv: only when the target is at the hypervisor level

+
The option requires at least one branch type among any, any_call, any_ret, ind_call.
The privilege levels may be ommitted, in which case, the privilege levels of the associated
event are applied to the branch filter. Both kernel (k) and hypervisor (hv) privilege
levels are subject to permissions.  When sampling on multiple events, branch stack sampling
is enabled for all the sampling events. The sampled branch type is the same for all events.
The various filters must be specified as a comma separated list: --branch-filter any_ret,u,k
Note that this feature may not be available on all processors.

SEE ALSO
--------
linkperf:perf-stat[1], linkperf:perf-list[1]