aboutsummaryrefslogtreecommitdiffstats
blob: 12fd3caffd2b7b3c8a794fee57d5f6e38df25de4 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
/*
 * This program is free software; you can redistribute it and/or modify
 * it under the terms of the GNU General Public License as published by
 * the Free Software Foundation; either version 2 of the License.
 *
 * This program is distributed in the hope that it will be useful,
 * but WITHOUT ANY WARRANTY; without even the implied warranty of
 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
 * GNU General Public License for more details.
 *
 * You should have received a copy of the GNU General Public License
 * along with this program; if not, write to the Free Software
 * Foundation, 51 Franklin Street, Fifth Floor, Boston, MA  02110-1301, USA.
 */

#ifndef __KVM_IODEV_H__
#define __KVM_IODEV_H__

#include <linux/kvm_types.h>
#include <asm/errno.h>

struct kvm_io_device;

/**
 * kvm_io_device_ops are called under kvm slots_lock.
 * read and write handlers return 0 if the transaction has been handled,
 * or non-zero to have it passed to the next device.
 **/
struct kvm_io_device_ops {
	int (*read)(struct kvm_io_device *this,
		    gpa_t addr,
		    int len,
		    void *val);
	int (*write)(struct kvm_io_device *this,
		     gpa_t addr,
		     int len,
		     const void *val);
	void (*destructor)(struct kvm_io_device *this);
};


struct kvm_io_device {
	const struct kvm_io_device_ops *ops;
};

static inline void kvm_iodevice_init(struct kvm_io_device *dev,
				     const struct kvm_io_device_ops *ops)
{
	dev->ops = ops;
}

static inline int kvm_iodevice_read(struct kvm_io_device *dev,
				    gpa_t addr, int l, void *v)
{
	return dev->ops->read ? dev->ops->read(dev, addr, l, v) : -EOPNOTSUPP;
}

static inline int kvm_iodevice_write(struct kvm_io_device *dev,
				     gpa_t addr, int l, const void *v)
{
	return dev->ops->write ? dev->ops->write(dev, addr, l, v) : -EOPNOTSUPP;
}

static inline void kvm_iodevice_destructor(struct kvm_io_device *dev)
{
	if (dev->ops->destructor)
		dev->ops->destructor(dev);
}

#endif /* __KVM_IODEV_H__ */