diff options
author | Glauber Costa | 2012-12-18 16:22:40 -0600 |
---|---|---|
committer | Linus Torvalds | 2012-12-18 17:02:14 -0600 |
commit | d7f25f8a2f81252d1ac134470ba1d0a287cf8fcd (patch) | |
tree | ecde8b5d98762e15a6fa1984d098ddf86646942b /init | |
parent | 55007d849759252ddd573aeb36143b947202d509 (diff) | |
download | kernel-video-d7f25f8a2f81252d1ac134470ba1d0a287cf8fcd.tar.gz kernel-video-d7f25f8a2f81252d1ac134470ba1d0a287cf8fcd.tar.xz kernel-video-d7f25f8a2f81252d1ac134470ba1d0a287cf8fcd.zip |
memcg: infrastructure to match an allocation to the right cache
The page allocator is able to bind a page to a memcg when it is
allocated. But for the caches, we'd like to have as many objects as
possible in a page belonging to the same cache.
This is done in this patch by calling memcg_kmem_get_cache in the
beginning of every allocation function. This function is patched out by
static branches when kernel memory controller is not being used.
It assumes that the task allocating, which determines the memcg in the
page allocator, belongs to the same cgroup throughout the whole process.
Misaccounting can happen if the task calls memcg_kmem_get_cache() while
belonging to a cgroup, and later on changes. This is considered
acceptable, and should only happen upon task migration.
Before the cache is created by the memcg core, there is also a possible
imbalance: the task belongs to a memcg, but the cache being allocated from
is the global cache, since the child cache is not yet guaranteed to be
ready. This case is also fine, since in this case the GFP_KMEMCG will not
be passed and the page allocator will not attempt any cgroup accounting.
Signed-off-by: Glauber Costa <glommer@parallels.com>
Cc: Christoph Lameter <cl@linux.com>
Cc: David Rientjes <rientjes@google.com>
Cc: Frederic Weisbecker <fweisbec@redhat.com>
Cc: Greg Thelen <gthelen@google.com>
Cc: Johannes Weiner <hannes@cmpxchg.org>
Cc: JoonSoo Kim <js1304@gmail.com>
Cc: KAMEZAWA Hiroyuki <kamezawa.hiroyu@jp.fujitsu.com>
Cc: Mel Gorman <mel@csn.ul.ie>
Cc: Michal Hocko <mhocko@suse.cz>
Cc: Pekka Enberg <penberg@cs.helsinki.fi>
Cc: Rik van Riel <riel@redhat.com>
Cc: Suleiman Souhlal <suleiman@google.com>
Cc: Tejun Heo <tj@kernel.org>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Diffstat (limited to 'init')
-rw-r--r-- | init/Kconfig | 1 |
1 files changed, 0 insertions, 1 deletions
diff --git a/init/Kconfig b/init/Kconfig index 19ccb33c99d..7d30240e5bf 100644 --- a/init/Kconfig +++ b/init/Kconfig | |||
@@ -883,7 +883,6 @@ config MEMCG_KMEM | |||
883 | bool "Memory Resource Controller Kernel Memory accounting (EXPERIMENTAL)" | 883 | bool "Memory Resource Controller Kernel Memory accounting (EXPERIMENTAL)" |
884 | depends on MEMCG && EXPERIMENTAL | 884 | depends on MEMCG && EXPERIMENTAL |
885 | depends on SLUB || SLAB | 885 | depends on SLUB || SLAB |
886 | default n | ||
887 | help | 886 | help |
888 | The Kernel Memory extension for Memory Resource Controller can limit | 887 | The Kernel Memory extension for Memory Resource Controller can limit |
889 | the amount of memory used by kernel objects in the system. Those are | 888 | the amount of memory used by kernel objects in the system. Those are |