diff options
author | Praneeth Bajjuri | 2013-04-16 17:52:14 -0500 |
---|---|---|
committer | Praneeth Bajjuri | 2013-04-16 17:52:14 -0500 |
commit | 79b8cdc3f1d584ba364133a5995755e2e5913368 (patch) | |
tree | e3bbf01b0601c6c1e0c0f80df17fbc5ddbe22c95 /net | |
parent | dfb23ecfcb8a7f9d5b5555edcf6369a162d4397c (diff) | |
parent | 19a56e50a91f875597920d593060c4e81d7a2838 (diff) | |
download | kernel-video-79b8cdc3f1d584ba364133a5995755e2e5913368.tar.gz kernel-video-79b8cdc3f1d584ba364133a5995755e2e5913368.tar.xz kernel-video-79b8cdc3f1d584ba364133a5995755e2e5913368.zip |
Merge remote-tracking branch 'origin/p-ti-linux-3.8.y' into p-ti-android-3.8.y
* origin/p-ti-linux-3.8.y: (114 commits)
drm.h: Fix DRM compilation with bare-metal toolchain
Revert "ARM: OMAP4+: omap2plus_defconfig: Enable audio via TWL6040 as module"
mmc:fix max discard sectors limit
arm: configs: disable unused sata configs
ARM: dts: omap3-beagle-xm: Add USB Host support
dmaengine: OMAP: Register SDMA controller with Device Tree DMA driver
ARM: OMAP3: Beagle: Fix USB Host on beagle xM Ax/Bx
USB: ehci-omap: Fix stale dma_mask on repeated modprobe/rmmod
ARM: omap2plus_defconfig: Enable USB Video class drivers
usb: dwc3: set 'mode' based on selected Kconfig choices
usb: dwc3: remove dwc3 dependency on host AND gadget.
drivers: usb: otg: palmas: enable VBUS on ID connect interrupt
drivers: regulator: palmas: add an API to set/clear the switch bit on SMPS10
usb: dwc3: gadget: free trb pool only from epnum 2
ARM: OMAP: Display: Fix compile issues
ARM: DTS: OMAP5-uevm: pull-up Palmas MSECURE line
ARM/dts: omap5-sevm: Enable palmas on i2c1 bus
ARM: OMAP2+: omap2plus_defconfig: Enable RTC support
ARM: dts: AM33XX: Enable system power off control in am335x-bone
ARM: dts: AM33XX: Set pmic-shutdown-controller for BeagleBone
...
Conflicts:
drivers/hid/hid-magicmouse.c
Signed-off-by: Praneeth Bajjuri <praneeth@ti.com>
Diffstat (limited to 'net')
-rw-r--r-- | net/can/gw.c | 6 | ||||
-rw-r--r-- | net/mac80211/cfg.c | 6 | ||||
-rw-r--r-- | net/mac80211/ieee80211_i.h | 3 | ||||
-rw-r--r-- | net/mac80211/offchannel.c | 23 | ||||
-rw-r--r-- | net/sunrpc/clnt.c | 4 |
5 files changed, 27 insertions, 15 deletions
diff --git a/net/can/gw.c b/net/can/gw.c index 574dda78eb0..28e7bdc9df8 100644 --- a/net/can/gw.c +++ b/net/can/gw.c | |||
@@ -436,7 +436,7 @@ static int cgw_notifier(struct notifier_block *nb, | |||
436 | if (gwj->src.dev == dev || gwj->dst.dev == dev) { | 436 | if (gwj->src.dev == dev || gwj->dst.dev == dev) { |
437 | hlist_del(&gwj->list); | 437 | hlist_del(&gwj->list); |
438 | cgw_unregister_filter(gwj); | 438 | cgw_unregister_filter(gwj); |
439 | kfree(gwj); | 439 | kmem_cache_free(cgw_cache, gwj); |
440 | } | 440 | } |
441 | } | 441 | } |
442 | } | 442 | } |
@@ -829,7 +829,7 @@ static void cgw_remove_all_jobs(void) | |||
829 | hlist_for_each_entry_safe(gwj, n, nx, &cgw_list, list) { | 829 | hlist_for_each_entry_safe(gwj, n, nx, &cgw_list, list) { |
830 | hlist_del(&gwj->list); | 830 | hlist_del(&gwj->list); |
831 | cgw_unregister_filter(gwj); | 831 | cgw_unregister_filter(gwj); |
832 | kfree(gwj); | 832 | kmem_cache_free(cgw_cache, gwj); |
833 | } | 833 | } |
834 | } | 834 | } |
835 | 835 | ||
@@ -885,7 +885,7 @@ static int cgw_remove_job(struct sk_buff *skb, struct nlmsghdr *nlh, void *arg) | |||
885 | 885 | ||
886 | hlist_del(&gwj->list); | 886 | hlist_del(&gwj->list); |
887 | cgw_unregister_filter(gwj); | 887 | cgw_unregister_filter(gwj); |
888 | kfree(gwj); | 888 | kmem_cache_free(cgw_cache, gwj); |
889 | err = 0; | 889 | err = 0; |
890 | break; | 890 | break; |
891 | } | 891 | } |
diff --git a/net/mac80211/cfg.c b/net/mac80211/cfg.c index 15d886c639e..30fb87f4275 100644 --- a/net/mac80211/cfg.c +++ b/net/mac80211/cfg.c | |||
@@ -2554,7 +2554,7 @@ static int ieee80211_cancel_roc(struct ieee80211_local *local, | |||
2554 | list_del(&dep->list); | 2554 | list_del(&dep->list); |
2555 | mutex_unlock(&local->mtx); | 2555 | mutex_unlock(&local->mtx); |
2556 | 2556 | ||
2557 | ieee80211_roc_notify_destroy(dep); | 2557 | ieee80211_roc_notify_destroy(dep, true); |
2558 | return 0; | 2558 | return 0; |
2559 | } | 2559 | } |
2560 | 2560 | ||
@@ -2594,7 +2594,7 @@ static int ieee80211_cancel_roc(struct ieee80211_local *local, | |||
2594 | ieee80211_start_next_roc(local); | 2594 | ieee80211_start_next_roc(local); |
2595 | mutex_unlock(&local->mtx); | 2595 | mutex_unlock(&local->mtx); |
2596 | 2596 | ||
2597 | ieee80211_roc_notify_destroy(found); | 2597 | ieee80211_roc_notify_destroy(found, true); |
2598 | } else { | 2598 | } else { |
2599 | /* work may be pending so use it all the time */ | 2599 | /* work may be pending so use it all the time */ |
2600 | found->abort = true; | 2600 | found->abort = true; |
@@ -2604,6 +2604,8 @@ static int ieee80211_cancel_roc(struct ieee80211_local *local, | |||
2604 | 2604 | ||
2605 | /* work will clean up etc */ | 2605 | /* work will clean up etc */ |
2606 | flush_delayed_work(&found->work); | 2606 | flush_delayed_work(&found->work); |
2607 | WARN_ON(!found->to_be_freed); | ||
2608 | kfree(found); | ||
2607 | } | 2609 | } |
2608 | 2610 | ||
2609 | return 0; | 2611 | return 0; |
diff --git a/net/mac80211/ieee80211_i.h b/net/mac80211/ieee80211_i.h index 5fba867d9e2..ec14647b63f 100644 --- a/net/mac80211/ieee80211_i.h +++ b/net/mac80211/ieee80211_i.h | |||
@@ -346,6 +346,7 @@ struct ieee80211_roc_work { | |||
346 | struct ieee80211_channel *chan; | 346 | struct ieee80211_channel *chan; |
347 | 347 | ||
348 | bool started, abort, hw_begun, notified; | 348 | bool started, abort, hw_begun, notified; |
349 | bool to_be_freed; | ||
349 | 350 | ||
350 | unsigned long hw_start_time; | 351 | unsigned long hw_start_time; |
351 | 352 | ||
@@ -1372,7 +1373,7 @@ void ieee80211_offchannel_return(struct ieee80211_local *local); | |||
1372 | void ieee80211_roc_setup(struct ieee80211_local *local); | 1373 | void ieee80211_roc_setup(struct ieee80211_local *local); |
1373 | void ieee80211_start_next_roc(struct ieee80211_local *local); | 1374 | void ieee80211_start_next_roc(struct ieee80211_local *local); |
1374 | void ieee80211_roc_purge(struct ieee80211_sub_if_data *sdata); | 1375 | void ieee80211_roc_purge(struct ieee80211_sub_if_data *sdata); |
1375 | void ieee80211_roc_notify_destroy(struct ieee80211_roc_work *roc); | 1376 | void ieee80211_roc_notify_destroy(struct ieee80211_roc_work *roc, bool free); |
1376 | void ieee80211_sw_roc_work(struct work_struct *work); | 1377 | void ieee80211_sw_roc_work(struct work_struct *work); |
1377 | void ieee80211_handle_roc_started(struct ieee80211_roc_work *roc); | 1378 | void ieee80211_handle_roc_started(struct ieee80211_roc_work *roc); |
1378 | 1379 | ||
diff --git a/net/mac80211/offchannel.c b/net/mac80211/offchannel.c index 82baf5b6ecf..057f3ccd707 100644 --- a/net/mac80211/offchannel.c +++ b/net/mac80211/offchannel.c | |||
@@ -302,10 +302,13 @@ void ieee80211_start_next_roc(struct ieee80211_local *local) | |||
302 | } | 302 | } |
303 | } | 303 | } |
304 | 304 | ||
305 | void ieee80211_roc_notify_destroy(struct ieee80211_roc_work *roc) | 305 | void ieee80211_roc_notify_destroy(struct ieee80211_roc_work *roc, bool free) |
306 | { | 306 | { |
307 | struct ieee80211_roc_work *dep, *tmp; | 307 | struct ieee80211_roc_work *dep, *tmp; |
308 | 308 | ||
309 | if (WARN_ON(roc->to_be_freed)) | ||
310 | return; | ||
311 | |||
309 | /* was never transmitted */ | 312 | /* was never transmitted */ |
310 | if (roc->frame) { | 313 | if (roc->frame) { |
311 | cfg80211_mgmt_tx_status(&roc->sdata->wdev, | 314 | cfg80211_mgmt_tx_status(&roc->sdata->wdev, |
@@ -321,9 +324,12 @@ void ieee80211_roc_notify_destroy(struct ieee80211_roc_work *roc) | |||
321 | GFP_KERNEL); | 324 | GFP_KERNEL); |
322 | 325 | ||
323 | list_for_each_entry_safe(dep, tmp, &roc->dependents, list) | 326 | list_for_each_entry_safe(dep, tmp, &roc->dependents, list) |
324 | ieee80211_roc_notify_destroy(dep); | 327 | ieee80211_roc_notify_destroy(dep, true); |
325 | 328 | ||
326 | kfree(roc); | 329 | if (free) |
330 | kfree(roc); | ||
331 | else | ||
332 | roc->to_be_freed = true; | ||
327 | } | 333 | } |
328 | 334 | ||
329 | void ieee80211_sw_roc_work(struct work_struct *work) | 335 | void ieee80211_sw_roc_work(struct work_struct *work) |
@@ -336,6 +342,9 @@ void ieee80211_sw_roc_work(struct work_struct *work) | |||
336 | 342 | ||
337 | mutex_lock(&local->mtx); | 343 | mutex_lock(&local->mtx); |
338 | 344 | ||
345 | if (roc->to_be_freed) | ||
346 | goto out_unlock; | ||
347 | |||
339 | if (roc->abort) | 348 | if (roc->abort) |
340 | goto finish; | 349 | goto finish; |
341 | 350 | ||
@@ -375,7 +384,7 @@ void ieee80211_sw_roc_work(struct work_struct *work) | |||
375 | finish: | 384 | finish: |
376 | list_del(&roc->list); | 385 | list_del(&roc->list); |
377 | started = roc->started; | 386 | started = roc->started; |
378 | ieee80211_roc_notify_destroy(roc); | 387 | ieee80211_roc_notify_destroy(roc, !roc->abort); |
379 | 388 | ||
380 | if (started) { | 389 | if (started) { |
381 | drv_flush(local, false); | 390 | drv_flush(local, false); |
@@ -415,7 +424,7 @@ static void ieee80211_hw_roc_done(struct work_struct *work) | |||
415 | 424 | ||
416 | list_del(&roc->list); | 425 | list_del(&roc->list); |
417 | 426 | ||
418 | ieee80211_roc_notify_destroy(roc); | 427 | ieee80211_roc_notify_destroy(roc, true); |
419 | 428 | ||
420 | /* if there's another roc, start it now */ | 429 | /* if there's another roc, start it now */ |
421 | ieee80211_start_next_roc(local); | 430 | ieee80211_start_next_roc(local); |
@@ -465,12 +474,14 @@ void ieee80211_roc_purge(struct ieee80211_sub_if_data *sdata) | |||
465 | list_for_each_entry_safe(roc, tmp, &tmp_list, list) { | 474 | list_for_each_entry_safe(roc, tmp, &tmp_list, list) { |
466 | if (local->ops->remain_on_channel) { | 475 | if (local->ops->remain_on_channel) { |
467 | list_del(&roc->list); | 476 | list_del(&roc->list); |
468 | ieee80211_roc_notify_destroy(roc); | 477 | ieee80211_roc_notify_destroy(roc, true); |
469 | } else { | 478 | } else { |
470 | ieee80211_queue_delayed_work(&local->hw, &roc->work, 0); | 479 | ieee80211_queue_delayed_work(&local->hw, &roc->work, 0); |
471 | 480 | ||
472 | /* work will clean up etc */ | 481 | /* work will clean up etc */ |
473 | flush_delayed_work(&roc->work); | 482 | flush_delayed_work(&roc->work); |
483 | WARN_ON(!roc->to_be_freed); | ||
484 | kfree(roc); | ||
474 | } | 485 | } |
475 | } | 486 | } |
476 | 487 | ||
diff --git a/net/sunrpc/clnt.c b/net/sunrpc/clnt.c index 507b5e84fbd..716aa41aa4d 100644 --- a/net/sunrpc/clnt.c +++ b/net/sunrpc/clnt.c | |||
@@ -511,7 +511,7 @@ static struct rpc_clnt *__rpc_clone_client(struct rpc_create_args *args, | |||
511 | new = rpc_new_client(args, xprt); | 511 | new = rpc_new_client(args, xprt); |
512 | if (IS_ERR(new)) { | 512 | if (IS_ERR(new)) { |
513 | err = PTR_ERR(new); | 513 | err = PTR_ERR(new); |
514 | goto out_put; | 514 | goto out_err; |
515 | } | 515 | } |
516 | 516 | ||
517 | atomic_inc(&clnt->cl_count); | 517 | atomic_inc(&clnt->cl_count); |
@@ -524,8 +524,6 @@ static struct rpc_clnt *__rpc_clone_client(struct rpc_create_args *args, | |||
524 | new->cl_chatty = clnt->cl_chatty; | 524 | new->cl_chatty = clnt->cl_chatty; |
525 | return new; | 525 | return new; |
526 | 526 | ||
527 | out_put: | ||
528 | xprt_put(xprt); | ||
529 | out_err: | 527 | out_err: |
530 | dprintk("RPC: %s: returned error %d\n", __func__, err); | 528 | dprintk("RPC: %s: returned error %d\n", __func__, err); |
531 | return ERR_PTR(err); | 529 | return ERR_PTR(err); |