diff options
author | Linus Torvalds | 2005-04-16 17:20:36 -0500 |
---|---|---|
committer | Linus Torvalds | 2005-04-16 17:20:36 -0500 |
commit | 1da177e4c3f41524e886b7f1b8a0c1fc7321cac2 (patch) | |
tree | 0bba044c4ce775e45a88a51686b5d9f90697ea9d /usr | |
download | kernel-video-1da177e4c3f41524e886b7f1b8a0c1fc7321cac2.tar.gz kernel-video-1da177e4c3f41524e886b7f1b8a0c1fc7321cac2.tar.xz kernel-video-1da177e4c3f41524e886b7f1b8a0c1fc7321cac2.zip |
Linux-2.6.12-rc2v2.6.12-rc2
Initial git repository build. I'm not bothering with the full history,
even though we have it. We can create a separate "historical" git
archive of that later if we want to, and in the meantime it's about
3.2GB when imported into git - space that would just make the early
git days unnecessarily complicated, when we don't have a lot of good
infrastructure for it.
Let it rip!
Diffstat (limited to 'usr')
-rw-r--r-- | usr/Makefile | 65 | ||||
-rw-r--r-- | usr/gen_init_cpio.c | 512 | ||||
-rw-r--r-- | usr/initramfs_data.S | 30 |
3 files changed, 607 insertions, 0 deletions
diff --git a/usr/Makefile b/usr/Makefile new file mode 100644 index 00000000000..248d5551029 --- /dev/null +++ b/usr/Makefile | |||
@@ -0,0 +1,65 @@ | |||
1 | |||
2 | obj-y := initramfs_data.o | ||
3 | |||
4 | hostprogs-y := gen_init_cpio | ||
5 | |||
6 | clean-files := initramfs_data.cpio.gz initramfs_list | ||
7 | |||
8 | # initramfs_data.o contains the initramfs_data.cpio.gz image. | ||
9 | # The image is included using .incbin, a dependency which is not | ||
10 | # tracked automatically. | ||
11 | $(obj)/initramfs_data.o: $(obj)/initramfs_data.cpio.gz FORCE | ||
12 | |||
13 | ifdef CONFIG_INITRAMFS_ROOT_UID | ||
14 | gen_initramfs_args += -u $(CONFIG_INITRAMFS_ROOT_UID) | ||
15 | endif | ||
16 | |||
17 | ifdef CONFIG_INITRAMFS_ROOT_GID | ||
18 | gen_initramfs_args += -g $(CONFIG_INITRAMFS_ROOT_GID) | ||
19 | endif | ||
20 | |||
21 | # The $(shell echo $(CONFIG_INITRAMFS_SOURCE)) is to remove the | ||
22 | # gratuitous begin and end quotes from the Kconfig string type. | ||
23 | # Internal, escaped quotes in the Kconfig string will loose the | ||
24 | # escape and become active quotes. | ||
25 | quotefixed_initramfs_source := $(shell echo $(CONFIG_INITRAMFS_SOURCE)) | ||
26 | |||
27 | filechk_initramfs_list = $(CONFIG_SHELL) \ | ||
28 | $(srctree)/scripts/gen_initramfs_list.sh $(gen_initramfs_args) $(quotefixed_initramfs_source) | ||
29 | |||
30 | $(obj)/initramfs_list: FORCE | ||
31 | $(call filechk,initramfs_list) | ||
32 | |||
33 | quiet_cmd_cpio = CPIO $@ | ||
34 | cmd_cpio = ./$< $(obj)/initramfs_list > $@ | ||
35 | |||
36 | |||
37 | # Check if the INITRAMFS_SOURCE is a cpio archive | ||
38 | ifneq (,$(findstring .cpio,$(quotefixed_initramfs_source))) | ||
39 | |||
40 | # INITRAMFS_SOURCE has a cpio archive - verify that it's a single file | ||
41 | ifneq (1,$(words $(quotefixed_initramfs_source))) | ||
42 | $(error Only a single file may be specified in CONFIG_INITRAMFS_SOURCE (="$(quotefixed_initramfs_source)") when a cpio archive is directly specified.) | ||
43 | endif | ||
44 | # Now use the cpio archive directly | ||
45 | initramfs_data_cpio = $(quotefixed_initramfs_source) | ||
46 | targets += $(quotefixed_initramfs_source) | ||
47 | |||
48 | else | ||
49 | |||
50 | # INITRAMFS_SOURCE is not a cpio archive - create one | ||
51 | $(obj)/initramfs_data.cpio: $(obj)/gen_init_cpio \ | ||
52 | $(initramfs-y) $(obj)/initramfs_list FORCE | ||
53 | $(call if_changed,cpio) | ||
54 | |||
55 | targets += initramfs_data.cpio | ||
56 | initramfs_data_cpio = $(obj)/initramfs_data.cpio | ||
57 | |||
58 | endif | ||
59 | |||
60 | |||
61 | $(obj)/initramfs_data.cpio.gz: $(initramfs_data_cpio) FORCE | ||
62 | $(call if_changed,gzip) | ||
63 | |||
64 | targets += initramfs_data.cpio.gz | ||
65 | |||
diff --git a/usr/gen_init_cpio.c b/usr/gen_init_cpio.c new file mode 100644 index 00000000000..33dbcbf77c5 --- /dev/null +++ b/usr/gen_init_cpio.c | |||
@@ -0,0 +1,512 @@ | |||
1 | #include <stdio.h> | ||
2 | #include <stdlib.h> | ||
3 | #include <sys/types.h> | ||
4 | #include <sys/stat.h> | ||
5 | #include <string.h> | ||
6 | #include <unistd.h> | ||
7 | #include <time.h> | ||
8 | #include <fcntl.h> | ||
9 | #include <errno.h> | ||
10 | #include <ctype.h> | ||
11 | #include <limits.h> | ||
12 | |||
13 | /* | ||
14 | * Original work by Jeff Garzik | ||
15 | * | ||
16 | * External file lists, symlink, pipe and fifo support by Thayne Harbaugh | ||
17 | */ | ||
18 | |||
19 | #define xstr(s) #s | ||
20 | #define str(s) xstr(s) | ||
21 | |||
22 | static unsigned int offset; | ||
23 | static unsigned int ino = 721; | ||
24 | |||
25 | struct file_handler { | ||
26 | const char *type; | ||
27 | int (*handler)(const char *line); | ||
28 | }; | ||
29 | |||
30 | static void push_string(const char *name) | ||
31 | { | ||
32 | unsigned int name_len = strlen(name) + 1; | ||
33 | |||
34 | fputs(name, stdout); | ||
35 | putchar(0); | ||
36 | offset += name_len; | ||
37 | } | ||
38 | |||
39 | static void push_pad (void) | ||
40 | { | ||
41 | while (offset & 3) { | ||
42 | putchar(0); | ||
43 | offset++; | ||
44 | } | ||
45 | } | ||
46 | |||
47 | static void push_rest(const char *name) | ||
48 | { | ||
49 | unsigned int name_len = strlen(name) + 1; | ||
50 | unsigned int tmp_ofs; | ||
51 | |||
52 | fputs(name, stdout); | ||
53 | putchar(0); | ||
54 | offset += name_len; | ||
55 | |||
56 | tmp_ofs = name_len + 110; | ||
57 | while (tmp_ofs & 3) { | ||
58 | putchar(0); | ||
59 | offset++; | ||
60 | tmp_ofs++; | ||
61 | } | ||
62 | } | ||
63 | |||
64 | static void push_hdr(const char *s) | ||
65 | { | ||
66 | fputs(s, stdout); | ||
67 | offset += 110; | ||
68 | } | ||
69 | |||
70 | static void cpio_trailer(void) | ||
71 | { | ||
72 | char s[256]; | ||
73 | const char name[] = "TRAILER!!!"; | ||
74 | |||
75 | sprintf(s, "%s%08X%08X%08lX%08lX%08X%08lX" | ||
76 | "%08X%08X%08X%08X%08X%08X%08X", | ||
77 | "070701", /* magic */ | ||
78 | 0, /* ino */ | ||
79 | 0, /* mode */ | ||
80 | (long) 0, /* uid */ | ||
81 | (long) 0, /* gid */ | ||
82 | 1, /* nlink */ | ||
83 | (long) 0, /* mtime */ | ||
84 | 0, /* filesize */ | ||
85 | 0, /* major */ | ||
86 | 0, /* minor */ | ||
87 | 0, /* rmajor */ | ||
88 | 0, /* rminor */ | ||
89 | (unsigned)strlen(name)+1, /* namesize */ | ||
90 | 0); /* chksum */ | ||
91 | push_hdr(s); | ||
92 | push_rest(name); | ||
93 | |||
94 | while (offset % 512) { | ||
95 | putchar(0); | ||
96 | offset++; | ||
97 | } | ||
98 | } | ||
99 | |||
100 | static int cpio_mkslink(const char *name, const char *target, | ||
101 | unsigned int mode, uid_t uid, gid_t gid) | ||
102 | { | ||
103 | char s[256]; | ||
104 | time_t mtime = time(NULL); | ||
105 | |||
106 | sprintf(s,"%s%08X%08X%08lX%08lX%08X%08lX" | ||
107 | "%08X%08X%08X%08X%08X%08X%08X", | ||
108 | "070701", /* magic */ | ||
109 | ino++, /* ino */ | ||
110 | S_IFLNK | mode, /* mode */ | ||
111 | (long) uid, /* uid */ | ||
112 | (long) gid, /* gid */ | ||
113 | 1, /* nlink */ | ||
114 | (long) mtime, /* mtime */ | ||
115 | (unsigned)strlen(target)+1, /* filesize */ | ||
116 | 3, /* major */ | ||
117 | 1, /* minor */ | ||
118 | 0, /* rmajor */ | ||
119 | 0, /* rminor */ | ||
120 | (unsigned)strlen(name) + 1,/* namesize */ | ||
121 | 0); /* chksum */ | ||
122 | push_hdr(s); | ||
123 | push_string(name); | ||
124 | push_pad(); | ||
125 | push_string(target); | ||
126 | push_pad(); | ||
127 | return 0; | ||
128 | } | ||
129 | |||
130 | static int cpio_mkslink_line(const char *line) | ||
131 | { | ||
132 | char name[PATH_MAX + 1]; | ||
133 | char target[PATH_MAX + 1]; | ||
134 | unsigned int mode; | ||
135 | int uid; | ||
136 | int gid; | ||
137 | int rc = -1; | ||
138 | |||
139 | if (5 != sscanf(line, "%" str(PATH_MAX) "s %" str(PATH_MAX) "s %o %d %d", name, target, &mode, &uid, &gid)) { | ||
140 | fprintf(stderr, "Unrecognized dir format '%s'", line); | ||
141 | goto fail; | ||
142 | } | ||
143 | rc = cpio_mkslink(name, target, mode, uid, gid); | ||
144 | fail: | ||
145 | return rc; | ||
146 | } | ||
147 | |||
148 | static int cpio_mkgeneric(const char *name, unsigned int mode, | ||
149 | uid_t uid, gid_t gid) | ||
150 | { | ||
151 | char s[256]; | ||
152 | time_t mtime = time(NULL); | ||
153 | |||
154 | sprintf(s,"%s%08X%08X%08lX%08lX%08X%08lX" | ||
155 | "%08X%08X%08X%08X%08X%08X%08X", | ||
156 | "070701", /* magic */ | ||
157 | ino++, /* ino */ | ||
158 | mode, /* mode */ | ||
159 | (long) uid, /* uid */ | ||
160 | (long) gid, /* gid */ | ||
161 | 2, /* nlink */ | ||
162 | (long) mtime, /* mtime */ | ||
163 | 0, /* filesize */ | ||
164 | 3, /* major */ | ||
165 | 1, /* minor */ | ||
166 | 0, /* rmajor */ | ||
167 | 0, /* rminor */ | ||
168 | (unsigned)strlen(name) + 1,/* namesize */ | ||
169 | 0); /* chksum */ | ||
170 | push_hdr(s); | ||
171 | push_rest(name); | ||
172 | return 0; | ||
173 | } | ||
174 | |||
175 | enum generic_types { | ||
176 | GT_DIR, | ||
177 | GT_PIPE, | ||
178 | GT_SOCK | ||
179 | }; | ||
180 | |||
181 | struct generic_type { | ||
182 | const char *type; | ||
183 | mode_t mode; | ||
184 | }; | ||
185 | |||
186 | static struct generic_type generic_type_table[] = { | ||
187 | [GT_DIR] = { | ||
188 | .type = "dir", | ||
189 | .mode = S_IFDIR | ||
190 | }, | ||
191 | [GT_PIPE] = { | ||
192 | .type = "pipe", | ||
193 | .mode = S_IFIFO | ||
194 | }, | ||
195 | [GT_SOCK] = { | ||
196 | .type = "sock", | ||
197 | .mode = S_IFSOCK | ||
198 | } | ||
199 | }; | ||
200 | |||
201 | static int cpio_mkgeneric_line(const char *line, enum generic_types gt) | ||
202 | { | ||
203 | char name[PATH_MAX + 1]; | ||
204 | unsigned int mode; | ||
205 | int uid; | ||
206 | int gid; | ||
207 | int rc = -1; | ||
208 | |||
209 | if (4 != sscanf(line, "%" str(PATH_MAX) "s %o %d %d", name, &mode, &uid, &gid)) { | ||
210 | fprintf(stderr, "Unrecognized %s format '%s'", | ||
211 | line, generic_type_table[gt].type); | ||
212 | goto fail; | ||
213 | } | ||
214 | mode |= generic_type_table[gt].mode; | ||
215 | rc = cpio_mkgeneric(name, mode, uid, gid); | ||
216 | fail: | ||
217 | return rc; | ||
218 | } | ||
219 | |||
220 | static int cpio_mkdir_line(const char *line) | ||
221 | { | ||
222 | return cpio_mkgeneric_line(line, GT_DIR); | ||
223 | } | ||
224 | |||
225 | static int cpio_mkpipe_line(const char *line) | ||
226 | { | ||
227 | return cpio_mkgeneric_line(line, GT_PIPE); | ||
228 | } | ||
229 | |||
230 | static int cpio_mksock_line(const char *line) | ||
231 | { | ||
232 | return cpio_mkgeneric_line(line, GT_SOCK); | ||
233 | } | ||
234 | |||
235 | static int cpio_mknod(const char *name, unsigned int mode, | ||
236 | uid_t uid, gid_t gid, char dev_type, | ||
237 | unsigned int maj, unsigned int min) | ||
238 | { | ||
239 | char s[256]; | ||
240 | time_t mtime = time(NULL); | ||
241 | |||
242 | if (dev_type == 'b') | ||
243 | mode |= S_IFBLK; | ||
244 | else | ||
245 | mode |= S_IFCHR; | ||
246 | |||
247 | sprintf(s,"%s%08X%08X%08lX%08lX%08X%08lX" | ||
248 | "%08X%08X%08X%08X%08X%08X%08X", | ||
249 | "070701", /* magic */ | ||
250 | ino++, /* ino */ | ||
251 | mode, /* mode */ | ||
252 | (long) uid, /* uid */ | ||
253 | (long) gid, /* gid */ | ||
254 | 1, /* nlink */ | ||
255 | (long) mtime, /* mtime */ | ||
256 | 0, /* filesize */ | ||
257 | 3, /* major */ | ||
258 | 1, /* minor */ | ||
259 | maj, /* rmajor */ | ||
260 | min, /* rminor */ | ||
261 | (unsigned)strlen(name) + 1,/* namesize */ | ||
262 | 0); /* chksum */ | ||
263 | push_hdr(s); | ||
264 | push_rest(name); | ||
265 | return 0; | ||
266 | } | ||
267 | |||
268 | static int cpio_mknod_line(const char *line) | ||
269 | { | ||
270 | char name[PATH_MAX + 1]; | ||
271 | unsigned int mode; | ||
272 | int uid; | ||
273 | int gid; | ||
274 | char dev_type; | ||
275 | unsigned int maj; | ||
276 | unsigned int min; | ||
277 | int rc = -1; | ||
278 | |||
279 | if (7 != sscanf(line, "%" str(PATH_MAX) "s %o %d %d %c %u %u", | ||
280 | name, &mode, &uid, &gid, &dev_type, &maj, &min)) { | ||
281 | fprintf(stderr, "Unrecognized nod format '%s'", line); | ||
282 | goto fail; | ||
283 | } | ||
284 | rc = cpio_mknod(name, mode, uid, gid, dev_type, maj, min); | ||
285 | fail: | ||
286 | return rc; | ||
287 | } | ||
288 | |||
289 | /* Not marked static to keep the compiler quiet, as no one uses this yet... */ | ||
290 | static int cpio_mkfile(const char *name, const char *location, | ||
291 | unsigned int mode, uid_t uid, gid_t gid) | ||
292 | { | ||
293 | char s[256]; | ||
294 | char *filebuf = NULL; | ||
295 | struct stat buf; | ||
296 | int file = -1; | ||
297 | int retval; | ||
298 | int rc = -1; | ||
299 | |||
300 | mode |= S_IFREG; | ||
301 | |||
302 | retval = stat (location, &buf); | ||
303 | if (retval) { | ||
304 | fprintf (stderr, "File %s could not be located\n", location); | ||
305 | goto error; | ||
306 | } | ||
307 | |||
308 | file = open (location, O_RDONLY); | ||
309 | if (file < 0) { | ||
310 | fprintf (stderr, "File %s could not be opened for reading\n", location); | ||
311 | goto error; | ||
312 | } | ||
313 | |||
314 | filebuf = malloc(buf.st_size); | ||
315 | if (!filebuf) { | ||
316 | fprintf (stderr, "out of memory\n"); | ||
317 | goto error; | ||
318 | } | ||
319 | |||
320 | retval = read (file, filebuf, buf.st_size); | ||
321 | if (retval < 0) { | ||
322 | fprintf (stderr, "Can not read %s file\n", location); | ||
323 | goto error; | ||
324 | } | ||
325 | |||
326 | sprintf(s,"%s%08X%08X%08lX%08lX%08X%08lX" | ||
327 | "%08X%08X%08X%08X%08X%08X%08X", | ||
328 | "070701", /* magic */ | ||
329 | ino++, /* ino */ | ||
330 | mode, /* mode */ | ||
331 | (long) uid, /* uid */ | ||
332 | (long) gid, /* gid */ | ||
333 | 1, /* nlink */ | ||
334 | (long) buf.st_mtime, /* mtime */ | ||
335 | (int) buf.st_size, /* filesize */ | ||
336 | 3, /* major */ | ||
337 | 1, /* minor */ | ||
338 | 0, /* rmajor */ | ||
339 | 0, /* rminor */ | ||
340 | (unsigned)strlen(name) + 1,/* namesize */ | ||
341 | 0); /* chksum */ | ||
342 | push_hdr(s); | ||
343 | push_string(name); | ||
344 | push_pad(); | ||
345 | |||
346 | fwrite(filebuf, buf.st_size, 1, stdout); | ||
347 | offset += buf.st_size; | ||
348 | push_pad(); | ||
349 | rc = 0; | ||
350 | |||
351 | error: | ||
352 | if (filebuf) free(filebuf); | ||
353 | if (file >= 0) close(file); | ||
354 | return rc; | ||
355 | } | ||
356 | |||
357 | static int cpio_mkfile_line(const char *line) | ||
358 | { | ||
359 | char name[PATH_MAX + 1]; | ||
360 | char location[PATH_MAX + 1]; | ||
361 | unsigned int mode; | ||
362 | int uid; | ||
363 | int gid; | ||
364 | int rc = -1; | ||
365 | |||
366 | if (5 != sscanf(line, "%" str(PATH_MAX) "s %" str(PATH_MAX) "s %o %d %d", name, location, &mode, &uid, &gid)) { | ||
367 | fprintf(stderr, "Unrecognized file format '%s'", line); | ||
368 | goto fail; | ||
369 | } | ||
370 | rc = cpio_mkfile(name, location, mode, uid, gid); | ||
371 | fail: | ||
372 | return rc; | ||
373 | } | ||
374 | |||
375 | void usage(const char *prog) | ||
376 | { | ||
377 | fprintf(stderr, "Usage:\n" | ||
378 | "\t%s <cpio_list>\n" | ||
379 | "\n" | ||
380 | "<cpio_list> is a file containing newline separated entries that\n" | ||
381 | "describe the files to be included in the initramfs archive:\n" | ||
382 | "\n" | ||
383 | "# a comment\n" | ||
384 | "file <name> <location> <mode> <uid> <gid>\n" | ||
385 | "dir <name> <mode> <uid> <gid>\n" | ||
386 | "nod <name> <mode> <uid> <gid> <dev_type> <maj> <min>\n" | ||
387 | "slink <name> <target> <mode> <uid> <gid>\n" | ||
388 | "pipe <name> <mode> <uid> <gid>\n" | ||
389 | "sock <name> <mode> <uid> <gid>\n" | ||
390 | "\n" | ||
391 | "<name> name of the file/dir/nod/etc in the archive\n" | ||
392 | "<location> location of the file in the current filesystem\n" | ||
393 | "<target> link target\n" | ||
394 | "<mode> mode/permissions of the file\n" | ||
395 | "<uid> user id (0=root)\n" | ||
396 | "<gid> group id (0=root)\n" | ||
397 | "<dev_type> device type (b=block, c=character)\n" | ||
398 | "<maj> major number of nod\n" | ||
399 | "<min> minor number of nod\n" | ||
400 | "\n" | ||
401 | "example:\n" | ||
402 | "# A simple initramfs\n" | ||
403 | "dir /dev 0755 0 0\n" | ||
404 | "nod /dev/console 0600 0 0 c 5 1\n" | ||
405 | "dir /root 0700 0 0\n" | ||
406 | "dir /sbin 0755 0 0\n" | ||
407 | "file /sbin/kinit /usr/src/klibc/kinit/kinit 0755 0 0\n", | ||
408 | prog); | ||
409 | } | ||
410 | |||
411 | struct file_handler file_handler_table[] = { | ||
412 | { | ||
413 | .type = "file", | ||
414 | .handler = cpio_mkfile_line, | ||
415 | }, { | ||
416 | .type = "nod", | ||
417 | .handler = cpio_mknod_line, | ||
418 | }, { | ||
419 | .type = "dir", | ||
420 | .handler = cpio_mkdir_line, | ||
421 | }, { | ||
422 | .type = "slink", | ||
423 | .handler = cpio_mkslink_line, | ||
424 | }, { | ||
425 | .type = "pipe", | ||
426 | .handler = cpio_mkpipe_line, | ||
427 | }, { | ||
428 | .type = "sock", | ||
429 | .handler = cpio_mksock_line, | ||
430 | }, { | ||
431 | .type = NULL, | ||
432 | .handler = NULL, | ||
433 | } | ||
434 | }; | ||
435 | |||
436 | #define LINE_SIZE (2 * PATH_MAX + 50) | ||
437 | |||
438 | int main (int argc, char *argv[]) | ||
439 | { | ||
440 | FILE *cpio_list; | ||
441 | char line[LINE_SIZE]; | ||
442 | char *args, *type; | ||
443 | int ec = 0; | ||
444 | int line_nr = 0; | ||
445 | |||
446 | if (2 != argc) { | ||
447 | usage(argv[0]); | ||
448 | exit(1); | ||
449 | } | ||
450 | |||
451 | if (! (cpio_list = fopen(argv[1], "r"))) { | ||
452 | fprintf(stderr, "ERROR: unable to open '%s': %s\n\n", | ||
453 | argv[1], strerror(errno)); | ||
454 | usage(argv[0]); | ||
455 | exit(1); | ||
456 | } | ||
457 | |||
458 | while (fgets(line, LINE_SIZE, cpio_list)) { | ||
459 | int type_idx; | ||
460 | size_t slen = strlen(line); | ||
461 | |||
462 | line_nr++; | ||
463 | |||
464 | if ('#' == *line) { | ||
465 | /* comment - skip to next line */ | ||
466 | continue; | ||
467 | } | ||
468 | |||
469 | if (! (type = strtok(line, " \t"))) { | ||
470 | fprintf(stderr, | ||
471 | "ERROR: incorrect format, could not locate file type line %d: '%s'\n", | ||
472 | line_nr, line); | ||
473 | ec = -1; | ||
474 | } | ||
475 | |||
476 | if ('\n' == *type) { | ||
477 | /* a blank line */ | ||
478 | continue; | ||
479 | } | ||
480 | |||
481 | if (slen == strlen(type)) { | ||
482 | /* must be an empty line */ | ||
483 | continue; | ||
484 | } | ||
485 | |||
486 | if (! (args = strtok(NULL, "\n"))) { | ||
487 | fprintf(stderr, | ||
488 | "ERROR: incorrect format, newline required line %d: '%s'\n", | ||
489 | line_nr, line); | ||
490 | ec = -1; | ||
491 | } | ||
492 | |||
493 | for (type_idx = 0; file_handler_table[type_idx].type; type_idx++) { | ||
494 | int rc; | ||
495 | if (! strcmp(line, file_handler_table[type_idx].type)) { | ||
496 | if ((rc = file_handler_table[type_idx].handler(args))) { | ||
497 | ec = rc; | ||
498 | fprintf(stderr, " line %d\n", line_nr); | ||
499 | } | ||
500 | break; | ||
501 | } | ||
502 | } | ||
503 | |||
504 | if (NULL == file_handler_table[type_idx].type) { | ||
505 | fprintf(stderr, "unknown file type line %d: '%s'\n", | ||
506 | line_nr, line); | ||
507 | } | ||
508 | } | ||
509 | cpio_trailer(); | ||
510 | |||
511 | exit(ec); | ||
512 | } | ||
diff --git a/usr/initramfs_data.S b/usr/initramfs_data.S new file mode 100644 index 00000000000..c2e1ad424f4 --- /dev/null +++ b/usr/initramfs_data.S | |||
@@ -0,0 +1,30 @@ | |||
1 | /* | ||
2 | initramfs_data includes the compressed binary that is the | ||
3 | filesystem used for early user space. | ||
4 | Note: Older versions of "as" (prior to binutils 2.11.90.0.23 | ||
5 | released on 2001-07-14) dit not support .incbin. | ||
6 | If you are forced to use older binutils than that then the | ||
7 | following trick can be applied to create the resulting binary: | ||
8 | |||
9 | |||
10 | ld -m elf_i386 --format binary --oformat elf32-i386 -r \ | ||
11 | -T initramfs_data.scr initramfs_data.cpio.gz -o initramfs_data.o | ||
12 | ld -m elf_i386 -r -o built-in.o initramfs_data.o | ||
13 | |||
14 | initramfs_data.scr looks like this: | ||
15 | SECTIONS | ||
16 | { | ||
17 | .init.ramfs : { *(.data) } | ||
18 | } | ||
19 | |||
20 | The above example is for i386 - the parameters vary from architectures. | ||
21 | Eventually look up LDFLAGS_BLOB in an older version of the | ||
22 | arch/$(ARCH)/Makefile to see the flags used before .incbin was introduced. | ||
23 | |||
24 | Using .incbin has the advantage over ld that the correct flags are set | ||
25 | in the ELF header, as required by certain architectures. | ||
26 | */ | ||
27 | |||
28 | .section .init.ramfs,"a" | ||
29 | .incbin "usr/initramfs_data.cpio.gz" | ||
30 | |||