/* * Copyright (C) 2001 Jens Axboe * * This program is free software; you can redistribute it and/or modify * it under the terms of the GNU General Public License version 2 as * published by the Free Software Foundation. * * This program is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the * GNU General Public License for more details. * * You should have received a copy of the GNU General Public Licens * along with this program; if not, write to the Free Software * Foundation, Inc., 59 Temple Place, Suite 330, Boston, MA 02111- * */ #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include struct blk_cmd_filter { unsigned long read_ok[BLK_SCSI_CMD_PER_LONG]; unsigned long write_ok[BLK_SCSI_CMD_PER_LONG]; }; static struct blk_cmd_filter blk_default_cmd_filter; /* Command group 3 is reserved and should never be used. */ const unsigned char scsi_command_size_tbl[8] = { 6, 10, 10, 12, 16, 12, 10, 10 }; EXPORT_SYMBOL(scsi_command_size_tbl); #include static int sg_get_version(int __user *p) { static const int sg_version_num = 30527; return put_user(sg_version_num, p); } static int scsi_get_idlun(struct request_queue *q, int __user *p) { return put_user(0, p); } static int scsi_get_bus(struct request_queue *q, int __user *p) { return put_user(0, p); } static int sg_get_timeout(struct request_queue *q) { return jiffies_to_clock_t(q->sg_timeout); } static int sg_set_timeout(struct request_queue *q, int __user *p) { int timeout, err = get_user(timeout, p); if (!err) q->sg_timeout = clock_t_to_jiffies(timeout); return err; } static int sg_get_reserved_size(struct request_queue *q, int __user *p) { unsigned val = min(q->sg_reserved_size, queue_max_sectors(q) << 9); return put_user(val, p); } static int sg_set_reserved_size(struct request_queue *q, int __user *p) { int size, err = get_user(size, p); if (err) return err; if (size < 0) return -EINVAL; if (size > (queue_max_sectors(q) << 9)) size = queue_max_sectors(q) << 9; q->sg_reserved_size = size; return 0; } /* * will always return that we are ATAPI even for a real SCSI drive, I'm not * so sure this is worth doing anything about (why would you care??) */ static int sg_emulated_host(struct request_queue *q, int __user *p) { return put_user(1, p); } static void blk_set_cmd_filter_defaults(struct blk_cmd_filter *filter) { /* Basic read-only commands */ __set_bit(TEST_UNIT_READY, filter->read_ok); __set_bit(REQUEST_SENSE, filter->read_ok); __set_bit(READ_6, filter->read_ok); __set_bit(READ_10, filter->read_ok); __set_bit(READ_12, filter->read_ok); __set_bit(READ_16, filter->read_ok); __set_bit(READ_BUFFER, filter->read_ok); __set_bit(READ_DEFECT_DATA, filter->read_ok); __set_bit(READ_CAPACITY, filter->read_ok); __set_bit(READ_LONG, filter->read_ok); __set_bit(INQUIRY, filter->read_ok); __set_bit(MODE_SENSE, filter->read_ok); __set_bit(MODE_SENSE_10, filter->read_ok); __set_bit(LOG_SENSE, filter->read_ok); __set_bit(START_STOP, filter->read_ok); __set_bit(GPCMD_VERIFY_10, filter->read_ok); __set_bit(VERIFY_16, filter->read_ok); __set_bit(REPORT_LUNS, filter->read_ok); __set_bit(SERVICE_ACTION_IN, filter->read_ok); __set_bit(RECEIVE_DIAGNOSTIC, filter->read_ok); __set_bit(MAINTENANCE_IN, filter->read_ok); __set_bit(GPCMD_READ_BUFFER_CAPACITY, filter->read_ok); /* Audio CD commands */ __set_bit(GPCMD_PLAY_CD, filter->read_ok); __set_bit(GPCMD_PLAY_AUDIO_10, filter->read_ok); __set_bit(GPCMD_PLAY_AUDIO_MSF, filter->read_ok); __set_bit(GPCMD_PLAY_AUDIO_TI, filter->read_ok); __set_bit(GPCMD_PAUSE_RESUME, filter->read_ok); /* CD/DVD data reading */ __set_bit(GPCMD_READ_CD, filter->read_ok); __set_bit(GPCMD_READ_CD_MSF, filter->read_ok); __set_bit(GPCMD_READ_DISC_INFO, filter->read_ok); __set_bit(GPCMD_READ_CDVD_CAPACITY, filter->read_ok); __set_bit(GPCMD_READ_DVD_STRUCTURE, filter->read_ok); __set_bit(GPCMD_READ_HEADER, filter->read_ok); __set_bit(GPCMD_READ_TRACK_RZONE_INFO, filter->read_ok); __set_bit(GPCMD_READ_SUBCHANNEL, filter->read_ok); __set_bit(GPCMD_READ_TOC_PMA_ATIP, filter->read_ok); __set_bit(GPCMD_REPORT_KEY, filter->read_ok); __set_bit(GPCMD_SCAN, filter->read_ok); __set_bit(GPCMD_GET_CONFIGURATION, filter->read_ok); __set_bit(GPCMD_READ_FORMAT_CAPACITIES, filter->read_ok); __set_bit(GPCMD_GET_EVENT_STATUS_NOTIFICATION, filter->read_ok); __set_bit(GPCMD_GET_PERFORMANCE, filter->read_ok); __set_bit(GPCMD_SEEK, filter->read_ok); __set_bit(GPCMD_STOP_PLAY_SCAN, filter->read_ok); /* Basic writing commands */ __set_bit(WRITE_6, filter->write_ok); __set_bit(WRITE_10, filter->write_ok); __set_bit(WRITE_VERIFY, filter->write_ok); __set_bit(WRITE_12, filter->write_ok); __set_bit(WRITE_VERIFY_12, filter->write_ok); __set_bit(WRITE_16, filter->write_ok); __set_bit(WRITE_LONG, filter->write_ok); __set_bit(WRITE_LONG_2, filter->write_ok); __set_bit(ERASE, filter->write_ok); __set_bit(GPCMD_MODE_SELECT_10, filter->write_ok); __set_bit(MODE_SELECT, filter->write_ok); __set_bit(LOG_SELECT, filter->write_ok); __set_bit(GPCMD_BLANK, filter->write_ok); __set_bit(GPCMD_CLOSE_TRACK, filter->write_ok); __set_bit(GPCMD_FLUSH_CACHE, filter->write_ok); __set_bit(GPCMD_FORMAT_UNIT, filter->write_ok); __set_bit(GPCMD_REPAIR_RZONE_TRACK, filter->write_ok); __set_bit(GPCMD_RESERVE_RZONE_TRACK, filter->write_ok); __set_bit(GPCMD_SEND_DVD_STRUCTURE, filter->write_ok); __set_bit(GPCMD_SEND_EVENT, filter->write_ok); __set_bit(GPCMD_SEND_KEY, filter->write_ok); __set_bit(GPCMD_SEND_OPC, filter->write_ok); __set_bit(GPCMD_SEND_CUE_SHEET, filter->write_ok); __set_bit(GPCMD_SET_SPEED, filter->write_ok); __set_bit(GPCMD_PREVENT_ALLOW_MEDIUM_REMOVAL, filter->write_ok); __set_bit(GPCMD_LOAD_UNLOAD, filter->write_ok); __set_bit(GPCMD_SET_STREAMING, filter->write_ok); __set_bit(GPCMD_SET_READ_AHEAD, filter->write_ok); } int blk_verify_command(unsigned char *cmd, fmode_t has_write_perm) { struct blk_cmd_filter *filter = &blk_default_cmd_filter; /* root can do any command. */ if (capable(CAP_SYS_RAWIO)) return 0; /* if there's no filter set, assume we're filtering everything out */ if (!filter) return -EPERM; /* Anybody who can open the device can do a read-safe command */ if (test_bit(cmd[0], filter->read_ok)) return 0; /* Write-safe commands require a writable open */ if (test_bit(cmd[0], filter->write_ok) && has_write_perm) return 0; return -EPERM; } EXPORT_SYMBOL(blk_verify_command); static int blk_fill_sghdr_rq(struct request_queue *q, struct request *rq, struct sg_io_hdr *hdr, fmode_t mode) { if (copy_from_user(rq->cmd, hdr->cmdp, hdr->cmd_len)) return -EFAULT; if (blk_verify_command(rq->cmd, mode & FMODE_WRITE)) return -EPERM; /* * fill in request structure */ rq->cmd_len = hdr->cmd_len; rq->cmd_type = REQ_TYPE_BLOCK_PC; rq->timeout = msecs_to_jiffies(hdr->timeout); if (!rq->timeout) rq->timeout = q->sg_timeout; if (!rq->timeout) rq->timeout = BLK_DEFAULT_SG_TIMEOUT; if (rq->timeout < BLK_MIN_SG_TIMEOUT) rq->timeout = BLK_MIN_SG_TIMEOUT; return 0; } static int blk_complete_sghdr_rq(struct request *rq, struct sg_io_hdr *hdr, struct bio *bio) { int r, ret = 0; /* * fill in all the output members */ hdr->status = rq->errors & 0xff; hdr->masked_status = status_byte(rq->errors); hdr->msg_status = msg_byte(rq->errors); hdr->host_status = host_byte(rq->errors); hdr->driver_status = driver_byte(rq->errors); hdr->info = 0; if (hdr->masked_status || hdr->host_status || hdr->driver_status) hdr->info |= SG_INFO_CHECK; hdr->resid = rq->resid_len; hdr->sb_len_wr = 0; if (rq->sense_len && hdr->sbp) { int len = min((unsigned int) hdr->mx_sb_len, rq->sense_len); if (!copy_to_user(hdr->sbp, rq->sense, len)) hdr->sb_len_wr = len; else ret = -EFAULT; } r = blk_rq_unmap_user(bio); if (!ret) ret = r; blk_put_request(rq); return ret; } static int sg_io(struct request_queue *q, struct gendisk *bd_disk, struct sg_io_hdr *hdr, fmode_t mode) { unsigned long start_time; int writing = 0, ret = 0; struct request *rq; char sense[SCSI_SENSE_BUFFERSIZE]; struct bio *bio; if (hdr->interface_id != 'S') return -EINVAL; if (hdr->cmd_len > BLK_MAX_CDB) return -EINVAL; if (hdr->dxfer_len > (queue_max_hw_sectors(q) << 9)) return -EIO; if (hdr->dxfer_len) switch (hdr->dxfer_direction) { default: return -EINVAL; case SG_DXFER_TO_DEV: writing = 1; break; case SG_DXFER_TO_FROM_DEV: case SG_DXFER_FROM_DEV: break; } rq = blk_get_request(q, writing ? WRITE : READ, GFP_KERNEL); if (!rq) return -ENOMEM; if (blk_fill_sghdr_rq(q, rq, hdr, mode)) { blk_put_request(rq); return -EFAULT; } if (hdr->iovec_count) { const int size = sizeof(struct sg_iovec) * hdr->iovec_count; size_t iov_data_len; struct sg_iovec *sg_iov; struct iovec *iov; int i; sg_iov = kmalloc(size, GFP_KERNEL); if (!sg_iov) { ret = -ENOMEM; goto out; } if (copy_from_user(sg_iov, hdr->dxferp, size)) { kfree(sg_iov); ret = -EFAULT; goto out; } /* * Sum up the vecs, making sure they don't overflow */ iov = (struct iovec *) sg_iov; iov_data_len = 0; for (i = 0; i < hdr->iovec_count; i++) { if (iov_data_len + iov[i].iov_len < iov_data_len) { kfree(sg_iov); ret = -EINVAL; goto out; } iov_data_len += iov[i].iov_len; } /* SG_IO howto says that the shorter of the two wins */ if (hdr->dxfer_len < iov_data_len) { hdr->iovec_count = iov_shorten(iov, hdr->iovec_count, hdr->dxfer_len); iov_data_len = hdr->dxfer_len; } ret = blk_rq_map_user_iov(q, rq, NULL, sg_iov, hdr->iovec_count, iov_data_len, GFP_KERNEL); kfree(sg_iov); } else if (hdr->dxfer_len) ret = blk_rq_map_user(q, rq, NULL, hdr->dxferp, hdr->dxfer_len, GFP_KERNEL); if (ret) goto out; bio = rq->bio; memset(sense, 0, sizeof(sense)); rq->sense = sense; rq->sense_len = 0; rq->retries = 0; start_time = jiffies; /* ignore return value. All information is passed back to caller * (if he doesn't check that is his problem). * N.B. a non-zero SCSI status is _not_ necessarily an error. */ blk_execute_rq(q, bd_disk, rq, 0); hdr->duration = jiffies_to_msecs(jiffies - start_time); return blk_complete_sghdr_rq(rq, hdr, bio); out: blk_put_request(rq); return ret; } /** * sg_scsi_ioctl -- handle deprecated SCSI_IOCTL_SEND_COMMAND ioctl * @file: file this ioctl operates on (optional) * @q: request queue to send scsi commands down * @disk: gendisk to operate on (option) * @sic: userspace structure describing the command to perform * * Send down the scsi command described by @sic to the device below * the request queue @q. If @file is non-NULL it's used to perform * fine-grained permission checks that allow users to send down * non-destructive SCSI commands. If the caller has a struct gendisk * available it should be passed in as @disk to allow the low level * driver to use the information contained in it. A non-NULL @disk * is only allowed if the caller knows that the low level driver doesn't * need it (e.g. in the scsi subsystem). * * Notes: * - This interface is deprecated - users should use the SG_IO * interface instead, as this is a more flexible approach to * performing SCSI commands on a device. * - The SCSI command length is determined by examining the 1st byte * of the given command. There is no way to override this. * - Data transfers are limited to PAGE_SIZE * - The length (x + y) must be at least OMAX_SB_LEN bytes long to * accommodate the sense buffer when an error occurs. * The sense buffer is truncated to OMAX_SB_LEN (16) bytes so that * old code will not be surprised. * - If a Unix error occurs (e.g. ENOMEM) then the user will receive * a negative return and the Unix error code in 'errno'. * If the SCSI command succeeds then 0 is returned. * Positive numbers returned are the compacted SCSI error codes (4 * bytes in one int) where the lowest byte is the SCSI status. */ #define OMAX_SB_LEN 16 /* For backward compatibility */ int sg_scsi_ioctl(struct request_queue *q, struct gendisk *disk, fmode_t mode, struct scsi_ioctl_command __user *sic) { struct request *rq; int err; unsigned int in_len, out_len, bytes, opcode, cmdlen; char *buffer = NULL, sense[SCSI_SENSE_BUFFERSIZE]; if (!sic) return -EINVAL; /* * get in an out lengths, verify they don't exceed a page worth of data */ if (get_user(in_len, &sic->inlen)) return -EFAULT; if (get_user(out_len, &sic->outlen)) return -EFAULT; if (in_len > PAGE_SIZE || out_len > PAGE_SIZE) return -EINVAL; if (get_user(opcode, sic->data)) return -EFAULT; bytes = max(in_len, out_len); if (bytes) { buffer = kzalloc(bytes, q->bounce_gfp | GFP_USER| __GFP_NOWARN); if (!buffer) return -ENOMEM; } rq = blk_get_request(q, in_len ? WRITE : READ, __GFP_WAIT); cmdlen = COMMAND_SIZE(opcode); /* * get command and data to send to device, if any */ err = -EFAULT; rq->cmd_len = cmdlen; if (copy_from_user(rq->cmd, sic->data, cmdlen)) goto error; if (in_len && copy_from_user(buffer, sic->data + cmdlen, in_len)) goto error; err = blk_verify_command(rq->cmd, mode & FMODE_WRITE); if (err) goto error; /* default. possible overriden later */ rq->retries = 5; switch (opcode) { case SEND_DIAGNOSTIC: case FORMAT_UNIT: rq->timeout = FORMAT_UNIT_TIMEOUT; rq->retries = 1; break; case START_STOP: rq->timeout = START_STOP_TIMEOUT; break; case MOVE_MEDIUM: rq->timeout = MOVE_MEDIUM_TIMEOUT; break; case READ_ELEMENT_STATUS: rq->timeout = READ_ELEMENT_STATUS_TIMEOUT; break; case READ_DEFECT_DATA: rq->timeout = READ_DEFECT_DATA_TIMEOUT; rq->retries = 1; break; default: rq->timeout = BLK_DEFAULT_SG_TIMEOUT; break; } if (bytes && blk_rq_map_kern(q, rq, buffer, bytes, __GFP_WAIT)) { err = DRIVER_ERROR << 24; goto out; } memset(sense, 0, sizeof(sense)); rq->sense = sense; rq->sense_len = 0; rq->cmd_type = REQ_TYPE_BLOCK_PC; blk_execute_rq(q, disk, rq, 0); out: err = rq->errors & 0xff; /* only 8 bit SCSI status */ if (err) { if (rq->sense_len && rq->sense) { bytes = (OMAX_SB_LEN > rq->sense_len) ? rq->sense_len : OMAX_SB_LEN; if (copy_to_user(sic->data, rq->sense, bytes)) err = -EFAULT; } } else { if (copy_to_user(sic->data, buffer, out_len)) err = -EFAULT; } error: kfree(buffer); blk_put_request(rq); return err; } EXPORT_SYMBOL_GPL(sg_scsi_ioctl); /* Send basic block requests */ static int __blk_send_generic(struct request_queue *q, struct gendisk *bd_disk, int cmd, int data) { struct request *rq; int err; rq = blk_get_request(q, WRITE, __GFP_WAIT); rq->cmd_type = REQ_TYPE_BLOCK_PC; rq->timeout = BLK_DEFAULT_SG_TIMEOUT; rq->cmd[0] = cmd; rq->cmd[4] = data; rq->cmd_len = 6; err = blk_execute_rq(q, bd_disk, rq, 0); blk_put_request(rq); return err; } static inline int blk_send_start_stop(struct request_queue *q, struct gendisk *bd_disk, int data) { return __blk_send_generic(q, bd_disk, GPCMD_START_STOP_UNIT, data); } int scsi_cmd_ioctl(struct request_queue *q, struct gendisk *bd_disk, fmode_t mode, unsigned int cmd, void __user *arg) { int err; if (!q) return -ENXIO; switch (cmd) { /* * new sgv3 interface */ case SG_GET_VERSION_NUM: err = sg_get_version(arg); break; case SCSI_IOCTL_GET_IDLUN: err = scsi_get_idlun(q, arg); break; case SCSI_IOCTL_GET_BUS_NUMBER: err = scsi_get_bus(q, arg); break; case SG_SET_TIMEOUT: err = sg_set_timeout(q, arg); break; case SG_GET_TIMEOUT: err = sg_get_timeout(q); break; case SG_GET_RESERVED_SIZE: err = sg_get_reserved_size(q, arg); break; case SG_SET_RESERVED_SIZE: err = sg_set_reserved_size(q, arg); break; case SG_EMULATED_HOST: err = sg_emulated_host(q, arg); break; case SG_IO: { struct sg_io_hdr hdr; err = -EFAULT; if (copy_from_user(&hdr, arg, sizeof(hdr))) break; err = sg_io(q, bd_disk, &hdr, mode); if (err == -EFAULT) break; if (copy_to_user(arg, &hdr, sizeof(hdr))) err = -EFAULT; break; } case CDROM_SEND_PACKET: { struct cdrom_generic_command cgc; struct sg_io_hdr hdr; err = -EFAULT; if (copy_from_user(&cgc, arg, sizeof(cgc))) break; cgc.timeout = clock_t_to_jiffies(cgc.timeout); memset(&hdr, 0, sizeof(hdr)); hdr.interface_id = 'S'; hdr.cmd_len = sizeof(cgc.cmd); hdr.dxfer_len = cgc.buflen; err = 0; switch (cgc.data_direction) { case CGC_DATA_UNKNOWN: hdr.dxfer_direction = SG_DXFER_UNKNOWN; break; case CGC_DATA_WRITE: hdr.dxfer_direction = SG_DXFER_TO_DEV; break; case CGC_DATA_READ: hdr.dxfer_direction = SG_DXFER_FROM_DEV; break; case CGC_DATA_NONE: hdr.dxfer_direction = SG_DXFER_NONE; break; default: err = -EINVAL; } if (err) break; hdr.dxferp = cgc.buffer; hdr.sbp = cgc.sense; if (hdr.sbp) hdr.mx_sb_len = sizeof(struct request_sense); hdr.timeout = jiffies_to_msecs(cgc.timeout); hdr.cmdp = ((struct cdrom_generic_command __user*) arg)->cmd; hdr.cmd_len = sizeof(cgc.cmd); err = sg_io(q, bd_disk, &hdr, mode); if (err == -EFAULT) break; if (hdr.status) err = -EIO; cgc.stat = err; cgc.buflen = hdr.resid; if (copy_to_user(arg, &cgc, sizeof(cgc))) err = -EFAULT; break; } /* * old junk scsi send command ioctl */ case SCSI_IOCTL_SEND_COMMAND: printk(KERN_WARNING "program %s is using a deprecated SCSI ioctl, please convert it to SG_IO\n", current->comm); err = -EINVAL; if (!arg) break; err = sg_scsi_ioctl(q, bd_disk, mode, arg); break; case CDROMCLOSETRAY: err = blk_send_start_stop(q, bd_disk, 0x03); break; case CDROMEJECT: err = blk_send_start_stop(q, bd_disk, 0x02); break; default: err = -ENOTTY; } return err; } EXPORT_SYMBOL(scsi_cmd_ioctl); int scsi_verify_blk_ioctl(struct block_device *bd, unsigned int cmd) { if (bd && bd == bd->bd_contains) return 0; /* Actually none of these is particularly useful on a partition, * but they are safe. */ switch (cmd) { case SCSI_IOCTL_GET_IDLUN: case SCSI_IOCTL_GET_BUS_NUMBER: case SCSI_IOCTL_GET_PCI: case SCSI_IOCTL_PROBE_HOST: case SG_GET_VERSION_NUM: case SG_SET_TIMEOUT: case SG_GET_TIMEOUT: case SG_GET_RESERVED_SIZE: case SG_SET_RESERVED_SIZE: case SG_EMULATED_HOST: return 0; case CDROM_GET_CAPABILITY: /* Keep this until we remove the printk below. udev sends it * and we do not want to spam dmesg about it. CD-ROMs do * not have partitions, so we get here only for disks. */ return -ENOIOCTLCMD; default: break; } if (capable(CAP_SYS_RAWIO)) return 0; /* In particular, rule out all resets and host-specific ioctls. */ printk_ratelimited(KERN_WARNING "%s: sending ioctl %x to a partition!\n", current->comm, cmd); return -ENOIOCTLCMD; } EXPORT_SYMBOL(scsi_verify_blk_ioctl); int scsi_cmd_blk_ioctl(struct block_device *bd, fmode_t mode, unsigned int cmd, void __user *arg) { int ret; ret = scsi_verify_blk_ioctl(bd, cmd); if (ret < 0) return ret; return scsi_cmd_ioctl(bd->bd_disk->queue, bd->bd_disk, mode, cmd, arg); } EXPORT_SYMBOL(scsi_cmd_blk_ioctl); static int __init blk_scsi_ioctl_init(void) { blk_set_cmd_filter_defaults(&blk_default_cmd_filter); return 0; } fs_initcall(blk_scsi_ioctl_init);